MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
INPUTMUX: Input Multiplexing Driver

Overview

The MCUXpresso SDK provides a driver for the Input multiplexing (INPUTMUX).
It configures the inputs to the pin interrupt block, DMA trigger, and frequency measure function. Once configured, the clock is not needed for the inputmux.

Input Multiplexing Driver operation

INPUTMUX_AttachSignal function configures the specified input

Typical use case

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/inputmux

Files

file  fsl_inputmux.h
 

Functions

void INPUTMUX_Init (INPUTMUX_Type *base)
 Initialize INPUTMUX peripheral. More...
 
void INPUTMUX_AttachSignal (INPUTMUX_Type *base, uint32_t index, inputmux_connection_t connection)
 Attaches a signal. More...
 
void INPUTMUX_Deinit (INPUTMUX_Type *base)
 Deinitialize INPUTMUX peripheral. More...
 

Driver version

#define FSL_INPUTMUX_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))
 Group interrupt driver version for SDK. More...
 

Macro Definition Documentation

#define FSL_INPUTMUX_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))

Version 2.0.1.

Function Documentation

void INPUTMUX_Init ( INPUTMUX_Type *  base)

This function enables the INPUTMUX clock.

Parameters
baseBase address of the INPUTMUX peripheral.
Return values
None.
void INPUTMUX_AttachSignal ( INPUTMUX_Type *  base,
uint32_t  index,
inputmux_connection_t  connection 
)

This function gates the INPUTPMUX clock.

Parameters
baseBase address of the INPUTMUX peripheral.
indexDestination peripheral to attach the signal to.
connectionSelects connection.
Return values
None.
void INPUTMUX_Deinit ( INPUTMUX_Type *  base)

This function disables the INPUTMUX clock.

Parameters
baseBase address of the INPUTMUX peripheral.
Return values
None.