![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | i2c_master_dma_handle_t |
| I2C master dma transfer structure. More... | |
Macros | |
| #define | I2C_MAX_DMA_TRANSFER_COUNT 1024 |
| Maximum lenght of single DMA transfer (determined by capability of the DMA engine) | |
Typedefs | |
| typedef void(* | i2c_master_dma_transfer_callback_t )(I2C_Type *base, i2c_master_dma_handle_t *handle, status_t status, void *userData) |
| I2C master dma transfer callback typedef. More... | |
Driver version | |
| #define | FSL_I2C_DMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 4)) |
| I2C DMA driver version 2.0.4. More... | |
I2C Block DMA Transfer Operation | |
| void | I2C_MasterTransferCreateHandleDMA (I2C_Type *base, i2c_master_dma_handle_t *handle, i2c_master_dma_transfer_callback_t callback, void *userData, dma_handle_t *dmaHandle) |
| Init the I2C handle which is used in transactional functions. More... | |
| status_t | I2C_MasterTransferDMA (I2C_Type *base, i2c_master_dma_handle_t *handle, i2c_master_transfer_t *xfer) |
| Performs a master dma non-blocking transfer on the I2C bus. More... | |
| status_t | I2C_MasterTransferGetCountDMA (I2C_Type *base, i2c_master_dma_handle_t *handle, size_t *count) |
| Get master transfer status during a dma non-blocking transfer. More... | |
| void | I2C_MasterTransferAbortDMA (I2C_Type *base, i2c_master_dma_handle_t *handle) |
| Abort a master dma non-blocking transfer in a early time. More... | |
| struct _i2c_master_dma_handle |
I2C master dma handle typedef.
Data Fields | |
| uint8_t | state |
| Transfer state machine current state. More... | |
| uint32_t | transferCount |
| Indicates progress of the transfer. | |
| uint32_t | remainingBytesDMA |
| Remaining byte count to be transferred using DMA. More... | |
| uint8_t * | buf |
| Buffer pointer for current state. More... | |
| dma_handle_t * | dmaHandle |
| The DMA handler used. More... | |
| i2c_master_transfer_t | transfer |
| Copy of the current transfer info. More... | |
| i2c_master_dma_transfer_callback_t | completionCallback |
| Callback function called after dma transfer finished. More... | |
| void * | userData |
| Callback parameter passed to callback function. More... | |
| uint8_t i2c_master_dma_handle_t::state |
| uint32_t i2c_master_dma_handle_t::remainingBytesDMA |
| uint8_t* i2c_master_dma_handle_t::buf |
| dma_handle_t* i2c_master_dma_handle_t::dmaHandle |
| i2c_master_transfer_t i2c_master_dma_handle_t::transfer |
| i2c_master_dma_transfer_callback_t i2c_master_dma_handle_t::completionCallback |
| void* i2c_master_dma_handle_t::userData |
| #define FSL_I2C_DMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 4)) |
| typedef void(* i2c_master_dma_transfer_callback_t)(I2C_Type *base, i2c_master_dma_handle_t *handle, status_t status, void *userData) |
| void I2C_MasterTransferCreateHandleDMA | ( | I2C_Type * | base, |
| i2c_master_dma_handle_t * | handle, | ||
| i2c_master_dma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | dmaHandle | ||
| ) |
| base | I2C peripheral base address |
| handle | pointer to i2c_master_dma_handle_t structure |
| callback | pointer to user callback function |
| userData | user param passed to the callback function |
| dmaHandle | DMA handle pointer |
| status_t I2C_MasterTransferDMA | ( | I2C_Type * | base, |
| i2c_master_dma_handle_t * | handle, | ||
| i2c_master_transfer_t * | xfer | ||
| ) |
| base | I2C peripheral base address |
| handle | pointer to i2c_master_dma_handle_t structure |
| xfer | pointer to transfer structure of i2c_master_transfer_t |
| kStatus_Success | Sucessully complete the data transmission. |
| kStatus_I2C_Busy | Previous transmission still not finished. |
| kStatus_I2C_Timeout | Transfer error, wait signal timeout. |
| kStatus_I2C_ArbitrationLost | Transfer error, arbitration lost. |
| kStataus_I2C_Nak | Transfer error, receive Nak during transfer. |
| status_t I2C_MasterTransferGetCountDMA | ( | I2C_Type * | base, |
| i2c_master_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | I2C peripheral base address |
| handle | pointer to i2c_master_dma_handle_t structure |
| count | Number of bytes transferred so far by the non-blocking transaction. |
| void I2C_MasterTransferAbortDMA | ( | I2C_Type * | base, |
| i2c_master_dma_handle_t * | handle | ||
| ) |
| base | I2C peripheral base address |
| handle | pointer to i2c_master_dma_handle_t structure |