This section describes the programming interface of the spi Cortex Microcontroller Software Interface Standard (CMSIS) driver. And this driver defines generic peripheral driver interfaces for middleware making it reusable across a wide range of supported microcontroller devices. The API connects microcontroller peripherals with middleware that implements for example communication stacks, file systems, or graphic user interfaces. More information and usage methord please refer to http://www.keil.com/pack/doc/cmsis/Driver/html/index.html.
Function groups
SPI CMSIS GetVersion Operation
This function group will return the DSPI CMSIS Driver version to user.
SPI CMSIS GetCapabilities Operation
This function group will return the capabilities of this driver.
SPI CMSIS Initialize and Uninitialize Operation
This function will initialize and uninitialize the instance in master mode or slave mode. And this API must be called before you configure an instance or after you Deinit an instance.The right steps to start an instance is that you must initialize the instance which been slected firstly,then you can power on the instance.After these all have been done,you can configure the instance by using control operation.If you want to Uninitialize the instance, you must power off the instance first.
SPI CMSIS Transfer Operation
This function group controls the transfer, master send/receive data, and slave send/receive data.
SPI CMSIS Status Operation
This function group gets the spi transfer status.
SPI CMSIS Control Operation
This function can select instance as master mode or slave mode, set baudrate for master mode transfer, get current baudrate of master mode transfer,set transfer data bits and set other control command.
Typical use case
Master Operation
uint8_t masterRxData[TRANSFER_SIZE] = {0U};
uint8_t masterTxData[TRANSFER_SIZE] = {0U};
Driver_SPI0.Initialize(DSPI_MasterSignalEvent_t);
Driver_SPI0.PowerControl(ARM_POWER_FULL);
Driver_SPI0.Control(ARM_SPI_MODE_MASTER, TRANSFER_BAUDRATE);
Driver_SPI0.Transfer(masterTxData, masterRxData, TRANSFER_SIZE);
Driver_SPI0.PowerControl(ARM_POWER_OFF);
Driver_SPI0.Uninitialize();
Slave Operation
uint8_t slaveRxData[TRANSFER_SIZE] = {0U};
uint8_t slaveTxData[TRANSFER_SIZE] = {0U};
Driver_SPI2.Initialize(DSPI_SlaveSignalEvent_t);
Driver_SPI2.PowerControl(ARM_POWER_FULL);
Driver_SPI2.Control(ARM_SPI_MODE_SLAVE, false);
Driver_SPI2.Transfer(slaveTxData, slaveRxData, TRANSFER_SIZE);
Driver_SPI2.PowerControl(ARM_POWER_OFF);
Driver_SPI2.Uninitialize();
This section describes the programming interface of the SPI DMA driver.
|
| #define | SPI_DUMMYDATA (0xFFU) |
| | SPI dummy transfer data, the data is sent while txBuff is NULL. More...
|
| |
|
| enum | spi_xfer_option_t {
kSPI_FrameDelay = (SPI_TXDATCTL_EOF_MASK),
kSPI_FrameAssert = (SPI_TXDATCTL_EOT_MASK),
kSPI_ReceiveIgnore = (SPI_TXDATCTL_RXIGNORE_MASK)
} |
| | SPI transfer option. More...
|
| |
| enum | spi_shift_direction_t {
kSPI_MsbFirst = 0U,
kSPI_LsbFirst = 1U
} |
| | SPI data shifter direction options. More...
|
| |
| enum | spi_clock_polarity_t {
kSPI_ClockPolarityActiveHigh = 0x0U,
kSPI_ClockPolarityActiveLow = 0x1U
} |
| | SPI clock polarity configuration. More...
|
| |
| enum | spi_clock_phase_t {
kSPI_ClockPhaseFirstEdge = 0x0U,
kSPI_ClockPhaseSecondEdge = 0x1U
} |
| | SPI clock phase configuration. More...
|
| |
| enum | spi_fifo_direction_t {
kSPI_FifoTx = 1U,
kSPI_FifoRx = 2U
} |
| | SPI FIFO driection. More...
|
| |
| enum | spi_data_width_t {
kSPI_Data1Bits = 0,
kSPI_Data2Bits = 1,
kSPI_Data3Bits = 2,
kSPI_Data4Bits = 3,
kSPI_Data5Bits = 4,
kSPI_Data6Bits = 5,
kSPI_Data7Bits = 6,
kSPI_Data8Bits = 7,
kSPI_Data9Bits = 8,
kSPI_Data10Bits = 9,
kSPI_Data11Bits = 10,
kSPI_Data12Bits = 11,
kSPI_Data13Bits = 12,
kSPI_Data14Bits = 13,
kSPI_Data15Bits = 14,
kSPI_Data16Bits = 15
} |
| | Transfer data width. More...
|
| |
| enum | spi_ssel_t {
kSPI_Ssel0 = 0,
kSPI_Ssel1 = 1,
kSPI_Ssel2 = 2,
kSPI_Ssel3 = 3
} |
| | Slave select. More...
|
| |
| enum | spi_spol_t |
| | ssel polarity
|
| |
| enum | _spi_status {
kStatus_SPI_Busy = MAKE_STATUS(kStatusGroup_LPC_SPI, 0),
kStatus_SPI_Idle = MAKE_STATUS(kStatusGroup_LPC_SPI, 1),
kStatus_SPI_Error = MAKE_STATUS(kStatusGroup_LPC_SPI, 2),
kStatus_SPI_BaudrateNotSupport
} |
| | SPI transfer status. More...
|
| |
| enum | _spi_interrupt_enable {
kSPI_RxReadyInterruptEnable = SPI_INTENSET_RXRDYEN_MASK,
kSPI_TxReadyInterruptEnable = SPI_INTENSET_TXRDYEN_MASK,
kSPI_RxOverrunInterruptEnable = SPI_INTENSET_RXOVEN_MASK,
kSPI_TxUnderrunInterruptEnable = SPI_INTENSET_TXUREN_MASK,
kSPI_SlaveSelectAssertInterruptEnable = SPI_INTENSET_SSAEN_MASK,
kSPI_SlaveSelectDeassertInterruptEnable = SPI_INTENSET_SSDEN_MASK,
kSPI_MasterIdleInterruptEnable = SPI_INTENSET_MSTIDLEEN_MASK
} |
| | SPI interrupt sources. More...
|
| |
| enum | _spi_fifo_interrupt_enable {
kSPI_RxFifoThresholdInterruptEnable,
kSPI_TxFifoThresholdInterruptEnable,
kSPI_RxFifoTimeoutInterruptEnable = VFIFO_SPI_CTLSETSPI_RXTIMEOUTINTEN_MASK
} |
| | SPI FIFO interrupt sources. More...
|
| |
| enum | _spi_status_flags {
kSPI_RxReadyFlag = SPI_STAT_RXRDY_MASK,
kSPI_TxReadyFlag = SPI_STAT_TXRDY_MASK,
kSPI_RxOverrunFlag = SPI_STAT_RXOV_MASK,
kSPI_TxUnderrunFlag = SPI_STAT_TXUR_MASK,
kSPI_SlaveSelectAssertFlag = SPI_STAT_SSA_MASK,
kSPI_SlaveSelectDeassertFlag = SPI_STAT_SSD_MASK,
kSPI_StallFlag = SPI_STAT_STALLED_MASK,
kSPI_EndTransferFlag = SPI_STAT_ENDTRANSFER_MASK,
kSPI_MasterIdleFlag = SPI_STAT_MSTIDLE_MASK
} |
| | SPI status flags. More...
|
| |
| enum | _spi_fifo_status_flags {
kSPI_RxFifoThresholdFlag = (VFIFO_SPI_STATSPI_RXTH_MASK),
kSPI_TxFifoThresholdFlag = (VFIFO_SPI_STATSPI_TXTH_MASK),
kSPI_RxFifoTimeOutFlag = (VFIFO_SPI_STATSPI_RXTIMEOUT_MASK),
kSPI_FifoBusErrorFlag = (VFIFO_SPI_STATSPI_BUSERR_MASK),
kSPI_RxFifoEmptyFlag = (VFIFO_SPI_STATSPI_RXEMPTY_MASK),
kSPI_TxFifoEmptyFlag = (VFIFO_SPI_STATSPI_TXEMPTY_MASK)
} |
| | SPI FIFO status flags. More...
|
| |
|
| status_t | SPI_MasterTransferCreateHandle (SPI_Type *base, spi_master_handle_t *handle, spi_master_callback_t callback, void *userData) |
| | Initializes the SPI master handle. More...
|
| |
| status_t | SPI_MasterTransferBlocking (SPI_Type *base, spi_transfer_t *xfer) |
| | Transfers a block of data using a polling method. More...
|
| |
| status_t | SPI_MasterTransferNonBlocking (SPI_Type *base, spi_master_handle_t *handle, spi_transfer_t *xfer) |
| | Performs a non-blocking SPI interrupt transfer. More...
|
| |
| status_t | SPI_MasterHalfDuplexTransferBlocking (SPI_Type *base, spi_half_duplex_transfer_t *xfer) |
| | Transfers a block of data using a polling method. More...
|
| |
| status_t | SPI_MasterHalfDuplexTransferNonBlocking (SPI_Type *base, spi_master_handle_t *handle, spi_half_duplex_transfer_t *xfer) |
| | Performs a non-blocking SPI interrupt transfer. More...
|
| |
| status_t | SPI_MasterTransferGetCount (SPI_Type *base, spi_master_handle_t *handle, size_t *count) |
| | Gets the master transfer count. More...
|
| |
| void | SPI_MasterTransferAbort (SPI_Type *base, spi_master_handle_t *handle) |
| | SPI master aborts a transfer using an interrupt. More...
|
| |
| void | SPI_MasterTransferHandleIRQ (SPI_Type *base, spi_master_handle_t *handle) |
| | Interrupts the handler for the SPI. More...
|
| |
| status_t | SPI_SlaveTransferCreateHandle (SPI_Type *base, spi_slave_handle_t *handle, spi_slave_callback_t callback, void *userData) |
| | Initializes the SPI slave handle. More...
|
| |
| status_t | SPI_SlaveTransferNonBlocking (SPI_Type *base, spi_slave_handle_t *handle, spi_transfer_t *xfer) |
| | Performs a non-blocking SPI slave interrupt transfer. More...
|
| |
| static status_t | SPI_SlaveTransferGetCount (SPI_Type *base, spi_slave_handle_t *handle, size_t *count) |
| | Gets the slave transfer count. More...
|
| |
| static void | SPI_SlaveTransferAbort (SPI_Type *base, spi_slave_handle_t *handle) |
| | SPI slave aborts a transfer using an interrupt. More...
|
| |
| void | SPI_SlaveTransferHandleIRQ (SPI_Type *base, spi_slave_handle_t *handle) |
| | Interrupts a handler for the SPI slave. More...
|
| |
| struct spi_delay_config_t |
| uint8_t spi_delay_config_t::preDelay |
| uint8_t spi_delay_config_t::postDelay |
| uint8_t spi_delay_config_t::frameDelay |
| uint8_t spi_delay_config_t::transferDelay |
| struct spi_master_config_t |
| struct spi_slave_config_t |
| uint32_t spi_transfer_t::configFlags |
| struct spi_half_duplex_transfer_t |
| uint32_t spi_half_duplex_transfer_t::configFlags |
| bool spi_half_duplex_transfer_t::isPcsAssertInTransfer |
true for assert and false for deassert.
| bool spi_half_duplex_transfer_t::isTransmitFirst |
| struct _spi_master_handle |
| bool spi_master_handle_t::isTxFifoEnabled |
| bool spi_master_handle_t::isRxFifoEnabled |
| uint8_t spi_master_handle_t::rxFIFOSize |
| uint32_t spi_master_handle_t::commonCommand |
| uint32_t spi_master_handle_t::lastCommand |
| #define SPI_DUMMYDATA (0xFFU) |
| Enumerator |
|---|
| kSPI_FrameDelay |
A delay may be inserted, defined in the DLY register.
|
| kSPI_FrameAssert |
SSEL will be deasserted at the end of a transfer.
|
| kSPI_ReceiveIgnore |
Ignore the receive data.
|
| Enumerator |
|---|
| kSPI_MsbFirst |
Data transfers start with most significant bit.
|
| kSPI_LsbFirst |
Data transfers start with least significant bit.
|
| Enumerator |
|---|
| kSPI_ClockPolarityActiveHigh |
Active-high SPI clock (idles low).
|
| kSPI_ClockPolarityActiveLow |
Active-low SPI clock (idles high).
|
| Enumerator |
|---|
| kSPI_ClockPhaseFirstEdge |
First edge on SCK occurs at the middle of the first cycle of a data transfer.
|
| kSPI_ClockPhaseSecondEdge |
First edge on SCK occurs at the start of the first cycle of a data transfer.
|
| Enumerator |
|---|
| kSPI_FifoTx |
FIFO direction for transmit.
|
| kSPI_FifoRx |
FIFO direction for receive.
|
| Enumerator |
|---|
| kSPI_Data1Bits |
1 bits data width,when LEN = 0, the underrun status is not meaningful.
|
| kSPI_Data2Bits |
2 bits data width
|
| kSPI_Data3Bits |
3 bits data width
|
| kSPI_Data4Bits |
4 bits data width
|
| kSPI_Data5Bits |
5 bits data width
|
| kSPI_Data6Bits |
6 bits data width
|
| kSPI_Data7Bits |
7 bits data width
|
| kSPI_Data8Bits |
8 bits data width
|
| kSPI_Data9Bits |
9 bits data width
|
| kSPI_Data10Bits |
10 bits data width
|
| kSPI_Data11Bits |
11 bits data width
|
| kSPI_Data12Bits |
12 bits data width
|
| kSPI_Data13Bits |
13 bits data width
|
| kSPI_Data14Bits |
14 bits data width
|
| kSPI_Data15Bits |
15 bits data width
|
| kSPI_Data16Bits |
16 bits data width
|
| Enumerator |
|---|
| kSPI_Ssel0 |
Slave select 0.
|
| kSPI_Ssel1 |
Slave select 1.
|
| kSPI_Ssel2 |
Slave select 2.
|
| kSPI_Ssel3 |
Slave select 3.
|
| Enumerator |
|---|
| kStatus_SPI_Busy |
SPI bus is busy.
|
| kStatus_SPI_Idle |
SPI is idle.
|
| kStatus_SPI_Error |
SPI error.
|
| kStatus_SPI_BaudrateNotSupport |
Baudrate is not support in current clock source.
|
| Enumerator |
|---|
| kSPI_RxReadyInterruptEnable |
Rx ready interrupt.
|
| kSPI_TxReadyInterruptEnable |
Tx ready interrupt.
|
| kSPI_RxOverrunInterruptEnable |
Rx overrun interrupt.
|
| kSPI_TxUnderrunInterruptEnable |
Tx underrun interrupt.
|
| kSPI_SlaveSelectAssertInterruptEnable |
Slave select assert interrupt.
|
| kSPI_SlaveSelectDeassertInterruptEnable |
Slave select deassert interrupt.
|
| kSPI_MasterIdleInterruptEnable |
Master idle interrupt.
|
| Enumerator |
|---|
| kSPI_RxFifoThresholdInterruptEnable |
Rx FIFO reach the threshold interrupt.
|
| kSPI_TxFifoThresholdInterruptEnable |
Tx FIFO reach the threshold interrupt.
|
| kSPI_RxFifoTimeoutInterruptEnable |
Rx FIfo timeout interrupt.
|
| Enumerator |
|---|
| kSPI_RxReadyFlag |
Receive ready flag.
|
| kSPI_TxReadyFlag |
Transmit ready flag.
|
| kSPI_RxOverrunFlag |
Receive overrun flag.
|
| kSPI_TxUnderrunFlag |
Transmit underrun flag.
|
| kSPI_SlaveSelectAssertFlag |
Slave select assert flag.
|
| kSPI_SlaveSelectDeassertFlag |
slave select deassert flag.
|
| kSPI_StallFlag |
Stall flag.
|
| kSPI_EndTransferFlag |
End transfer bit.
|
| kSPI_MasterIdleFlag |
Master in idle status flag.
|
| Enumerator |
|---|
| kSPI_RxFifoThresholdFlag |
Receive FIFO threshold reached flag.
|
| kSPI_TxFifoThresholdFlag |
Transmit FIFO threshold reached flag.
|
| kSPI_RxFifoTimeOutFlag |
Receive time out flag.
|
| kSPI_FifoBusErrorFlag |
FIFO bus error flag.
|
| kSPI_RxFifoEmptyFlag |
Receive fifo buffer empty flag.
|
| kSPI_TxFifoEmptyFlag |
transmit fifo buffer empty flag.
|
| uint32_t SPI_GetInstance |
( |
SPI_Type * |
base | ) |
|
The purpose of this API is to get the configuration structure initialized for use in SPI_MasterInit(). User may use the initialized structure unchanged in SPI_MasterInit(), or modify some fields of the structure before calling SPI_MasterInit(). After calling this API, the master is ready to transfer. Example:
- Parameters
-
| config | pointer to master config structure |
The configuration structure can be filled by user from scratch, or be set with default values by SPI_MasterGetDefaultConfig(). After calling this API, the slave is ready to transfer. Example
- Parameters
-
| base | SPI base pointer |
| config | pointer to master configuration structure |
| srcClock_Hz | Source clock frequency. |
The purpose of this API is to get the configuration structure initialized for use in SPI_SlaveInit(). Modify some fields of the structure before calling SPI_SlaveInit(). Example:
- Parameters
-
| config | pointer to slave configuration structure |
The configuration structure can be filled by user from scratch or be set with default values by SPI_SlaveGetDefaultConfig(). After calling this API, the slave is ready to transfer. Example
- Parameters
-
| base | SPI base pointer |
| config | pointer to slave configuration structure |
| void SPI_Deinit |
( |
SPI_Type * |
base | ) |
|
Calling this API resets the SPI module, gates the SPI clock. Disable the fifo if enabled. The SPI module can't work unless calling the SPI_MasterInit/SPI_SlaveInit to initialize module.
- Parameters
-
| static void SPI_Enable |
( |
SPI_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | SPI base pointer |
| enable | or disable ( true = enable, false = disable) |
| static uint32_t SPI_GetStatusFlags |
( |
SPI_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
- Returns
- SPI Status, use status flag to AND _spi_status_flags could get the related status.
| uint32_t SPI_GetFifoStatusFlags |
( |
SPI_Type * |
base | ) |
|
| void SPI_ClearFifoStatusFlags |
( |
SPI_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
Only kSPI_RxFifoTimeOutFlag and kSPI_FifoBusErrorFlag can be cleared.
- Parameters
-
| base | SPI base pointer |
| mask | use status flag to AND _spi_status_flags could get the related status. |
| static void SPI_EnableInterrupts |
( |
SPI_Type * |
base, |
|
|
uint32_t |
irqs |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | SPI base pointer |
| irqs | SPI interrupt source. The parameter can be any combination of the following values:
- kSPI_RxReadyInterruptEnable
- kSPI_TxReadyInterruptEnable
|
| static void SPI_DisableInterrupts |
( |
SPI_Type * |
base, |
|
|
uint32_t |
irqs |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | SPI base pointer |
| irqs | SPI interrupt source. The parameter can be any combination of the following values:
- kSPI_RxReadyInterruptEnable
- kSPI_TxReadyInterruptEnable
|
| void SPI_EnableFifoInterrupts |
( |
SPI_Type * |
base, |
|
|
uint32_t |
irqs |
|
) |
| |
- Parameters
-
| base | SPI base pointer |
| irqs | SPI interrupt source. The parameter can be any combination of the following values:
- kSPI_RxFifoThresholdInterruptEnable
- kSPI_TxFifoThresholdInterruptEnable
|
| void SPI_DisableFifoInterrupts |
( |
SPI_Type * |
base, |
|
|
uint32_t |
irqs |
|
) |
| |
- Parameters
-
| base | SPI base pointer |
| irqs | SPI interrupt source. The parameter can be any combination of the following values:
- kSPI_RxFifoThresholdInterruptEnable
- kSPI_TxFifoThresholdInterruptEnable
|
| static bool SPI_IsMaster |
( |
SPI_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | SPI peripheral address. |
- Returns
- Returns true if the module is in master mode or false if the module is in slave mode.
| void* SPI_GetConfig |
( |
SPI_Type * |
base | ) |
|
- Parameters
-
| base | SPI peripheral address. |
- Returns
- return configurations which contain datawidth and SSEL numbers. return data type is a pointer of spi_config_t.
| status_t SPI_MasterSetBaud |
( |
SPI_Type * |
base, |
|
|
uint32_t |
baudrate_Bps, |
|
|
uint32_t |
srcClock_Hz |
|
) |
| |
This is only used in master.
- Parameters
-
| base | SPI base pointer |
| baudrate_Bps | baud rate needed in Hz. |
| srcClock_Hz | SPI source clock frequency in Hz. |
| void SPI_WriteData |
( |
SPI_Type * |
base, |
|
|
uint16_t |
data, |
|
|
uint32_t |
configFlags |
|
) |
| |
- Parameters
-
| base | SPI base pointer |
| data | needs to be write. |
| configFlags | transfer configuration options spi_xfer_option_t |
| uint32_t SPI_ReadData |
( |
SPI_Type * |
base | ) |
|
- Parameters
-
- Returns
- Data in the register.
the delay uint is SPI clock time, maximum value is 0xF.
- Parameters
-
| void SPI_SetDummyData |
( |
SPI_Type * |
base, |
|
|
uint8_t |
dummyData |
|
) |
| |
- Parameters
-
| base | SPI peripheral address. |
| dummyData | Data to be transferred when tx buffer is NULL. |
This function will enable the FIFO for SPI according to pointer of the configure struct. Note: If this API is called, please reset the baudrate to adapt your demand after this API was called.
- Parameters
-
| base | SPI peripheral base address. |
| config | pointer to FIFO configuration structure. |
| void SPI_DisableFifo |
( |
SPI_Type * |
base | ) |
|
This function will Disable the FIFO for SPI transfer. disable interrupts, clear status flags, disable the TX/RX FIFO, set fifo size to zero. But will not disable the system FIFO, because other instance like USART may using the FIFO.
- Parameters
-
| base | SPI peripheral base address. |
| config | pointer to FIFO configuration structure. |
| bool SPI_IsTxFifoEnabled |
( |
SPI_Type * |
base | ) |
|
This function will return status if the transmit fifo is enabled. true for enabled and false for not enabled.
- Parameters
-
| base | SPI peripheral base address. |
- Returns
- true for enabled and false for not enabled.
| bool SPI_IsRxFifoEnabled |
( |
SPI_Type * |
base | ) |
|
This function will return status if the receive fifo is enabled. true for enabled and false for not enabled.
- Parameters
-
| base | SPI peripheral base address. |
- Returns
- true for enabled and false for not enabled.
| void SPI_FifoFlush |
( |
SPI_Type * |
base, |
|
|
uint32_t |
direction |
|
) |
| |
This function will Flush tHE fifo buffer.
- Parameters
-
| base | SPI peripheral base address. |
| direction | the fifo direction need to flushed, Tx FIFO or Rx FIFO. |
This function initializes the SPI master handle which can be used for other SPI master transactional APIs. Usually, for a specified SPI instance, call this API once to get the initialized handle.
- Parameters
-
| base | SPI peripheral base address. |
| handle | SPI handle pointer. |
| callback | Callback function. |
| userData | User data. |
- Parameters
-
| base | SPI base pointer |
| xfer | pointer to spi_xfer_config_t structure |
- Return values
-
| kStatus_Success | Successfully start a transfer. |
| kStatus_InvalidArgument | Input argument is invalid. |
| status_t SPI_MasterTransferNonBlocking |
( |
SPI_Type * |
base, |
|
|
spi_master_handle_t * |
handle, |
|
|
spi_transfer_t * |
xfer |
|
) |
| |
- Parameters
-
| base | SPI peripheral base address. |
| handle | pointer to spi_master_handle_t structure which stores the transfer state |
| xfer | pointer to spi_xfer_config_t structure |
- Return values
-
| kStatus_Success | Successfully start a transfer. |
| kStatus_InvalidArgument | Input argument is invalid. |
| kStatus_SPI_Busy | SPI is not idle, is running another transfer. |
This function will do a half-duplex transfer for SPI master, This is a blocking function, which does not retuen until all transfer have been completed. And data transfer will be half-duplex, users can set transmit first or receive first.
- Parameters
-
- Returns
- status of status_t.
This function using polling way to do the first half transimission and using interrupts to do the srcond half transimission, the transfer mechanism is half-duplex. When do the second half transimission, code will return right away. When all data is transferred, the callback function is called.
- Parameters
-
| base | SPI peripheral base address. |
| handle | pointer to spi_master_handle_t structure which stores the transfer state |
| xfer | pointer to spi_half_duplex_transfer_t structure |
- Returns
- status of status_t.
| status_t SPI_MasterTransferGetCount |
( |
SPI_Type * |
base, |
|
|
spi_master_handle_t * |
handle, |
|
|
size_t * |
count |
|
) |
| |
This function gets the master transfer count.
- Parameters
-
| base | SPI peripheral base address. |
| handle | Pointer to the spi_master_handle_t structure which stores the transfer state. |
| count | The number of bytes transferred by using the non-blocking transaction. |
- Returns
- status of status_t.
| void SPI_MasterTransferAbort |
( |
SPI_Type * |
base, |
|
|
spi_master_handle_t * |
handle |
|
) |
| |
This function aborts a transfer using an interrupt.
- Parameters
-
| base | SPI peripheral base address. |
| handle | Pointer to the spi_master_handle_t structure which stores the transfer state. |
| void SPI_MasterTransferHandleIRQ |
( |
SPI_Type * |
base, |
|
|
spi_master_handle_t * |
handle |
|
) |
| |
- Parameters
-
| base | SPI peripheral base address. |
| handle | pointer to spi_master_handle_t structure which stores the transfer state. |
This function initializes the SPI slave handle which can be used for other SPI slave transactional APIs. Usually, for a specified SPI instance, call this API once to get the initialized handle.
- Parameters
-
| base | SPI peripheral base address. |
| handle | SPI handle pointer. |
| callback | Callback function. |
| userData | User data. |
- Note
- The API returns immediately after the transfer initialization is finished.
- Parameters
-
| base | SPI peripheral base address. |
| handle | pointer to spi_master_handle_t structure which stores the transfer state |
| xfer | pointer to spi_xfer_config_t structure |
- Return values
-
| kStatus_Success | Successfully start a transfer. |
| kStatus_InvalidArgument | Input argument is invalid. |
| kStatus_SPI_Busy | SPI is not idle, is running another transfer. |
This function gets the slave transfer count.
- Parameters
-
| base | SPI peripheral base address. |
| handle | Pointer to the spi_master_handle_t structure which stores the transfer state. |
| count | The number of bytes transferred by using the non-blocking transaction. |
- Returns
- status of status_t.
This function aborts a transfer using an interrupt.
- Parameters
-
| base | SPI peripheral base address. |
| handle | Pointer to the spi_slave_handle_t structure which stores the transfer state. |
- Parameters
-
| base | SPI peripheral base address. |
| handle | pointer to spi_slave_handle_t structure which stores the transfer state |
| volatile uint8_t s_dummyData[] |