MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
FLEXRAM: on-chip RAM manager

Overview

The MCUXpresso SDK provides a driver for the FLEXRAM module of MCUXpresso SDK devices.

The FLEXRAM module intergrates the ITCM, DTCM, and OCRAM controller, and supports parameterized RAM array and RAM array portioning.

This example code shows how to allocate RAM using the FLEXRAM driver.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/flexram

Data Structures

struct  flexram_allocate_ram_t
 FLEXRAM allocate ocram, itcm, dtcm size. More...
 

Enumerations

enum  _flexram_wr_rd_sel {
  kFLEXRAM_Read = 0U,
  kFLEXRAM_Write = 1U
}
 flexram write read sel More...
 
enum  _flexram_interrupt_status {
  kFLEXRAM_OCRAMAccessError = FLEXRAM_INT_STATUS_OCRAM_ERR_STATUS_MASK,
  kFLEXRAM_DTCMAccessError = FLEXRAM_INT_STATUS_DTCM_ERR_STATUS_MASK,
  kFLEXRAM_ITCMAccessError = FLEXRAM_INT_STATUS_ITCM_ERR_STATUS_MASK,
  kFLEXRAM_InterruptStatusAll
}
 Interrupt status flag mask. More...
 
enum  flexram_tcm_access_mode_t {
  kFLEXRAM_TCMAccessFastMode = 0U,
  kFLEXRAM_TCMAccessWaitMode = 1U
}
 FLEXRAM TCM access mode Fast access mode expected to be finished in 1-cycle Wait access mode expected to be finished in 2-cycle Wait access mode is a feature of the flexram and it should be used when the cpu clock too fast to finish tcm access in 1-cycle. More...
 
enum  _flexram_bank_type {
  kFLEXRAM_BankNotUsed = 0U,
  kFLEXRAM_BankOCRAM = 1U,
  kFLEXRAM_BankDTCM = 2U,
  kFLEXRAM_BankITCM = 3U
}
 FLEXRAM bank type. More...
 
enum  _flexram_tcm_size {
  kFLEXRAM_TCMSize32KB = 32 * 1024U,
  kFLEXRAM_TCMSize64KB = 64 * 1024U,
  kFLEXRAM_TCMSize128KB = 128 * 1024U,
  kFLEXRAM_TCMSize256KB = 256 * 1024U,
  kFLEXRAM_TCMSize512KB = 512 * 1024U
}
 FLEXRAM tcm support size. More...
 
enum  flexram_bank_allocate_src_t {
  kFLEXRAM_BankAllocateThroughHardwareFuse = 0U,
  kFLEXRAM_BankAllocateThroughBankCfg = 1U
}
 FLEXRAM bank allocate source. More...
 

Variables

const uint8_t flexram_allocate_ram_t::ocramBankNum
 ocram banknumber which the SOC support
 
const uint8_t flexram_allocate_ram_t::dtcmBankNum
 dtcm bank number to allocate, the number should be power of 2
 
const uint8_t flexram_allocate_ram_t::itcmBankNum
 itcm bank number to allocate, the number should be power of 2
 

Driver version

#define FSL_FLEXRAM_DRIVER_VERSION   (MAKE_VERSION(2U, 0U, 5U))
 Driver version 2.0.5. More...
 

Initialization and deinitialization

void FLEXRAM_Init (FLEXRAM_Type *base)
 FLEXRAM module initialization function. More...
 
void FLEXRAN_Deinit (FLEXRAM_Type *base)
 Deinitializes the FLEXRAM.
 

Status

static uint32_t FLEXRAM_GetInterruptStatus (FLEXRAM_Type *base)
 FLEXRAM module get interrupt status. More...
 
static void FLEXRAM_ClearInterruptStatus (FLEXRAM_Type *base, uint32_t status)
 FLEXRAM module clear interrupt status. More...
 
static void FLEXRAM_EnableInterruptStatus (FLEXRAM_Type *base, uint32_t status)
 FLEXRAM module enable interrupt status. More...
 
static void FLEXRAM_DisableInterruptStatus (FLEXRAM_Type *base, uint32_t status)
 FLEXRAM module disable interrupt status. More...
 

Interrupts

static void FLEXRAM_EnableInterruptSignal (FLEXRAM_Type *base, uint32_t status)
 FLEXRAM module enable interrupt. More...
 
static void FLEXRAM_DisableInterruptSignal (FLEXRAM_Type *base, uint32_t status)
 FLEXRAM module disable interrupt. More...
 

functional

static void FLEXRAM_SetTCMReadAccessMode (FLEXRAM_Type *base, flexram_tcm_access_mode_t mode)
 FLEXRAM module set TCM read access mode. More...
 
static void FLEXRAM_SetTCMWriteAccessMode (FLEXRAM_Type *base, flexram_tcm_access_mode_t mode)
 FLEXRAM module set TCM write access mode. More...
 
static void FLEXRAM_EnableForceRamClockOn (FLEXRAM_Type *base, bool enable)
 FLEXRAM module force ram clock on. More...
 
status_t FLEXRAM_AllocateRam (flexram_allocate_ram_t *config)
 FLEXRAM allocate on-chip ram for OCRAM,ITCM,DTCM This function is independent of FLEXRAM_Init, it can be called directly if ram re-allocate is needed. More...
 
static void FLEXRAM_SetAllocateRamSrc (flexram_bank_allocate_src_t src)
 FLEXRAM set allocate on-chip ram source. More...
 
void FLEXRAM_SetTCMSize (uint8_t itcmBankNum, uint8_t dtcmBankNum)
 FLEXRAM configure TCM size This function is used to set the TCM to the target size. More...
 

Data Structure Documentation

struct flexram_allocate_ram_t

Data Fields

const uint8_t ocramBankNum
 ocram banknumber which the SOC support
 
const uint8_t dtcmBankNum
 dtcm bank number to allocate, the number should be power of 2
 
const uint8_t itcmBankNum
 itcm bank number to allocate, the number should be power of 2
 

Macro Definition Documentation

#define FSL_FLEXRAM_DRIVER_VERSION   (MAKE_VERSION(2U, 0U, 5U))

Enumeration Type Documentation

Enumerator
kFLEXRAM_Read 

read

kFLEXRAM_Write 

write

Enumerator
kFLEXRAM_OCRAMAccessError 

ocram access unallocated address

kFLEXRAM_DTCMAccessError 

dtcm access unallocated address

kFLEXRAM_ITCMAccessError 

itcm access unallocated address

kFLEXRAM_InterruptStatusAll 

all the interrupt status mask

Normally, fast mode is the default mode, the efficiency of the tcm access will better.

Enumerator
kFLEXRAM_TCMAccessFastMode 

fast access mode

kFLEXRAM_TCMAccessWaitMode 

wait access mode

Enumerator
kFLEXRAM_BankNotUsed 

bank is not used

kFLEXRAM_BankOCRAM 

bank is OCRAM

kFLEXRAM_BankDTCM 

bank is DTCM

kFLEXRAM_BankITCM 

bank is ITCM

Enumerator
kFLEXRAM_TCMSize32KB 

TCM total size 32KB.

kFLEXRAM_TCMSize64KB 

TCM total size 64KB.

kFLEXRAM_TCMSize128KB 

TCM total size 128KB.

kFLEXRAM_TCMSize256KB 

TCM total size 256KB.

kFLEXRAM_TCMSize512KB 

TCM total size 512KB.

Enumerator
kFLEXRAM_BankAllocateThroughHardwareFuse 

allocate ram through hardware fuse value

kFLEXRAM_BankAllocateThroughBankCfg 

allocate ram through FLEXRAM_BANK_CFG

Function Documentation

void FLEXRAM_Init ( FLEXRAM_Type *  base)
Parameters
baseFLEXRAM base address.
static uint32_t FLEXRAM_GetInterruptStatus ( FLEXRAM_Type *  base)
inlinestatic
Parameters
baseFLEXRAM base address.
static void FLEXRAM_ClearInterruptStatus ( FLEXRAM_Type *  base,
uint32_t  status 
)
inlinestatic
Parameters
baseFLEXRAM base address.
statusstatus to clear.
static void FLEXRAM_EnableInterruptStatus ( FLEXRAM_Type *  base,
uint32_t  status 
)
inlinestatic
Parameters
baseFLEXRAM base address.
statusstatus to enable.
static void FLEXRAM_DisableInterruptStatus ( FLEXRAM_Type *  base,
uint32_t  status 
)
inlinestatic
Parameters
baseFLEXRAM base address.
statusstatus to disable.
static void FLEXRAM_EnableInterruptSignal ( FLEXRAM_Type *  base,
uint32_t  status 
)
inlinestatic
Parameters
baseFLEXRAM base address.
statusstatus interrupt to enable.
static void FLEXRAM_DisableInterruptSignal ( FLEXRAM_Type *  base,
uint32_t  status 
)
inlinestatic
Parameters
baseFLEXRAM base address.
statusstatus interrupt to disable.
static void FLEXRAM_SetTCMReadAccessMode ( FLEXRAM_Type *  base,
flexram_tcm_access_mode_t  mode 
)
inlinestatic
Parameters
baseFLEXRAM base address.
modeaccess mode.
static void FLEXRAM_SetTCMWriteAccessMode ( FLEXRAM_Type *  base,
flexram_tcm_access_mode_t  mode 
)
inlinestatic
Parameters
baseFLEXRAM base address.
modeaccess mode.
static void FLEXRAM_EnableForceRamClockOn ( FLEXRAM_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseFLEXRAM base address.
enableenable or disable clock force on.
status_t FLEXRAM_AllocateRam ( flexram_allocate_ram_t *  config)
Parameters
configallocate configuration.
Return values
kStatus_InvalidArgumentthe argument is invalid kStatus_Success allocate success
static void FLEXRAM_SetAllocateRamSrc ( flexram_bank_allocate_src_t  src)
inlinestatic
Parameters
srcbank config source select value.
void FLEXRAM_SetTCMSize ( uint8_t  itcmBankNum,
uint8_t  dtcmBankNum 
)

If a odd bank number is used, a new banknumber will be used which is bigger than target value, application can set tcm size to the biggest bank number always, then boundary access error can be captured by flexram only. When access to the TCM memory boundary ,hardfault will raised by core.

Parameters
itcmBankNumitcm bank number to allocate
dtcmBankNumdtcm bank number to allocate