![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Packet32.h contains the data structures and the definitions used by packet.dll. The file is used both by the Win9x and the WinNTx versions of packet.dll, and can be included by the applications that use the functions of this library
Data Structures | |
| struct | NetType |
| Network type structure. More... | |
| struct | bpf_program |
| A BPF pseudo-assembly program. More... | |
| struct | bpf_insn |
| A single BPF pseudo-instruction. More... | |
| struct | bpf_stat |
| Structure that contains a couple of statistics values on the current capture. More... | |
| struct | bpf_hdr |
| Packet header. More... | |
| struct | dump_bpf_hdr |
| Dump packet header. More... | |
| struct | npf_if_addr |
| Addresses of a network adapter. More... | |
| struct | LPADAPTER |
| Describes an opened network adapter. More... | |
| struct | LPPACKET |
| Structure that contains a group of packets coming from the driver. More... | |
| struct | PPACKET_OID_DATA |
| Structure containing an OID request. More... | |
Variables | |
| UINT | NetType::LinkType |
| The MAC of the current network adapter (see function PacketGetNetType() for more information) | |
| ULONGLONG | NetType::LinkSpeed |
| The speed of the network in bits per second. | |
| UINT | bpf_program::bf_len |
| Indicates the number of instructions of the program, i.e. the number of struct bpf_insn that will follow. | |
| struct bpf_insn * | bpf_program::bf_insns |
| A pointer to the first instruction of the program. | |
| USHORT | bpf_insn::code |
| Instruction type and addressing mode. | |
| UCHAR | bpf_insn::jt |
| Jump if true. | |
| UCHAR | bpf_insn::jf |
| Jump if false. | |
| int | bpf_insn::k |
| Generic field used for various purposes. | |
| UINT | bpf_stat::bs_recv |
| UINT | bpf_stat::bs_drop |
| UINT | bpf_stat::ps_ifdrop |
| drops by interface. XXX not yet supported | |
| UINT | bpf_stat::bs_capt |
| struct timeval | bpf_hdr::bh_tstamp |
| UINT | bpf_hdr::bh_caplen |
| UINT | bpf_hdr::bh_datalen |
| Original length of packet. | |
| USHORT | bpf_hdr::bh_hdrlen |
| struct timeval | dump_bpf_hdr::ts |
| Time stamp of the packet. | |
| UINT | dump_bpf_hdr::caplen |
| UINT | dump_bpf_hdr::len |
| Length of the original packet (off wire). | |
| struct sockaddr_storage | npf_if_addr::IPAddress |
| IP address. | |
| struct sockaddr_storage | npf_if_addr::SubnetMask |
| Netmask for that address. | |
| struct sockaddr_storage | npf_if_addr::Broadcast |
| Broadcast address. | |
| HANDLE | LPADAPTER::ReadEvent |
| UINT | LPADAPTER::Flags |
| Adapter's flags. Tell if this adapter must be treated in a different way, using the Netmon API or the dagc API. | |
| HANDLE | LPPACKET::hEvent |
| OVERLAPPED | LPPACKET::OverLapped |
| PVOID | LPPACKET::Buffer |
| UINT | LPPACKET::Length |
| Length of the buffer. | |
| DWORD | LPPACKET::ulBytesReceived |
| BOOLEAN | LPPACKET::bIoComplete |
| ULONG | PPACKET_OID_DATA::Oid |
| ULONG | PPACKET_OID_DATA::Length |
| Length of the data field. | |
| UCHAR | PPACKET_OID_DATA::Data [1] |
| typedef struct WAN_ADAPTER_INT | WAN_ADAPTER |
| Describes an opened wan (dialup, VPN...) network adapter using the NetMon API. | |
| typedef WAN_ADAPTER * | PWAN_ADAPTER |
| Describes an opened wan (dialup, VPN...) network adapter using the NetMon API. | |
| #define | PACKET_MODE_CAPT 0x0 |
| Capture mode. | |
| #define | PACKET_MODE_STAT 0x1 |
| Statistical mode. | |
| #define | PACKET_MODE_MON 0x2 |
| Monitoring mode. | |
| #define | PACKET_MODE_DUMP 0x10 |
| Dump mode. | |
| #define | PACKET_MODE_STAT_DUMP MODE_DUMP | MODE_STAT |
| Statistical dump Mode. | |
| #define | Packet_ALIGNMENT sizeof(int) |
| Alignment macro. Defines the alignment size. | |
| #define | Packet_WORDALIGN(x) (((x)+(Packet_ALIGNMENT-1))&~(Packet_ALIGNMENT-1)) |
| Alignment macro. Rounds up to the next even multiple of Packet_ALIGNMENT. | |
| #define | NdisMediumNull -1 |
| Custom linktype: NDIS doesn't provide an equivalent. | |
| #define | NdisMediumCHDLC -2 |
| Custom linktype: NDIS doesn't provide an equivalent. | |
| #define | NdisMediumPPPSerial -3 |
| Custom linktype: NDIS doesn't provide an equivalent. | |
| #define | NdisMediumBare80211 -4 |
| Custom linktype: NDIS doesn't provide an equivalent. | |
| #define | NdisMediumRadio80211 -5 |
| Custom linktype: NDIS doesn't provide an equivalent. | |
| #define | NdisMediumPpi -6 |
| Custom linktype: NDIS doesn't provide an equivalent. | |
| #define | NPF_DISABLE_LOOPBACK 1 |
| Drop the packets sent by the NPF driver. | |
| #define | NPF_ENABLE_LOOPBACK 2 |
| Capture the packets sent by the NPF driver. | |
| #define | DOSNAMEPREFIX TEXT("Packet_") |
| Prefix added to the adapters device names to create the WinPcap devices. | |
| #define | ADAPTER_NAME_LENGTH 256 + 12 |
| Maximum length for the name of an adapter. The value is the same used by the IP Helper API. | |
| #define | ADAPTER_DESC_LENGTH 128 |
| Maximum length for the description of an adapter. The value is the same used by the IP Helper API. | |
| #define | MAX_MAC_ADDR_LENGTH 8 |
| Maximum length for the link layer address of an adapter. The value is the same used by the IP Helper API. | |
| #define | MAX_NETWORK_ADDRESSES 16 |
| Maximum length for the link layer address of an adapter. The value is the same used by the IP Helper API. | |
| #define | INFO_FLAG_NDIS_ADAPTER 0 |
| Flag for ADAPTER_INFO: this is a traditional ndis adapter. | |
| #define | INFO_FLAG_NDISWAN_ADAPTER 1 |
| Flag for ADAPTER_INFO: this is a NdisWan adapter, and it's managed by WANPACKET. | |
| #define | INFO_FLAG_DAG_CARD 2 |
| Flag for ADAPTER_INFO: this is a DAG card. | |
| #define | INFO_FLAG_DAG_FILE 6 |
| Flag for ADAPTER_INFO: this is a DAG file. | |
| #define | INFO_FLAG_DONT_EXPORT 8 |
| Flag for ADAPTER_INFO: when this flag is set, the adapter will not be listed or openend by winpcap. This allows to prevent exporting broken network adapters, like for example FireWire ones. | |
| #define | INFO_FLAG_AIRPCAP_CARD 16 |
| Flag for ADAPTER_INFO: this is an airpcap card. | |
| struct NetType |
This structure is used by the PacketGetNetType() function to return information on the current adapter's type and speed.
Data Fields | |
| UINT | LinkType |
| The MAC of the current network adapter (see function PacketGetNetType() for more information) | |
| ULONGLONG | LinkSpeed |
| The speed of the network in bits per second. | |
| struct bpf_program |
The program will be injected in the kernel by the PacketSetBPF() function and applied to every incoming packet.
Data Fields | |
| UINT | bf_len |
| Indicates the number of instructions of the program, i.e. the number of struct bpf_insn that will follow. | |
| struct bpf_insn * | bf_insns |
| A pointer to the first instruction of the program. | |
| struct bpf_insn |
| struct bpf_stat |
| struct bpf_hdr |
This structure defines the header associated with every packet delivered to the application.
Data Fields | |
| struct timeval | bh_tstamp |
| UINT | bh_caplen |
| UINT | bh_datalen |
| Original length of packet. | |
| USHORT | bh_hdrlen |
| struct dump_bpf_hdr |
This structure defines the header associated with the packets in a buffer to be used with PacketSendPackets(). It is simpler than the bpf_hdr, because it corresponds to the header associated by WinPcap and libpcap to a packet in a dump file. This makes straightforward sending WinPcap dump files to the network.
Data Fields | |
| struct timeval | ts |
| Time stamp of the packet. | |
| UINT | caplen |
| UINT | len |
| Length of the original packet (off wire). | |
| struct npf_if_addr |
This structure is used by the PacketGetNetInfoEx() function to return the IP addresses associated with an adapter.
Data Fields | |
| struct sockaddr_storage | IPAddress |
| IP address. | |
| struct sockaddr_storage | SubnetMask |
| Netmask for that address. | |
| struct sockaddr_storage | Broadcast |
| Broadcast address. | |
| struct ADAPTER |
This structure is the most important for the functioning of packet.dll, but the great part of its fields should be ignored by the user, since the library offers functions that avoid to cope with low-level parameters
Data Fields | |
| HANDLE | ReadEvent |
| UINT | Flags |
| Adapter's flags. Tell if this adapter must be treated in a different way, using the Netmon API or the dagc API. | |
| struct PACKET |
This structure defines the header associated with every packet delivered to the application.
Data Fields | |
| HANDLE | hEvent |
| OVERLAPPED | OverLapped |
| PVOID | Buffer |
| UINT | Length |
| Length of the buffer. | |
| DWORD | ulBytesReceived |
| BOOLEAN | bIoComplete |
| struct _PACKET_OID_DATA |
It is used by the PacketRequest() function to send an OID to the interface card driver. It can be used, for example, to retrieve the status of the error counters on the adapter, its MAC address, the list of the multicast groups defined on it, and so on.
Data Fields | |
| ULONG | Oid |
| ULONG | Length |
| Length of the data field. | |
| UCHAR | Data [1] |
| UINT bpf_stat::bs_recv |
Number of packets that the driver received from the network adapter from the beginning of the current capture. This value includes the packets lost by the driver.
| UINT bpf_stat::bs_drop |
number of packets that the driver lost from the beginning of a capture. Basically, a packet is lost when the the buffer of the driver is full. In this situation the packet cannot be stored and the driver rejects it.
| UINT bpf_stat::bs_capt |
number of packets that pass the filter, find place in the kernel buffer and thus reach the application.
| struct timeval bpf_hdr::bh_tstamp |
The timestamp associated with the captured packet. It is stored in a TimeVal structure.
| UINT bpf_hdr::bh_caplen |
Length of captured portion. The captured portion can be different from the original packet, because it is possible (with a proper filter) to instruct the driver to capture only a portion of the packets.
| USHORT bpf_hdr::bh_hdrlen |
Length of bpf header (this struct plus alignment padding). In some cases, a padding could be added between the end of this structure and the packet data for performance reasons. This filed can be used to retrieve the actual data of the packet.
| UINT dump_bpf_hdr::caplen |
Length of captured portion. The captured portion can smaller than the the original packet, because it is possible (with a proper filter) to instruct the driver to capture only a portion of the packets.
| HANDLE LPADAPTER::ReadEvent |
A notification event associated with the read calls on the adapter. It can be passed to standard Win32 functions (like WaitForSingleObject or WaitForMultipleObjects) to wait until the driver's buffer contains some data. It is particularly useful in GUI applications that need to wait concurrently on several events. In Windows NT/2000 the PacketSetMinToCopy() function can be used to define the minimum amount of data in the kernel buffer that will cause the event to be signalled.
| HANDLE LPPACKET::hEvent |
| OVERLAPPED LPPACKET::OverLapped |
| PVOID LPPACKET::Buffer |
Buffer with containing the packets. See the PacketReceivePacket() for details about the organization of the data in this buffer
| DWORD LPPACKET::ulBytesReceived |
Number of valid bytes present in the buffer, i.e. amount of data received by the last call to PacketReceivePacket()
| BOOLEAN LPPACKET::bIoComplete |
| ULONG PPACKET_OID_DATA::Oid |
OID code. See the Microsoft DDK documentation or the file ntddndis.h for a complete list of valid codes.
| UCHAR PPACKET_OID_DATA::Data[1] |
variable-lenght field that contains the information passed to or received from the adapter.