The MCUXpresso SDK provides a peripheral driver for the LCD Interface v2(LCDIFv2)
The LCDIFv2 supports RGB mode (dot clock mode), it supports up to maximum 8 layers of alpha blending.
Shadow load
Shadow registers are used for LCDIFv2 layer configuration, when layer configurations are set, they are written to the shadow registers and do not take effect, after the function LCDIFV2_TriggerLayerShadowLoad is called, the new configuration are loaded to the active control registers at next vertical blank period. This mechanism ensures that all configurations are loaded at the same time.
Frame store
The LCDIFv2 supports saving the output frame data to memory, application can choose two mode:
- One shot mode
- Repeat mode
In one shot mode, the store process stops after one frame store finished. In repeat mode, the LCDIFv2 continues storing the new frame to the same address, it does not stop storing until reset.
Typical use case
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/lcdifv2
|
| enum | _lcdifv2_polarity_flags {
kLCDIFV2_VsyncActiveLow = LCDIFV2_CTRL_INV_VS_MASK,
kLCDIFV2_VsyncActiveHigh = 0U,
kLCDIFV2_HsyncActiveLow = LCDIFV2_CTRL_INV_HS_MASK,
kLCDIFV2_HsyncActiveHigh = 0U,
kLCDIFV2_DataEnableActiveLow = LCDIFV2_CTRL_INV_DE_MASK,
kLCDIFV2_DataEnableActiveHigh = 0U,
kLCDIFV2_DriveDataOnFallingClkEdge = LCDIFV2_CTRL_INV_PXCK_MASK,
kLCDIFV2_DriveDataOnRisingClkEdge = 0U,
kLCDIFV2_DataActiveLow = LCDIFV2_CTRL_NEG_MASK,
kLCDIFV2_DataActiveHigh = 0U
} |
| | LCDIF v2 signal polarity flags. More...
|
| |
| enum | _lcdifv2_interrupt {
kLCDIFV2_Layer0FifoEmptyInterrupt = LCDIFV2_MAKE_FIFO_EMPTY_INTERRUPT(0),
kLCDIFV2_Layer1FifoEmptyInterrupt = LCDIFV2_MAKE_FIFO_EMPTY_INTERRUPT(1),
kLCDIFV2_Layer2FifoEmptyInterrupt = LCDIFV2_MAKE_FIFO_EMPTY_INTERRUPT(2),
kLCDIFV2_Layer3FifoEmptyInterrupt = LCDIFV2_MAKE_FIFO_EMPTY_INTERRUPT(3),
kLCDIFV2_Layer4FifoEmptyInterrupt = LCDIFV2_MAKE_FIFO_EMPTY_INTERRUPT(4),
kLCDIFV2_Layer5FifoEmptyInterrupt = LCDIFV2_MAKE_FIFO_EMPTY_INTERRUPT(5),
kLCDIFV2_Layer6FifoEmptyInterrupt = LCDIFV2_MAKE_FIFO_EMPTY_INTERRUPT(6),
kLCDIFV2_Layer7FifoEmptyInterrupt = LCDIFV2_MAKE_FIFO_EMPTY_INTERRUPT(7),
kLCDIFV2_Layer0DmaDoneInterrupt = LCDIFV2_MAKE_DMA_DONE_INTERRUPT(0),
kLCDIFV2_Layer1DmaDoneInterrupt = LCDIFV2_MAKE_DMA_DONE_INTERRUPT(1),
kLCDIFV2_Layer2DmaDoneInterrupt = LCDIFV2_MAKE_DMA_DONE_INTERRUPT(2),
kLCDIFV2_Layer3DmaDoneInterrupt = LCDIFV2_MAKE_DMA_DONE_INTERRUPT(3),
kLCDIFV2_Layer4DmaDoneInterrupt = LCDIFV2_MAKE_DMA_DONE_INTERRUPT(4),
kLCDIFV2_Layer5DmaDoneInterrupt = LCDIFV2_MAKE_DMA_DONE_INTERRUPT(5),
kLCDIFV2_Layer6DmaDoneInterrupt = LCDIFV2_MAKE_DMA_DONE_INTERRUPT(6),
kLCDIFV2_Layer7DmaDoneInterrupt = LCDIFV2_MAKE_DMA_DONE_INTERRUPT(7),
kLCDIFV2_Layer0DmaErrorInterrupt = LCDIFV2_MAKE_DMA_ERROR_INTERRUPT(0),
kLCDIFV2_Layer1DmaErrorInterrupt = LCDIFV2_MAKE_DMA_ERROR_INTERRUPT(1),
kLCDIFV2_Layer2DmaErrorInterrupt = LCDIFV2_MAKE_DMA_ERROR_INTERRUPT(2),
kLCDIFV2_Layer3DmaErrorInterrupt = LCDIFV2_MAKE_DMA_ERROR_INTERRUPT(3),
kLCDIFV2_Layer4DmaErrorInterrupt = LCDIFV2_MAKE_DMA_ERROR_INTERRUPT(4),
kLCDIFV2_Layer5DmaErrorInterrupt = LCDIFV2_MAKE_DMA_ERROR_INTERRUPT(5),
kLCDIFV2_Layer6DmaErrorInterrupt = LCDIFV2_MAKE_DMA_ERROR_INTERRUPT(6),
kLCDIFV2_Layer7DmaErrorInterrupt = LCDIFV2_MAKE_DMA_ERROR_INTERRUPT(7),
kLCDIFV2_StoreErrorInterrupt = (1U << 5U),
kLCDIFV2_StoreFrameDoneInterrupt = (1U << 4U),
kLCDIFV2_VerticalBlankingInterrupt = (1U << 2U),
kLCDIFV2_OutputUnderrunInterrupt = (1U << 1U),
kLCDIFV2_VsyncEdgeInterrupt = (1U << 0U)
} |
| | The LCDIF v2 interrupts. More...
|
| |
| enum | lcdifv2_line_order_t {
kLCDIFV2_LineOrderRGB = 0,
kLCDIFV2_LineOrderRBG,
kLCDIFV2_LineOrderGBR,
kLCDIFV2_LineOrderGRB,
kLCDIFV2_LineOrderBRG,
kLCDIFV2_LineOrderBGR
} |
| | The LCDIF v2 output line order. More...
|
| |
| enum | lcdifv2_csc_mode_t {
kLCDIFV2_CscDisable = 0U,
kLCDIFV2_CscYUV2RGB,
kLCDIFV2_CscYCbCr2RGB
} |
| | LCDIF v2 color space conversion mode. More...
|
| |
| enum | lcdifv2_pixel_format_t {
kLCDIFV2_PixelFormatIndex1BPP = LCDIFV2_CTRLDESCL5_BPP(0U),
kLCDIFV2_PixelFormatIndex2BPP = LCDIFV2_CTRLDESCL5_BPP(1U),
kLCDIFV2_PixelFormatIndex4BPP = LCDIFV2_CTRLDESCL5_BPP(2U),
kLCDIFV2_PixelFormatIndex8BPP = LCDIFV2_CTRLDESCL5_BPP(3U),
kLCDIFV2_PixelFormatRGB565 = LCDIFV2_CTRLDESCL5_BPP(4U),
kLCDIFV2_PixelFormatARGB1555 = LCDIFV2_CTRLDESCL5_BPP(5U),
kLCDIFV2_PixelFormatARGB4444 = LCDIFV2_CTRLDESCL5_BPP(6U),
kLCDIFV2_PixelFormatUYVY,
kLCDIFV2_PixelFormatVYUY,
kLCDIFV2_PixelFormatYUYV,
kLCDIFV2_PixelFormatYVYU,
kLCDIFV2_PixelFormatRGB888 = LCDIFV2_CTRLDESCL5_BPP(8U),
kLCDIFV2_PixelFormatARGB8888 = LCDIFV2_CTRLDESCL5_BPP(9U),
kLCDIFV2_PixelFormatABGR8888 = LCDIFV2_CTRLDESCL5_BPP(10U)
} |
| |
| enum | lcdifv2_alpha_mode_t {
kLCDIFV2_AlphaDisable,
kLCDIFV2_AlphaOverride,
kLCDIFV2_AlphaEmbedded,
kLCDIFV2_AlphaPoterDuff
} |
| | LCDIF v2 layer alpha blending mode. More...
|
| |
| enum | lcdifv2_pd_alpha_mode_t {
kLCDIFV2_PD_AlphaStraight = 0,
kLCDIFV2_PD_AlphaInversed = 1
} |
| | LCDIF v2 PoterDuff alpha mode. More...
|
| |
| enum | lcdifv2_pd_color_mode_t {
kLCDIFV2_PD_ColorStraight = 0,
kLCDIFV2_PD_ColorInversed = 1
} |
| | LCDIF v2 PoterDuff color mode. More...
|
| |
| enum | lcdifv2_pd_global_alpha_mode_t {
kLCDIFV2_PD_GlobalAlpha = 0,
kLCDIFV2_PD_LocalAlpha = 1,
kLCDIFV2_PD_ScaledAlpha = 2
} |
| | LCDIF v2 PoterDuff global alpha mode. More...
|
| |
| enum | lcdifv2_pd_factor_mode_t {
kLCDIFV2_PD_FactorOne = 0,
kLCDIFV2_PD_FactorZero = 1,
kLCDIFV2_PD_FactorStraightAlpha = 2,
kLCDIFV2_PD_FactorInversedAlpha = 3
} |
| | LCDIF v2 PoterDuff factor mode. More...
|
| |
| enum | lcdifv2_store_pixel_format_t {
kLCDIFV2_StorePixelFormatARGB8888,
kLCDIFV2_StorePixelFormatRGB888
} |
| | LCDIF v2 write buffer pixel format. More...
|
| |
|
| uint16_t | lcdifv2_display_config_t::panelWidth |
| | Display panel width, pixels per line. More...
|
| |
| uint16_t | lcdifv2_display_config_t::panelHeight |
| | Display panel height, how many lines per panel. More...
|
| |
| uint8_t | lcdifv2_display_config_t::hsw |
| | HSYNC pulse width. More...
|
| |
| uint8_t | lcdifv2_display_config_t::hfp |
| | Horizontal front porch. More...
|
| |
| uint8_t | lcdifv2_display_config_t::hbp |
| | Horizontal back porch. More...
|
| |
| uint8_t | lcdifv2_display_config_t::vsw |
| | VSYNC pulse width. More...
|
| |
| uint8_t | lcdifv2_display_config_t::vfp |
| | Vrtical front porch. More...
|
| |
| uint8_t | lcdifv2_display_config_t::vbp |
| | Vertical back porch. More...
|
| |
| uint32_t | lcdifv2_display_config_t::polarityFlags |
| | OR'ed value of _lcdifv2_polarity_flags, used to contol the signal polarity. More...
|
| |
| lcdifv2_line_order_t | lcdifv2_display_config_t::lineOrder |
| | Line order. More...
|
| |
| uint16_t | lcdifv2_buffer_config_t::strideBytes |
| | Number of bytes between two vertically adjacent pixels, suggest 64-bit aligned. More...
|
| |
| lcdifv2_pixel_format_t | lcdifv2_buffer_config_t::pixelFormat |
| | Source buffer pixel format. More...
|
| |
|
uint8_t | lcdifv2_blend_config_t::globalAlpha |
| | Global alpha value, only used when alphaMode is kLCDIFV2_AlphaOverride or kLCDIFV2_AlphaPoterDuff.
|
| |
| lcdifv2_alpha_mode_t | lcdifv2_blend_config_t::alphaMode |
| | Alpha mode. More...
|
| |
|
lcdifv2_pd_alpha_mode_t | lcdifv2_blend_config_t::pdAlphaMode |
| | PoterDuff alpha mode, only used when alphaMode is kLCDIFV2_AlphaPoterDuff.
|
| |
|
lcdifv2_pd_color_mode_t | lcdifv2_blend_config_t::pdColorMode |
| | PoterDuff color mode, only used when alphaMode is kLCDIFV2_AlphaPoterDuff.
|
| |
|
lcdifv2_pd_global_alpha_mode_t | lcdifv2_blend_config_t::pdGlobalAlphaMode |
| | PoterDuff global alpha mode, only used when @ref alphaMode is
kLCDIFV2_AlphaPoterDuff
|
| |
|
lcdifv2_pd_factor_mode_t | lcdifv2_blend_config_t::pdFactorMode |
| | PoterDuff factor mode, only used when @ref alphaMode is @ref
kLCDIFV2_AlphaPoterDuff
|
| |
| uint32_t | lcdifv2_store_buffer_config_t::bufferAddr |
| | Output buffer address, suggest 64-bit aligned for better performance. More...
|
| |
| uint16_t | lcdifv2_store_buffer_config_t::strideBytes |
| | Number of bytes between two vertically adjacent pixels, suggest 64-bit aligned for better performance. More...
|
| |
| lcdifv2_store_pixel_format_t | lcdifv2_store_buffer_config_t::pixelFormat |
| | Store pixel format. More...
|
| |
| struct lcdifv2_display_config_t |
| struct lcdifv2_buffer_config_t |
| struct lcdifv2_blend_config_t |
| #define LCDIFV2_MAKE_FIFO_EMPTY_INTERRUPT |
( |
|
layer | ) |
(1U << ((uint32_t)(layer) + 24U)) |
| #define LCDIFV2_MAKE_DMA_DONE_INTERRUPT |
( |
|
layer | ) |
(1U << ((uint32_t)(layer) + 16U)) |
| #define LCDIFV2_MAKE_DMA_ERROR_INTERRUPT |
( |
|
layer | ) |
(1U << ((uint32_t)(layer) + 8U)) |
| Enumerator |
|---|
| kLCDIFV2_VsyncActiveLow |
VSYNC active low.
|
| kLCDIFV2_VsyncActiveHigh |
VSYNC active high.
|
| kLCDIFV2_HsyncActiveLow |
HSYNC active low.
|
| kLCDIFV2_HsyncActiveHigh |
HSYNC active high.
|
| kLCDIFV2_DataEnableActiveLow |
Data enable line active low.
|
| kLCDIFV2_DataEnableActiveHigh |
Data enable line active high.
|
| kLCDIFV2_DriveDataOnFallingClkEdge |
Drive data on falling clock edge, capture data on rising clock edge.
|
| kLCDIFV2_DriveDataOnRisingClkEdge |
Drive data on falling clock edge, capture data on rising clock edge.
|
| kLCDIFV2_DataActiveLow |
Data active high.
|
| kLCDIFV2_DataActiveHigh |
Data active high.
|
| Enumerator |
|---|
| kLCDIFV2_Layer0FifoEmptyInterrupt |
Layer 0 FIFO empty.
|
| kLCDIFV2_Layer1FifoEmptyInterrupt |
Layer 1 FIFO empty.
|
| kLCDIFV2_Layer2FifoEmptyInterrupt |
Layer 2 FIFO empty.
|
| kLCDIFV2_Layer3FifoEmptyInterrupt |
Layer 3 FIFO empty.
|
| kLCDIFV2_Layer4FifoEmptyInterrupt |
Layer 4 FIFO empty.
|
| kLCDIFV2_Layer5FifoEmptyInterrupt |
Layer 5 FIFO empty.
|
| kLCDIFV2_Layer6FifoEmptyInterrupt |
Layer 6 FIFO empty.
|
| kLCDIFV2_Layer7FifoEmptyInterrupt |
Layer 7 FIFO empty.
|
| kLCDIFV2_Layer0DmaDoneInterrupt |
Layer 0 DMA done.
|
| kLCDIFV2_Layer1DmaDoneInterrupt |
Layer 1 DMA done.
|
| kLCDIFV2_Layer2DmaDoneInterrupt |
Layer 2 DMA done.
|
| kLCDIFV2_Layer3DmaDoneInterrupt |
Layer 3 DMA done.
|
| kLCDIFV2_Layer4DmaDoneInterrupt |
Layer 4 DMA done.
|
| kLCDIFV2_Layer5DmaDoneInterrupt |
Layer 5 DMA done.
|
| kLCDIFV2_Layer6DmaDoneInterrupt |
Layer 6 DMA done.
|
| kLCDIFV2_Layer7DmaDoneInterrupt |
Layer 7 DMA done.
|
| kLCDIFV2_Layer0DmaErrorInterrupt |
Layer 0 DMA error.
|
| kLCDIFV2_Layer1DmaErrorInterrupt |
Layer 1 DMA error.
|
| kLCDIFV2_Layer2DmaErrorInterrupt |
Layer 2 DMA error.
|
| kLCDIFV2_Layer3DmaErrorInterrupt |
Layer 3 DMA error.
|
| kLCDIFV2_Layer4DmaErrorInterrupt |
Layer 4 DMA error.
|
| kLCDIFV2_Layer5DmaErrorInterrupt |
Layer 5 DMA error.
|
| kLCDIFV2_Layer6DmaErrorInterrupt |
Layer 6 DMA error.
|
| kLCDIFV2_Layer7DmaErrorInterrupt |
Layer 7 DMA error.
|
| kLCDIFV2_StoreErrorInterrupt |
Store frame error on AXI interface.
|
| kLCDIFV2_StoreFrameDoneInterrupt |
Current frame being stored has finished.
|
| kLCDIFV2_VerticalBlankingInterrupt |
Start of vertical blanking period.
|
| kLCDIFV2_OutputUnderrunInterrupt |
Output buffer underrun.
|
| kLCDIFV2_VsyncEdgeInterrupt |
Interrupt at VSYNC edge.
|
| Enumerator |
|---|
| kLCDIFV2_LineOrderRGB |
RGB.
|
| kLCDIFV2_LineOrderRBG |
RBG.
|
| kLCDIFV2_LineOrderGBR |
GBR.
|
| kLCDIFV2_LineOrderGRB |
GRB.
|
| kLCDIFV2_LineOrderBRG |
BRG.
|
| kLCDIFV2_LineOrderBGR |
BGR.
|
| Enumerator |
|---|
| kLCDIFV2_CscDisable |
Disable the CSC.
|
| kLCDIFV2_CscYUV2RGB |
YUV to RGB.
|
| kLCDIFV2_CscYCbCr2RGB |
YCbCr to RGB.
|
| Enumerator |
|---|
| kLCDIFV2_PixelFormatIndex1BPP |
LUT index 1 bit.
|
| kLCDIFV2_PixelFormatIndex2BPP |
LUT index 2 bit.
|
| kLCDIFV2_PixelFormatIndex4BPP |
LUT index 4 bit.
|
| kLCDIFV2_PixelFormatIndex8BPP |
LUT index 8 bit.
|
| kLCDIFV2_PixelFormatRGB565 |
RGB565, two pixels use 32 bits.
|
| kLCDIFV2_PixelFormatARGB1555 |
ARGB1555, two pixels use 32 bits.
|
| kLCDIFV2_PixelFormatARGB4444 |
ARGB4444, two pixels use 32 bits.
|
| kLCDIFV2_PixelFormatUYVY |
UYVY, only layer 0 and layer 1 support this.
|
| kLCDIFV2_PixelFormatVYUY |
VYUY, only layer 0 and layer 1 support this.
|
| kLCDIFV2_PixelFormatYUYV |
YUYV, only layer 0 and layer 1 support this.
|
| kLCDIFV2_PixelFormatYVYU |
YVYU, only layer 0 and layer 1 support this.
|
| kLCDIFV2_PixelFormatRGB888 |
RGB888 packed, one pixel uses 24 bits.
|
| kLCDIFV2_PixelFormatARGB8888 |
ARGB8888 unpacked, one pixel uses 32 bits.
|
| kLCDIFV2_PixelFormatABGR8888 |
ABGR8888 unpacked, one pixel uses 32 bits.
|
| Enumerator |
|---|
| kLCDIFV2_AlphaDisable |
Disable alpha blend.
|
| kLCDIFV2_AlphaOverride |
Use the gobal alpha value, pixel defined alpha value is overridden.
|
| kLCDIFV2_AlphaEmbedded |
Use the pixel defined alpha value.
|
| kLCDIFV2_AlphaPoterDuff |
Use the PoterDuff alpha blending.
|
| Enumerator |
|---|
| kLCDIFV2_PD_AlphaStraight |
Straight mode.
|
| kLCDIFV2_PD_AlphaInversed |
Inversed mode.
|
| Enumerator |
|---|
| kLCDIFV2_PD_ColorStraight |
Straight mode.
|
| kLCDIFV2_PD_ColorInversed |
Inversed mode.
|
| Enumerator |
|---|
| kLCDIFV2_PD_GlobalAlpha |
Use global alpha.
|
| kLCDIFV2_PD_LocalAlpha |
Use local alpha.
|
| kLCDIFV2_PD_ScaledAlpha |
Use scaled alpha.
|
| Enumerator |
|---|
| kLCDIFV2_PD_FactorOne |
Use 1.
|
| kLCDIFV2_PD_FactorZero |
Use 0.
|
| kLCDIFV2_PD_FactorStraightAlpha |
Use straight alpha.
|
| kLCDIFV2_PD_FactorInversedAlpha |
Use inversed alpha.
|
| Enumerator |
|---|
| kLCDIFV2_StorePixelFormatARGB8888 |
32-bpp ARGB8888.
|
| kLCDIFV2_StorePixelFormatRGB888 |
24-bpp RGB888.
|
| void LCDIFV2_Init |
( |
LCDIFV2_Type * |
base | ) |
|
This function ungates the LCDIF v2 clock and release the peripheral reset.
- Parameters
-
| base | LCDIF v2 peripheral base address. |
| void LCDIFV2_Deinit |
( |
LCDIFV2_Type * |
base | ) |
|
- Parameters
-
| base | LCDIF peripheral base address. |
| static void LCDIFV2_Reset |
( |
LCDIFV2_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | LCDIF peripheral base address. |
| enable | Enable or disable. |
| uint16_t lcdifv2_display_config_t::panelWidth |
| uint16_t lcdifv2_display_config_t::panelHeight |
| uint8_t lcdifv2_display_config_t::hsw |
| uint8_t lcdifv2_display_config_t::hfp |
| uint8_t lcdifv2_display_config_t::hbp |
| uint8_t lcdifv2_display_config_t::vsw |
| uint8_t lcdifv2_display_config_t::vfp |
| uint8_t lcdifv2_display_config_t::vbp |
| uint32_t lcdifv2_display_config_t::polarityFlags |
| uint16_t lcdifv2_buffer_config_t::strideBytes |
| uint32_t lcdifv2_store_buffer_config_t::bufferAddr |
| uint16_t lcdifv2_store_buffer_config_t::strideBytes |