![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Error codes returned by the SOCKETS API. More...
Note that SOCKETS API may also propagate port-specific error codes when they are more descriptive. See your port's error codes for more details. PORT_SPECIFIC_LINK
Macros | |
| #define | SOCKETS_ERROR_NONE ( 0 ) |
| No error. More... | |
| #define | SOCKETS_SOCKET_ERROR ( -1 ) |
| Catch-all sockets error code. More... | |
| #define | SOCKETS_EWOULDBLOCK ( -11 ) |
| A resource is temporarily unavailable. More... | |
| #define | SOCKETS_ENOMEM ( -12 ) |
| Memory allocation failed. More... | |
| #define | SOCKETS_EINVAL ( -22 ) |
| Invalid argument. More... | |
| #define | SOCKETS_ENOPROTOOPT ( -109 ) |
| A bad option was specified . More... | |
| #define | SOCKETS_ENOTCONN ( -126 ) |
| The supplied socket is not connected. More... | |
| #define | SOCKETS_EISCONN ( -127 ) |
| The supplied socket is already connected. More... | |
| #define | SOCKETS_ECLOSED ( -128 ) |
| The supplied socket has already been closed. More... | |
| #define | SOCKETS_TLS_INIT_ERROR ( -1001 ) |
| TLS initialization failed. More... | |
| #define | SOCKETS_TLS_HANDSHAKE_ERROR ( -1002 ) |
| TLS handshake failed. More... | |
| #define | SOCKETS_TLS_SERVER_UNVERIFIED ( -1003 ) |
| A connection was made but the server could not be verified. More... | |
| #define | SOCKETS_TLS_RECV_ERROR ( -1004 ) |
| TLS receive operation failed. More... | |
| #define | SOCKETS_TLS_SEND_ERROR ( -1005 ) |
| TLS send operation failed. More... | |
| #define | SOCKETS_PERIPHERAL_RESET ( -1006 ) |
| Communications peripheral has been reset. More... | |
| #define SOCKETS_ERROR_NONE ( 0 ) |
| #define SOCKETS_SOCKET_ERROR ( -1 ) |
| #define SOCKETS_EWOULDBLOCK ( -11 ) |
| #define SOCKETS_ENOMEM ( -12 ) |
| #define SOCKETS_EINVAL ( -22 ) |
| #define SOCKETS_ENOPROTOOPT ( -109 ) |
| #define SOCKETS_ENOTCONN ( -126 ) |
| #define SOCKETS_EISCONN ( -127 ) |
| #define SOCKETS_ECLOSED ( -128 ) |
| #define SOCKETS_TLS_INIT_ERROR ( -1001 ) |
| #define SOCKETS_TLS_HANDSHAKE_ERROR ( -1002 ) |
| #define SOCKETS_TLS_SERVER_UNVERIFIED ( -1003 ) |
It is recommended that the socket be closed.
| #define SOCKETS_TLS_RECV_ERROR ( -1004 ) |
| #define SOCKETS_TLS_SEND_ERROR ( -1005 ) |
| #define SOCKETS_PERIPHERAL_RESET ( -1006 ) |