![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Options for lOptionName in SOCKETS_SetSockOpt(). More...
Macros | |
| #define | SOCKETS_SO_RCVTIMEO ( 0 ) |
| #define | SOCKETS_SO_SNDTIMEO ( 1 ) |
| #define | SOCKETS_SO_SNDBUF ( 4 ) |
| #define | SOCKETS_SO_RCVBUF ( 5 ) |
| #define | SOCKETS_SO_SERVER_NAME_INDICATION ( 6 ) |
| #define | SOCKETS_SO_TRUSTED_SERVER_CERTIFICATE ( 7 ) |
| #define | SOCKETS_SO_REQUIRE_TLS ( 8 ) |
| #define | SOCKETS_SO_NONBLOCK ( 9 ) |
| #define | SOCKETS_SO_ALPN_PROTOCOLS ( 10 ) |
| #define | SOCKETS_SO_WAKEUP_CALLBACK ( 17 ) |
| #define SOCKETS_SO_RCVTIMEO ( 0 ) |
Set the receive timeout.
| #define SOCKETS_SO_SNDTIMEO ( 1 ) |
Set the send timeout.
| #define SOCKETS_SO_SNDBUF ( 4 ) |
Set the size of the send buffer (TCP only).
| #define SOCKETS_SO_RCVBUF ( 5 ) |
Set the size of the receive buffer (TCP only).
| #define SOCKETS_SO_SERVER_NAME_INDICATION ( 6 ) |
Toggle client use of TLS SNI.
| #define SOCKETS_SO_TRUSTED_SERVER_CERTIFICATE ( 7 ) |
Override default TLS server certificate trust. Must be PEM encoded and length must include null terminator.
| #define SOCKETS_SO_REQUIRE_TLS ( 8 ) |
Toggle client enforcement of TLS.
| #define SOCKETS_SO_NONBLOCK ( 9 ) |
Socket is nonblocking.
| #define SOCKETS_SO_ALPN_PROTOCOLS ( 10 ) |
Application protocol list to be included in TLS ClientHello.
| #define SOCKETS_SO_WAKEUP_CALLBACK ( 17 ) |
Set the callback to be called whenever there is data available on the socket for reading.