![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
nand Disk Function | |
| DSTATUS | nand_disk_initialize (uint8_t physicalDrive) |
| Initializes nand disk. More... | |
| DSTATUS | nand_disk_status (uint8_t physicalDrive) |
| Gets nand disk status. More... | |
| DRESULT | nand_disk_read (uint8_t physicalDrive, uint8_t *buffer, uint32_t sector, uint8_t count) |
| Reads nand disk. More... | |
| DRESULT | nand_disk_write (uint8_t physicalDrive, const uint8_t *buffer, uint32_t sector, uint8_t count) |
| Writes nand disk. More... | |
| DRESULT | nand_disk_ioctl (uint8_t physicalDrive, uint8_t command, void *buffer) |
| nand disk IO operation. More... | |
| DSTATUS nand_disk_initialize | ( | uint8_t | physicalDrive | ) |
| physicalDrive | Physical drive number. |
| STA_NOINIT | Failed. |
| RES_OK | Success. |
| DSTATUS nand_disk_status | ( | uint8_t | physicalDrive | ) |
| physicalDrive | Physical drive number. |
| STA_NOINIT | Failed. |
| RES_OK | Success. |
| DRESULT nand_disk_read | ( | uint8_t | physicalDrive, |
| uint8_t * | buffer, | ||
| uint32_t | sector, | ||
| uint8_t | count | ||
| ) |
| physicalDrive | Physical drive number. |
| buffer | The data buffer pointer to store read content. |
| sector | The start sector number to be read. |
| count | The sector count to be read. |
| RES_PARERR | Failed. |
| RES_OK | Success. |
| DRESULT nand_disk_write | ( | uint8_t | physicalDrive, |
| const uint8_t * | buffer, | ||
| uint32_t | sector, | ||
| uint8_t | count | ||
| ) |
| physicalDrive | Physical drive number. |
| buffer | The data buffer pointer to store write content. |
| sector | The start sector number to be written. |
| count | The sector count to be written. |
| RES_PARERR | Failed. |
| RES_OK | Success. |
| DRESULT nand_disk_ioctl | ( | uint8_t | physicalDrive, |
| uint8_t | command, | ||
| void * | buffer | ||
| ) |
| physicalDrive | Physical drive number. |
| command | The command to be set. |
| buffer | The buffer to store command result. |
| RES_PARERR | Failed. |
| RES_OK | Success. |