![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
ASN1 Error codes | |
These error codes are OR'ed to X509 error codes for higher error granularity. ASN1 is a standard to specify data structures. | |
| #define | MBEDTLS_ERR_ASN1_OUT_OF_DATA -0x0060 |
| #define | MBEDTLS_ERR_ASN1_UNEXPECTED_TAG -0x0062 |
| #define | MBEDTLS_ERR_ASN1_INVALID_LENGTH -0x0064 |
| #define | MBEDTLS_ERR_ASN1_LENGTH_MISMATCH -0x0066 |
| #define | MBEDTLS_ERR_ASN1_INVALID_DATA -0x0068 |
| #define | MBEDTLS_ERR_ASN1_ALLOC_FAILED -0x006A |
| #define | MBEDTLS_ERR_ASN1_BUF_TOO_SMALL -0x006C |
| #define MBEDTLS_ERR_ASN1_OUT_OF_DATA -0x0060 |
Out of data when parsing an ASN1 data structure.
| #define MBEDTLS_ERR_ASN1_UNEXPECTED_TAG -0x0062 |
ASN1 tag was of an unexpected value.
| #define MBEDTLS_ERR_ASN1_INVALID_LENGTH -0x0064 |
Error when trying to determine the length or invalid length.
| #define MBEDTLS_ERR_ASN1_LENGTH_MISMATCH -0x0066 |
Actual length differs from expected length.
| #define MBEDTLS_ERR_ASN1_INVALID_DATA -0x0068 |
Data is invalid. (not used)
| #define MBEDTLS_ERR_ASN1_ALLOC_FAILED -0x006A |
Memory allocation failed
| #define MBEDTLS_ERR_ASN1_BUF_TOO_SMALL -0x006C |
Buffer too small when writing ASN.1 data structure.