![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | sai_edma_handle_t | 
| SAI DMA transfer handle, users should not touch the content of the handle.  More... | |
Typedefs | |
| typedef void(* | sai_edma_callback_t )(I2S_Type *base, sai_edma_handle_t *handle, status_t status, void *userData) | 
| SAI eDMA transfer callback function for finish and error.  | |
Driver version | |
| #define | FSL_SAI_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 2, 0)) | 
| Version 2.2.0.  | |
eDMA Transactional | |
| void | SAI_TransferTxCreateHandleEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_edma_callback_t callback, void *userData, edma_handle_t *dmaHandle) | 
| Initializes the SAI eDMA handle.  More... | |
| void | SAI_TransferRxCreateHandleEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_edma_callback_t callback, void *userData, edma_handle_t *dmaHandle) | 
| Initializes the SAI Rx eDMA handle.  More... | |
| void | SAI_TransferTxSetFormatEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz) | 
| Configures the SAI Tx audio format.  More... | |
| void | SAI_TransferRxSetFormatEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz) | 
| Configures the SAI Rx audio format.  More... | |
| void | SAI_TransferTxSetConfigEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transceiver_t *saiConfig) | 
| Configures the SAI Tx.  More... | |
| void | SAI_TransferRxSetConfigEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transceiver_t *saiConfig) | 
| Configures the SAI Rx.  More... | |
| status_t | SAI_TransferSendEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transfer_t *xfer) | 
| Performs a non-blocking SAI transfer using DMA.  More... | |
| status_t | SAI_TransferReceiveEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transfer_t *xfer) | 
| Performs a non-blocking SAI receive using eDMA.  More... | |
| void | SAI_TransferTerminateSendEDMA (I2S_Type *base, sai_edma_handle_t *handle) | 
| Terminate all SAI send.  More... | |
| void | SAI_TransferTerminateReceiveEDMA (I2S_Type *base, sai_edma_handle_t *handle) | 
| Terminate all SAI receive.  More... | |
| void | SAI_TransferAbortSendEDMA (I2S_Type *base, sai_edma_handle_t *handle) | 
| Aborts a SAI transfer using eDMA.  More... | |
| void | SAI_TransferAbortReceiveEDMA (I2S_Type *base, sai_edma_handle_t *handle) | 
| Aborts a SAI receive using eDMA.  More... | |
| status_t | SAI_TransferGetSendCountEDMA (I2S_Type *base, sai_edma_handle_t *handle, size_t *count) | 
| Gets byte count sent by SAI.  More... | |
| status_t | SAI_TransferGetReceiveCountEDMA (I2S_Type *base, sai_edma_handle_t *handle, size_t *count) | 
| Gets byte count received by SAI.  More... | |
| struct _sai_edma_handle | 
Data Fields | |
| edma_handle_t * | dmaHandle | 
| DMA handler for SAI send.  | |
| uint8_t | nbytes | 
| eDMA minor byte transfer count initially configured.  More... | |
| uint8_t | bytesPerFrame | 
| Bytes in a frame.  | |
| uint8_t | channel | 
| Which data channel.  | |
| uint8_t | count | 
| The transfer data count in a DMA request.  | |
| uint32_t | state | 
| Internal state for SAI eDMA transfer.  | |
| sai_edma_callback_t | callback | 
| Callback for users while transfer finish or error occurs.  | |
| void * | userData | 
| User callback parameter.  | |
| uint8_t | tcd [(SAI_XFER_QUEUE_SIZE+1U)*sizeof(edma_tcd_t)] | 
| TCD pool for eDMA transfer.  More... | |
| sai_transfer_t | saiQueue [SAI_XFER_QUEUE_SIZE] | 
| Transfer queue storing queued transfer.  More... | |
| size_t | transferSize [SAI_XFER_QUEUE_SIZE] | 
| Data bytes need to transfer.  | |
| volatile uint8_t | queueUser | 
| Index for user to queue transfer.  More... | |
| volatile uint8_t | queueDriver | 
| Index for driver to get the transfer data and size.  | |
| uint8_t sai_edma_handle_t::nbytes | 
| uint8_t sai_edma_handle_t::tcd[(SAI_XFER_QUEUE_SIZE+1U)*sizeof(edma_tcd_t)] | 
| sai_transfer_t sai_edma_handle_t::saiQueue[SAI_XFER_QUEUE_SIZE] | 
| volatile uint8_t sai_edma_handle_t::queueUser | 
| void SAI_TransferTxCreateHandleEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | dmaHandle | ||
| ) | 
This function initializes the SAI master DMA handle, which can be used for other SAI master transactional APIs. Usually, for a specified SAI instance, call this API once to get the initialized handle.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| base | SAI peripheral base address. | 
| callback | Pointer to user callback function. | 
| userData | User parameter passed to the callback function. | 
| dmaHandle | eDMA handle pointer, this handle shall be static allocated by users. | 
| void SAI_TransferRxCreateHandleEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | dmaHandle | ||
| ) | 
This function initializes the SAI slave DMA handle, which can be used for other SAI master transactional APIs. Usually, for a specified SAI instance, call this API once to get the initialized handle.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| base | SAI peripheral base address. | 
| callback | Pointer to user callback function. | 
| userData | User parameter passed to the callback function. | 
| dmaHandle | eDMA handle pointer, this handle shall be static allocated by users. | 
| void SAI_TransferTxSetFormatEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_transfer_format_t * | format, | ||
| uint32_t | mclkSourceClockHz, | ||
| uint32_t | bclkSourceClockHz | ||
| ) | 
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred. This function also sets the eDMA parameter according to formatting requirements.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| format | Pointer to SAI audio data format structure. | 
| mclkSourceClockHz | SAI master clock source frequency in Hz. | 
| bclkSourceClockHz | SAI bit clock source frequency in Hz. If bit clock source is master clock, this value should equals to masterClockHz in format. | 
| kStatus_Success | Audio format set successfully. | 
| kStatus_InvalidArgument | The input argument is invalid. | 
| void SAI_TransferRxSetFormatEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_transfer_format_t * | format, | ||
| uint32_t | mclkSourceClockHz, | ||
| uint32_t | bclkSourceClockHz | ||
| ) | 
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred. This function also sets the eDMA parameter according to formatting requirements.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| format | Pointer to SAI audio data format structure. | 
| mclkSourceClockHz | SAI master clock source frequency in Hz. | 
| bclkSourceClockHz | SAI bit clock source frequency in Hz. If a bit clock source is the master clock, this value should equal to masterClockHz in format. | 
| kStatus_Success | Audio format set successfully. | 
| kStatus_InvalidArgument | The input argument is invalid. | 
| void SAI_TransferTxSetConfigEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_transceiver_t * | saiConfig | ||
| ) | 
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| saiConfig | sai configurations. | 
| void SAI_TransferRxSetConfigEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_transceiver_t * | saiConfig | ||
| ) | 
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| saiConfig | sai configurations. | 
| status_t SAI_TransferSendEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_transfer_t * | xfer | ||
| ) | 
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| xfer | Pointer to the DMA transfer structure. | 
| kStatus_Success | Start a SAI eDMA send successfully. | 
| kStatus_InvalidArgument | The input argument is invalid. | 
| kStatus_TxBusy | SAI is busy sending data. | 
| status_t SAI_TransferReceiveEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_transfer_t * | xfer | ||
| ) | 
| base | SAI base pointer | 
| handle | SAI eDMA handle pointer. | 
| xfer | Pointer to DMA transfer structure. | 
| kStatus_Success | Start a SAI eDMA receive successfully. | 
| kStatus_InvalidArgument | The input argument is invalid. | 
| kStatus_RxBusy | SAI is busy receiving data. | 
| void SAI_TransferTerminateSendEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle | ||
| ) | 
This function will clear all transfer slots buffered in the sai queue. If users only want to abort the current transfer slot, please call SAI_TransferAbortSendEDMA.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| void SAI_TransferTerminateReceiveEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle | ||
| ) | 
This function will clear all transfer slots buffered in the sai queue. If users only want to abort the current transfer slot, please call SAI_TransferAbortReceiveEDMA.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| void SAI_TransferAbortSendEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle | ||
| ) | 
This function only aborts the current transfer slots, the other transfer slots' information still kept in the handler. If users want to terminate all transfer slots, just call SAI_TransferTerminateSendEDMA.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| void SAI_TransferAbortReceiveEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle | ||
| ) | 
This function only aborts the current transfer slots, the other transfer slots' information still kept in the handler. If users want to terminate all transfer slots, just call SAI_TransferTerminateReceiveEDMA.
| base | SAI base pointer | 
| handle | SAI eDMA handle pointer. | 
| status_t SAI_TransferGetSendCountEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| count | Bytes count sent by SAI. | 
| kStatus_Success | Succeed get the transfer count. | 
| kStatus_NoTransferInProgress | There is no non-blocking transaction in progress. | 
| status_t SAI_TransferGetReceiveCountEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | SAI base pointer | 
| handle | SAI eDMA handle pointer. | 
| count | Bytes count received by SAI. | 
| kStatus_Success | Succeed get the transfer count. | 
| kStatus_NoTransferInProgress | There is no non-blocking transaction in progress. |