![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | flexio_uart_edma_handle_t | 
| UART eDMA handle.  More... | |
Typedefs | |
| typedef void(* | flexio_uart_edma_transfer_callback_t )(FLEXIO_UART_Type *base, flexio_uart_edma_handle_t *handle, status_t status, void *userData) | 
| UART transfer callback function.  More... | |
Driver version | |
| #define | FSL_FLEXIO_UART_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 4)) | 
| FlexIO UART EDMA driver version 2.1.4.  More... | |
eDMA transactional | |
| status_t | FLEXIO_UART_TransferCreateHandleEDMA (FLEXIO_UART_Type *base, flexio_uart_edma_handle_t *handle, flexio_uart_edma_transfer_callback_t callback, void *userData, edma_handle_t *txEdmaHandle, edma_handle_t *rxEdmaHandle) | 
| Initializes the UART handle which is used in transactional functions.  More... | |
| status_t | FLEXIO_UART_TransferSendEDMA (FLEXIO_UART_Type *base, flexio_uart_edma_handle_t *handle, flexio_uart_transfer_t *xfer) | 
| Sends data using eDMA.  More... | |
| status_t | FLEXIO_UART_TransferReceiveEDMA (FLEXIO_UART_Type *base, flexio_uart_edma_handle_t *handle, flexio_uart_transfer_t *xfer) | 
| Receives data using eDMA.  More... | |
| void | FLEXIO_UART_TransferAbortSendEDMA (FLEXIO_UART_Type *base, flexio_uart_edma_handle_t *handle) | 
| Aborts the sent data which using eDMA.  More... | |
| void | FLEXIO_UART_TransferAbortReceiveEDMA (FLEXIO_UART_Type *base, flexio_uart_edma_handle_t *handle) | 
| Aborts the receive data which using eDMA.  More... | |
| status_t | FLEXIO_UART_TransferGetSendCountEDMA (FLEXIO_UART_Type *base, flexio_uart_edma_handle_t *handle, size_t *count) | 
| Gets the number of bytes sent out.  More... | |
| status_t | FLEXIO_UART_TransferGetReceiveCountEDMA (FLEXIO_UART_Type *base, flexio_uart_edma_handle_t *handle, size_t *count) | 
| Gets the number of bytes received.  More... | |
| struct _flexio_uart_edma_handle | 
Data Fields | |
| flexio_uart_edma_transfer_callback_t | callback | 
| Callback function.  More... | |
| void * | userData | 
| UART callback function parameter.  More... | |
| size_t | txDataSizeAll | 
| Total bytes to be sent.  More... | |
| size_t | rxDataSizeAll | 
| Total bytes to be received.  More... | |
| edma_handle_t * | txEdmaHandle | 
| The eDMA TX channel used.  More... | |
| edma_handle_t * | rxEdmaHandle | 
| The eDMA RX channel used.  More... | |
| uint8_t | nbytes | 
| eDMA minor byte transfer count initially configured.  More... | |
| volatile uint8_t | txState | 
| TX transfer state.  More... | |
| volatile uint8_t | rxState | 
| RX transfer state.  | |
| flexio_uart_edma_transfer_callback_t flexio_uart_edma_handle_t::callback | 
| void* flexio_uart_edma_handle_t::userData | 
| size_t flexio_uart_edma_handle_t::txDataSizeAll | 
| size_t flexio_uart_edma_handle_t::rxDataSizeAll | 
| edma_handle_t* flexio_uart_edma_handle_t::txEdmaHandle | 
| edma_handle_t* flexio_uart_edma_handle_t::rxEdmaHandle | 
| uint8_t flexio_uart_edma_handle_t::nbytes | 
| volatile uint8_t flexio_uart_edma_handle_t::txState | 
| #define FSL_FLEXIO_UART_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 4)) | 
| typedef void(* flexio_uart_edma_transfer_callback_t)(FLEXIO_UART_Type *base, flexio_uart_edma_handle_t *handle, status_t status, void *userData) | 
| status_t FLEXIO_UART_TransferCreateHandleEDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_edma_handle_t * | handle, | ||
| flexio_uart_edma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | txEdmaHandle, | ||
| edma_handle_t * | rxEdmaHandle | ||
| ) | 
| base | Pointer to FLEXIO_UART_Type. | 
| handle | Pointer to flexio_uart_edma_handle_t structure. | 
| callback | The callback function. | 
| userData | The parameter of the callback function. | 
| rxEdmaHandle | User requested DMA handle for RX DMA transfer. | 
| txEdmaHandle | User requested DMA handle for TX DMA transfer. | 
| kStatus_Success | Successfully create the handle. | 
| kStatus_OutOfRange | The FlexIO SPI eDMA type/handle table out of range. | 
| status_t FLEXIO_UART_TransferSendEDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_edma_handle_t * | handle, | ||
| flexio_uart_transfer_t * | xfer | ||
| ) | 
This function sends data using eDMA. This is a non-blocking function, which returns right away. When all data is sent out, the send callback function is called.
| base | Pointer to FLEXIO_UART_Type | 
| handle | UART handle pointer. | 
| xfer | UART eDMA transfer structure, see flexio_uart_transfer_t. | 
| kStatus_Success | if succeed, others failed. | 
| kStatus_FLEXIO_UART_TxBusy | Previous transfer on going. | 
| status_t FLEXIO_UART_TransferReceiveEDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_edma_handle_t * | handle, | ||
| flexio_uart_transfer_t * | xfer | ||
| ) | 
This function receives data using eDMA. This is a non-blocking function, which returns right away. When all data is received, the receive callback function is called.
| base | Pointer to FLEXIO_UART_Type | 
| handle | Pointer to flexio_uart_edma_handle_t structure | 
| xfer | UART eDMA transfer structure, see flexio_uart_transfer_t. | 
| kStatus_Success | if succeed, others failed. | 
| kStatus_UART_RxBusy | Previous transfer on going. | 
| void FLEXIO_UART_TransferAbortSendEDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_edma_handle_t * | handle | ||
| ) | 
This function aborts sent data which using eDMA.
| base | Pointer to FLEXIO_UART_Type | 
| handle | Pointer to flexio_uart_edma_handle_t structure | 
| void FLEXIO_UART_TransferAbortReceiveEDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_edma_handle_t * | handle | ||
| ) | 
This function aborts the receive data which using eDMA.
| base | Pointer to FLEXIO_UART_Type | 
| handle | Pointer to flexio_uart_edma_handle_t structure | 
| status_t FLEXIO_UART_TransferGetSendCountEDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
This function gets the number of bytes sent out.
| base | Pointer to FLEXIO_UART_Type | 
| handle | Pointer to flexio_uart_edma_handle_t structure | 
| count | Number of bytes sent so far by the non-blocking transaction. | 
| kStatus_NoTransferInProgress | transfer has finished or no transfer in progress. | 
| kStatus_Success | Successfully return the count. | 
| status_t FLEXIO_UART_TransferGetReceiveCountEDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
This function gets the number of bytes received.
| base | Pointer to FLEXIO_UART_Type | 
| handle | Pointer to flexio_uart_edma_handle_t structure | 
| count | Number of bytes received so far by the non-blocking transaction. | 
| kStatus_NoTransferInProgress | transfer has finished or no transfer in progress. | 
| kStatus_Success | Successfully return the count. |