![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | lpi2c_master_config_t | 
| Structure with settings to initialize the LPI2C master module.  More... | |
| struct | lpi2c_data_match_config_t | 
| LPI2C master data match configuration structure.  More... | |
| struct | lpi2c_master_transfer_t | 
| Non-blocking transfer descriptor structure.  More... | |
| struct | lpi2c_master_handle_t | 
| Driver handle for master non-blocking APIs.  More... | |
Typedefs | |
| typedef void(* | lpi2c_master_transfer_callback_t )(LPI2C_Type *base, lpi2c_master_handle_t *handle, status_t completionStatus, void *userData) | 
| Master completion callback function pointer type.  More... | |
Initialization and deinitialization | |
| void | LPI2C_MasterGetDefaultConfig (lpi2c_master_config_t *masterConfig) | 
| Provides a default configuration for the LPI2C master peripheral.  More... | |
| void | LPI2C_MasterInit (LPI2C_Type *base, const lpi2c_master_config_t *masterConfig, uint32_t sourceClock_Hz) | 
| Initializes the LPI2C master peripheral.  More... | |
| void | LPI2C_MasterDeinit (LPI2C_Type *base) | 
| Deinitializes the LPI2C master peripheral.  More... | |
| void | LPI2C_MasterConfigureDataMatch (LPI2C_Type *base, const lpi2c_data_match_config_t *config) | 
| Configures LPI2C master data match feature.  More... | |
| status_t | LPI2C_MasterCheckAndClearError (LPI2C_Type *base, uint32_t status) | 
| status_t | LPI2C_CheckForBusyBus (LPI2C_Type *base) | 
| static void | LPI2C_MasterReset (LPI2C_Type *base) | 
| Performs a software reset.  More... | |
| static void | LPI2C_MasterEnable (LPI2C_Type *base, bool enable) | 
| Enables or disables the LPI2C module as master.  More... | |
Status | |
| static uint32_t | LPI2C_MasterGetStatusFlags (LPI2C_Type *base) | 
| Gets the LPI2C master status flags.  More... | |
| static void | LPI2C_MasterClearStatusFlags (LPI2C_Type *base, uint32_t statusMask) | 
| Clears the LPI2C master status flag state.  More... | |
Interrupts | |
| static void | LPI2C_MasterEnableInterrupts (LPI2C_Type *base, uint32_t interruptMask) | 
| Enables the LPI2C master interrupt requests.  More... | |
| static void | LPI2C_MasterDisableInterrupts (LPI2C_Type *base, uint32_t interruptMask) | 
| Disables the LPI2C master interrupt requests.  More... | |
| static uint32_t | LPI2C_MasterGetEnabledInterrupts (LPI2C_Type *base) | 
| Returns the set of currently enabled LPI2C master interrupt requests.  More... | |
DMA control | |
| static void | LPI2C_MasterEnableDMA (LPI2C_Type *base, bool enableTx, bool enableRx) | 
| Enables or disables LPI2C master DMA requests.  More... | |
| static uint32_t | LPI2C_MasterGetTxFifoAddress (LPI2C_Type *base) | 
| Gets LPI2C master transmit data register address for DMA transfer.  More... | |
| static uint32_t | LPI2C_MasterGetRxFifoAddress (LPI2C_Type *base) | 
| Gets LPI2C master receive data register address for DMA transfer.  More... | |
FIFO control | |
| static void | LPI2C_MasterSetWatermarks (LPI2C_Type *base, size_t txWords, size_t rxWords) | 
| Sets the watermarks for LPI2C master FIFOs.  More... | |
| static void | LPI2C_MasterGetFifoCounts (LPI2C_Type *base, size_t *rxCount, size_t *txCount) | 
| Gets the current number of words in the LPI2C master FIFOs.  More... | |
Bus operations | |
| void | LPI2C_MasterSetBaudRate (LPI2C_Type *base, uint32_t sourceClock_Hz, uint32_t baudRate_Hz) | 
| Sets the I2C bus frequency for master transactions.  More... | |
| static bool | LPI2C_MasterGetBusIdleState (LPI2C_Type *base) | 
| Returns whether the bus is idle.  More... | |
| status_t | LPI2C_MasterStart (LPI2C_Type *base, uint8_t address, lpi2c_direction_t dir) | 
| Sends a START signal and slave address on the I2C bus.  More... | |
| static status_t | LPI2C_MasterRepeatedStart (LPI2C_Type *base, uint8_t address, lpi2c_direction_t dir) | 
| Sends a repeated START signal and slave address on the I2C bus.  More... | |
| status_t | LPI2C_MasterSend (LPI2C_Type *base, void *txBuff, size_t txSize) | 
| Performs a polling send transfer on the I2C bus.  More... | |
| status_t | LPI2C_MasterReceive (LPI2C_Type *base, void *rxBuff, size_t rxSize) | 
| Performs a polling receive transfer on the I2C bus.  More... | |
| status_t | LPI2C_MasterStop (LPI2C_Type *base) | 
| Sends a STOP signal on the I2C bus.  More... | |
| status_t | LPI2C_MasterTransferBlocking (LPI2C_Type *base, lpi2c_master_transfer_t *transfer) | 
| Performs a master polling transfer on the I2C bus.  More... | |
Non-blocking | |
| void | LPI2C_MasterTransferCreateHandle (LPI2C_Type *base, lpi2c_master_handle_t *handle, lpi2c_master_transfer_callback_t callback, void *userData) | 
| Creates a new handle for the LPI2C master non-blocking APIs.  More... | |
| status_t | LPI2C_MasterTransferNonBlocking (LPI2C_Type *base, lpi2c_master_handle_t *handle, lpi2c_master_transfer_t *transfer) | 
| Performs a non-blocking transaction on the I2C bus.  More... | |
| status_t | LPI2C_MasterTransferGetCount (LPI2C_Type *base, lpi2c_master_handle_t *handle, size_t *count) | 
| Returns number of bytes transferred so far.  More... | |
| void | LPI2C_MasterTransferAbort (LPI2C_Type *base, lpi2c_master_handle_t *handle) | 
| Terminates a non-blocking LPI2C master transmission early.  More... | |
IRQ handler | |
| void | LPI2C_MasterTransferHandleIRQ (LPI2C_Type *base, lpi2c_master_handle_t *handle) | 
| Reusable routine to handle master interrupts.  More... | |
| struct lpi2c_master_config_t | 
This structure holds configuration settings for the LPI2C peripheral. To initialize this structure to reasonable defaults, call the LPI2C_MasterGetDefaultConfig() function and pass a pointer to your configuration structure instance.
The configuration structure can be made constant so it resides in flash.
Data Fields | |
| bool | enableMaster | 
| Whether to enable master mode.  More... | |
| bool | enableDoze | 
| Whether master is enabled in doze mode.  More... | |
| bool | debugEnable | 
| Enable transfers to continue when halted in debug mode.  More... | |
| bool | ignoreAck | 
| Whether to ignore ACK/NACK.  More... | |
| lpi2c_master_pin_config_t | pinConfig | 
| The pin configuration option.  More... | |
| uint32_t | baudRate_Hz | 
| Desired baud rate in Hertz.  More... | |
| uint32_t | busIdleTimeout_ns | 
| Bus idle timeout in nanoseconds.  More... | |
| uint32_t | pinLowTimeout_ns | 
| Pin low timeout in nanoseconds.  More... | |
| uint8_t | sdaGlitchFilterWidth_ns | 
| Width in nanoseconds of glitch filter on SDA pin.  More... | |
| uint8_t | sclGlitchFilterWidth_ns | 
| Width in nanoseconds of glitch filter on SCL pin.  More... | |
| struct { | |
| bool enable | |
| Enable host request.  More... | |
| lpi2c_host_request_source_t source | |
| Host request source.  More... | |
| lpi2c_host_request_polarity_t polarity | |
| Host request pin polarity.  More... | |
| } | hostRequest | 
| Host request options.  More... | |
| bool lpi2c_master_config_t::enableMaster | 
| bool lpi2c_master_config_t::enableDoze | 
| bool lpi2c_master_config_t::debugEnable | 
| bool lpi2c_master_config_t::ignoreAck | 
| lpi2c_master_pin_config_t lpi2c_master_config_t::pinConfig | 
| uint32_t lpi2c_master_config_t::baudRate_Hz | 
| uint32_t lpi2c_master_config_t::busIdleTimeout_ns | 
Set to 0 to disable.
| uint32_t lpi2c_master_config_t::pinLowTimeout_ns | 
Set to 0 to disable.
| uint8_t lpi2c_master_config_t::sdaGlitchFilterWidth_ns | 
Set to 0 to disable.
| uint8_t lpi2c_master_config_t::sclGlitchFilterWidth_ns | 
Set to 0 to disable.
| bool lpi2c_master_config_t::enable | 
| lpi2c_host_request_source_t lpi2c_master_config_t::source | 
| lpi2c_host_request_polarity_t lpi2c_master_config_t::polarity | 
| struct { ... } lpi2c_master_config_t::hostRequest | 
| struct lpi2c_data_match_config_t | 
Data Fields | |
| lpi2c_data_match_config_mode_t | matchMode | 
| Data match configuration setting.  More... | |
| bool | rxDataMatchOnly | 
| When set to true, received data is ignored until a successful match.  More... | |
| uint32_t | match0 | 
| Match value 0.  More... | |
| uint32_t | match1 | 
| Match value 1.  More... | |
| lpi2c_data_match_config_mode_t lpi2c_data_match_config_t::matchMode | 
| bool lpi2c_data_match_config_t::rxDataMatchOnly | 
| uint32_t lpi2c_data_match_config_t::match0 | 
| uint32_t lpi2c_data_match_config_t::match1 | 
| struct _lpi2c_master_transfer | 
This structure is used to pass transaction parameters to the LPI2C_MasterTransferNonBlocking() API.
Data Fields | |
| uint32_t | flags | 
| Bit mask of options for the transfer.  More... | |
| uint16_t | slaveAddress | 
| The 7-bit slave address.  More... | |
| lpi2c_direction_t | direction | 
| Either kLPI2C_Read or kLPI2C_Write.  More... | |
| uint32_t | subaddress | 
| Sub address.  More... | |
| size_t | subaddressSize | 
| Length of sub address to send in bytes.  More... | |
| void * | data | 
| Pointer to data to transfer.  More... | |
| size_t | dataSize | 
| Number of bytes to transfer.  More... | |
| uint32_t lpi2c_master_transfer_t::flags | 
See enumeration _lpi2c_master_transfer_flags for available options. Set to 0 or kLPI2C_TransferDefaultFlag for normal transfers.
| uint16_t lpi2c_master_transfer_t::slaveAddress | 
| lpi2c_direction_t lpi2c_master_transfer_t::direction | 
| uint32_t lpi2c_master_transfer_t::subaddress | 
Transferred MSB first.
| size_t lpi2c_master_transfer_t::subaddressSize | 
Maximum size is 4 bytes.
| void* lpi2c_master_transfer_t::data | 
| size_t lpi2c_master_transfer_t::dataSize | 
| struct _lpi2c_master_handle | 
Data Fields | |
| uint8_t | state | 
| Transfer state machine current state.  More... | |
| uint16_t | remainingBytes | 
| Remaining byte count in current state.  More... | |
| uint8_t * | buf | 
| Buffer pointer for current state.  More... | |
| uint16_t | commandBuffer [7] | 
| LPI2C command sequence.  More... | |
| lpi2c_master_transfer_t | transfer | 
| Copy of the current transfer info.  More... | |
| lpi2c_master_transfer_callback_t | completionCallback | 
| Callback function pointer.  More... | |
| void * | userData | 
| Application data passed to callback.  More... | |
| uint8_t lpi2c_master_handle_t::state | 
| uint16_t lpi2c_master_handle_t::remainingBytes | 
| uint8_t* lpi2c_master_handle_t::buf | 
| uint16_t lpi2c_master_handle_t::commandBuffer[7] | 
| lpi2c_master_transfer_t lpi2c_master_handle_t::transfer | 
| lpi2c_master_transfer_callback_t lpi2c_master_handle_t::completionCallback | 
| void* lpi2c_master_handle_t::userData | 
| typedef void(* lpi2c_master_transfer_callback_t)(LPI2C_Type *base, lpi2c_master_handle_t *handle, status_t completionStatus, void *userData) | 
This callback is used only for the non-blocking master transfer API. Specify the callback you wish to use in the call to LPI2C_MasterTransferCreateHandle().
| base | The LPI2C peripheral base address. | 
| completionStatus | Either #kStatus_Success or an error code describing how the transfer completed. | 
| userData | Arbitrary pointer-sized value passed from the application. | 
| anonymous enum | 
The following status register flags can be cleared:
All flags except kLPI2C_MasterBusyFlag and kLPI2C_MasterBusBusyFlag can be enabled as interrupts.
| enum lpi2c_direction_t | 
| void LPI2C_MasterGetDefaultConfig | ( | lpi2c_master_config_t * | masterConfig | ) | 
This function provides the following default configuration for the LPI2C master peripheral:
After calling this function, you can override any settings in order to customize the configuration, prior to initializing the master driver with LPI2C_MasterInit().
| [out] | masterConfig | User provided configuration structure for default values. Refer to lpi2c_master_config_t. | 
| void LPI2C_MasterInit | ( | LPI2C_Type * | base, | 
| const lpi2c_master_config_t * | masterConfig, | ||
| uint32_t | sourceClock_Hz | ||
| ) | 
This function enables the peripheral clock and initializes the LPI2C master peripheral as described by the user provided configuration. A software reset is performed prior to configuration.
| base | The LPI2C peripheral base address. | 
| masterConfig | User provided peripheral configuration. Use LPI2C_MasterGetDefaultConfig() to get a set of defaults that you can override. | 
| sourceClock_Hz | Frequency in Hertz of the LPI2C functional clock. Used to calculate the baud rate divisors, filter widths, and timeout periods. | 
| void LPI2C_MasterDeinit | ( | LPI2C_Type * | base | ) | 
This function disables the LPI2C master peripheral and gates the clock. It also performs a software reset to restore the peripheral to reset conditions.
| base | The LPI2C peripheral base address. | 
| void LPI2C_MasterConfigureDataMatch | ( | LPI2C_Type * | base, | 
| const lpi2c_data_match_config_t * | config | ||
| ) | 
| base | The LPI2C peripheral base address. | 
| config | Settings for the data match feature. | 
      
  | 
  inlinestatic | 
Restores the LPI2C master peripheral to reset conditions.
| base | The LPI2C peripheral base address. | 
      
  | 
  inlinestatic | 
| base | The LPI2C peripheral base address. | 
| enable | Pass true to enable or false to disable the specified LPI2C as master. | 
      
  | 
  inlinestatic | 
A bit mask with the state of all LPI2C master status flags is returned. For each flag, the corresponding bit in the return value is set if the flag is asserted.
| base | The LPI2C peripheral base address. | 
      
  | 
  inlinestatic | 
The following status register flags can be cleared:
Attempts to clear other flags has no effect.
| base | The LPI2C peripheral base address. | 
| statusMask | A bitmask of status flags that are to be cleared. The mask is composed of #_lpi2c_master_flags enumerators OR'd together. You may pass the result of a previous call to LPI2C_MasterGetStatusFlags(). | 
      
  | 
  inlinestatic | 
All flags except kLPI2C_MasterBusyFlag and kLPI2C_MasterBusBusyFlag can be enabled as interrupts.
| base | The LPI2C peripheral base address. | 
| interruptMask | Bit mask of interrupts to enable. See #_lpi2c_master_flags for the set of constants that should be OR'd together to form the bit mask. | 
      
  | 
  inlinestatic | 
All flags except kLPI2C_MasterBusyFlag and kLPI2C_MasterBusBusyFlag can be enabled as interrupts.
| base | The LPI2C peripheral base address. | 
| interruptMask | Bit mask of interrupts to disable. See #_lpi2c_master_flags for the set of constants that should be OR'd together to form the bit mask. | 
      
  | 
  inlinestatic | 
| base | The LPI2C peripheral base address. | 
      
  | 
  inlinestatic | 
| base | The LPI2C peripheral base address. | 
| enableTx | Enable flag for transmit DMA request. Pass true for enable, false for disable. | 
| enableRx | Enable flag for receive DMA request. Pass true for enable, false for disable. | 
      
  | 
  inlinestatic | 
| base | The LPI2C peripheral base address. | 
      
  | 
  inlinestatic | 
| base | The LPI2C peripheral base address. | 
      
  | 
  inlinestatic | 
| base | The LPI2C peripheral base address. | 
| txWords | Transmit FIFO watermark value in words. The kLPI2C_MasterTxReadyFlag flag is set whenever the number of words in the transmit FIFO is equal or less than txWords. Writing a value equal or greater than the FIFO size is truncated. | 
| rxWords | Receive FIFO watermark value in words. The kLPI2C_MasterRxReadyFlag flag is set whenever the number of words in the receive FIFO is greater than rxWords. Writing a value equal or greater than the FIFO size is truncated. | 
      
  | 
  inlinestatic | 
| base | The LPI2C peripheral base address. | |
| [out] | txCount | Pointer through which the current number of words in the transmit FIFO is returned. Pass NULL if this value is not required. | 
| [out] | rxCount | Pointer through which the current number of words in the receive FIFO is returned. Pass NULL if this value is not required. | 
| void LPI2C_MasterSetBaudRate | ( | LPI2C_Type * | base, | 
| uint32_t | sourceClock_Hz, | ||
| uint32_t | baudRate_Hz | ||
| ) | 
The LPI2C master is automatically disabled and re-enabled as necessary to configure the baud rate. Do not call this function during a transfer, or the transfer is aborted.
| base | The LPI2C peripheral base address. | 
| sourceClock_Hz | LPI2C functional clock frequency in Hertz. | 
| baudRate_Hz | Requested bus frequency in Hertz. | 
      
  | 
  inlinestatic | 
Requires the master mode to be enabled.
| base | The LPI2C peripheral base address. | 
| true | Bus is busy. | 
| false | Bus is idle. | 
| status_t LPI2C_MasterStart | ( | LPI2C_Type * | base, | 
| uint8_t | address, | ||
| lpi2c_direction_t | dir | ||
| ) | 
This function is used to initiate a new master mode transfer. First, the bus state is checked to ensure that another master is not occupying the bus. Then a START signal is transmitted, followed by the 7-bit address specified in the address parameter. Note that this function does not actually wait until the START and address are successfully sent on the bus before returning.
| base | The LPI2C peripheral base address. | 
| address | 7-bit slave device address, in bits [6:0]. | 
| dir | Master transfer direction, either kLPI2C_Read or kLPI2C_Write. This parameter is used to set the R/w bit (bit 0) in the transmitted slave address. | 
| #kStatus_Success | START signal and address were successfully enqueued in the transmit FIFO. | 
| kStatus_LPI2C_Busy | Another master is currently utilizing the bus. | 
      
  | 
  inlinestatic | 
This function is used to send a Repeated START signal when a transfer is already in progress. Like LPI2C_MasterStart(), it also sends the specified 7-bit address.
| base | The LPI2C peripheral base address. | 
| address | 7-bit slave device address, in bits [6:0]. | 
| dir | Master transfer direction, either kLPI2C_Read or kLPI2C_Write. This parameter is used to set the R/w bit (bit 0) in the transmitted slave address. | 
| #kStatus_Success | Repeated START signal and address were successfully enqueued in the transmit FIFO. | 
| kStatus_LPI2C_Busy | Another master is currently utilizing the bus. | 
| status_t LPI2C_MasterSend | ( | LPI2C_Type * | base, | 
| void * | txBuff, | ||
| size_t | txSize | ||
| ) | 
Sends up to txSize number of bytes to the previously addressed slave device. The slave may reply with a NAK to any byte in order to terminate the transfer early. If this happens, this function returns kStatus_LPI2C_Nak.
| base | The LPI2C peripheral base address. | 
| txBuff | The pointer to the data to be transferred. | 
| txSize | The length in bytes of the data to be transferred. | 
| #kStatus_Success | Data was sent successfully. | 
| kStatus_LPI2C_Busy | Another master is currently utilizing the bus. | 
| kStatus_LPI2C_Nak | The slave device sent a NAK in response to a byte. | 
| kStatus_LPI2C_FifoError | FIFO under run or over run. | 
| kStatus_LPI2C_ArbitrationLost | Arbitration lost error. | 
| kStatus_LPI2C_PinLowTimeout | SCL or SDA were held low longer than the timeout. | 
| status_t LPI2C_MasterReceive | ( | LPI2C_Type * | base, | 
| void * | rxBuff, | ||
| size_t | rxSize | ||
| ) | 
| base | The LPI2C peripheral base address. | 
| rxBuff | The pointer to the data to be transferred. | 
| rxSize | The length in bytes of the data to be transferred. | 
| #kStatus_Success | Data was received successfully. | 
| kStatus_LPI2C_Busy | Another master is currently utilizing the bus. | 
| kStatus_LPI2C_Nak | The slave device sent a NAK in response to a byte. | 
| kStatus_LPI2C_FifoError | FIFO under run or overrun. | 
| kStatus_LPI2C_ArbitrationLost | Arbitration lost error. | 
| kStatus_LPI2C_PinLowTimeout | SCL or SDA were held low longer than the timeout. | 
| status_t LPI2C_MasterStop | ( | LPI2C_Type * | base | ) | 
This function does not return until the STOP signal is seen on the bus, or an error occurs.
| base | The LPI2C peripheral base address. | 
| #kStatus_Success | The STOP signal was successfully sent on the bus and the transaction terminated. | 
| kStatus_LPI2C_Busy | Another master is currently utilizing the bus. | 
| kStatus_LPI2C_Nak | The slave device sent a NAK in response to a byte. | 
| kStatus_LPI2C_FifoError | FIFO under run or overrun. | 
| kStatus_LPI2C_ArbitrationLost | Arbitration lost error. | 
| kStatus_LPI2C_PinLowTimeout | SCL or SDA were held low longer than the timeout. | 
| status_t LPI2C_MasterTransferBlocking | ( | LPI2C_Type * | base, | 
| lpi2c_master_transfer_t * | transfer | ||
| ) | 
| base | The LPI2C peripheral base address. | 
| transfer | Pointer to the transfer structure. | 
| #kStatus_Success | Data was received successfully. | 
| kStatus_LPI2C_Busy | Another master is currently utilizing the bus. | 
| kStatus_LPI2C_Nak | The slave device sent a NAK in response to a byte. | 
| kStatus_LPI2C_FifoError | FIFO under run or overrun. | 
| kStatus_LPI2C_ArbitrationLost | Arbitration lost error. | 
| kStatus_LPI2C_PinLowTimeout | SCL or SDA were held low longer than the timeout. | 
| void LPI2C_MasterTransferCreateHandle | ( | LPI2C_Type * | base, | 
| lpi2c_master_handle_t * | handle, | ||
| lpi2c_master_transfer_callback_t | callback, | ||
| void * | userData | ||
| ) | 
The creation of a handle is for use with the non-blocking APIs. Once a handle is created, there is not a corresponding destroy handle. If the user wants to terminate a transfer, the LPI2C_MasterTransferAbort() API shall be called.
| base | The LPI2C peripheral base address. | |
| [out] | handle | Pointer to the LPI2C master driver handle. | 
| callback | User provided pointer to the asynchronous callback function. | |
| userData | User provided pointer to the application callback data. | 
| status_t LPI2C_MasterTransferNonBlocking | ( | LPI2C_Type * | base, | 
| lpi2c_master_handle_t * | handle, | ||
| lpi2c_master_transfer_t * | transfer | ||
| ) | 
| base | The LPI2C peripheral base address. | 
| handle | Pointer to the LPI2C master driver handle. | 
| transfer | The pointer to the transfer descriptor. | 
| #kStatus_Success | The transaction was started successfully. | 
| kStatus_LPI2C_Busy | Either another master is currently utilizing the bus, or a non-blocking transaction is already in progress. | 
| status_t LPI2C_MasterTransferGetCount | ( | LPI2C_Type * | base, | 
| lpi2c_master_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | The LPI2C peripheral base address. | |
| handle | Pointer to the LPI2C master driver handle. | |
| [out] | count | Number of bytes transferred so far by the non-blocking transaction. | 
| #kStatus_Success | |
| #kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. | 
| void LPI2C_MasterTransferAbort | ( | LPI2C_Type * | base, | 
| lpi2c_master_handle_t * | handle | ||
| ) | 
| base | The LPI2C peripheral base address. | 
| handle | Pointer to the LPI2C master driver handle. | 
| #kStatus_Success | A transaction was successfully aborted. | 
| kStatus_LPI2C_Idle | There is not a non-blocking transaction currently in progress. | 
| void LPI2C_MasterTransferHandleIRQ | ( | LPI2C_Type * | base, | 
| lpi2c_master_handle_t * | handle | ||
| ) | 
| base | The LPI2C peripheral base address. | 
| handle | Pointer to the LPI2C master driver handle. |