![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Set these values to 1 or 0 to enable or disable the typedefs, respectively. These typedefs should only be disabled if they conflict with system typedefs.
Macros | |
| #define | posixconfigENABLE_CLOCK_T 1 | 
| #define | posixconfigENABLE_CLOCKID_T 1 | 
| #define | posixconfigENABLE_MODE_T 1 | 
| #define | posixconfigENABLE_PID_T 1 | 
| #define | posixconfigENABLE_PTHREAD_ATTR_T 1 | 
| #define | posixconfigENABLE_PTHREAD_COND_T 1 | 
| #define | posixconfigENABLE_PTHREAD_CONDATTR_T 1 | 
| #define | posixconfigENABLE_PTHREAD_MUTEX_T 1 | 
| #define | posixconfigENABLE_PTHREAD_MUTEXATTR_T 1 | 
| #define | posixconfigENABLE_PTHREAD_T 1 | 
| #define | posixconfigENABLE_SSIZE_T 1 | 
| #define | posixconfigENABLE_TIME_T 1 | 
| #define | posixconfigENABLE_TIMER_T 1 | 
| #define | posixconfigENABLE_USECONDS_T 1 | 
| #define | posixconfigENABLE_TIMESPEC 1 | 
| #define | posixconfigENABLE_ITIMERSPEC 1 | 
| #define | posixconfigENABLE_TM 1 | 
| #define | posixconfigENABLE_SEM_T 1 | 
| #define | posixconfigENABLE_PTHREAD_BARRIER_T 1 | 
| #define posixconfigENABLE_CLOCK_T 1 | 
clock_t in sys/types.h
| #define posixconfigENABLE_CLOCKID_T 1 | 
clockid_t in sys/types.h
| #define posixconfigENABLE_MODE_T 1 | 
mode_t in sys/types.h
| #define posixconfigENABLE_PID_T 1 | 
pid_t in sys/types.h
| #define posixconfigENABLE_PTHREAD_ATTR_T 1 | 
pthread_attr_t in sys/types.h
| #define posixconfigENABLE_PTHREAD_COND_T 1 | 
pthread_cond_t in sys/types.h
| #define posixconfigENABLE_PTHREAD_CONDATTR_T 1 | 
pthread_condattr_t in sys/types.h
| #define posixconfigENABLE_PTHREAD_MUTEX_T 1 | 
pthread_mutex_t in sys/types.h
| #define posixconfigENABLE_PTHREAD_MUTEXATTR_T 1 | 
pthread_mutexattr_t in sys/types.h
| #define posixconfigENABLE_PTHREAD_T 1 | 
pthread_t in sys/types.h
| #define posixconfigENABLE_SSIZE_T 1 | 
ssize_t in sys/types.h
| #define posixconfigENABLE_TIME_T 1 | 
time_t in sys/types.h
| #define posixconfigENABLE_TIMER_T 1 | 
timer_t in sys/types.h
| #define posixconfigENABLE_USECONDS_T 1 | 
useconds_t in sys/types.h
| #define posixconfigENABLE_TIMESPEC 1 | 
struct timespec in time.h
| #define posixconfigENABLE_ITIMERSPEC 1 | 
struct itimerspec in time.h
| #define posixconfigENABLE_TM 1 | 
struct tm in time.h
| #define posixconfigENABLE_SEM_T 1 | 
struct sem_t in semaphore.h
| #define posixconfigENABLE_PTHREAD_BARRIER_T 1 | 
pthread_barrier_t in sys/types.h