![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
nand Disk Function | |
| DSTATUS | nand_disk_initialize (uint8_t physicalDrive) | 
| Initializes nand disk.  More... | |
| DSTATUS | nand_disk_status (uint8_t physicalDrive) | 
| Gets nand disk status.  More... | |
| DRESULT | nand_disk_read (uint8_t physicalDrive, uint8_t *buffer, uint32_t sector, uint8_t count) | 
| Reads nand disk.  More... | |
| DRESULT | nand_disk_write (uint8_t physicalDrive, const uint8_t *buffer, uint32_t sector, uint8_t count) | 
| Writes nand disk.  More... | |
| DRESULT | nand_disk_ioctl (uint8_t physicalDrive, uint8_t command, void *buffer) | 
| nand disk IO operation.  More... | |
| DSTATUS nand_disk_initialize | ( | uint8_t | physicalDrive | ) | 
| physicalDrive | Physical drive number. | 
| STA_NOINIT | Failed. | 
| RES_OK | Success. | 
| DSTATUS nand_disk_status | ( | uint8_t | physicalDrive | ) | 
| physicalDrive | Physical drive number. | 
| STA_NOINIT | Failed. | 
| RES_OK | Success. | 
| DRESULT nand_disk_read | ( | uint8_t | physicalDrive, | 
| uint8_t * | buffer, | ||
| uint32_t | sector, | ||
| uint8_t | count | ||
| ) | 
| physicalDrive | Physical drive number. | 
| buffer | The data buffer pointer to store read content. | 
| sector | The start sector number to be read. | 
| count | The sector count to be read. | 
| RES_PARERR | Failed. | 
| RES_OK | Success. | 
| DRESULT nand_disk_write | ( | uint8_t | physicalDrive, | 
| const uint8_t * | buffer, | ||
| uint32_t | sector, | ||
| uint8_t | count | ||
| ) | 
| physicalDrive | Physical drive number. | 
| buffer | The data buffer pointer to store write content. | 
| sector | The start sector number to be written. | 
| count | The sector count to be written. | 
| RES_PARERR | Failed. | 
| RES_OK | Success. | 
| DRESULT nand_disk_ioctl | ( | uint8_t | physicalDrive, | 
| uint8_t | command, | ||
| void * | buffer | ||
| ) | 
| physicalDrive | Physical drive number. | 
| command | The command to be set. | 
| buffer | The buffer to store command result. | 
| RES_PARERR | Failed. | 
| RES_OK | Success. |