MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Packet.dll definitions and data structures

Overview

Packet32.h contains the data structures and the definitions used by packet.dll. The file is used both by the Win9x and the WinNTx versions of packet.dll, and can be included by the applications that use the functions of this library

Data Structures

struct  NetType
 Network type structure. More...
 
struct  bpf_program
 A BPF pseudo-assembly program. More...
 
struct  bpf_insn
 A single BPF pseudo-instruction. More...
 
struct  bpf_stat
 Structure that contains a couple of statistics values on the current capture. More...
 
struct  bpf_hdr
 Packet header. More...
 
struct  dump_bpf_hdr
 Dump packet header. More...
 
struct  npf_if_addr
 Addresses of a network adapter. More...
 
struct  LPADAPTER
 Describes an opened network adapter. More...
 
struct  LPPACKET
 Structure that contains a group of packets coming from the driver. More...
 
struct  PPACKET_OID_DATA
 Structure containing an OID request. More...
 

Variables

UINT NetType::LinkType
 The MAC of the current network adapter (see function PacketGetNetType() for more information)
 
ULONGLONG NetType::LinkSpeed
 The speed of the network in bits per second.
 
UINT bpf_program::bf_len
 Indicates the number of instructions of the program, i.e. the number of struct bpf_insn that will follow.
 
struct bpf_insn * bpf_program::bf_insns
 A pointer to the first instruction of the program.
 
USHORT bpf_insn::code
 Instruction type and addressing mode.
 
UCHAR bpf_insn::jt
 Jump if true.
 
UCHAR bpf_insn::jf
 Jump if false.
 
int bpf_insn::k
 Generic field used for various purposes.
 
UINT bpf_stat::bs_recv
 
UINT bpf_stat::bs_drop
 
UINT bpf_stat::ps_ifdrop
 drops by interface. XXX not yet supported
 
UINT bpf_stat::bs_capt
 
struct timeval bpf_hdr::bh_tstamp
 
UINT bpf_hdr::bh_caplen
 
UINT bpf_hdr::bh_datalen
 Original length of packet.
 
USHORT bpf_hdr::bh_hdrlen
 
struct timeval dump_bpf_hdr::ts
 Time stamp of the packet.
 
UINT dump_bpf_hdr::caplen
 
UINT dump_bpf_hdr::len
 Length of the original packet (off wire).
 
struct sockaddr_storage npf_if_addr::IPAddress
 IP address.
 
struct sockaddr_storage npf_if_addr::SubnetMask
 Netmask for that address.
 
struct sockaddr_storage npf_if_addr::Broadcast
 Broadcast address.
 
HANDLE LPADAPTER::ReadEvent
 
UINT LPADAPTER::Flags
 Adapter's flags. Tell if this adapter must be treated in a different way, using the Netmon API or the dagc API.
 
HANDLE LPPACKET::hEvent
 
OVERLAPPED LPPACKET::OverLapped
 
PVOID LPPACKET::Buffer
 
UINT LPPACKET::Length
 Length of the buffer.
 
DWORD LPPACKET::ulBytesReceived
 
BOOLEAN LPPACKET::bIoComplete
 
ULONG PPACKET_OID_DATA::Oid
 
ULONG PPACKET_OID_DATA::Length
 Length of the data field.
 
UCHAR PPACKET_OID_DATA::Data [1]
 
typedef struct WAN_ADAPTER_INT WAN_ADAPTER
 Describes an opened wan (dialup, VPN...) network adapter using the NetMon API.
 
typedef WAN_ADAPTER * PWAN_ADAPTER
 Describes an opened wan (dialup, VPN...) network adapter using the NetMon API.
 
#define PACKET_MODE_CAPT   0x0
 Capture mode.
 
#define PACKET_MODE_STAT   0x1
 Statistical mode.
 
#define PACKET_MODE_MON   0x2
 Monitoring mode.
 
#define PACKET_MODE_DUMP   0x10
 Dump mode.
 
#define PACKET_MODE_STAT_DUMP   MODE_DUMP | MODE_STAT
 Statistical dump Mode.
 
#define Packet_ALIGNMENT   sizeof(int)
 Alignment macro. Defines the alignment size.
 
#define Packet_WORDALIGN(x)   (((x)+(Packet_ALIGNMENT-1))&~(Packet_ALIGNMENT-1))
 Alignment macro. Rounds up to the next even multiple of Packet_ALIGNMENT.
 
#define NdisMediumNull   -1
 Custom linktype: NDIS doesn't provide an equivalent.
 
#define NdisMediumCHDLC   -2
 Custom linktype: NDIS doesn't provide an equivalent.
 
#define NdisMediumPPPSerial   -3
 Custom linktype: NDIS doesn't provide an equivalent.
 
#define NdisMediumBare80211   -4
 Custom linktype: NDIS doesn't provide an equivalent.
 
#define NdisMediumRadio80211   -5
 Custom linktype: NDIS doesn't provide an equivalent.
 
#define NdisMediumPpi   -6
 Custom linktype: NDIS doesn't provide an equivalent.
 
#define NPF_DISABLE_LOOPBACK   1
 Drop the packets sent by the NPF driver.
 
#define NPF_ENABLE_LOOPBACK   2
 Capture the packets sent by the NPF driver.
 
#define DOSNAMEPREFIX   TEXT("Packet_")
 Prefix added to the adapters device names to create the WinPcap devices.
 
#define ADAPTER_NAME_LENGTH   256 + 12
 Maximum length for the name of an adapter. The value is the same used by the IP Helper API.
 
#define ADAPTER_DESC_LENGTH   128
 Maximum length for the description of an adapter. The value is the same used by the IP Helper API.
 
#define MAX_MAC_ADDR_LENGTH   8
 Maximum length for the link layer address of an adapter. The value is the same used by the IP Helper API.
 
#define MAX_NETWORK_ADDRESSES   16
 Maximum length for the link layer address of an adapter. The value is the same used by the IP Helper API.
 
#define INFO_FLAG_NDIS_ADAPTER   0
 Flag for ADAPTER_INFO: this is a traditional ndis adapter.
 
#define INFO_FLAG_NDISWAN_ADAPTER   1
 Flag for ADAPTER_INFO: this is a NdisWan adapter, and it's managed by WANPACKET.
 
#define INFO_FLAG_DAG_CARD   2
 Flag for ADAPTER_INFO: this is a DAG card.
 
#define INFO_FLAG_DAG_FILE   6
 Flag for ADAPTER_INFO: this is a DAG file.
 
#define INFO_FLAG_DONT_EXPORT   8
 Flag for ADAPTER_INFO: when this flag is set, the adapter will not be listed or openend by winpcap. This allows to prevent exporting broken network adapters, like for example FireWire ones.
 
#define INFO_FLAG_AIRPCAP_CARD   16
 Flag for ADAPTER_INFO: this is an airpcap card.
 

Data Structure Documentation

struct NetType

This structure is used by the PacketGetNetType() function to return information on the current adapter's type and speed.

Data Fields

UINT LinkType
 The MAC of the current network adapter (see function PacketGetNetType() for more information)
 
ULONGLONG LinkSpeed
 The speed of the network in bits per second.
 
struct bpf_program

The program will be injected in the kernel by the PacketSetBPF() function and applied to every incoming packet.

Data Fields

UINT bf_len
 Indicates the number of instructions of the program, i.e. the number of struct bpf_insn that will follow.
 
struct bpf_insn * bf_insns
 A pointer to the first instruction of the program.
 
struct bpf_insn

bpf_insn contains a single instruction for the BPF register-machine. It is used to send a filter program to the driver.

Data Fields

USHORT code
 Instruction type and addressing mode.
 
UCHAR jt
 Jump if true.
 
UCHAR jf
 Jump if false.
 
int k
 Generic field used for various purposes.
 
struct bpf_stat

It is used by packet.dll to return statistics about a capture session.

Data Fields

UINT bs_recv
 
UINT bs_drop
 
UINT ps_ifdrop
 drops by interface. XXX not yet supported
 
UINT bs_capt
 
struct bpf_hdr

This structure defines the header associated with every packet delivered to the application.

Data Fields

struct timeval bh_tstamp
 
UINT bh_caplen
 
UINT bh_datalen
 Original length of packet.
 
USHORT bh_hdrlen
 
struct dump_bpf_hdr

This structure defines the header associated with the packets in a buffer to be used with PacketSendPackets(). It is simpler than the bpf_hdr, because it corresponds to the header associated by WinPcap and libpcap to a packet in a dump file. This makes straightforward sending WinPcap dump files to the network.

Data Fields

struct timeval ts
 Time stamp of the packet.
 
UINT caplen
 
UINT len
 Length of the original packet (off wire).
 
struct npf_if_addr

This structure is used by the PacketGetNetInfoEx() function to return the IP addresses associated with an adapter.

Data Fields

struct sockaddr_storage IPAddress
 IP address.
 
struct sockaddr_storage SubnetMask
 Netmask for that address.
 
struct sockaddr_storage Broadcast
 Broadcast address.
 
struct ADAPTER

This structure is the most important for the functioning of packet.dll, but the great part of its fields should be ignored by the user, since the library offers functions that avoid to cope with low-level parameters

Data Fields

HANDLE ReadEvent
 
UINT Flags
 Adapter's flags. Tell if this adapter must be treated in a different way, using the Netmon API or the dagc API.
 
struct PACKET

This structure defines the header associated with every packet delivered to the application.

Data Fields

HANDLE hEvent
 
OVERLAPPED OverLapped
 
PVOID Buffer
 
UINT Length
 Length of the buffer.
 
DWORD ulBytesReceived
 
BOOLEAN bIoComplete
 
struct _PACKET_OID_DATA

It is used by the PacketRequest() function to send an OID to the interface card driver. It can be used, for example, to retrieve the status of the error counters on the adapter, its MAC address, the list of the multicast groups defined on it, and so on.

Data Fields

ULONG Oid
 
ULONG Length
 Length of the data field.
 
UCHAR Data [1]
 

Variable Documentation

UINT bpf_stat::bs_recv

Number of packets that the driver received from the network adapter from the beginning of the current capture. This value includes the packets lost by the driver.

UINT bpf_stat::bs_drop

number of packets that the driver lost from the beginning of a capture. Basically, a packet is lost when the the buffer of the driver is full. In this situation the packet cannot be stored and the driver rejects it.

UINT bpf_stat::bs_capt

number of packets that pass the filter, find place in the kernel buffer and thus reach the application.

struct timeval bpf_hdr::bh_tstamp

The timestamp associated with the captured packet. It is stored in a TimeVal structure.

UINT bpf_hdr::bh_caplen

Length of captured portion. The captured portion can be different from the original packet, because it is possible (with a proper filter) to instruct the driver to capture only a portion of the packets.

USHORT bpf_hdr::bh_hdrlen

Length of bpf header (this struct plus alignment padding). In some cases, a padding could be added between the end of this structure and the packet data for performance reasons. This filed can be used to retrieve the actual data of the packet.

UINT dump_bpf_hdr::caplen

Length of captured portion. The captured portion can smaller than the the original packet, because it is possible (with a proper filter) to instruct the driver to capture only a portion of the packets.

HANDLE LPADAPTER::ReadEvent

A notification event associated with the read calls on the adapter. It can be passed to standard Win32 functions (like WaitForSingleObject or WaitForMultipleObjects) to wait until the driver's buffer contains some data. It is particularly useful in GUI applications that need to wait concurrently on several events. In Windows NT/2000 the PacketSetMinToCopy() function can be used to define the minimum amount of data in the kernel buffer that will cause the event to be signalled.

HANDLE LPPACKET::hEvent
OVERLAPPED LPPACKET::OverLapped
PVOID LPPACKET::Buffer

Buffer with containing the packets. See the PacketReceivePacket() for details about the organization of the data in this buffer

DWORD LPPACKET::ulBytesReceived

Number of valid bytes present in the buffer, i.e. amount of data received by the last call to PacketReceivePacket()

BOOLEAN LPPACKET::bIoComplete
ULONG PPACKET_OID_DATA::Oid

OID code. See the Microsoft DDK documentation or the file ntddndis.h for a complete list of valid codes.

UCHAR PPACKET_OID_DATA::Data[1]

variable-lenght field that contains the information passed to or received from the adapter.