MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
CSI: CMOS Sensor Interface

Overview

The MCUXpresso SDK provides a driver for the CMOS Sensor Interface (CSI)

The CSI enables the chip to connect directly to external CMOS image sensors. The CSI driver provides functional APIs and transactional APIs for the CSI module. The functional APIs implement the basic functions, so the user can construct them for a special use case. The transactional APIs provide a queue mechanism in order for the user to submit an empty frame buffer and get a fully-filled frame buffer easily.

Frame Buffer Queue

The CSI transactional functions maintain a frame buffer queue. The queue size is defined by the macro CSI_DRIVER_QUEUE_SIZE. The queue size is 4 by default, but the user can override it by redefining the macro value in the project setting.
To use transactional APIs, first call CSI_TransferCreateHandle to create a handle to save the CSI driver state. This function initializes the frame buffer queue to empty status.
After the handle is created, the function CSI_TransferSubmitEmptyBuffer can be used to submit the empty frame buffer to the queue. If the queue does not have room to save the new empty frame buffers, this function returns with an error. It is not necessary to check the queue rooms before submitting an empty frame buffer. After this step, the application can call CSI_TransferStart to start the transfer. There must be at least two empty buffers in the queue, otherwise this function returns an error. The incoming frames are saved to the empty buffers one by one, and a callback is provided when every frame completed. To get the fully-filled frame buffer, call the function CSI_TransferGetFullBuffer. This function returns an error if the frame buffer queue does not have full buffers. Therefore, it is not necessary to check the full buffer number in the queue before this function.
To stop the transfer, call the function CSI_TransferStop at anytime. If the queue has some full frame buffers, the application can still read them out after this stop function.
Once the transfer is started by calling CSI_TransferStart, the CSI device starts to receive frames and save into buffer. The CSI devices does not stop until CSI_TransferStop is called. If application does not submit empty buffer to CSI driver, the CSI driver always writes to the last submited empty buffer, this buffer will never be sent into full buffer queue until new empty buffer submited. In other words, one frame buffer is reserved by CSI driver, if application submits N empty buffers, it could get (N-1) full buffers.

Fragment Mode

The frame buffer queue mechanism needs large memory, it is not suitable for some special case, for example, no SDRAM used. Fragment mode is designed for this purpose, it needs two types of buffers:

  1. DMA buffer. It could be as small as (camera frame width x 2 x 2) bytes, CSI DMA writes the input data to this buffer.
  2. Frame buffer. The input data is copied to this buffer at last. What is more, user could define a window (in other words, region of interest), only image in this window will be copied to the frame buffer. If input data is YUV422 format, user can only save Y component optionally.

Limitations:

  1. Fragment mode could not be used together with frame buffer queue mode.
  2. In fragment mode, user should pay attention to the system payload. When the payload is high, the image capture might be broken.

Typical use case

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/csi

Data Structures

struct  csi_config_t
 Configuration to initialize the CSI module. More...
 
struct  csi_handle_t
 CSI handle structure. More...
 

Macros

#define CSI_DRIVER_QUEUE_SIZE   4U
 Size of the frame buffer queue used in CSI transactional function. More...
 
#define CSI_DRIVER_FRAG_MODE   0U
 Enable fragment capture function or not. More...
 

Typedefs

typedef void(* csi_transfer_callback_t )(CSI_Type *base, csi_handle_t *handle, status_t status, void *userData)
 CSI transfer callback function. More...
 

Enumerations

enum  _csi_status {
  kStatus_CSI_NoEmptyBuffer = MAKE_STATUS(kStatusGroup_CSI, 0),
  kStatus_CSI_NoFullBuffer = MAKE_STATUS(kStatusGroup_CSI, 1),
  kStatus_CSI_QueueFull = MAKE_STATUS(kStatusGroup_CSI, 2),
  kStatus_CSI_FrameDone = MAKE_STATUS(kStatusGroup_CSI, 3)
}
 Error codes for the CSI driver. More...
 
enum  csi_work_mode_t {
  kCSI_GatedClockMode = CSI_CSICR1_GCLK_MODE(1U),
  kCSI_NonGatedClockMode = 0U,
  kCSI_CCIR656ProgressiveMode = CSI_CSICR1_CCIR_EN(1U)
}
 CSI work mode. More...
 
enum  csi_data_bus_t {
  kCSI_DataBus8Bit,
  kCSI_DataBus16Bit,
  kCSI_DataBus24Bit
}
 CSI data bus witdh. More...
 
enum  _csi_polarity_flags {
  kCSI_HsyncActiveLow = 0U,
  kCSI_HsyncActiveHigh = CSI_CSICR1_HSYNC_POL_MASK,
  kCSI_DataLatchOnRisingEdge = CSI_CSICR1_REDGE_MASK,
  kCSI_DataLatchOnFallingEdge = 0U,
  kCSI_VsyncActiveHigh = 0U,
  kCSI_VsyncActiveLow = CSI_CSICR1_SOF_POL_MASK
}
 CSI signal polarity. More...
 
enum  csi_fifo_t {
  kCSI_RxFifo = (1U << 0U),
  kCSI_StatFifo = (1U << 1U),
  kCSI_AllFifo = 0x01 | 0x02
}
 The CSI FIFO, used for FIFO operation. More...
 
enum  _csi_interrupt_enable {
  kCSI_EndOfFrameInterruptEnable = CSI_CSICR1_EOF_INT_EN_MASK,
  kCSI_ChangeOfFieldInterruptEnable = CSI_CSICR1_COF_INT_EN_MASK,
  kCSI_StatFifoOverrunInterruptEnable = CSI_CSICR1_SF_OR_INTEN_MASK,
  kCSI_RxFifoOverrunInterruptEnable = CSI_CSICR1_RF_OR_INTEN_MASK,
  kCSI_StatFifoDmaDoneInterruptEnable,
  kCSI_StatFifoFullInterruptEnable = CSI_CSICR1_STATFF_INTEN_MASK,
  kCSI_RxBuffer1DmaDoneInterruptEnable,
  kCSI_RxBuffer0DmaDoneInterruptEnable,
  kCSI_RxFifoFullInterruptEnable = CSI_CSICR1_RXFF_INTEN_MASK,
  kCSI_StartOfFrameInterruptEnable = CSI_CSICR1_SOF_INTEN_MASK,
  kCSI_EccErrorInterruptEnable = CSI_CSICR3_ECC_INT_EN_MASK,
  kCSI_AhbResErrorInterruptEnable = CSI_CSICR3_HRESP_ERR_EN_MASK,
  kCSI_BaseAddrChangeErrorInterruptEnable,
  kCSI_Field0DoneInterruptEnable = CSI_CSICR18_FIELD0_DONE_IE_MASK << 6U,
  kCSI_Field1DoneInterruptEnable = CSI_CSICR18_DMA_FIELD1_DONE_IE_MASK << 6U
}
 CSI feature interrupt source. More...
 
enum  _csi_flags {
  kCSI_RxFifoDataReadyFlag = CSI_CSISR_DRDY_MASK,
  kCSI_EccErrorFlag = CSI_CSISR_ECC_INT_MASK,
  kCSI_AhbResErrorFlag = CSI_CSISR_HRESP_ERR_INT_MASK,
  kCSI_ChangeOfFieldFlag = CSI_CSISR_COF_INT_MASK,
  kCSI_Field0PresentFlag = CSI_CSISR_F1_INT_MASK,
  kCSI_Field1PresentFlag = CSI_CSISR_F2_INT_MASK,
  kCSI_StartOfFrameFlag = CSI_CSISR_SOF_INT_MASK,
  kCSI_EndOfFrameFlag = CSI_CSISR_EOF_INT_MASK,
  kCSI_RxFifoFullFlag = CSI_CSISR_RxFF_INT_MASK,
  kCSI_RxBuffer1DmaDoneFlag = CSI_CSISR_DMA_TSF_DONE_FB2_MASK,
  kCSI_RxBuffer0DmaDoneFlag = CSI_CSISR_DMA_TSF_DONE_FB1_MASK,
  kCSI_StatFifoFullFlag = CSI_CSISR_STATFF_INT_MASK,
  kCSI_StatFifoDmaDoneFlag = CSI_CSISR_DMA_TSF_DONE_SFF_MASK,
  kCSI_StatFifoOverrunFlag = CSI_CSISR_SF_OR_INT_MASK,
  kCSI_RxFifoOverrunFlag = CSI_CSISR_RF_OR_INT_MASK,
  kCSI_Field0DoneFlag = CSI_CSISR_DMA_FIELD0_DONE_MASK,
  kCSI_Field1DoneFlag = CSI_CSISR_DMA_FIELD1_DONE_MASK,
  kCSI_BaseAddrChangeErrorFlag = CSI_CSISR_BASEADDR_CHHANGE_ERROR_MASK
}
 CSI status flags. More...
 

Driver version

#define FSL_CSI_DRIVER_VERSION   (MAKE_VERSION(2, 0, 4))
 

Initialization and deinitialization

status_t CSI_Init (CSI_Type *base, const csi_config_t *config)
 Initialize the CSI. More...
 
void CSI_Deinit (CSI_Type *base)
 De-initialize the CSI. More...
 
void CSI_Reset (CSI_Type *base)
 Reset the CSI. More...
 
void CSI_GetDefaultConfig (csi_config_t *config)
 Get the default configuration for to initialize the CSI. More...
 

Module operation

void CSI_ClearFifo (CSI_Type *base, csi_fifo_t fifo)
 Clear the CSI FIFO. More...
 
void CSI_ReflashFifoDma (CSI_Type *base, csi_fifo_t fifo)
 Reflash the CSI FIFO DMA. More...
 
void CSI_EnableFifoDmaRequest (CSI_Type *base, csi_fifo_t fifo, bool enable)
 Enable or disable the CSI FIFO DMA request. More...
 
static void CSI_Start (CSI_Type *base)
 Start to receive data. More...
 
static void CSI_Stop (CSI_Type *base)
 Stop to receiving data. More...
 
void CSI_SetRxBufferAddr (CSI_Type *base, uint8_t index, uint32_t addr)
 Set the RX frame buffer address. More...
 

Interrupts

void CSI_EnableInterrupts (CSI_Type *base, uint32_t mask)
 Enables CSI interrupt requests. More...
 
void CSI_DisableInterrupts (CSI_Type *base, uint32_t mask)
 Disable CSI interrupt requests. More...
 

Status

static uint32_t CSI_GetStatusFlags (CSI_Type *base)
 Gets the CSI status flags. More...
 
static void CSI_ClearStatusFlags (CSI_Type *base, uint32_t statusMask)
 Clears the CSI status flag. More...
 

Transactional

status_t CSI_TransferCreateHandle (CSI_Type *base, csi_handle_t *handle, csi_transfer_callback_t callback, void *userData)
 Initializes the CSI handle. More...
 
status_t CSI_TransferStart (CSI_Type *base, csi_handle_t *handle)
 Start the transfer using transactional functions. More...
 
status_t CSI_TransferStop (CSI_Type *base, csi_handle_t *handle)
 Stop the transfer using transactional functions. More...
 
status_t CSI_TransferSubmitEmptyBuffer (CSI_Type *base, csi_handle_t *handle, uint32_t frameBuffer)
 Submit empty frame buffer to queue. More...
 
status_t CSI_TransferGetFullBuffer (CSI_Type *base, csi_handle_t *handle, uint32_t *frameBuffer)
 Get one full frame buffer from queue. More...
 
void CSI_TransferHandleIRQ (CSI_Type *base, csi_handle_t *handle)
 CSI IRQ handle function. More...
 

Data Structure Documentation

struct csi_config_t

Data Fields

uint16_t width
 Pixels of the input frame. More...
 
uint16_t height
 Lines of the input frame. More...
 
uint32_t polarityFlags
 Timing signal polarity flags, OR'ed value of _csi_polarity_flags. More...
 
uint8_t bytesPerPixel
 Bytes per pixel, valid values are: More...
 
uint16_t linePitch_Bytes
 Frame buffer line pitch, must be 8-byte aligned. More...
 
csi_work_mode_t workMode
 CSI work mode. More...
 
csi_data_bus_t dataBus
 Data bus width. More...
 
bool useExtVsync
 In CCIR656 progressive mode, set true to use external VSYNC signal, set false to use internal VSYNC signal decoded from SOF. More...
 

Field Documentation

uint16_t csi_config_t::width
uint16_t csi_config_t::height
uint32_t csi_config_t::polarityFlags
uint8_t csi_config_t::bytesPerPixel
  • 2: Used for RGB565, YUV422, and so on.
  • 4: Used for XRGB8888, XYUV444, and so on.
uint16_t csi_config_t::linePitch_Bytes
csi_work_mode_t csi_config_t::workMode
csi_data_bus_t csi_config_t::dataBus
bool csi_config_t::useExtVsync
struct _csi_handle

Please see the user guide for the details of the CSI driver queue mechanism.

Data Fields

uint32_t frameBufferQueue [CSI_DRIVER_ACTUAL_QUEUE_SIZE]
 Frame buffer queue. More...
 
volatile uint8_t queueWriteIdx
 Pointer to save incoming item. More...
 
volatile uint8_t queueReadIdx
 Pointer to read out the item. More...
 
void *volatile emptyBuffer
 Pointer to maintain the empty frame buffers. More...
 
volatile uint8_t emptyBufferCnt
 Empty frame buffers count. More...
 
volatile uint8_t activeBufferNum
 How many frame buffers are in progres currently. More...
 
volatile bool transferStarted
 User has called CSI_TransferStart to start frame receiving. More...
 
csi_transfer_callback_t callback
 Callback function. More...
 
void * userData
 CSI callback function parameter. More...
 

Field Documentation

uint32_t csi_handle_t::frameBufferQueue[CSI_DRIVER_ACTUAL_QUEUE_SIZE]
volatile uint8_t csi_handle_t::queueWriteIdx
volatile uint8_t csi_handle_t::queueReadIdx
void* volatile csi_handle_t::emptyBuffer
volatile uint8_t csi_handle_t::emptyBufferCnt
volatile uint8_t csi_handle_t::activeBufferNum
volatile bool csi_handle_t::transferStarted
csi_transfer_callback_t csi_handle_t::callback
void* csi_handle_t::userData

Macro Definition Documentation

#define CSI_DRIVER_QUEUE_SIZE   4U
#define CSI_DRIVER_FRAG_MODE   0U

Typedef Documentation

typedef void(* csi_transfer_callback_t)(CSI_Type *base, csi_handle_t *handle, status_t status, void *userData)

When a new frame is received and saved to the frame buffer queue, the callback is called and the pass the status kStatus_CSI_FrameDone to upper layer.

Enumeration Type Documentation

Enumerator
kStatus_CSI_NoEmptyBuffer 

No empty frame buffer in queue to load to CSI.

kStatus_CSI_NoFullBuffer 

No full frame buffer in queue to read out.

kStatus_CSI_QueueFull 

Queue is full, no room to save new empty buffer.

kStatus_CSI_FrameDone 

New frame received and saved to queue.

The CCIR656 interlace mode is not supported currently.

Enumerator
kCSI_GatedClockMode 

HSYNC, VSYNC, and PIXCLK signals are used.

kCSI_NonGatedClockMode 

VSYNC, and PIXCLK signals are used.

kCSI_CCIR656ProgressiveMode 

CCIR656 progressive mode.

Enumerator
kCSI_DataBus8Bit 

8-bit data bus.

kCSI_DataBus16Bit 

16-bit data bus.

kCSI_DataBus24Bit 

24-bit data bus.

Enumerator
kCSI_HsyncActiveLow 

HSYNC is active low.

kCSI_HsyncActiveHigh 

HSYNC is active high.

kCSI_DataLatchOnRisingEdge 

Pixel data latched at rising edge of pixel clock.

kCSI_DataLatchOnFallingEdge 

Pixel data latched at falling edge of pixel clock.

kCSI_VsyncActiveHigh 

VSYNC is active high.

kCSI_VsyncActiveLow 

VSYNC is active low.

enum csi_fifo_t
Enumerator
kCSI_RxFifo 

RXFIFO.

kCSI_StatFifo 

STAT FIFO.

kCSI_AllFifo 

Both RXFIFO and STAT FIFO.

Enumerator
kCSI_EndOfFrameInterruptEnable 

End of frame interrupt enable.

kCSI_ChangeOfFieldInterruptEnable 

Change of field interrupt enable.

kCSI_StatFifoOverrunInterruptEnable 

STAT FIFO overrun interrupt enable.

kCSI_RxFifoOverrunInterruptEnable 

RXFIFO overrun interrupt enable.

kCSI_StatFifoDmaDoneInterruptEnable 

STAT FIFO DMA done interrupt enable.

kCSI_StatFifoFullInterruptEnable 

STAT FIFO full interrupt enable.

kCSI_RxBuffer1DmaDoneInterruptEnable 

RX frame buffer 1 DMA transfer done.

kCSI_RxBuffer0DmaDoneInterruptEnable 

RX frame buffer 0 DMA transfer done.

kCSI_RxFifoFullInterruptEnable 

RXFIFO full interrupt enable.

kCSI_StartOfFrameInterruptEnable 

Start of frame (SOF) interrupt enable.

kCSI_EccErrorInterruptEnable 

ECC error detection interrupt enable.

kCSI_AhbResErrorInterruptEnable 

AHB response Error interrupt enable.

kCSI_BaseAddrChangeErrorInterruptEnable 

The DMA output buffer base address changes before DMA completed.

kCSI_Field0DoneInterruptEnable 

Field 0 done interrupt enable.

kCSI_Field1DoneInterruptEnable 

Field 1 done interrupt enable.

enum _csi_flags

The following status register flags can be cleared:

  • kCSI_EccErrorFlag
  • kCSI_AhbResErrorFlag
  • kCSI_ChangeOfFieldFlag
  • kCSI_StartOfFrameFlag
  • kCSI_EndOfFrameFlag
  • kCSI_RxBuffer1DmaDoneFlag
  • kCSI_RxBuffer0DmaDoneFlag
  • kCSI_StatFifoDmaDoneFlag
  • kCSI_StatFifoOverrunFlag
  • kCSI_RxFifoOverrunFlag
  • kCSI_Field0DoneFlag
  • kCSI_Field1DoneFlag
  • kCSI_BaseAddrChangeErrorFlag
Enumerator
kCSI_RxFifoDataReadyFlag 

RXFIFO data ready.

kCSI_EccErrorFlag 

ECC error detected.

kCSI_AhbResErrorFlag 

Hresponse (AHB bus response) Error.

kCSI_ChangeOfFieldFlag 

Change of field.

kCSI_Field0PresentFlag 

Field 0 present in CCIR mode.

kCSI_Field1PresentFlag 

Field 1 present in CCIR mode.

kCSI_StartOfFrameFlag 

Start of frame (SOF) detected.

kCSI_EndOfFrameFlag 

End of frame (EOF) detected.

kCSI_RxFifoFullFlag 

RXFIFO full (Number of data reaches trigger level).

kCSI_RxBuffer1DmaDoneFlag 

RX frame buffer 1 DMA transfer done.

kCSI_RxBuffer0DmaDoneFlag 

RX frame buffer 0 DMA transfer done.

kCSI_StatFifoFullFlag 

STAT FIFO full (Reach trigger level).

kCSI_StatFifoDmaDoneFlag 

STAT FIFO DMA transfer done.

kCSI_StatFifoOverrunFlag 

STAT FIFO overrun.

kCSI_RxFifoOverrunFlag 

RXFIFO overrun.

kCSI_Field0DoneFlag 

Field 0 transfer done.

kCSI_Field1DoneFlag 

Field 1 transfer done.

kCSI_BaseAddrChangeErrorFlag 

The DMA output buffer base address changes before DMA completed.

Function Documentation

status_t CSI_Init ( CSI_Type *  base,
const csi_config_t *  config 
)

This function enables the CSI peripheral clock, and resets the CSI registers.

Parameters
baseCSI peripheral base address.
configPointer to the configuration structure.
Return values
kStatus_SuccessInitialize successfully.
kStatus_InvalidArgumentInitialize failed because of invalid argument.
void CSI_Deinit ( CSI_Type *  base)

This function disables the CSI peripheral clock.

Parameters
baseCSI peripheral base address.
void CSI_Reset ( CSI_Type *  base)

This function resets the CSI peripheral registers to default status.

Parameters
baseCSI peripheral base address.
void CSI_GetDefaultConfig ( csi_config_t *  config)

The default configuration value is:

config->width = 320U;
config->height = 240U;
config->bytesPerPixel = 2U;
config->linePitch_Bytes = 320U * 2U;
config->workMode = kCSI_GatedClockMode;
config->dataBus = kCSI_DataBus8Bit;
config->useExtVsync = true;
Parameters
configPointer to the CSI configuration.
void CSI_ClearFifo ( CSI_Type *  base,
csi_fifo_t  fifo 
)

This function clears the CSI FIFO.

Parameters
baseCSI peripheral base address.
fifoThe FIFO to clear.
void CSI_ReflashFifoDma ( CSI_Type *  base,
csi_fifo_t  fifo 
)

This function reflashes the CSI FIFO DMA.

For RXFIFO, there are two frame buffers. When the CSI module started, it saves the frames to frame buffer 0 then frame buffer 1, the two buffers will be written by turns. After reflash DMA using this function, the CSI is reset to save frame to buffer 0.

Parameters
baseCSI peripheral base address.
fifoThe FIFO DMA to reflash.
void CSI_EnableFifoDmaRequest ( CSI_Type *  base,
csi_fifo_t  fifo,
bool  enable 
)
Parameters
baseCSI peripheral base address.
fifoThe FIFO DMA reques to enable or disable.
enableTrue to enable, false to disable.
static void CSI_Start ( CSI_Type *  base)
inlinestatic
Parameters
baseCSI peripheral base address.
static void CSI_Stop ( CSI_Type *  base)
inlinestatic
Parameters
baseCSI peripheral base address.
void CSI_SetRxBufferAddr ( CSI_Type *  base,
uint8_t  index,
uint32_t  addr 
)
Parameters
baseCSI peripheral base address.
indexBuffer index.
addrFrame buffer address to set.
void CSI_EnableInterrupts ( CSI_Type *  base,
uint32_t  mask 
)
Parameters
baseCSI peripheral base address.
maskThe interrupts to enable, pass in as OR'ed value of _csi_interrupt_enable.
void CSI_DisableInterrupts ( CSI_Type *  base,
uint32_t  mask 
)
Parameters
baseCSI peripheral base address.
maskThe interrupts to disable, pass in as OR'ed value of _csi_interrupt_enable.
static uint32_t CSI_GetStatusFlags ( CSI_Type *  base)
inlinestatic
Parameters
baseCSI peripheral base address.
Returns
status flag, it is OR'ed value of _csi_flags.
static void CSI_ClearStatusFlags ( CSI_Type *  base,
uint32_t  statusMask 
)
inlinestatic

The flags to clear are passed in as OR'ed value of _csi_flags. The following flags are cleared automatically by hardware:

Parameters
baseCSI peripheral base address.
statusMaskThe status flags mask, OR'ed value of _csi_flags.
status_t CSI_TransferCreateHandle ( CSI_Type *  base,
csi_handle_t *  handle,
csi_transfer_callback_t  callback,
void *  userData 
)

This function initializes CSI handle, it should be called before any other CSI transactional functions.

Parameters
baseCSI peripheral base address.
handlePointer to the handle structure.
callbackCallback function for CSI transfer.
userDataCallback function parameter.
Return values
kStatus_SuccessHandle created successfully.
status_t CSI_TransferStart ( CSI_Type *  base,
csi_handle_t *  handle 
)

When the empty frame buffers have been submit to CSI driver using function CSI_TransferSubmitEmptyBuffer, user could call this function to start the transfer. The incoming frame will be saved to the empty frame buffer, and user could be optionally notified through callback function.

Parameters
baseCSI peripheral base address.
handlePointer to the handle structure.
Return values
kStatus_SuccessStarted successfully.
kStatus_CSI_NoEmptyBufferCould not start because no empty frame buffer in queue.
status_t CSI_TransferStop ( CSI_Type *  base,
csi_handle_t *  handle 
)

The driver does not clean the full frame buffers in queue. In other words, after calling this function, user still could get the full frame buffers in queue using function CSI_TransferGetFullBuffer.

Parameters
baseCSI peripheral base address.
handlePointer to the handle structure.
Return values
kStatus_SuccessStoped successfully.
status_t CSI_TransferSubmitEmptyBuffer ( CSI_Type *  base,
csi_handle_t *  handle,
uint32_t  frameBuffer 
)

This function could be called before CSI_TransferStart or after CSI_TransferStart. If there is no room in queue to store the empty frame buffer, this function returns error.

Parameters
baseCSI peripheral base address.
handlePointer to the handle structure.
frameBufferEmpty frame buffer to submit.
Return values
kStatus_SuccessStarted successfully.
kStatus_CSI_QueueFullCould not submit because there is no room in queue.
status_t CSI_TransferGetFullBuffer ( CSI_Type *  base,
csi_handle_t *  handle,
uint32_t *  frameBuffer 
)

After the transfer started using function CSI_TransferStart, the incoming frames will be saved to the empty frame buffers in queue. This function gets the full-filled frame buffer from the queue. If there is no full frame buffer in queue, this function returns error.

Parameters
baseCSI peripheral base address.
handlePointer to the handle structure.
frameBufferFull frame buffer.
Return values
kStatus_SuccessStarted successfully.
kStatus_CSI_NoFullBufferThere is no full frame buffer in queue.
void CSI_TransferHandleIRQ ( CSI_Type *  base,
csi_handle_t *  handle 
)

This function handles the CSI IRQ request to work with CSI driver transactional APIs.

Parameters
baseCSI peripheral base address.
handleCSI handle pointer.