![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
struct | flexio_mculcd_smartdma_handle_t |
FlexIO MCULCD SMARTDMA transfer handle, users should not touch the content of the handle. More... | |
struct | flexio_mculcd_smartdma_config_t |
FlexIO MCULCD SMARTDMA configuration. More... | |
Macros | |
#define | FSL_FLEXIO_MCULCD_SMARTDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
FlexIO MCULCD SMARTDMA driver version 2.0.0. More... | |
#define | FLEXIO_MCULCD_SMARTDMA_TX_LEN_ALIGN 64U |
SMARTDMA transfer size should be multiple of 64 bytes. More... | |
#define | FLEXIO_MCULCD_SMARTDMA_TX_ADDR_ALIGN 4U |
SMARTDMA transfer memory address should be 4 byte aligned. More... | |
Typedefs | |
typedef void(* | flexio_mculcd_smartdma_transfer_callback_t )(FLEXIO_MCULCD_Type *base, flexio_mculcd_smartdma_handle_t *handle, status_t status, void *userData) |
FlexIO MCULCD master callback for transfer complete. More... | |
SMARTDMA Transactional | |
status_t | FLEXIO_MCULCD_TransferCreateHandleSMARTDMA (FLEXIO_MCULCD_Type *base, flexio_mculcd_smartdma_handle_t *handle, const flexio_mculcd_smartdma_config_t *config, flexio_mculcd_smartdma_transfer_callback_t callback, void *userData) |
Initializes the FLEXO MCULCD master SMARTDMA handle. More... | |
status_t | FLEXIO_MCULCD_TransferSMARTDMA (FLEXIO_MCULCD_Type *base, flexio_mculcd_smartdma_handle_t *handle, flexio_mculcd_transfer_t *xfer) |
Performs a non-blocking FlexIO MCULCD transfer using SMARTDMA. More... | |
void | FLEXIO_MCULCD_TransferAbortSMARTDMA (FLEXIO_MCULCD_Type *base, flexio_mculcd_smartdma_handle_t *handle) |
Aborts a FlexIO MCULCD transfer using SMARTDMA. More... | |
status_t | FLEXIO_MCULCD_TransferGetCountSMARTDMA (FLEXIO_MCULCD_Type *base, flexio_mculcd_smartdma_handle_t *handle, size_t *count) |
Gets the remaining bytes for FlexIO MCULCD SMARTDMA transfer. More... | |
struct _flexio_mculcd_smartdma_handle |
typedef for flexio_mculcd_smartdma_handle_t in advance.
Data Fields | |
FLEXIO_MCULCD_Type * | base |
Pointer to the FLEXIO_MCULCD_Type. More... | |
size_t | dataCount |
Total count to be transferred. More... | |
uint32_t | dataAddrOrSameValue |
When sending the same value for many times, this is the value to send. More... | |
size_t | dataCountUsingEzh |
Data transfered using SMARTDMA. More... | |
volatile size_t | remainingCount |
Remaining count to transfer. More... | |
volatile uint32_t | state |
FlexIO MCULCD driver internal state. More... | |
uint8_t | smartdmaApi |
The SMARTDMA API used during transfer. More... | |
bool | needColorConvert |
Need color convert or not. More... | |
uint8_t | blockingXferBuffer [FLEXIO_MCULCD_SMARTDMA_TX_LEN_ALIGN *3/2] |
Used for blocking method color space convet. More... | |
flexio_mculcd_smartdma_transfer_callback_t | completionCallback |
Callback for MCULCD SMARTDMA transfer. | |
void * | userData |
User Data for MCULCD SMARTDMA callback. | |
FLEXIO_MCULCD_Type* flexio_mculcd_smartdma_handle_t::base |
size_t flexio_mculcd_smartdma_handle_t::dataCount |
uint32_t flexio_mculcd_smartdma_handle_t::dataAddrOrSameValue |
When writing or reading array, this is the address of the data array.
size_t flexio_mculcd_smartdma_handle_t::dataCountUsingEzh |
volatile size_t flexio_mculcd_smartdma_handle_t::remainingCount |
volatile uint32_t flexio_mculcd_smartdma_handle_t::state |
uint8_t flexio_mculcd_smartdma_handle_t::smartdmaApi |
bool flexio_mculcd_smartdma_handle_t::needColorConvert |
uint8_t flexio_mculcd_smartdma_handle_t::blockingXferBuffer[FLEXIO_MCULCD_SMARTDMA_TX_LEN_ALIGN *3/2] |
struct flexio_mculcd_smartdma_config_t |
Data Fields | |
flexio_mculcd_pixel_format_t | inputPixelFormat |
The pixel format in the frame buffer. More... | |
flexio_mculcd_pixel_format_t | outputPixelFormat |
The pixel format on the 8080/68k bus. More... | |
flexio_mculcd_pixel_format_t flexio_mculcd_smartdma_config_t::inputPixelFormat |
flexio_mculcd_pixel_format_t flexio_mculcd_smartdma_config_t::outputPixelFormat |
#define FSL_FLEXIO_MCULCD_SMARTDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
#define FLEXIO_MCULCD_SMARTDMA_TX_LEN_ALIGN 64U |
#define FLEXIO_MCULCD_SMARTDMA_TX_ADDR_ALIGN 4U |
typedef void(* flexio_mculcd_smartdma_transfer_callback_t)(FLEXIO_MCULCD_Type *base, flexio_mculcd_smartdma_handle_t *handle, status_t status, void *userData) |
When transfer finished, the callback function is called and returns the status
as kStatus_FLEXIO_MCULCD_Idle.
status_t FLEXIO_MCULCD_TransferCreateHandleSMARTDMA | ( | FLEXIO_MCULCD_Type * | base, |
flexio_mculcd_smartdma_handle_t * | handle, | ||
const flexio_mculcd_smartdma_config_t * | config, | ||
flexio_mculcd_smartdma_transfer_callback_t | callback, | ||
void * | userData | ||
) |
This function initializes the FLEXO MCULCD master SMARTDMA handle which can be used for other FLEXO MCULCD transactional APIs. For a specified FLEXO MCULCD instance, call this API once to get the initialized handle.
base | Pointer to FLEXIO_MCULCD_Type structure. |
handle | Pointer to flexio_mculcd_smartdma_handle_t structure to store the transfer state. |
config | Pointer to the configuration. |
callback | MCULCD transfer complete callback, NULL means no callback. |
userData | callback function parameter. |
kStatus_Success | Successfully create the handle. |
status_t FLEXIO_MCULCD_TransferSMARTDMA | ( | FLEXIO_MCULCD_Type * | base, |
flexio_mculcd_smartdma_handle_t * | handle, | ||
flexio_mculcd_transfer_t * | xfer | ||
) |
This function returns immediately after transfer initiates. Use the callback function to check whether the transfer is completed.
base | pointer to FLEXIO_MCULCD_Type structure. |
handle | pointer to flexio_mculcd_smartdma_handle_t structure to store the transfer state. |
xfer | Pointer to FlexIO MCULCD transfer structure. |
kStatus_Success | Successfully start a transfer. |
kStatus_InvalidArgument | Input argument is invalid. |
kStatus_FLEXIO_MCULCD_Busy | FlexIO MCULCD is not idle, it is running another transfer. |
void FLEXIO_MCULCD_TransferAbortSMARTDMA | ( | FLEXIO_MCULCD_Type * | base, |
flexio_mculcd_smartdma_handle_t * | handle | ||
) |
base | pointer to FLEXIO_MCULCD_Type structure. |
handle | FlexIO MCULCD SMARTDMA handle pointer. |
status_t FLEXIO_MCULCD_TransferGetCountSMARTDMA | ( | FLEXIO_MCULCD_Type * | base, |
flexio_mculcd_smartdma_handle_t * | handle, | ||
size_t * | count | ||
) |
base | pointer to FLEXIO_MCULCD_Type structure. |
handle | FlexIO MCULCD SMARTDMA handle pointer. |
count | Number of count transferred so far by the SMARTDMA transaction. |
kStatus_Success | Get the transferred count Successfully. |
kStatus_NoTransferInProgress | No transfer in process. |