![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Files | |
| file | fsl_iap.h |
Data Structures | |
| struct | flash_ecc_log_t |
| Flash ECC log info. More... | |
| struct | flash_mode_config_t |
| Flash controller paramter config. More... | |
| struct | flash_ffr_config_t |
| Flash controller paramter config. More... | |
| struct | flash_config_t |
| Flash driver state information. More... | |
Variables | |
| uint32_t | flash_config_t::PFlashBlockBase |
| A base address of the first PFlash block. | |
| uint32_t | flash_config_t::PFlashTotalSize |
| The size of the combined PFlash block. More... | |
| uint32_t | flash_config_t::PFlashBlockCount |
| A number of PFlash blocks. More... | |
| uint32_t | flash_config_t::PFlashPageSize |
| The size in bytes of a page of PFlash. More... | |
| uint32_t | flash_config_t::PFlashSectorSize |
| The size in bytes of a sector of PFlash. More... | |
Flash version | |
| enum | _flash_driver_version_constants { kFLASH_DriverVersionName = 'F', kFLASH_DriverVersionMajor = 2, kFLASH_DriverVersionMinor = 0, kFLASH_DriverVersionBugfix = 2 } |
| Flash driver version for ROM. More... | |
| #define | MAKE_VERSION(major, minor, bugfix) (((major) << 16) | ((minor) << 8) | (bugfix)) |
| Constructs the version number for drivers. More... | |
| #define | FSL_FLASH_DRIVER_VERSION (MAKE_VERSION(2, 0, 2)) |
| Flash driver version for SDK. More... | |
Flash configuration | |
| #define | FSL_FEATURE_FLASH_IP_IS_C040HD_ATFC (1) |
| Flash IP Type. More... | |
| #define | FSL_FEATURE_FLASH_IP_IS_C040HD_FC (0) |
Flash API key | |
| enum | _flash_driver_api_keys { kFLASH_ApiEraseKey = FOUR_CHAR_CODE('l', 'f', 'e', 'k') } |
| Enumeration for Flash driver API keys. More... | |
| #define | FOUR_CHAR_CODE(a, b, c, d) (((d) << 24) | ((c) << 16) | ((b) << 8) | ((a))) |
| Constructs the four character code for the Flash driver API key. More... | |
Initialization | |
| status_t | FLASH_Init (flash_config_t *config) |
| Initializes the global flash properties structure members. More... | |
Erasing | |
| status_t | FLASH_Erase (flash_config_t *config, uint32_t start, uint32_t lengthInBytes, uint32_t key) |
| Erases the flash sectors encompassed by parameters passed into function. More... | |
Programming | |
| status_t | FLASH_Program (flash_config_t *config, uint32_t start, uint8_t *src, uint32_t lengthInBytes) |
| Programs flash with data at locations passed in through parameters. More... | |
Verification | |
| status_t | FLASH_VerifyErase (flash_config_t *config, uint32_t start, uint32_t lengthInBytes) |
| Verifies an erasure of the desired flash area at a specified margin level. More... | |
| status_t | FLASH_VerifyProgram (flash_config_t *config, uint32_t start, uint32_t lengthInBytes, const uint8_t *expectedData, uint32_t *failedAddress, uint32_t *failedData) |
| Verifies programming of the desired flash area at a specified margin level. More... | |
Properties | |
| status_t | FLASH_GetProperty (flash_config_t *config, flash_property_tag_t whichProperty, uint32_t *value) |
| Returns the desired flash property. More... | |
| struct flash_ecc_log_t |
| struct flash_mode_config_t |
| struct flash_ffr_config_t |
| struct flash_config_t |
An instance of this structure is allocated by the user of the flash driver and passed into each of the driver APIs.
Data Fields | |
| uint32_t | PFlashBlockBase |
| A base address of the first PFlash block. | |
| uint32_t | PFlashTotalSize |
| The size of the combined PFlash block. More... | |
| uint32_t | PFlashBlockCount |
| A number of PFlash blocks. More... | |
| uint32_t | PFlashPageSize |
| The size in bytes of a page of PFlash. More... | |
| uint32_t | PFlashSectorSize |
| The size in bytes of a sector of PFlash. More... | |
| #define MAKE_VERSION | ( | major, | |
| minor, | |||
| bugfix | |||
| ) | (((major) << 16) | ((minor) << 8) | (bugfix)) |
| #define FSL_FLASH_DRIVER_VERSION (MAKE_VERSION(2, 0, 2)) |
Version 2.0.2
| #define FSL_FEATURE_FLASH_IP_IS_C040HD_ATFC (1) |
| #define kStatusGroupGeneric 0 |
| #define MAKE_STATUS | ( | group, | |
| code | |||
| ) | ((((group)*100) + (code))) |
| #define FOUR_CHAR_CODE | ( | a, | |
| b, | |||
| c, | |||
| d | |||
| ) | (((d) << 24) | ((c) << 16) | ((b) << 8) | ((a))) |
| enum _flash_status |
| enum flash_property_tag_t |
| status_t FLASH_Init | ( | flash_config_t * | config | ) |
This function checks and initializes the Flash module for the other Flash APIs.
| config | Pointer to the storage for the driver runtime state. |
| kStatus_FLASH_Success | API was executed successfully. |
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. |
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. |
| kStatus_FLASH_CommandNotSupported | Flash API is not supported. |
| kStatus_FLASH_EccError | A correctable or uncorrectable error during command execution. |
| status_t FLASH_Erase | ( | flash_config_t * | config, |
| uint32_t | start, | ||
| uint32_t | lengthInBytes, | ||
| uint32_t | key | ||
| ) |
This function erases the appropriate number of flash sectors based on the desired start address and length.
| config | The pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be erased. The start address need to be 512bytes-aligned. |
| lengthInBytes | The length, given in bytes (not words or long-words) to be erased. Must be 512bytes-aligned. |
| key | The value used to validate all flash erase APIs. |
| kStatus_FLASH_Success | API was executed successfully. |
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. |
| kStatus_FLASH_AlignmentError | The parameter is not aligned with the specified baseline. |
| kStatus_FLASH_AddressError | The address is out of range. |
| kStatus_FLASH_EraseKeyError | The API erase key is invalid. |
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. |
| kStatus_FLASH_CommandNotSupported | Flash API is not supported. |
| kStatus_FLASH_EccError | A correctable or uncorrectable error during command execution. |
| status_t FLASH_Program | ( | flash_config_t * | config, |
| uint32_t | start, | ||
| uint8_t * | src, | ||
| uint32_t | lengthInBytes | ||
| ) |
This function programs the flash memory with the desired data for a given flash area as determined by the start address and the length.
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be programmed. Must be 512bytes-aligned. |
| src | A pointer to the source buffer of data that is to be programmed into the flash. |
| lengthInBytes | The length, given in bytes (not words or long-words), to be programmed. Must be 512bytes-aligned. |
| kStatus_FLASH_Success | API was executed successfully. |
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. |
| kStatus_FLASH_AlignmentError | Parameter is not aligned with the specified baseline. |
| kStatus_FLASH_AddressError | Address is out of range. |
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. |
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. |
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. |
| kStatus_FLASH_CommandNotSupported | Flash API is not supported. |
| kStatus_FLASH_EccError | A correctable or uncorrectable error during command execution. |
| status_t FLASH_VerifyErase | ( | flash_config_t * | config, |
| uint32_t | start, | ||
| uint32_t | lengthInBytes | ||
| ) |
This function checks the appropriate number of flash sectors based on the desired start address and length to check whether the flash is erased to the specified read margin level.
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be verified. The start address need to be 512bytes-aligned. |
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be 512bytes-aligned. |
| margin | Read margin choice. |
| kStatus_FLASH_Success | API was executed successfully. |
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. |
| kStatus_FLASH_AlignmentError | Parameter is not aligned with specified baseline. |
| kStatus_FLASH_AddressError | Address is out of range. |
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. |
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. |
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. |
| kStatus_FLASH_CommandNotSupported | Flash API is not supported. |
| kStatus_FLASH_EccError | A correctable or uncorrectable error during command execution. |
| status_t FLASH_VerifyProgram | ( | flash_config_t * | config, |
| uint32_t | start, | ||
| uint32_t | lengthInBytes, | ||
| const uint8_t * | expectedData, | ||
| uint32_t * | failedAddress, | ||
| uint32_t * | failedData | ||
| ) |
This function verifies the data programed in the flash memory using the Flash Program Check Command and compares it to the expected data for a given flash area as determined by the start address and length.
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be verified. need be 512bytes-aligned. |
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. need be 512bytes-aligned. |
| expectedData | A pointer to the expected data that is to be verified against. |
| margin | Read margin choice. |
| failedAddress | A pointer to the returned failing address. |
| failedData | A pointer to the returned failing data. Some derivatives do not include failed data as part of the FCCOBx registers. In this case, zeros are returned upon failure. |
| kStatus_FLASH_Success | API was executed successfully. |
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. |
| kStatus_FLASH_AlignmentError | Parameter is not aligned with specified baseline. |
| kStatus_FLASH_AddressError | Address is out of range. |
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. |
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. |
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. |
| kStatus_FLASH_CommandNotSupported | Flash API is not supported. |
| kStatus_FLASH_EccError | A correctable or uncorrectable error during command execution. |
| status_t FLASH_GetProperty | ( | flash_config_t * | config, |
| flash_property_tag_t | whichProperty, | ||
| uint32_t * | value | ||
| ) |
| config | A pointer to the storage for the driver runtime state. |
| whichProperty | The desired property from the list of properties in enum flash_property_tag_t |
| value | A pointer to the value returned for the desired flash property. |
| kStatus_FLASH_Success | API was executed successfully. |
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. |
| kStatus_FLASH_UnknownProperty | An unknown property tag. |
| uint32_t flash_config_t::PFlashTotalSize |
| uint32_t flash_config_t::PFlashBlockCount |
| uint32_t flash_config_t::PFlashPageSize |
| uint32_t flash_config_t::PFlashSectorSize |