MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
IRQ: external interrupt (IRQ) module

Overview

The MCUXpresso SDK provides a peripheral driver for the external interrupt (IRQ) module of MCUXpresso SDK devices.

The IRQ Initialize is to initialize for common configure: gate the IRQ clock, configure enabled IRQ pins for pullup, edge select and detect mode, then enable the IRQ module. The IRQ Deinitialize is used to ungate the clock.

The IRQ provides the function to enable/disable interrupts. IRQ still provides functions to get and clear IRQF flags.

Typical use case

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/irq

Files

file  fsl_irq.h
 

Data Structures

struct  irq_config_t
 The IRQ pin configuration structure. More...
 

Enumerations

enum  irq_edge_t {
  kIRQ_FallingEdgeorLowlevel = 0U,
  kIRQ_RisingEdgeorHighlevel = 1U
}
 Interrupt Request (IRQ) Edge Select. More...
 
enum  irq_mode_t {
  kIRQ_DetectOnEdgesOnly = 0U,
  kIRQ_DetectOnEdgesAndEdges = 1U
}
 Interrupt Request (IRQ) Detection Mode. More...
 

Driver version

#define FSL_IRQ_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))
 Version 2.0.2. More...
 

IRQ Configuration

uint32_t IRQ_GetInstance (IRQ_Type *base)
 Get irq instance. More...
 
void IRQ_Init (IRQ_Type *base, const irq_config_t *config)
 Initializes the IRQ pin used by the board. More...
 
void IRQ_Deinit (IRQ_Type *base)
 Deinitialize IRQ peripheral. More...
 
static void IRQ_Enable (IRQ_Type *base, bool enable)
 Enable/disable IRQ pin. More...
 

IRQ interrupt Operations

static void IRQ_EnableInterrupt (IRQ_Type *base, bool enable)
 Enable/disable IRQ pin interrupt. More...
 
static void IRQ_ClearIRQFlag (IRQ_Type *base)
 Clear IRQF flag. More...
 
static uint32_t IRQ_GetIRQFlag (IRQ_Type *base)
 Get IRQF flag. More...
 

Data Structure Documentation

struct irq_config_t

Data Fields

bool enablePullDevice
 Enable/disable the internal pullup device when the IRQ pin is enabled.
 
irq_edge_t edgeSelect
 Select the polarity of edges or levels on the IRQ pin that cause IRQF to be set.
 
irq_mode_t detectMode
 select either edge-only detection or edge-and-level detection
 

Macro Definition Documentation

#define FSL_IRQ_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))

Enumeration Type Documentation

enum irq_edge_t
Enumerator
kIRQ_FallingEdgeorLowlevel 

IRQ is falling-edge or falling-edge/low-level sensitive.

kIRQ_RisingEdgeorHighlevel 

IRQ is rising-edge or rising-edge/high-level sensitive.

enum irq_mode_t
Enumerator
kIRQ_DetectOnEdgesOnly 

IRQ event is detected only on falling/rising edges.

kIRQ_DetectOnEdgesAndEdges 

IRQ event is detected on falling/rising edges and low/high levels.

Function Documentation

uint32_t IRQ_GetInstance ( IRQ_Type *  base)
Parameters
baseIRQ peripheral base pointer
Return values
Irqinstance number.
void IRQ_Init ( IRQ_Type *  base,
const irq_config_t *  config 
)

To initialize the IRQ pin, define a irq configuration, specify whhether enable pull-up, the edge and detect mode. Then, call the IRQ_Init() function.

This is an example to initialize irq configuration.

Parameters
baseIRQ peripheral base pointer
configIRQ configuration pointer
void IRQ_Deinit ( IRQ_Type *  base)

This function disables the IRQ clock.

Parameters
baseIRQ peripheral base pointer.
Return values
None.
static void IRQ_Enable ( IRQ_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseIRQ peripheral base pointer.
enabletrue to enable IRQ pin, else disable IRQ pin.
Return values
None.
static void IRQ_EnableInterrupt ( IRQ_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseIRQ peripheral base pointer.
enabletrue to enable IRQF assert interrupt request, else disable.
Return values
None.
static void IRQ_ClearIRQFlag ( IRQ_Type *  base)
inlinestatic

This function clears the IRQF flag.

Parameters
baseIRQ peripheral base pointer.
Return values
None.
static uint32_t IRQ_GetIRQFlag ( IRQ_Type *  base)
inlinestatic

This function returns the IRQF flag.

Parameters
baseIRQ peripheral base pointer.
Return values
status= 0 IRQF flag deasserted. = 1 IRQF flag asserted.