![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Files | |
| file | fsl_gpio.h |
Data Structures | |
| struct | gpio_pin_config_t |
| The GPIO pin configuration structure. More... | |
Enumerations | |
| enum | gpio_pin_direction_t { kGPIO_DigitalInput = 0U, kGPIO_DigitalOutput = 1U } |
| LPC GPIO direction definition. More... | |
| enum | gpio_interrupt_mode_t { kGPIO_IntDisabled = 0U, kGPIO_IntLowLevel = 1U, kGPIO_IntHighLevel = 2U, kGPIO_IntRisingEdge = 3U, kGPIO_IntFallingEdge = 4U, kGPIO_IntRisingOrFallingEdge = 5U } |
| GPIO interrupt mode definition. More... | |
Functions | |
| void | GPIO_PinInit (GPIO_Type *base, uint32_t pin, const gpio_pin_config_t *Config) |
| Initializes a GPIO pin used by the board. More... | |
| void | GPIO_PortInit (GPIO_Type *base, uint32_t port) |
| Initializes the GPIO peripheral. More... | |
| void | GPIO_PinSetInterruptConfig (GPIO_Type *base, uint32_t pin, gpio_interrupt_mode_t pinInterruptMode) |
| Initializes the GPIO peripheral. More... | |
Driver version | |
| #define | FSL_GPIO_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
| LPC GPIO driver version 2.0.0. More... | |
| struct gpio_pin_config_t |
Every pin can only be configured as either output pin or input pin at a time. If configured as a input pin, then leave the outputConfig unused.
Data Fields | |
| gpio_pin_direction_t | direction |
| Specifies the pin direction. More... | |
| uint8_t | outputLogic |
| Set a default output logic, which has no use in input. | |
| gpio_pin_direction_t gpio_pin_config_t::direction |
| #define FSL_GPIO_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
| enum gpio_pin_direction_t |
| void GPIO_PinInit | ( | GPIO_Type * | base, |
| uint32_t | pin, | ||
| const gpio_pin_config_t * | Config | ||
| ) |
To initialize the GPIO, define a pin configuration, either input or output, in the user file. Then, call the GPIO_PinInit() function.
This is an example to define an input pin or output pin configuration:
| base | GPIO peripheral base pointer(Typically GPIO) |
| pin | GPIO pin number |
| config | GPIO pin configuration pointer |
| void GPIO_PortInit | ( | GPIO_Type * | base, |
| uint32_t | port | ||
| ) |
This function ungates the GPIO clock.
| base | GPIO peripheral base pointer. |
| port | GPIO port number. |
| void GPIO_PinSetInterruptConfig | ( | GPIO_Type * | base, |
| uint32_t | pin, | ||
| gpio_interrupt_mode_t | pinInterruptMode | ||
| ) |
This function ungates the GPIO clock.
| base | GPIO peripheral base pointer. |
| pin | GPIO pin number |
| pinInterruptMode | GPIO interrupt mode |