![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the Reset Control Module (RCM) module of MCUXpresso SDK devices.
Data Structures | |
| struct | rcm_reset_pin_filter_config_t |
| Reset pin filter configuration. More... | |
Enumerations | |
| enum | rcm_reset_source_t { kRCM_SourceWakeup = RCM_SRS0_WAKEUP_MASK, kRCM_SourceLvd = RCM_SRS0_LVD_MASK, kRCM_SourceWdog = RCM_SRS0_WDOG_MASK, kRCM_SourcePin = RCM_SRS0_PIN_MASK, kRCM_SourcePor = RCM_SRS0_POR_MASK, kRCM_SourceLockup = RCM_SRS1_LOCKUP_MASK << 8U, kRCM_SourceSw = RCM_SRS1_SW_MASK << 8U, kRCM_SourceMdmap = RCM_SRS1_MDM_AP_MASK << 8U, kRCM_SourceSackerr = RCM_SRS1_SACKERR_MASK << 8U } |
| System Reset Source Name definitions. More... | |
| enum | rcm_run_wait_filter_mode_t { kRCM_FilterDisable = 0U, kRCM_FilterBusClock = 1U, kRCM_FilterLpoClock = 2U } |
| Reset pin filter select in Run and Wait modes. More... | |
| enum | rcm_boot_rom_config_t { kRCM_BootFlash = 0U, kRCM_BootRomCfg0 = 1U, kRCM_BootRomFopt = 2U, kRCM_BootRomBoth = 3U } |
| Boot from ROM configuration. More... | |
Driver version | |
| #define | FSL_RCM_DRIVER_VERSION (MAKE_VERSION(2, 0, 3)) |
| RCM driver version 2.0.3. More... | |
Reset Control Module APIs | |
| static uint32_t | RCM_GetPreviousResetSources (RCM_Type *base) |
| Gets the reset source status which caused a previous reset. More... | |
| static uint32_t | RCM_GetStickyResetSources (RCM_Type *base) |
| Gets the sticky reset source status. More... | |
| static void | RCM_ClearStickyResetSources (RCM_Type *base, uint32_t sourceMasks) |
| Clears the sticky reset source status. More... | |
| void | RCM_ConfigureResetPinFilter (RCM_Type *base, const rcm_reset_pin_filter_config_t *config) |
| Configures the reset pin filter. More... | |
| static rcm_boot_rom_config_t | RCM_GetBootRomSource (RCM_Type *base) |
| Gets the ROM boot source. More... | |
| static void | RCM_ClearBootRomSource (RCM_Type *base) |
| Clears the ROM boot source flag. More... | |
| void | RCM_SetForceBootRomSource (RCM_Type *base, rcm_boot_rom_config_t config) |
| Forces the boot from ROM. More... | |
| struct rcm_reset_pin_filter_config_t |
Data Fields | |
| bool | enableFilterInStop |
| Reset pin filter select in stop mode. More... | |
| rcm_run_wait_filter_mode_t | filterInRunWait |
| Reset pin filter in run/wait mode. More... | |
| uint8_t | busClockFilterCount |
| Reset pin bus clock filter width. More... | |
| bool rcm_reset_pin_filter_config_t::enableFilterInStop |
| rcm_run_wait_filter_mode_t rcm_reset_pin_filter_config_t::filterInRunWait |
| uint8_t rcm_reset_pin_filter_config_t::busClockFilterCount |
| #define FSL_RCM_DRIVER_VERSION (MAKE_VERSION(2, 0, 3)) |
| enum rcm_reset_source_t |
|
inlinestatic |
This function gets the current reset source status. Use source masks defined in the rcm_reset_source_t to get the desired source status.
This is an example.
| base | RCM peripheral base address. |
|
inlinestatic |
This function gets the current reset source status that has not been cleared by software for a specific source.
This is an example.
| base | RCM peripheral base address. |
|
inlinestatic |
This function clears the sticky system reset flags indicated by source masks.
This is an example.
| base | RCM peripheral base address. |
| sourceMasks | reset source status bit map |
| void RCM_ConfigureResetPinFilter | ( | RCM_Type * | base, |
| const rcm_reset_pin_filter_config_t * | config | ||
| ) |
This function sets the reset pin filter including the filter source, filter width, and so on.
| base | RCM peripheral base address. |
| config | Pointer to the configuration structure. |
|
inlinestatic |
This function gets the ROM boot source during the last chip reset.
| base | RCM peripheral base address. |
|
inlinestatic |
This function clears the ROM boot source flag.
| base | Register base address of RCM |
| void RCM_SetForceBootRomSource | ( | RCM_Type * | base, |
| rcm_boot_rom_config_t | config | ||
| ) |
This function forces booting from ROM during all subsequent system resets.
| base | RCM peripheral base address. |
| config | Boot configuration. |