![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the System Integration Module (SIM) of MCUXpresso SDK devices.
Data Structures | |
| struct | sim_uid_t |
| Unique ID. More... | |
Enumerations | |
| enum | _sim_flash_mode { kSIM_FlashDisableInWait = SIM_FCFG1_FLASHDOZE_MASK, kSIM_FlashDisable = SIM_FCFG1_FLASHDIS_MASK } |
| Flash enable mode. More... | |
Functions | |
| void | SIM_GetUniqueId (sim_uid_t *uid) |
| Gets the unique identification register value. More... | |
| static void | SIM_SetFlashMode (uint8_t mode) |
| Sets the flash enable mode. More... | |
Driver version | |
| #define | FSL_SIM_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
| struct sim_uid_t |
| enum _sim_flash_mode |
| void SIM_GetUniqueId | ( | sim_uid_t * | uid | ) |
| uid | Pointer to the structure to save the UID value. |
|
inlinestatic |
| mode | The mode to set; see _sim_flash_mode for mode details. |