![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | flexio_camera_edma_handle_t | 
| Camera eDMA handle.  More... | |
Typedefs | |
| typedef void(* | flexio_camera_edma_transfer_callback_t )(FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, status_t status, void *userData) | 
| Camera transfer callback function.  More... | |
Driver version | |
| #define | FSL_FLEXIO_CAMERA_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 2)) | 
| FlexIO Camera EDMA driver version 2.1.2.  More... | |
eDMA transactional | |
| status_t | FLEXIO_CAMERA_TransferCreateHandleEDMA (FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, flexio_camera_edma_transfer_callback_t callback, void *userData, edma_handle_t *rxEdmaHandle) | 
| Initializes the Camera handle, which is used in transactional functions.  More... | |
| status_t | FLEXIO_CAMERA_TransferReceiveEDMA (FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, flexio_camera_transfer_t *xfer) | 
| Receives data using eDMA.  More... | |
| void | FLEXIO_CAMERA_TransferAbortReceiveEDMA (FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle) | 
| Aborts the receive data which used the eDMA.  More... | |
| status_t | FLEXIO_CAMERA_TransferGetReceiveCountEDMA (FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, size_t *count) | 
| Gets the remaining bytes to be received.  More... | |
| struct _flexio_camera_edma_handle | 
Forward declaration of the handle typedef.
Data Fields | |
| flexio_camera_edma_transfer_callback_t | callback | 
| Callback function.  More... | |
| void * | userData | 
| Camera callback function parameter.  More... | |
| size_t | rxSize | 
| Total bytes to be received.  More... | |
| edma_handle_t * | rxEdmaHandle | 
| The eDMA RX channel used.  More... | |
| uint8_t | nbytes | 
| eDMA minor byte transfer count initially configured.  More... | |
| volatile uint8_t | rxState | 
| RX transfer state.  | |
| flexio_camera_edma_transfer_callback_t flexio_camera_edma_handle_t::callback | 
| void* flexio_camera_edma_handle_t::userData | 
| size_t flexio_camera_edma_handle_t::rxSize | 
| edma_handle_t* flexio_camera_edma_handle_t::rxEdmaHandle | 
| uint8_t flexio_camera_edma_handle_t::nbytes | 
| #define FSL_FLEXIO_CAMERA_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 2)) | 
| typedef void(* flexio_camera_edma_transfer_callback_t)(FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, status_t status, void *userData) | 
| status_t FLEXIO_CAMERA_TransferCreateHandleEDMA | ( | FLEXIO_CAMERA_Type * | base, | 
| flexio_camera_edma_handle_t * | handle, | ||
| flexio_camera_edma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | rxEdmaHandle | ||
| ) | 
| base | Pointer to the FLEXIO_CAMERA_Type. | 
| handle | Pointer to flexio_camera_edma_handle_t structure. | 
| callback | The callback function. | 
| userData | The parameter of the callback function. | 
| rxEdmaHandle | User requested DMA handle for RX DMA transfer. | 
| kStatus_Success | Successfully create the handle. | 
| kStatus_OutOfRange | The FlexIO Camera eDMA type/handle table out of range. | 
| status_t FLEXIO_CAMERA_TransferReceiveEDMA | ( | FLEXIO_CAMERA_Type * | base, | 
| flexio_camera_edma_handle_t * | handle, | ||
| flexio_camera_transfer_t * | xfer | ||
| ) | 
This function receives data using eDMA. This is a non-blocking function, which returns right away. When all data is received, the receive callback function is called.
| base | Pointer to the FLEXIO_CAMERA_Type. | 
| handle | Pointer to the flexio_camera_edma_handle_t structure. | 
| xfer | Camera eDMA transfer structure, see flexio_camera_transfer_t. | 
| kStatus_Success | if succeeded, others failed. | 
| kStatus_CAMERA_RxBusy | Previous transfer on going. | 
| void FLEXIO_CAMERA_TransferAbortReceiveEDMA | ( | FLEXIO_CAMERA_Type * | base, | 
| flexio_camera_edma_handle_t * | handle | ||
| ) | 
This function aborts the receive data which used the eDMA.
| base | Pointer to the FLEXIO_CAMERA_Type. | 
| handle | Pointer to the flexio_camera_edma_handle_t structure. | 
| status_t FLEXIO_CAMERA_TransferGetReceiveCountEDMA | ( | FLEXIO_CAMERA_Type * | base, | 
| flexio_camera_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
This function gets the number of bytes still not received.
| base | Pointer to the FLEXIO_CAMERA_Type. | 
| handle | Pointer to the flexio_camera_edma_handle_t structure. | 
| count | Number of bytes sent so far by the non-blocking transaction. | 
| kStatus_Success | Succeed get the transfer count. | 
| kStatus_InvalidArgument | The count parameter is invalid. |