![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | flexio_mculcd_dma_handle_t | 
| FlexIO MCULCD DMA transfer handle, users should not touch the content of the handle.  More... | |
Macros | |
| #define | FSL_FLEXIO_MCULCD_DMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) | 
| FlexIO MCULCD DMA driver version 2.0.0.  More... | |
Typedefs | |
| typedef void(* | flexio_mculcd_dma_transfer_callback_t )(FLEXIO_MCULCD_Type *base, flexio_mculcd_dma_handle_t *handle, status_t status, void *userData) | 
| FlexIO MCULCD master callback for transfer complete.  More... | |
DMA Transactional | |
| status_t | FLEXIO_MCULCD_TransferCreateHandleDMA (FLEXIO_MCULCD_Type *base, flexio_mculcd_dma_handle_t *handle, flexio_mculcd_dma_transfer_callback_t callback, void *userData, dma_handle_t *txDmaHandle, dma_handle_t *rxDmaHandle) | 
| Initializes the FLEXO MCULCD master DMA handle.  More... | |
| status_t | FLEXIO_MCULCD_TransferDMA (FLEXIO_MCULCD_Type *base, flexio_mculcd_dma_handle_t *handle, flexio_mculcd_transfer_t *xfer) | 
| Performs a non-blocking FlexIO MCULCD transfer using DMA.  More... | |
| void | FLEXIO_MCULCD_TransferAbortDMA (FLEXIO_MCULCD_Type *base, flexio_mculcd_dma_handle_t *handle) | 
| Aborts a FlexIO MCULCD transfer using DMA.  More... | |
| status_t | FLEXIO_MCULCD_TransferGetCountDMA (FLEXIO_MCULCD_Type *base, flexio_mculcd_dma_handle_t *handle, size_t *count) | 
| Gets the remaining bytes for FlexIO MCULCD DMA transfer.  More... | |
| struct _flexio_mculcd_dma_handle | 
typedef for flexio_mculcd_dma_handle_t in advance.
Data Fields | |
| FLEXIO_MCULCD_Type * | base | 
| Pointer to the FLEXIO_MCULCD_Type.  More... | |
| uint8_t | txShifterNum | 
| Number of shifters used for TX.  More... | |
| uint8_t | rxShifterNum | 
| Number of shifters used for RX.  More... | |
| dma_trigger_burst_t | txTriggerBurst | 
| Trigger burst setting for TX.  More... | |
| dma_trigger_burst_t | rxTriggerBurst | 
| Trigger burst setting for RX.  More... | |
| uint32_t | burstBytes | 
| DMA transfer bytes per burst.  More... | |
| uint32_t | dataAddrOrSameValue | 
| When sending the same value for many times, this is the value to send.  More... | |
| size_t | dataCount | 
| Total count to be transferred.  More... | |
| volatile size_t | remainingCount | 
| Remaining count still not transfered.  More... | |
| volatile uint32_t | state | 
| FlexIO MCULCD driver internal state.  More... | |
| dma_handle_t * | txDmaHandle | 
| DMA handle for MCULCD TX.  | |
| dma_handle_t * | rxDmaHandle | 
| DMA handle for MCULCD RX.  | |
| flexio_mculcd_dma_transfer_callback_t | completionCallback | 
| Callback for MCULCD DMA transfer.  | |
| void * | userData | 
| User Data for MCULCD DMA callback.  | |
| FLEXIO_MCULCD_Type* flexio_mculcd_dma_handle_t::base | 
| uint8_t flexio_mculcd_dma_handle_t::txShifterNum | 
| uint8_t flexio_mculcd_dma_handle_t::rxShifterNum | 
| dma_trigger_burst_t flexio_mculcd_dma_handle_t::txTriggerBurst | 
| dma_trigger_burst_t flexio_mculcd_dma_handle_t::rxTriggerBurst | 
| uint32_t flexio_mculcd_dma_handle_t::burstBytes | 
| uint32_t flexio_mculcd_dma_handle_t::dataAddrOrSameValue | 
When writing or reading array, this is the address of the data array.
| size_t flexio_mculcd_dma_handle_t::dataCount | 
| volatile size_t flexio_mculcd_dma_handle_t::remainingCount | 
| volatile uint32_t flexio_mculcd_dma_handle_t::state | 
| #define FSL_FLEXIO_MCULCD_DMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) | 
| typedef void(* flexio_mculcd_dma_transfer_callback_t)(FLEXIO_MCULCD_Type *base, flexio_mculcd_dma_handle_t *handle, status_t status, void *userData) | 
When transfer finished, the callback function is called and returns the status as kStatus_FLEXIO_MCULCD_Idle. 
| status_t FLEXIO_MCULCD_TransferCreateHandleDMA | ( | FLEXIO_MCULCD_Type * | base, | 
| flexio_mculcd_dma_handle_t * | handle, | ||
| flexio_mculcd_dma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | txDmaHandle, | ||
| dma_handle_t * | rxDmaHandle | ||
| ) | 
This function initializes the FLEXO MCULCD master DMA handle which can be used for other FLEXO MCULCD transactional APIs. For a specified FLEXO MCULCD instance, call this API once to get the initialized handle.
| base | Pointer to FLEXIO_MCULCD_Type structure. | 
| handle | Pointer to flexio_mculcd_dma_handle_t structure to store the transfer state. | 
| callback | MCULCD transfer complete callback, NULL means no callback. | 
| userData | callback function parameter. | 
| txDmaHandle | User requested DMA handle for FlexIO MCULCD DMA TX, the DMA request source of this handle should be the first of TX shifters. | 
| rxDmaHandle | User requested DMA handle for FlexIO MCULCD DMA RX, the DMA request source of this handle should be the last of RX shifters. | 
| kStatus_Success | Successfully create the handle. | 
| status_t FLEXIO_MCULCD_TransferDMA | ( | FLEXIO_MCULCD_Type * | base, | 
| flexio_mculcd_dma_handle_t * | handle, | ||
| flexio_mculcd_transfer_t * | xfer | ||
| ) | 
This function returns immediately after transfer initiates. To check whether the transfer is completed, user could:
| base | pointer to FLEXIO_MCULCD_Type structure. | 
| handle | pointer to flexio_mculcd_dma_handle_t structure to store the transfer state. | 
| xfer | Pointer to FlexIO MCULCD transfer structure. | 
| kStatus_Success | Successfully start a transfer. | 
| kStatus_InvalidArgument | Input argument is invalid. | 
| kStatus_FLEXIO_MCULCD_Busy | FlexIO MCULCD is not idle, it is running another transfer. | 
| void FLEXIO_MCULCD_TransferAbortDMA | ( | FLEXIO_MCULCD_Type * | base, | 
| flexio_mculcd_dma_handle_t * | handle | ||
| ) | 
| base | pointer to FLEXIO_MCULCD_Type structure. | 
| handle | FlexIO MCULCD DMA handle pointer. | 
| status_t FLEXIO_MCULCD_TransferGetCountDMA | ( | FLEXIO_MCULCD_Type * | base, | 
| flexio_mculcd_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | pointer to FLEXIO_MCULCD_Type structure. | 
| handle | FlexIO MCULCD DMA handle pointer. | 
| count | Number of count transferred so far by the DMA transaction. | 
| kStatus_Success | Get the transferred count Successfully. | 
| kStatus_NoTransferInProgress | No transfer in process. |