![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | flexio_mculcd_smartdma_handle_t | 
| FlexIO MCULCD SMARTDMA transfer handle, users should not touch the content of the handle.  More... | |
| struct | flexio_mculcd_smartdma_config_t | 
| FlexIO MCULCD SMARTDMA configuration.  More... | |
Macros | |
| #define | FSL_FLEXIO_MCULCD_SMARTDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) | 
| FlexIO MCULCD SMARTDMA driver version.  More... | |
| #define | FLEXIO_MCULCD_SMARTDMA_TX_LEN_ALIGN 64U | 
| SMARTDMA transfer size should be multiple of 64 bytes.  More... | |
| #define | FLEXIO_MCULCD_SMARTDMA_TX_ADDR_ALIGN 4U | 
| SMARTDMA transfer memory address should be 4 byte aligned.  More... | |
Typedefs | |
| typedef void(* | flexio_mculcd_smartdma_transfer_callback_t )(FLEXIO_MCULCD_Type *base, flexio_mculcd_smartdma_handle_t *handle, status_t status, void *userData) | 
| FlexIO MCULCD master callback for transfer complete.  More... | |
SMARTDMA Transactional | |
| status_t | FLEXIO_MCULCD_TransferCreateHandleSMARTDMA (FLEXIO_MCULCD_Type *base, flexio_mculcd_smartdma_handle_t *handle, const flexio_mculcd_smartdma_config_t *config, flexio_mculcd_smartdma_transfer_callback_t callback, void *userData) | 
| Initializes the FLEXO MCULCD master SMARTDMA handle.  More... | |
| status_t | FLEXIO_MCULCD_TransferSMARTDMA (FLEXIO_MCULCD_Type *base, flexio_mculcd_smartdma_handle_t *handle, flexio_mculcd_transfer_t *xfer) | 
| Performs a non-blocking FlexIO MCULCD transfer using SMARTDMA.  More... | |
| void | FLEXIO_MCULCD_TransferAbortSMARTDMA (FLEXIO_MCULCD_Type *base, flexio_mculcd_smartdma_handle_t *handle) | 
| Aborts a FlexIO MCULCD transfer using SMARTDMA.  More... | |
| status_t | FLEXIO_MCULCD_TransferGetCountSMARTDMA (FLEXIO_MCULCD_Type *base, flexio_mculcd_smartdma_handle_t *handle, size_t *count) | 
| Gets the remaining bytes for FlexIO MCULCD SMARTDMA transfer.  More... | |
| struct _flexio_mculcd_smartdma_handle | 
typedef for flexio_mculcd_smartdma_handle_t in advance.
Data Fields | |
| FLEXIO_MCULCD_Type * | base | 
| Pointer to the FLEXIO_MCULCD_Type.  More... | |
| size_t | dataCount | 
| Total count to be transferred.  More... | |
| uint32_t | dataAddrOrSameValue | 
| When sending the same value for many times, this is the value to send.  More... | |
| size_t | dataCountUsingEzh | 
| Data transfered using SMARTDMA.  More... | |
| volatile size_t | remainingCount | 
| Remaining count to transfer.  More... | |
| volatile uint32_t | state | 
| FlexIO MCULCD driver internal state.  More... | |
| uint8_t | smartdmaApi | 
| The SMARTDMA API used during transfer.  More... | |
| bool | needColorConvert | 
| Need color convert or not.  More... | |
| uint8_t | blockingXferBuffer [FLEXIO_MCULCD_SMARTDMA_TX_LEN_ALIGN *3/2] | 
| Used for blocking method color space convet.  More... | |
| flexio_mculcd_smartdma_transfer_callback_t | completionCallback | 
| Callback for MCULCD SMARTDMA transfer.  | |
| void * | userData | 
| User Data for MCULCD SMARTDMA callback.  | |
| smartdma_flexio_mculcd_param_t | smartdmaParam | 
| SMARTDMA function parameters.  More... | |
| uint32_t | smartdmaStack [1] | 
| SMARTDMA function stack.  More... | |
| FLEXIO_MCULCD_Type* flexio_mculcd_smartdma_handle_t::base | 
| size_t flexio_mculcd_smartdma_handle_t::dataCount | 
| uint32_t flexio_mculcd_smartdma_handle_t::dataAddrOrSameValue | 
When writing or reading array, this is the address of the data array.
| size_t flexio_mculcd_smartdma_handle_t::dataCountUsingEzh | 
| volatile size_t flexio_mculcd_smartdma_handle_t::remainingCount | 
| volatile uint32_t flexio_mculcd_smartdma_handle_t::state | 
| uint8_t flexio_mculcd_smartdma_handle_t::smartdmaApi | 
| bool flexio_mculcd_smartdma_handle_t::needColorConvert | 
| uint8_t flexio_mculcd_smartdma_handle_t::blockingXferBuffer[FLEXIO_MCULCD_SMARTDMA_TX_LEN_ALIGN *3/2] | 
| smartdma_flexio_mculcd_param_t flexio_mculcd_smartdma_handle_t::smartdmaParam | 
| uint32_t flexio_mculcd_smartdma_handle_t::smartdmaStack[1] | 
| struct flexio_mculcd_smartdma_config_t | 
Data Fields | |
| flexio_mculcd_pixel_format_t | inputPixelFormat | 
| The pixel format in the frame buffer.  More... | |
| flexio_mculcd_pixel_format_t | outputPixelFormat | 
| The pixel format on the 8080/68k bus.  More... | |
| flexio_mculcd_pixel_format_t flexio_mculcd_smartdma_config_t::inputPixelFormat | 
| flexio_mculcd_pixel_format_t flexio_mculcd_smartdma_config_t::outputPixelFormat | 
| #define FSL_FLEXIO_MCULCD_SMARTDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) | 
| #define FLEXIO_MCULCD_SMARTDMA_TX_LEN_ALIGN 64U | 
| #define FLEXIO_MCULCD_SMARTDMA_TX_ADDR_ALIGN 4U | 
| typedef void(* flexio_mculcd_smartdma_transfer_callback_t)(FLEXIO_MCULCD_Type *base, flexio_mculcd_smartdma_handle_t *handle, status_t status, void *userData) | 
When transfer finished, the callback function is called and returns the status as kStatus_FLEXIO_MCULCD_Idle. 
| status_t FLEXIO_MCULCD_TransferCreateHandleSMARTDMA | ( | FLEXIO_MCULCD_Type * | base, | 
| flexio_mculcd_smartdma_handle_t * | handle, | ||
| const flexio_mculcd_smartdma_config_t * | config, | ||
| flexio_mculcd_smartdma_transfer_callback_t | callback, | ||
| void * | userData | ||
| ) | 
This function initializes the FLEXO MCULCD master SMARTDMA handle which can be used for other FLEXO MCULCD transactional APIs. For a specified FLEXO MCULCD instance, call this API once to get the initialized handle.
| base | Pointer to FLEXIO_MCULCD_Type structure. | 
| handle | Pointer to flexio_mculcd_smartdma_handle_t structure to store the transfer state. | 
| config | Pointer to the configuration. | 
| callback | MCULCD transfer complete callback, NULL means no callback. | 
| userData | callback function parameter. | 
| kStatus_Success | Successfully create the handle. | 
| status_t FLEXIO_MCULCD_TransferSMARTDMA | ( | FLEXIO_MCULCD_Type * | base, | 
| flexio_mculcd_smartdma_handle_t * | handle, | ||
| flexio_mculcd_transfer_t * | xfer | ||
| ) | 
This function returns immediately after transfer initiates. Use the callback function to check whether the transfer is completed.
| base | pointer to FLEXIO_MCULCD_Type structure. | 
| handle | pointer to flexio_mculcd_smartdma_handle_t structure to store the transfer state. | 
| xfer | Pointer to FlexIO MCULCD transfer structure. | 
| kStatus_Success | Successfully start a transfer. | 
| kStatus_InvalidArgument | Input argument is invalid. | 
| kStatus_FLEXIO_MCULCD_Busy | FlexIO MCULCD is not idle, it is running another transfer. | 
| void FLEXIO_MCULCD_TransferAbortSMARTDMA | ( | FLEXIO_MCULCD_Type * | base, | 
| flexio_mculcd_smartdma_handle_t * | handle | ||
| ) | 
| base | pointer to FLEXIO_MCULCD_Type structure. | 
| handle | FlexIO MCULCD SMARTDMA handle pointer. | 
| status_t FLEXIO_MCULCD_TransferGetCountSMARTDMA | ( | FLEXIO_MCULCD_Type * | base, | 
| flexio_mculcd_smartdma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | pointer to FLEXIO_MCULCD_Type structure. | 
| handle | FlexIO MCULCD SMARTDMA handle pointer. | 
| count | Number of count transferred so far by the SMARTDMA transaction. | 
| kStatus_Success | Get the transferred count Successfully. | 
| kStatus_NoTransferInProgress | No transfer in process. |