![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | flexio_uart_dma_handle_t | 
| UART DMA handle.  More... | |
Typedefs | |
| typedef void(* | flexio_uart_dma_transfer_callback_t )(FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, status_t status, void *userData) | 
| UART transfer callback function.  More... | |
Driver version | |
| #define | FSL_FLEXIO_UART_DMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 6)) | 
| FlexIO UART DMA driver version 2.1.6.  More... | |
eDMA transactional | |
| status_t | FLEXIO_UART_TransferCreateHandleDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, flexio_uart_dma_transfer_callback_t callback, void *userData, dma_handle_t *txDmaHandle, dma_handle_t *rxDmaHandle) | 
| Initializes the FLEXIO_UART handle which is used in transactional functions.  More... | |
| status_t | FLEXIO_UART_TransferSendDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, flexio_uart_transfer_t *xfer) | 
| Sends data using DMA.  More... | |
| status_t | FLEXIO_UART_TransferReceiveDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, flexio_uart_transfer_t *xfer) | 
| Receives data using DMA.  More... | |
| void | FLEXIO_UART_TransferAbortSendDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle) | 
| Aborts the sent data which using DMA.  More... | |
| void | FLEXIO_UART_TransferAbortReceiveDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle) | 
| Aborts the receive data which using DMA.  More... | |
| status_t | FLEXIO_UART_TransferGetSendCountDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, size_t *count) | 
| Gets the number of bytes sent out.  More... | |
| status_t | FLEXIO_UART_TransferGetReceiveCountDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, size_t *count) | 
| Gets the number of bytes received.  More... | |
| struct _flexio_uart_dma_handle | 
Data Fields | |
| flexio_uart_dma_transfer_callback_t | callback | 
| Callback function.  More... | |
| void * | userData | 
| UART callback function parameter.  More... | |
| size_t | txDataSizeAll | 
| Total bytes to be sent.  More... | |
| size_t | rxDataSizeAll | 
| Total bytes to be received.  More... | |
| dma_handle_t * | txDmaHandle | 
| The DMA TX channel used.  More... | |
| dma_handle_t * | rxDmaHandle | 
| The DMA RX channel used.  More... | |
| volatile uint8_t | txState | 
| TX transfer state.  More... | |
| volatile uint8_t | rxState | 
| RX transfer state.  | |
| flexio_uart_dma_transfer_callback_t flexio_uart_dma_handle_t::callback | 
| void* flexio_uart_dma_handle_t::userData | 
| size_t flexio_uart_dma_handle_t::txDataSizeAll | 
| size_t flexio_uart_dma_handle_t::rxDataSizeAll | 
| dma_handle_t* flexio_uart_dma_handle_t::txDmaHandle | 
| dma_handle_t* flexio_uart_dma_handle_t::rxDmaHandle | 
| volatile uint8_t flexio_uart_dma_handle_t::txState | 
| #define FSL_FLEXIO_UART_DMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 6)) | 
| typedef void(* flexio_uart_dma_transfer_callback_t)(FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, status_t status, void *userData) | 
| status_t FLEXIO_UART_TransferCreateHandleDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_dma_handle_t * | handle, | ||
| flexio_uart_dma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | txDmaHandle, | ||
| dma_handle_t * | rxDmaHandle | ||
| ) | 
| base | Pointer to FLEXIO_UART_Type structure. | 
| handle | Pointer to flexio_uart_dma_handle_t structure. | 
| callback | FlexIO UART callback, NULL means no callback. | 
| userData | User callback function data. | 
| txDmaHandle | User requested DMA handle for TX DMA transfer. | 
| rxDmaHandle | User requested DMA handle for RX DMA transfer. | 
| kStatus_Success | Successfully create the handle. | 
| kStatus_OutOfRange | The FlexIO UART DMA type/handle table out of range. | 
| status_t FLEXIO_UART_TransferSendDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_dma_handle_t * | handle, | ||
| flexio_uart_transfer_t * | xfer | ||
| ) | 
This function send data using DMA. This is non-blocking function, which returns right away. When all data is sent out, the send callback function is called.
| base | Pointer to FLEXIO_UART_Type structure | 
| handle | Pointer to flexio_uart_dma_handle_t structure | 
| xfer | FLEXIO_UART DMA transfer structure, see flexio_uart_transfer_t. | 
| kStatus_Success | if succeed, others failed. | 
| kStatus_FLEXIO_UART_TxBusy | Previous transfer on going. | 
| status_t FLEXIO_UART_TransferReceiveDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_dma_handle_t * | handle, | ||
| flexio_uart_transfer_t * | xfer | ||
| ) | 
This function receives data using DMA. This is non-blocking function, which returns right away. When all data is received, the receive callback function is called.
| base | Pointer to FLEXIO_UART_Type structure | 
| handle | Pointer to flexio_uart_dma_handle_t structure | 
| xfer | FLEXIO_UART DMA transfer structure, see flexio_uart_transfer_t. | 
| kStatus_Success | if succeed, others failed. | 
| kStatus_FLEXIO_UART_RxBusy | Previous transfer on going. | 
| void FLEXIO_UART_TransferAbortSendDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_dma_handle_t * | handle | ||
| ) | 
This function aborts the sent data which using DMA.
| base | Pointer to FLEXIO_UART_Type structure | 
| handle | Pointer to flexio_uart_dma_handle_t structure | 
| void FLEXIO_UART_TransferAbortReceiveDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_dma_handle_t * | handle | ||
| ) | 
This function aborts the receive data which using DMA.
| base | Pointer to FLEXIO_UART_Type structure | 
| handle | Pointer to flexio_uart_dma_handle_t structure | 
| status_t FLEXIO_UART_TransferGetSendCountDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
This function gets the number of bytes sent out.
| base | Pointer to FLEXIO_UART_Type structure | 
| handle | Pointer to flexio_uart_dma_handle_t structure | 
| count | Number of bytes sent so far by the non-blocking transaction. | 
| kStatus_NoTransferInProgress | transfer has finished or no transfer in progress. | 
| kStatus_Success | Successfully return the count. | 
| status_t FLEXIO_UART_TransferGetReceiveCountDMA | ( | FLEXIO_UART_Type * | base, | 
| flexio_uart_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
This function gets the number of bytes received.
| base | Pointer to FLEXIO_UART_Type structure | 
| handle | Pointer to flexio_uart_dma_handle_t structure | 
| count | Number of bytes received so far by the non-blocking transaction. | 
| kStatus_NoTransferInProgress | transfer has finished or no transfer in progress. | 
| kStatus_Success | Successfully return the count. |