![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | flexspi_dma_handle_t | 
| FLEXSPI DMA transfer handle, users should not touch the content of the handle.  More... | |
Typedefs | |
| typedef void(* | flexspi_dma_callback_t )(FLEXSPI_Type *base, flexspi_dma_handle_t *handle, status_t status, void *userData) | 
| FLEXSPI dma transfer callback function for finish and error.  | |
Enumerations | |
| enum | flexspi_dma_transfer_nsize_t {  kFLEXPSI_DMAnSize1Bytes = 0x1U, kFLEXPSI_DMAnSize2Bytes = 0x2U, kFLEXPSI_DMAnSize4Bytes = 0x4U, kFLEXPSI_DMAnSize8Bytes = 0x8U, kFLEXPSI_DMAnSize32Bytes = 0x20U }  | 
| dma transfer configuration  More... | |
Driver version | |
| #define | FSL_FLEXSPI_DMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) | 
| FLEXSPI DMA driver version 2.0.0.  More... | |
FLEXSPI dma Transactional | |
| void | FLEXSPI_TransferCreateHandleDMA (FLEXSPI_Type *base, flexspi_dma_handle_t *handle, flexspi_dma_callback_t callback, void *userData, dma_handle_t *txDmaHandle, dma_handle_t *rxDmaHandle) | 
| Initializes the FLEXSPI handle for transfer which is used in transactional functions and set the callback.  More... | |
| void | FLEXSPI_TransferUpdateSizeDMA (FLEXSPI_Type *base, flexspi_dma_handle_t *handle, flexspi_dma_transfer_nsize_t nsize) | 
| Update FLEXSPI DMA transfer source data transfer size(SSIZE) and destination data transfer size(DSIZE).  More... | |
| status_t | FLEXSPI_TransferDMA (FLEXSPI_Type *base, flexspi_dma_handle_t *handle, flexspi_transfer_t *xfer) | 
| Transfers FLEXSPI data using an dma non-blocking method.  More... | |
| void | FLEXSPI_TransferAbortDMA (FLEXSPI_Type *base, flexspi_dma_handle_t *handle) | 
| Aborts the transfer data using dma.  More... | |
| status_t | FLEXSPI_TransferGetCountDMA (FLEXSPI_Type *base, flexspi_dma_handle_t *handle, size_t *count) | 
| Gets the transferred counts of transfer.  More... | |
| struct _flexspi_dma_handle | 
Data Fields | |
| dma_handle_t * | txDmaHandle | 
| dma handler for FLEXSPI Tx.  More... | |
| dma_handle_t * | rxDmaHandle | 
| dma handler for FLEXSPI Rx.  More... | |
| size_t | transferSize | 
| Bytes need to transfer.  More... | |
| flexspi_dma_transfer_nsize_t | nsize | 
| dma SSIZE/DSIZE in each transfer.  More... | |
| uint8_t | nbytes | 
| dma minor byte transfer count initially configured.  More... | |
| uint8_t | count | 
| The transfer data count in a DMA request.  More... | |
| uint32_t | state | 
| Internal state for FLEXSPI dma transfer.  More... | |
| flexspi_dma_callback_t | completionCallback | 
| A callback function called after the dma transfer is finished.  More... | |
| void * | userData | 
| User callback parameter.  | |
| dma_handle_t* flexspi_dma_handle_t::txDmaHandle | 
| dma_handle_t* flexspi_dma_handle_t::rxDmaHandle | 
| size_t flexspi_dma_handle_t::transferSize | 
| flexspi_dma_transfer_nsize_t flexspi_dma_handle_t::nsize | 
| uint8_t flexspi_dma_handle_t::nbytes | 
| uint8_t flexspi_dma_handle_t::count | 
| uint32_t flexspi_dma_handle_t::state | 
| flexspi_dma_callback_t flexspi_dma_handle_t::completionCallback | 
| #define FSL_FLEXSPI_DMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) | 
| void FLEXSPI_TransferCreateHandleDMA | ( | FLEXSPI_Type * | base, | 
| flexspi_dma_handle_t * | handle, | ||
| flexspi_dma_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | txDmaHandle, | ||
| dma_handle_t * | rxDmaHandle | ||
| ) | 
| base | FLEXSPI peripheral base address | 
| handle | Pointer to flexspi_dma_handle_t structure | 
| callback | FLEXSPI callback, NULL means no callback. | 
| userData | User callback function data. | 
| txDmaHandle | User requested DMA handle for TX DMA transfer. | 
| rxDmaHandle | User requested DMA handle for RX DMA transfer. | 
| void FLEXSPI_TransferUpdateSizeDMA | ( | FLEXSPI_Type * | base, | 
| flexspi_dma_handle_t * | handle, | ||
| flexspi_dma_transfer_nsize_t | nsize | ||
| ) | 
| base | FLEXSPI peripheral base address | 
| handle | Pointer to flexspi_dma_handle_t structure | 
| nsize | FLEXSPI DMA transfer data transfer size(SSIZE/DSIZE), by default the size is kFLEXPSI_DMAnSize1Bytes(one byte). | 
| status_t FLEXSPI_TransferDMA | ( | FLEXSPI_Type * | base, | 
| flexspi_dma_handle_t * | handle, | ||
| flexspi_transfer_t * | xfer | ||
| ) | 
This function writes/receives data to/from the FLEXSPI transmit/receive FIFO. This function is non-blocking.
| base | FLEXSPI peripheral base address. | 
| handle | Pointer to flexspi_dma_handle_t structure | 
| xfer | FLEXSPI transfer structure. | 
| kStatus_FLEXSPI_Busy | FLEXSPI is busy transfer. | 
| kStatus_InvalidArgument | The watermark configuration is invalid, the watermark should be power of 2 to do successfully DMA transfer. | 
| kStatus_Success | FLEXSPI successfully start dma transfer. | 
| void FLEXSPI_TransferAbortDMA | ( | FLEXSPI_Type * | base, | 
| flexspi_dma_handle_t * | handle | ||
| ) | 
This function aborts the transfer data using dma.
| base | FLEXSPI peripheral base address. | 
| handle | Pointer to flexspi_dma_handle_t structure | 
| status_t FLEXSPI_TransferGetCountDMA | ( | FLEXSPI_Type * | base, | 
| flexspi_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | FLEXSPI peripheral base address. | 
| handle | Pointer to flexspi_dma_handle_t structure. | 
| count | Bytes transfer. | 
| kStatus_Success | Succeed get the transfer count. | 
| kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |