![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | lpuart_edma_handle_t | 
| LPUART eDMA handle.  More... | |
Typedefs | |
| typedef void(* | lpuart_edma_transfer_callback_t )(LPUART_Type *base, lpuart_edma_handle_t *handle, status_t status, void *userData) | 
| LPUART transfer callback function.  More... | |
Driver version | |
| #define | FSL_LPUART_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 2, 8)) | 
| LPUART EDMA driver version 2.2.8.  More... | |
eDMA transactional | |
| void | LPUART_TransferCreateHandleEDMA (LPUART_Type *base, lpuart_edma_handle_t *handle, lpuart_edma_transfer_callback_t callback, void *userData, edma_handle_t *txEdmaHandle, edma_handle_t *rxEdmaHandle) | 
| Initializes the LPUART handle which is used in transactional functions.  More... | |
| status_t | LPUART_SendEDMA (LPUART_Type *base, lpuart_edma_handle_t *handle, lpuart_transfer_t *xfer) | 
| Sends data using eDMA.  More... | |
| status_t | LPUART_ReceiveEDMA (LPUART_Type *base, lpuart_edma_handle_t *handle, lpuart_transfer_t *xfer) | 
| Receives data using eDMA.  More... | |
| void | LPUART_TransferAbortSendEDMA (LPUART_Type *base, lpuart_edma_handle_t *handle) | 
| Aborts the sent data using eDMA.  More... | |
| void | LPUART_TransferAbortReceiveEDMA (LPUART_Type *base, lpuart_edma_handle_t *handle) | 
| Aborts the received data using eDMA.  More... | |
| status_t | LPUART_TransferGetSendCountEDMA (LPUART_Type *base, lpuart_edma_handle_t *handle, uint32_t *count) | 
| Gets the number of bytes written to the LPUART TX register.  More... | |
| status_t | LPUART_TransferGetReceiveCountEDMA (LPUART_Type *base, lpuart_edma_handle_t *handle, uint32_t *count) | 
| Gets the number of received bytes.  More... | |
| struct _lpuart_edma_handle | 
Data Fields | |
| lpuart_edma_transfer_callback_t | callback | 
| Callback function.  More... | |
| void * | userData | 
| LPUART callback function parameter.  More... | |
| size_t | rxDataSizeAll | 
| Size of the data to receive.  More... | |
| size_t | txDataSizeAll | 
| Size of the data to send out.  More... | |
| edma_handle_t * | txEdmaHandle | 
| The eDMA TX channel used.  More... | |
| edma_handle_t * | rxEdmaHandle | 
| The eDMA RX channel used.  More... | |
| uint8_t | nbytes | 
| eDMA minor byte transfer count initially configured.  More... | |
| volatile uint8_t | txState | 
| TX transfer state.  More... | |
| volatile uint8_t | rxState | 
| RX transfer state.  | |
| lpuart_edma_transfer_callback_t lpuart_edma_handle_t::callback | 
| void* lpuart_edma_handle_t::userData | 
| size_t lpuart_edma_handle_t::rxDataSizeAll | 
| size_t lpuart_edma_handle_t::txDataSizeAll | 
| edma_handle_t* lpuart_edma_handle_t::txEdmaHandle | 
| edma_handle_t* lpuart_edma_handle_t::rxEdmaHandle | 
| uint8_t lpuart_edma_handle_t::nbytes | 
| volatile uint8_t lpuart_edma_handle_t::txState | 
| #define FSL_LPUART_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 2, 8)) | 
| typedef void(* lpuart_edma_transfer_callback_t)(LPUART_Type *base, lpuart_edma_handle_t *handle, status_t status, void *userData) | 
| void LPUART_TransferCreateHandleEDMA | ( | LPUART_Type * | base, | 
| lpuart_edma_handle_t * | handle, | ||
| lpuart_edma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | txEdmaHandle, | ||
| edma_handle_t * | rxEdmaHandle | ||
| ) | 
| base | LPUART peripheral base address. | 
| handle | Pointer to lpuart_edma_handle_t structure. | 
| callback | Callback function. | 
| userData | User data. | 
| txEdmaHandle | User requested DMA handle for TX DMA transfer. | 
| rxEdmaHandle | User requested DMA handle for RX DMA transfer. | 
| status_t LPUART_SendEDMA | ( | LPUART_Type * | base, | 
| lpuart_edma_handle_t * | handle, | ||
| lpuart_transfer_t * | xfer | ||
| ) | 
This function sends data using eDMA. This is a non-blocking function, which returns right away. When all data is sent, the send callback function is called.
| base | LPUART peripheral base address. | 
| handle | LPUART handle pointer. | 
| xfer | LPUART eDMA transfer structure. See lpuart_transfer_t. | 
| kStatus_Success | if succeed, others failed. | 
| kStatus_LPUART_TxBusy | Previous transfer on going. | 
| kStatus_InvalidArgument | Invalid argument. | 
| status_t LPUART_ReceiveEDMA | ( | LPUART_Type * | base, | 
| lpuart_edma_handle_t * | handle, | ||
| lpuart_transfer_t * | xfer | ||
| ) | 
This function receives data using eDMA. This is non-blocking function, which returns right away. When all data is received, the receive callback function is called.
| base | LPUART peripheral base address. | 
| handle | Pointer to lpuart_edma_handle_t structure. | 
| xfer | LPUART eDMA transfer structure, see lpuart_transfer_t. | 
| kStatus_Success | if succeed, others fail. | 
| kStatus_LPUART_RxBusy | Previous transfer ongoing. | 
| kStatus_InvalidArgument | Invalid argument. | 
| void LPUART_TransferAbortSendEDMA | ( | LPUART_Type * | base, | 
| lpuart_edma_handle_t * | handle | ||
| ) | 
This function aborts the sent data using eDMA.
| base | LPUART peripheral base address. | 
| handle | Pointer to lpuart_edma_handle_t structure. | 
| void LPUART_TransferAbortReceiveEDMA | ( | LPUART_Type * | base, | 
| lpuart_edma_handle_t * | handle | ||
| ) | 
This function aborts the received data using eDMA.
| base | LPUART peripheral base address. | 
| handle | Pointer to lpuart_edma_handle_t structure. | 
| status_t LPUART_TransferGetSendCountEDMA | ( | LPUART_Type * | base, | 
| lpuart_edma_handle_t * | handle, | ||
| uint32_t * | count | ||
| ) | 
This function gets the number of bytes written to the LPUART TX register by DMA.
| base | LPUART peripheral base address. | 
| handle | LPUART handle pointer. | 
| count | Send bytes count. | 
| kStatus_NoTransferInProgress | No send in progress. | 
| kStatus_InvalidArgument | Parameter is invalid. | 
| kStatus_Success | Get successfully through the parameter count;  | 
| status_t LPUART_TransferGetReceiveCountEDMA | ( | LPUART_Type * | base, | 
| lpuart_edma_handle_t * | handle, | ||
| uint32_t * | count | ||
| ) | 
This function gets the number of received bytes.
| base | LPUART peripheral base address. | 
| handle | LPUART handle pointer. | 
| count | Receive bytes count. | 
| kStatus_NoTransferInProgress | No receive in progress. | 
| kStatus_InvalidArgument | Parameter is invalid. | 
| kStatus_Success | Get successfully through the parameter count;  |