![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | lpuart_rtos_config_t | 
| LPUART RTOS configuration structure.  More... | |
Driver version | |
| #define | FSL_LPUART_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 2, 8)) | 
| LPUART FreeRTOS driver version 2.2.8.  More... | |
LPUART RTOS Operation | |
| int | LPUART_RTOS_Init (lpuart_rtos_handle_t *handle, lpuart_handle_t *t_handle, const lpuart_rtos_config_t *cfg) | 
| Initializes an LPUART instance for operation in RTOS.  More... | |
| int | LPUART_RTOS_Deinit (lpuart_rtos_handle_t *handle) | 
| Deinitializes an LPUART instance for operation.  More... | |
LPUART transactional Operation | |
| int | LPUART_RTOS_Send (lpuart_rtos_handle_t *handle, const uint8_t *buffer, uint32_t length) | 
| Sends data in the background.  More... | |
| int | LPUART_RTOS_Receive (lpuart_rtos_handle_t *handle, uint8_t *buffer, uint32_t length, size_t *received) | 
| Receives data.  More... | |
| struct lpuart_rtos_config_t | 
Data Fields | |
| LPUART_Type * | base | 
| UART base address.  | |
| uint32_t | srcclk | 
| UART source clock in Hz.  | |
| uint32_t | baudrate | 
| Desired communication speed.  | |
| lpuart_parity_mode_t | parity | 
| Parity setting.  | |
| lpuart_stop_bit_count_t | stopbits | 
| Number of stop bits to use.  | |
| uint8_t * | buffer | 
| Buffer for background reception.  | |
| uint32_t | buffer_size | 
| Size of buffer for background reception.  | |
| bool | enableRxRTS | 
| RX RTS enable.  | |
| bool | enableTxCTS | 
| TX CTS enable.  | |
| lpuart_transmit_cts_source_t | txCtsSource | 
| TX CTS source.  | |
| lpuart_transmit_cts_config_t | txCtsConfig | 
| TX CTS configure.  | |
| #define FSL_LPUART_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 2, 8)) | 
| int LPUART_RTOS_Init | ( | lpuart_rtos_handle_t * | handle, | 
| lpuart_handle_t * | t_handle, | ||
| const lpuart_rtos_config_t * | cfg | ||
| ) | 
| handle | The RTOS LPUART handle, the pointer to an allocated space for RTOS context. | 
| t_handle | The pointer to an allocated space to store the transactional layer internal state. | 
| cfg | The pointer to the parameters required to configure the LPUART after initialization. | 
| int LPUART_RTOS_Deinit | ( | lpuart_rtos_handle_t * | handle | ) | 
This function deinitializes the LPUART module, sets all register value to the reset value, and releases the resources.
| handle | The RTOS LPUART handle. | 
| int LPUART_RTOS_Send | ( | lpuart_rtos_handle_t * | handle, | 
| const uint8_t * | buffer, | ||
| uint32_t | length | ||
| ) | 
This function sends data. It is an synchronous API. If the hardware buffer is full, the task is in the blocked state.
| handle | The RTOS LPUART handle. | 
| buffer | The pointer to buffer to send. | 
| length | The number of bytes to send. | 
| int LPUART_RTOS_Receive | ( | lpuart_rtos_handle_t * | handle, | 
| uint8_t * | buffer, | ||
| uint32_t | length, | ||
| size_t * | received | ||
| ) | 
This function receives data from LPUART. It is an synchronous API. If any data is immediately available it is returned immediately and the number of bytes received.
| handle | The RTOS LPUART handle. | 
| buffer | The pointer to buffer where to write received data. | 
| length | The number of bytes to receive. | 
| received | The pointer to a variable of size_t where the number of received data is filled. |