![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | spdif_edma_transfer_t | 
| SPDIF transfer structure.  More... | |
| struct | spdif_edma_handle_t | 
| SPDIF DMA transfer handle, users should not touch the content of the handle.  More... | |
Typedefs | |
| typedef void(* | spdif_edma_callback_t )(SPDIF_Type *base, spdif_edma_handle_t *handle, status_t status, void *userData) | 
| SPDIF eDMA transfer callback function for finish and error.  | |
Driver version | |
| #define | FSL_SPDIF_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 3)) | 
| Version 2.0.3.  | |
eDMA Transactional | |
| void | SPDIF_TransferTxCreateHandleEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle, spdif_edma_callback_t callback, void *userData, edma_handle_t *dmaLeftHandle, edma_handle_t *dmaRightHandle) | 
| Initializes the SPDIF eDMA handle.  More... | |
| void | SPDIF_TransferRxCreateHandleEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle, spdif_edma_callback_t callback, void *userData, edma_handle_t *dmaLeftHandle, edma_handle_t *dmaRightHandle) | 
| Initializes the SPDIF Rx eDMA handle.  More... | |
| status_t | SPDIF_TransferSendEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle, spdif_edma_transfer_t *xfer) | 
| Performs a non-blocking SPDIF transfer using DMA.  More... | |
| status_t | SPDIF_TransferReceiveEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle, spdif_edma_transfer_t *xfer) | 
| Performs a non-blocking SPDIF receive using eDMA.  More... | |
| void | SPDIF_TransferAbortSendEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle) | 
| Aborts a SPDIF transfer using eDMA.  More... | |
| void | SPDIF_TransferAbortReceiveEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle) | 
| Aborts a SPDIF receive using eDMA.  More... | |
| status_t | SPDIF_TransferGetSendCountEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle, size_t *count) | 
| Gets byte count sent by SPDIF.  More... | |
| status_t | SPDIF_TransferGetReceiveCountEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle, size_t *count) | 
| Gets byte count received by SPDIF.  More... | |
| struct spdif_edma_transfer_t | 
Data Fields | |
| uint8_t * | leftData | 
| Data start address to transfer.  More... | |
| uint8_t * | rightData | 
| Data start address to transfer.  More... | |
| size_t | dataSize | 
| Transfer size.  More... | |
| uint8_t* spdif_edma_transfer_t::leftData | 
| uint8_t* spdif_edma_transfer_t::rightData | 
| size_t spdif_edma_transfer_t::dataSize | 
| struct _spdif_edma_handle | 
Data Fields | |
| edma_handle_t * | dmaLeftHandle | 
| DMA handler for SPDIF left channel.  | |
| edma_handle_t * | dmaRightHandle | 
| DMA handler for SPDIF right channel.  | |
| uint8_t | nbytes | 
| eDMA minor byte transfer count initially configured.  More... | |
| uint8_t | count | 
| The transfer data count in a DMA request.  | |
| uint32_t | state | 
| Internal state for SPDIF eDMA transfer.  | |
| spdif_edma_callback_t | callback | 
| Callback for users while transfer finish or error occurs.  | |
| void * | userData | 
| User callback parameter.  | |
| edma_tcd_t | leftTcd [SPDIF_XFER_QUEUE_SIZE+1U] | 
| TCD pool for eDMA transfer.  More... | |
| edma_tcd_t | rightTcd [SPDIF_XFER_QUEUE_SIZE+1U] | 
| TCD pool for eDMA transfer.  More... | |
| spdif_edma_transfer_t | spdifQueue [SPDIF_XFER_QUEUE_SIZE] | 
| Transfer queue storing queued transfer.  More... | |
| size_t | transferSize [SPDIF_XFER_QUEUE_SIZE] | 
| Data bytes need to transfer, left and right are the same, so use one.  | |
| volatile uint8_t | queueUser | 
| Index for user to queue transfer.  More... | |
| volatile uint8_t | queueDriver | 
| Index for driver to get the transfer data and size.  | |
| uint8_t spdif_edma_handle_t::nbytes | 
| edma_tcd_t spdif_edma_handle_t::leftTcd[SPDIF_XFER_QUEUE_SIZE+1U] | 
| edma_tcd_t spdif_edma_handle_t::rightTcd[SPDIF_XFER_QUEUE_SIZE+1U] | 
| spdif_edma_transfer_t spdif_edma_handle_t::spdifQueue[SPDIF_XFER_QUEUE_SIZE] | 
| volatile uint8_t spdif_edma_handle_t::queueUser | 
| void SPDIF_TransferTxCreateHandleEDMA | ( | SPDIF_Type * | base, | 
| spdif_edma_handle_t * | handle, | ||
| spdif_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | dmaLeftHandle, | ||
| edma_handle_t * | dmaRightHandle | ||
| ) | 
This function initializes the SPDIF master DMA handle, which can be used for other SPDIF master transactional APIs. Usually, for a specified SPDIF instance, call this API once to get the initialized handle.
| base | SPDIF base pointer. | 
| handle | SPDIF eDMA handle pointer. | 
| base | SPDIF peripheral base address. | 
| callback | Pointer to user callback function. | 
| userData | User parameter passed to the callback function. | 
| dmaLeftHandle | eDMA handle pointer for left channel, this handle shall be static allocated by users. | 
| dmaRightHandle | eDMA handle pointer for right channel, this handle shall be static allocated by users. | 
| void SPDIF_TransferRxCreateHandleEDMA | ( | SPDIF_Type * | base, | 
| spdif_edma_handle_t * | handle, | ||
| spdif_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | dmaLeftHandle, | ||
| edma_handle_t * | dmaRightHandle | ||
| ) | 
This function initializes the SPDIF slave DMA handle, which can be used for other SPDIF master transactional APIs. Usually, for a specified SPDIF instance, call this API once to get the initialized handle.
| base | SPDIF base pointer. | 
| handle | SPDIF eDMA handle pointer. | 
| base | SPDIF peripheral base address. | 
| callback | Pointer to user callback function. | 
| userData | User parameter passed to the callback function. | 
| dmaLeftHandle | eDMA handle pointer for left channel, this handle shall be static allocated by users. | 
| dmaRightHandle | eDMA handle pointer for right channel, this handle shall be static allocated by users. | 
| status_t SPDIF_TransferSendEDMA | ( | SPDIF_Type * | base, | 
| spdif_edma_handle_t * | handle, | ||
| spdif_edma_transfer_t * | xfer | ||
| ) | 
| base | SPDIF base pointer. | 
| handle | SPDIF eDMA handle pointer. | 
| xfer | Pointer to the DMA transfer structure. | 
| kStatus_Success | Start a SPDIF eDMA send successfully. | 
| kStatus_InvalidArgument | The input argument is invalid. | 
| kStatus_TxBusy | SPDIF is busy sending data. | 
| status_t SPDIF_TransferReceiveEDMA | ( | SPDIF_Type * | base, | 
| spdif_edma_handle_t * | handle, | ||
| spdif_edma_transfer_t * | xfer | ||
| ) | 
| base | SPDIF base pointer | 
| handle | SPDIF eDMA handle pointer. | 
| xfer | Pointer to DMA transfer structure. | 
| kStatus_Success | Start a SPDIF eDMA receive successfully. | 
| kStatus_InvalidArgument | The input argument is invalid. | 
| kStatus_RxBusy | SPDIF is busy receiving data. | 
| void SPDIF_TransferAbortSendEDMA | ( | SPDIF_Type * | base, | 
| spdif_edma_handle_t * | handle | ||
| ) | 
| base | SPDIF base pointer. | 
| handle | SPDIF eDMA handle pointer. | 
| void SPDIF_TransferAbortReceiveEDMA | ( | SPDIF_Type * | base, | 
| spdif_edma_handle_t * | handle | ||
| ) | 
| base | SPDIF base pointer | 
| handle | SPDIF eDMA handle pointer. | 
| status_t SPDIF_TransferGetSendCountEDMA | ( | SPDIF_Type * | base, | 
| spdif_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | SPDIF base pointer. | 
| handle | SPDIF eDMA handle pointer. | 
| count | Bytes count sent by SPDIF. | 
| kStatus_Success | Succeed get the transfer count. | 
| kStatus_NoTransferInProgress | There is no non-blocking transaction in progress. | 
| status_t SPDIF_TransferGetReceiveCountEDMA | ( | SPDIF_Type * | base, | 
| spdif_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | SPDIF base pointer | 
| handle | SPDIF eDMA handle pointer. | 
| count | Bytes count received by SPDIF. | 
| kStatus_Success | Succeed get the transfer count. | 
| kStatus_NoTransferInProgress | There is no non-blocking transaction in progress. |