![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | i2c_master_edma_handle_t | 
| I2C master eDMA transfer structure.  More... | |
Typedefs | |
| typedef void(* | i2c_master_edma_transfer_callback_t )(I2C_Type *base, i2c_master_edma_handle_t *handle, status_t status, void *userData) | 
| I2C master eDMA transfer callback typedef.  More... | |
Driver version | |
| #define | FSL_I2C_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 8)) | 
| I2C EDMA driver version 2.0.8.  More... | |
I2C Block eDMA Transfer Operation | |
| void | I2C_MasterCreateEDMAHandle (I2C_Type *base, i2c_master_edma_handle_t *handle, i2c_master_edma_transfer_callback_t callback, void *userData, edma_handle_t *edmaHandle) | 
| Initializes the I2C handle which is used in transactional functions.  More... | |
| status_t | I2C_MasterTransferEDMA (I2C_Type *base, i2c_master_edma_handle_t *handle, i2c_master_transfer_t *xfer) | 
| Performs a master eDMA non-blocking transfer on the I2C bus.  More... | |
| status_t | I2C_MasterTransferGetCountEDMA (I2C_Type *base, i2c_master_edma_handle_t *handle, size_t *count) | 
| Gets a master transfer status during the eDMA non-blocking transfer.  More... | |
| void | I2C_MasterTransferAbortEDMA (I2C_Type *base, i2c_master_edma_handle_t *handle) | 
| Aborts a master eDMA non-blocking transfer early.  More... | |
| struct _i2c_master_edma_handle | 
Retry times for waiting flag.
I2C master eDMA handle typedef.
Data Fields | |
| i2c_master_transfer_t | transfer | 
| I2C master transfer structure.  More... | |
| size_t | transferSize | 
| Total bytes to be transferred.  More... | |
| uint8_t | nbytes | 
| eDMA minor byte transfer count initially configured.  More... | |
| uint8_t | state | 
| I2C master transfer status.  More... | |
| edma_handle_t * | dmaHandle | 
| The eDMA handler used.  More... | |
| i2c_master_edma_transfer_callback_t | completionCallback | 
| A callback function called after the eDMA transfer is finished.  More... | |
| void * | userData | 
| A callback parameter passed to the callback function.  More... | |
| i2c_master_transfer_t i2c_master_edma_handle_t::transfer | 
| size_t i2c_master_edma_handle_t::transferSize | 
| uint8_t i2c_master_edma_handle_t::nbytes | 
| uint8_t i2c_master_edma_handle_t::state | 
| edma_handle_t* i2c_master_edma_handle_t::dmaHandle | 
| i2c_master_edma_transfer_callback_t i2c_master_edma_handle_t::completionCallback | 
| void* i2c_master_edma_handle_t::userData | 
| #define FSL_I2C_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 8)) | 
| typedef void(* i2c_master_edma_transfer_callback_t)(I2C_Type *base, i2c_master_edma_handle_t *handle, status_t status, void *userData) | 
| void I2C_MasterCreateEDMAHandle | ( | I2C_Type * | base, | 
| i2c_master_edma_handle_t * | handle, | ||
| i2c_master_edma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | edmaHandle | ||
| ) | 
| base | I2C peripheral base address. | 
| handle | A pointer to the i2c_master_edma_handle_t structure. | 
| callback | A pointer to the user callback function. | 
| userData | A user parameter passed to the callback function. | 
| edmaHandle | eDMA handle pointer. | 
| status_t I2C_MasterTransferEDMA | ( | I2C_Type * | base, | 
| i2c_master_edma_handle_t * | handle, | ||
| i2c_master_transfer_t * | xfer | ||
| ) | 
| base | I2C peripheral base address. | 
| handle | A pointer to the i2c_master_edma_handle_t structure. | 
| xfer | A pointer to the transfer structure of i2c_master_transfer_t. | 
| kStatus_Success | Successfully completed the data transmission. | 
| kStatus_I2C_Busy | A previous transmission is still not finished. | 
| kStatus_I2C_Timeout | Transfer error, waits for a signal timeout. | 
| kStatus_I2C_ArbitrationLost | Transfer error, arbitration lost. | 
| kStataus_I2C_Nak | Transfer error, receive NAK during transfer. | 
| status_t I2C_MasterTransferGetCountEDMA | ( | I2C_Type * | base, | 
| i2c_master_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | I2C peripheral base address. | 
| handle | A pointer to the i2c_master_edma_handle_t structure. | 
| count | A number of bytes transferred by the non-blocking transaction. | 
| void I2C_MasterTransferAbortEDMA | ( | I2C_Type * | base, | 
| i2c_master_edma_handle_t * | handle | ||
| ) | 
| base | I2C peripheral base address. | 
| handle | A pointer to the i2c_master_edma_handle_t structure. |