| Enumerator | 
|---|
| kSerialManager_UsbVirtualControllerKhci0  | 
 KHCI 0U.  
 | 
| kSerialManager_UsbVirtualControllerKhci1  | 
 KHCI 1U, Currently, there are no platforms which have two KHCI IPs, this is reserved to be used in the future.  
 | 
| kSerialManager_UsbVirtualControllerEhci0  | 
 EHCI 0U.  
 | 
| kSerialManager_UsbVirtualControllerEhci1  | 
 EHCI 1U, Currently, there are no platforms which have two EHCI IPs, this is reserved to be used in the future.  
 | 
| kSerialManager_UsbVirtualControllerLpcIp3511Fs0  | 
 LPC USB IP3511 FS controller 0.  
 | 
| kSerialManager_UsbVirtualControllerLpcIp3511Fs1  | 
 LPC USB IP3511 FS controller 1, there are no platforms which have two IP3511 IPs, this is reserved to be used in the future.  
 | 
| kSerialManager_UsbVirtualControllerLpcIp3511Hs0  | 
 LPC USB IP3511 HS controller 0.  
 | 
| kSerialManager_UsbVirtualControllerLpcIp3511Hs1  | 
 LPC USB IP3511 HS controller 1, there are no platforms which have two IP3511 IPs, this is reserved to be used in the future.  
 | 
| kSerialManager_UsbVirtualControllerOhci0  | 
 OHCI 0U.  
 | 
| kSerialManager_UsbVirtualControllerOhci1  | 
 OHCI 1U, Currently, there are no platforms which have two OHCI IPs, this is reserved to be used in the future.  
 | 
| kSerialManager_UsbVirtualControllerIp3516Hs0  | 
 IP3516HS 0U.  
 | 
| kSerialManager_UsbVirtualControllerIp3516Hs1  | 
 IP3516HS 1U, Currently, there are no platforms which have two IP3516HS IPs, this is reserved to be used in the future.  
 |