![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Modules | |
| ftfx adapter | |
Macros | |
| #define | FTFx_DRIVER_HAS_FLASH1_SUPPORT (0U) | 
| Indicates whether the secondary flash is supported in the Flash driver.  | |
FTFx configuration | |
| #define | FTFx_DRIVER_IS_FLASH_RESIDENT 1U | 
| Flash driver location.  More... | |
| #define | FTFx_DRIVER_IS_EXPORTED 0U | 
| Flash Driver Export option.  More... | |
Secondary flash configuration | |
| #define | FTFx_FLASH1_HAS_PROT_CONTROL (0U) | 
| Indicates whether the secondary flash has its own protection register in flash module.  More... | |
| #define | FTFx_FLASH1_HAS_XACC_CONTROL (0U) | 
| Indicates whether the secondary flash has its own Execute-Only access register in flash module.  More... | |
| #define FTFx_DRIVER_IS_FLASH_RESIDENT 1U | 
Used for the flash resident application.
| #define FTFx_DRIVER_IS_EXPORTED 0U | 
Used for the MCUXpresso SDK application.
| #define FTFx_FLASH1_HAS_PROT_CONTROL (0U) | 
| #define FTFx_FLASH1_HAS_XACC_CONTROL (0U) |