MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

The MCUXpresso SDK provides a peripheral driver for the Universal Asynchronous Receiver/Transmitter (UART) module of MCUXpresso SDK devices.

The UART driver includes functional APIs and transactional APIs.

Functional APIs are used for UART initialization/configuration/operation for the purpose of optimization/customization. Using the functional API requires the knowledge of the UART peripheral and how to organize functional APIs to meet the application requirements. All functional APIs use the peripheral base address as the first parameter. UART functional operation groups provide the functional API set.

Transactional APIs can be used to enable the peripheral quickly and in the application if the code size and performance of transactional APIs can satisfy the requirements. If the code size and performance are critical requirements, see the transactional API implementation and write custom code. All transactional APIs use the uart_handle_t as the second parameter. Initialize the handle by calling the UART_TransferCreateHandle() API.

Transactional APIs support asynchronous transfer, which means that the functions UART_TransferSendNonBlocking() and UART_TransferReceiveNonBlocking() set up an interrupt for data transfer. When the transfer completes, the upper layer is notified through a callback function with the kStatus_UART_TxIdle and kStatus_UART_RxIdle.

Transactional receive APIs support the ring buffer. Prepare the memory for the ring buffer and pass in the start address and size while calling the UART_TransferCreateHandle(). If passing NULL, the ring buffer feature is disabled. When the ring buffer is enabled, the received data is saved to the ring buffer in the background. The UART_TransferReceiveNonBlocking() function first gets data from the ring buffer. If the ring buffer does not have enough data, the function first returns the data in the ring buffer and then saves the received data to user memory. When all data is received, the upper layer is informed through a callback with the kStatus_UART_RxIdle.

If the receive ring buffer is full, the upper layer is informed through a callback with the kStatus_UART_RxRingBufferOverrun. In the callback function, the upper layer reads data out from the ring buffer. If not, existing data is overwritten by the new data.

The ring buffer size is specified when creating the handle. Note that one byte is reserved for the ring buffer maintenance. When creating handle using the following code.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/uart In this example, the buffer size is 32, but only 31 bytes are used for saving data.

Typical use case

UART Send/receive using a polling method

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/uart

UART Send/receive using an interrupt method

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/uart

UART Receive using the ringbuffer feature

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/uart

UART automatic baud rate detect feature

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/uart

Data Structures

struct  uart_config_t
 UART configuration structure. More...
 
struct  uart_transfer_t
 UART transfer structure. More...
 
struct  uart_handle_t
 UART handle structure. More...
 

Typedefs

typedef void(* uart_transfer_callback_t )(UART_Type *base, uart_handle_t *handle, status_t status, void *userData)
 UART transfer callback function. More...
 

Enumerations

enum  {
  kStatus_UART_TxBusy = MAKE_STATUS(kStatusGroup_IUART, 0),
  kStatus_UART_RxBusy = MAKE_STATUS(kStatusGroup_IUART, 1),
  kStatus_UART_TxIdle = MAKE_STATUS(kStatusGroup_IUART, 2),
  kStatus_UART_RxIdle = MAKE_STATUS(kStatusGroup_IUART, 3),
  kStatus_UART_TxWatermarkTooLarge = MAKE_STATUS(kStatusGroup_IUART, 4),
  kStatus_UART_RxWatermarkTooLarge = MAKE_STATUS(kStatusGroup_IUART, 5),
  kStatus_UART_FlagCannotClearManually,
  kStatus_UART_Error = MAKE_STATUS(kStatusGroup_IUART, 7),
  kStatus_UART_RxRingBufferOverrun = MAKE_STATUS(kStatusGroup_IUART, 8),
  kStatus_UART_RxHardwareOverrun = MAKE_STATUS(kStatusGroup_IUART, 9),
  kStatus_UART_NoiseError = MAKE_STATUS(kStatusGroup_IUART, 10),
  kStatus_UART_FramingError = MAKE_STATUS(kStatusGroup_IUART, 11),
  kStatus_UART_ParityError = MAKE_STATUS(kStatusGroup_IUART, 12),
  kStatus_UART_BaudrateNotSupport,
  kStatus_UART_BreakDetect = MAKE_STATUS(kStatusGroup_IUART, 14)
}
 Error codes for the UART driver. More...
 
enum  uart_data_bits_t {
  kUART_SevenDataBits = 0x0U,
  kUART_EightDataBits = 0x1U
}
 UART data bits count. More...
 
enum  uart_parity_mode_t {
  kUART_ParityDisabled = 0x0U,
  kUART_ParityEven = 0x2U,
  kUART_ParityOdd = 0x3U
}
 UART parity mode. More...
 
enum  uart_stop_bit_count_t {
  kUART_OneStopBit = 0x0U,
  kUART_TwoStopBit = 0x1U
}
 UART stop bit count. More...
 
enum  uart_idle_condition_t {
  kUART_IdleFor4Frames = 0x0U,
  kUART_IdleFor8Frames = 0x1U,
  kUART_IdleFor16Frames = 0x2U,
  kUART_IdleFor32Frames = 0x3U
}
 UART idle condition detect. More...
 
enum  _uart_interrupt_enable
 This structure contains the settings for all of the UART interrupt configurations. More...
 
enum  _uart_flags {
  kUART_RxCharReadyFlag = 0x0000000FU,
  kUART_RxErrorFlag = 0x0000000EU,
  kUART_RxOverrunErrorFlag = 0x0000000DU,
  kUART_RxFrameErrorFlag = 0x0000000CU,
  kUART_RxBreakDetectFlag = 0x0000000BU,
  kUART_RxParityErrorFlag = 0x0000000AU,
  kUART_ParityErrorFlag = 0x0094000FU,
  kUART_RtsStatusFlag = 0x0094000EU,
  kUART_TxReadyFlag = 0x0094000DU,
  kUART_RtsDeltaFlag = 0x0094000CU,
  kUART_EscapeFlag = 0x0094000BU,
  kUART_FrameErrorFlag = 0x0094000AU,
  kUART_RxReadyFlag = 0x00940009U,
  kUART_AgingTimerFlag = 0x00940008U,
  kUART_DtrDeltaFlag = 0x00940007U,
  kUART_RxDsFlag = 0x00940006U,
  kUART_tAirWakeFlag = 0x00940005U,
  kUART_AwakeFlag = 0x00940004U,
  kUART_Rs485SlaveAddrMatchFlag = 0x00940003U,
  kUART_AutoBaudFlag = 0x0098000FU,
  kUART_TxEmptyFlag = 0x0098000EU,
  kUART_DtrFlag = 0x0098000DU,
  kUART_IdleFlag = 0x0098000CU,
  kUART_AutoBaudCntStopFlag = 0x0098000BU,
  kUART_RiDeltaFlag = 0x0098000AU,
  kUART_RiFlag = 0x00980009U,
  kUART_IrFlag = 0x00980008U,
  kUART_WakeFlag = 0x00980007U,
  kUART_DcdDeltaFlag = 0x00980006U,
  kUART_DcdFlag = 0x00980005U,
  kUART_RtsFlag = 0x00980004U,
  kUART_TxCompleteFlag = 0x00980003U,
  kUART_BreakDetectFlag = 0x00980002U,
  kUART_RxOverrunFlag = 0x00980001U,
  kUART_RxDataReadyFlag = 0x00980000U
}
 UART status flags. More...
 

Functions

uint32_t UART_GetInstance (UART_Type *base)
 Get the UART instance from peripheral base address. More...
 

Variables

uint32_t uart_config_t::baudRate_Bps
 UART baud rate. More...
 
uart_parity_mode_t uart_config_t::parityMode
 Parity error check mode of this module. More...
 
uart_data_bits_t uart_config_t::dataBitsCount
 Data bits count, eight (default), seven.
 
uart_stop_bit_count_t uart_config_t::stopBitCount
 Number of stop bits in one frame. More...
 
uint8_t uart_config_t::txFifoWatermark
 TX FIFO watermark.
 
uint8_t uart_config_t::rxFifoWatermark
 RX FIFO watermark.
 
bool uart_config_t::enableAutoBaudRate
 Enable automatic baud rate detection.
 
bool uart_config_t::enableTx
 Enable TX.
 
bool uart_config_t::enableRx
 Enable RX.
 
uint8_t * uart_transfer_t::data
 The buffer of data to be transfer. More...
 
size_t uart_transfer_t::dataSize
 The byte count to be transfer. More...
 
uint8_t *volatile uart_handle_t::txData
 Address of remaining data to send. More...
 
volatile size_t uart_handle_t::txDataSize
 Size of the remaining data to send. More...
 
size_t uart_handle_t::txDataSizeAll
 Size of the data to send out. More...
 
uint8_t *volatile uart_handle_t::rxData
 Address of remaining data to receive. More...
 
volatile size_t uart_handle_t::rxDataSize
 Size of the remaining data to receive. More...
 
size_t uart_handle_t::rxDataSizeAll
 Size of the data to receive. More...
 
uint8_t * uart_handle_t::rxRingBuffer
 Start address of the receiver ring buffer. More...
 
size_t uart_handle_t::rxRingBufferSize
 Size of the ring buffer. More...
 
volatile uint16_t uart_handle_t::rxRingBufferHead
 Index for the driver to store received data into ring buffer. More...
 
volatile uint16_t uart_handle_t::rxRingBufferTail
 Index for the user to get data from the ring buffer. More...
 
uart_transfer_callback_t uart_handle_t::callback
 Callback function. More...
 
void * uart_handle_t::userData
 UART callback function parameter. More...
 
volatile uint8_t uart_handle_t::txState
 TX transfer state. More...
 
volatile uint8_t uart_handle_t::rxState
 RX transfer state.
 

Driver version

#define FSL_UART_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))
 UART driver version 2.0.2. More...
 

Software Reset

static void UART_SoftwareReset (UART_Type *base)
 Resets the UART using software. More...
 

Initialization and deinitialization

status_t UART_Init (UART_Type *base, const uart_config_t *config, uint32_t srcClock_Hz)
 Initializes an UART instance with the user configuration structure and the peripheral clock. More...
 
void UART_Deinit (UART_Type *base)
 Deinitializes a UART instance. More...
 
void UART_GetDefaultConfig (uart_config_t *config)
 l More...
 
status_t UART_SetBaudRate (UART_Type *base, uint32_t baudRate_Bps, uint32_t srcClock_Hz)
 Sets the UART instance baud rate. More...
 
static void UART_Enable (UART_Type *base)
 This function is used to Enable the UART Module. More...
 
static void UART_SetIdleCondition (UART_Type *base, uart_idle_condition_t condition)
 This function is used to configure the IDLE line condition. More...
 
static void UART_Disable (UART_Type *base)
 This function is used to Disable the UART Module. More...
 

Status

bool UART_GetStatusFlag (UART_Type *base, uint32_t flag)
 This function is used to get the current status of specific UART status flag(including interrupt flag). More...
 
void UART_ClearStatusFlag (UART_Type *base, uint32_t flag)
 This function is used to clear the current status of specific UART status flag. More...
 

Interrupts

void UART_EnableInterrupts (UART_Type *base, uint32_t mask)
 Enables UART interrupts according to the provided mask. More...
 
void UART_DisableInterrupts (UART_Type *base, uint32_t mask)
 Disables the UART interrupts according to the provided mask. More...
 
uint32_t UART_GetEnabledInterrupts (UART_Type *base)
 Gets enabled UART interrupts. More...
 

Bus Operations

static void UART_EnableTx (UART_Type *base, bool enable)
 Enables or disables the UART transmitter. More...
 
static void UART_EnableRx (UART_Type *base, bool enable)
 Enables or disables the UART receiver. More...
 
static void UART_WriteByte (UART_Type *base, uint8_t data)
 Writes to the transmitter register. More...
 
static uint8_t UART_ReadByte (UART_Type *base)
 Reads the receiver register. More...
 
void UART_WriteBlocking (UART_Type *base, const uint8_t *data, size_t length)
 Writes to the TX register using a blocking method. More...
 
status_t UART_ReadBlocking (UART_Type *base, uint8_t *data, size_t length)
 Read RX data register using a blocking method. More...
 

Transactional

void UART_TransferCreateHandle (UART_Type *base, uart_handle_t *handle, uart_transfer_callback_t callback, void *userData)
 Initializes the UART handle. More...
 
void UART_TransferStartRingBuffer (UART_Type *base, uart_handle_t *handle, uint8_t *ringBuffer, size_t ringBufferSize)
 Sets up the RX ring buffer. More...
 
void UART_TransferStopRingBuffer (UART_Type *base, uart_handle_t *handle)
 Aborts the background transfer and uninstalls the ring buffer. More...
 
size_t UART_TransferGetRxRingBufferLength (uart_handle_t *handle)
 Get the length of received data in RX ring buffer. More...
 
status_t UART_TransferSendNonBlocking (UART_Type *base, uart_handle_t *handle, uart_transfer_t *xfer)
 Transmits a buffer of data using the interrupt method. More...
 
void UART_TransferAbortSend (UART_Type *base, uart_handle_t *handle)
 Aborts the interrupt-driven data transmit. More...
 
status_t UART_TransferGetSendCount (UART_Type *base, uart_handle_t *handle, uint32_t *count)
 Gets the number of bytes written to the UART TX register. More...
 
status_t UART_TransferReceiveNonBlocking (UART_Type *base, uart_handle_t *handle, uart_transfer_t *xfer, size_t *receivedBytes)
 Receives a buffer of data using an interrupt method. More...
 
void UART_TransferAbortReceive (UART_Type *base, uart_handle_t *handle)
 Aborts the interrupt-driven data receiving. More...
 
status_t UART_TransferGetReceiveCount (UART_Type *base, uart_handle_t *handle, uint32_t *count)
 Gets the number of bytes that have been received. More...
 
void UART_TransferHandleIRQ (UART_Type *base, uart_handle_t *handle)
 UART IRQ handle function. More...
 

DMA control functions.

static void UART_EnableTxDMA (UART_Type *base, bool enable)
 Enables or disables the UART transmitter DMA request. More...
 
static void UART_EnableRxDMA (UART_Type *base, bool enable)
 Enables or disables the UART receiver DMA request. More...
 

FIFO control functions.

static void UART_SetTxFifoWatermark (UART_Type *base, uint8_t watermark)
 This function is used to set the watermark of UART Tx FIFO. More...
 
static void UART_SetRxFifoWatermark (UART_Type *base, uint8_t watermark)
 This function is used to set the watermark of UART Rx FIFO. More...
 

Auto baud rate detection.

static void UART_EnableAutoBaudRate (UART_Type *base, bool enable)
 This function is used to set the enable condition of Automatic Baud Rate Detection feature. More...
 
static bool UART_IsAutoBaudRateComplete (UART_Type *base)
 This function is used to read if the automatic baud rate detection has finished. More...
 

Data Structure Documentation

struct uart_config_t

Data Fields

uint32_t baudRate_Bps
 UART baud rate. More...
 
uart_parity_mode_t parityMode
 Parity error check mode of this module. More...
 
uart_data_bits_t dataBitsCount
 Data bits count, eight (default), seven.
 
uart_stop_bit_count_t stopBitCount
 Number of stop bits in one frame. More...
 
uint8_t txFifoWatermark
 TX FIFO watermark.
 
uint8_t rxFifoWatermark
 RX FIFO watermark.
 
bool enableAutoBaudRate
 Enable automatic baud rate detection.
 
bool enableTx
 Enable TX.
 
bool enableRx
 Enable RX.
 
struct uart_transfer_t

Data Fields

uint8_t * data
 The buffer of data to be transfer. More...
 
size_t dataSize
 The byte count to be transfer. More...
 
struct _uart_handle

Forward declaration of the handle typedef.

Data Fields

uint8_t *volatile txData
 Address of remaining data to send. More...
 
volatile size_t txDataSize
 Size of the remaining data to send. More...
 
size_t txDataSizeAll
 Size of the data to send out. More...
 
uint8_t *volatile rxData
 Address of remaining data to receive. More...
 
volatile size_t rxDataSize
 Size of the remaining data to receive. More...
 
size_t rxDataSizeAll
 Size of the data to receive. More...
 
uint8_t * rxRingBuffer
 Start address of the receiver ring buffer. More...
 
size_t rxRingBufferSize
 Size of the ring buffer. More...
 
volatile uint16_t rxRingBufferHead
 Index for the driver to store received data into ring buffer. More...
 
volatile uint16_t rxRingBufferTail
 Index for the user to get data from the ring buffer. More...
 
uart_transfer_callback_t callback
 Callback function. More...
 
void * userData
 UART callback function parameter. More...
 
volatile uint8_t txState
 TX transfer state. More...
 
volatile uint8_t rxState
 RX transfer state.
 

Macro Definition Documentation

#define FSL_UART_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))

Typedef Documentation

typedef void(* uart_transfer_callback_t)(UART_Type *base, uart_handle_t *handle, status_t status, void *userData)

Enumeration Type Documentation

anonymous enum
Enumerator
kStatus_UART_TxBusy 

Transmitter is busy.

kStatus_UART_RxBusy 

Receiver is busy.

kStatus_UART_TxIdle 

UART transmitter is idle.

kStatus_UART_RxIdle 

UART receiver is idle.

kStatus_UART_TxWatermarkTooLarge 

TX FIFO watermark too large.

kStatus_UART_RxWatermarkTooLarge 

RX FIFO watermark too large.

kStatus_UART_FlagCannotClearManually 

UART flag can't be manually cleared.

kStatus_UART_Error 

Error happens on UART.

kStatus_UART_RxRingBufferOverrun 

UART RX software ring buffer overrun.

kStatus_UART_RxHardwareOverrun 

UART RX receiver overrun.

kStatus_UART_NoiseError 

UART noise error.

kStatus_UART_FramingError 

UART framing error.

kStatus_UART_ParityError 

UART parity error.

kStatus_UART_BaudrateNotSupport 

Baudrate is not support in current clock source.

kStatus_UART_BreakDetect 

Receiver detect BREAK signal.

Enumerator
kUART_SevenDataBits 

Seven data bit.

kUART_EightDataBits 

Eight data bit.

Enumerator
kUART_ParityDisabled 

Parity disabled.

kUART_ParityEven 

Even error check is selected.

kUART_ParityOdd 

Odd error check is selected.

Enumerator
kUART_OneStopBit 

One stop bit.

kUART_TwoStopBit 

Two stop bits.

Enumerator
kUART_IdleFor4Frames 

Idle for more than 4 frames.

kUART_IdleFor8Frames 

Idle for more than 8 frames.

kUART_IdleFor16Frames 

Idle for more than 16 frames.

kUART_IdleFor32Frames 

Idle for more than 32 frames.

This provides constants for the UART status flags for use in the UART functions.

Enumerator
kUART_RxCharReadyFlag 

Rx Character Ready Flag.

kUART_RxErrorFlag 

Rx Error Detect Flag.

kUART_RxOverrunErrorFlag 

Rx Overrun Flag.

kUART_RxFrameErrorFlag 

Rx Frame Error Flag.

kUART_RxBreakDetectFlag 

Rx Break Detect Flag.

kUART_RxParityErrorFlag 

Rx Parity Error Flag.

kUART_ParityErrorFlag 

Parity Error Interrupt Flag.

kUART_RtsStatusFlag 

RTS_B Pin Status Flag.

kUART_TxReadyFlag 

Transmitter Ready Interrupt/DMA Flag.

kUART_RtsDeltaFlag 

RTS Delta Flag.

kUART_EscapeFlag 

Escape Sequence Interrupt Flag.

kUART_FrameErrorFlag 

Frame Error Interrupt Flag.

kUART_RxReadyFlag 

Receiver Ready Interrupt/DMA Flag.

kUART_AgingTimerFlag 

Aging Timer Interrupt Flag.

kUART_DtrDeltaFlag 

DTR Delta Flag.

kUART_RxDsFlag 

Receiver IDLE Interrupt Flag.

kUART_tAirWakeFlag 

Asynchronous IR WAKE Interrupt Flag.

kUART_AwakeFlag 

Asynchronous WAKE Interrupt Flag.

kUART_Rs485SlaveAddrMatchFlag 

RS-485 Slave Address Detected Interrupt Flag.

kUART_AutoBaudFlag 

Automatic Baud Rate Detect Complete Flag.

kUART_TxEmptyFlag 

Transmit Buffer FIFO Empty.

kUART_DtrFlag 

DTR edge triggered interrupt flag.

kUART_IdleFlag 

Idle Condition Flag.

kUART_AutoBaudCntStopFlag 

Auto-baud Counter Stopped Flag.

kUART_RiDeltaFlag 

Ring Indicator Delta Flag.

kUART_RiFlag 

Ring Indicator Input Flag.

kUART_IrFlag 

Serial Infrared Interrupt Flag.

kUART_WakeFlag 

Wake Flag.

kUART_DcdDeltaFlag 

Data Carrier Detect Delta Flag.

kUART_DcdFlag 

Data Carrier Detect Input Flag.

kUART_RtsFlag 

RTS Edge Triggered Interrupt Flag.

kUART_TxCompleteFlag 

Transmitter Complete Flag.

kUART_BreakDetectFlag 

BREAK Condition Detected Flag.

kUART_RxOverrunFlag 

Overrun Error Flag.

kUART_RxDataReadyFlag 

Receive Data Ready Flag.

Function Documentation

uint32_t UART_GetInstance ( UART_Type *  base)
Parameters
baseUART peripheral base address.
Returns
UART instance.
static void UART_SoftwareReset ( UART_Type *  base)
inlinestatic

This function resets the transmit and receive state machines, all FIFOs and register USR1, USR2, UBIR, UBMR, UBRC , URXD, UTXD and UTS[6-3]

Parameters
baseUART peripheral base address.
status_t UART_Init ( UART_Type *  base,
const uart_config_t *  config,
uint32_t  srcClock_Hz 
)

This function configures the UART module with user-defined settings. Call the UART_GetDefaultConfig() function to configure the configuration structure and get the default configuration. The example below shows how to use this API to configure the UART.

* uart_config_t uartConfig;
* uartConfig.baudRate_Bps = 115200U;
* uartConfig.txFifoWatermark = 2;
* uartConfig.rxFifoWatermark = 1;
* uartConfig.enableAutoBaudrate = false;
* uartConfig.enableTx = true;
* uartConfig.enableRx = true;
* UART_Init(UART1, &uartConfig, 24000000U);
*
Parameters
baseUART peripheral base address.
configPointer to a user-defined configuration structure.
srcClock_HzUART clock source frequency in HZ.
Return values
kStatus_SuccessUART initialize succeed
void UART_Deinit ( UART_Type *  base)

This function waits for transmit to complete, disables TX and RX, and disables the UART clock.

Parameters
baseUART peripheral base address.
void UART_GetDefaultConfig ( uart_config_t *  config)

Gets the default configuration structure.

This function initializes the UART configuration structure to a default value. The default values are: uartConfig->baudRate_Bps = 115200U; uartConfig->parityMode = kUART_ParityDisabled; uartConfig->dataBitsCount = kUART_EightDataBits; uartConfig->stopBitCount = kUART_OneStopBit; uartConfig->txFifoWatermark = 2; uartConfig->rxFifoWatermark = 1; uartConfig->enableAutoBaudrate = flase; uartConfig->enableTx = false; uartConfig->enableRx = false;

Parameters
configPointer to a configuration structure.
status_t UART_SetBaudRate ( UART_Type *  base,
uint32_t  baudRate_Bps,
uint32_t  srcClock_Hz 
)

This function configures the UART module baud rate. This function is used to update the UART module baud rate after the UART module is initialized by the UART_Init.

* UART_SetBaudRate(UART1, 115200U, 20000000U);
*
Parameters
baseUART peripheral base address.
baudRate_BpsUART baudrate to be set.
srcClock_HzUART clock source frequency in Hz.
Return values
kStatus_UART_BaudrateNotSupportBaudrate is not support in the current clock source.
kStatus_SuccessSet baudrate succeeded.
static void UART_Enable ( UART_Type *  base)
inlinestatic
Parameters
baseUART base pointer.
static void UART_SetIdleCondition ( UART_Type *  base,
uart_idle_condition_t  condition 
)
inlinestatic
Parameters
baseUART base pointer.
conditionIDLE line detect condition of the enumerators in _uart_idle_condition.
static void UART_Disable ( UART_Type *  base)
inlinestatic
Parameters
baseUART base pointer.
bool UART_GetStatusFlag ( UART_Type *  base,
uint32_t  flag 
)

The available status flag can be select from uart_status_flag_t enumeration.

Parameters
baseUART base pointer.
flagStatus flag to check.
Return values
currentstate of corresponding status flag.
void UART_ClearStatusFlag ( UART_Type *  base,
uint32_t  flag 
)

The available status flag can be select from uart_status_flag_t enumeration.

Parameters
baseUART base pointer.
flagStatus flag to clear.
void UART_EnableInterrupts ( UART_Type *  base,
uint32_t  mask 
)

This function enables the UART interrupts according to the provided mask. The mask is a logical OR of enumeration members. See _uart_interrupt_enable. For example, to enable TX empty interrupt and RX data ready interrupt, do the following.

* UART_EnableInterrupts(UART1,kUART_TxEmptyEnable | kUART_RxDataReadyEnable);
*
Parameters
baseUART peripheral base address.
maskThe interrupts to enable. Logical OR of _uart_interrupt_enable.
void UART_DisableInterrupts ( UART_Type *  base,
uint32_t  mask 
)

This function disables the UART interrupts according to the provided mask. The mask is a logical OR of enumeration members. See _uart_interrupt_enable. For example, to disable TX empty interrupt and RX data ready interrupt do the following.

* UART_EnableInterrupts(UART1,kUART_TxEmptyEnable | kUART_RxDataReadyEnable);
*
Parameters
baseUART peripheral base address.
maskThe interrupts to disable. Logical OR of _uart_interrupt_enable.
uint32_t UART_GetEnabledInterrupts ( UART_Type *  base)

This function gets the enabled UART interrupts. The enabled interrupts are returned as the logical OR value of the enumerators _uart_interrupt_enable. To check a specific interrupt enable status, compare the return value with enumerators in _uart_interrupt_enable. For example, to check whether the TX empty interrupt is enabled:

* uint32_t enabledInterrupts = UART_GetEnabledInterrupts(UART1);
*
* if (kUART_TxEmptyEnable & enabledInterrupts)
* {
* ...
* }
*
Parameters
baseUART peripheral base address.
Returns
UART interrupt flags which are logical OR of the enumerators in _uart_interrupt_enable.
static void UART_EnableTx ( UART_Type *  base,
bool  enable 
)
inlinestatic

This function enables or disables the UART transmitter.

Parameters
baseUART peripheral base address.
enableTrue to enable, false to disable.
static void UART_EnableRx ( UART_Type *  base,
bool  enable 
)
inlinestatic

This function enables or disables the UART receiver.

Parameters
baseUART peripheral base address.
enableTrue to enable, false to disable.
static void UART_WriteByte ( UART_Type *  base,
uint8_t  data 
)
inlinestatic

This function is used to write data to transmitter register. The upper layer must ensure that the TX register is empty or that the TX FIFO has room before calling this function.

Parameters
baseUART peripheral base address.
dataData write to the TX register.
static uint8_t UART_ReadByte ( UART_Type *  base)
inlinestatic

This function is used to read data from receiver register. The upper layer must ensure that the receiver register is full or that the RX FIFO has data before calling this function.

Parameters
baseUART peripheral base address.
Returns
Data read from data register.
void UART_WriteBlocking ( UART_Type *  base,
const uint8_t *  data,
size_t  length 
)

This function polls the TX register, waits for the TX register to be empty or for the TX FIFO to have room and writes data to the TX buffer.

Parameters
baseUART peripheral base address.
dataStart address of the data to write.
lengthSize of the data to write.
status_t UART_ReadBlocking ( UART_Type *  base,
uint8_t *  data,
size_t  length 
)

This function polls the RX register, waits for the RX register to be full or for RX FIFO to have data, and reads data from the TX register.

Parameters
baseUART peripheral base address.
dataStart address of the buffer to store the received data.
lengthSize of the buffer.
Return values
kStatus_UART_RxHardwareOverrunReceiver overrun occurred while receiving data.
kStatus_UART_NoiseErrorA noise error occurred while receiving data.
kStatus_UART_FramingErrorA framing error occurred while receiving data.
kStatus_UART_ParityErrorA parity error occurred while receiving data.
kStatus_SuccessSuccessfully received all data.
void UART_TransferCreateHandle ( UART_Type *  base,
uart_handle_t *  handle,
uart_transfer_callback_t  callback,
void *  userData 
)

This function initializes the UART handle which can be used for other UART transactional APIs. Usually, for a specified UART instance, call this API once to get the initialized handle.

Parameters
baseUART peripheral base address.
handleUART handle pointer.
callbackThe callback function.
userDataThe parameter of the callback function.
void UART_TransferStartRingBuffer ( UART_Type *  base,
uart_handle_t *  handle,
uint8_t *  ringBuffer,
size_t  ringBufferSize 
)

This function sets up the RX ring buffer to a specific UART handle.

When the RX ring buffer is used, data received are stored into the ring buffer even when the user doesn't call the UART_TransferReceiveNonBlocking() API. If data is already received in the ring buffer, the user can get the received data from the ring buffer directly.

Note
When using the RX ring buffer, one byte is reserved for internal use. In other words, if ringBufferSize is 32, only 31 bytes are used for saving data.
Parameters
baseUART peripheral base address.
handleUART handle pointer.
ringBufferStart address of the ring buffer for background receiving. Pass NULL to disable the ring buffer.
ringBufferSizeSize of the ring buffer.
void UART_TransferStopRingBuffer ( UART_Type *  base,
uart_handle_t *  handle 
)

This function aborts the background transfer and uninstalls the ring buffer.

Parameters
baseUART peripheral base address.
handleUART handle pointer.
size_t UART_TransferGetRxRingBufferLength ( uart_handle_t *  handle)
Parameters
handleUART handle pointer.
Returns
Length of received data in RX ring buffer.
status_t UART_TransferSendNonBlocking ( UART_Type *  base,
uart_handle_t *  handle,
uart_transfer_t *  xfer 
)

This function sends data using an interrupt method. This is a non-blocking function, which returns directly without waiting for all data to be written to the TX register. When all data is written to the TX register in the ISR, the UART driver calls the callback function and passes the kStatus_UART_TxIdle as status parameter.

Note
The kStatus_UART_TxIdle is passed to the upper layer when all data is written to the TX register. However, it does not ensure that all data is sent out. Before disabling the TX, check the kUART_TransmissionCompleteFlag to ensure that the TX is finished.
Parameters
baseUART peripheral base address.
handleUART handle pointer.
xferUART transfer structure. See uart_transfer_t.
Return values
kStatus_SuccessSuccessfully start the data transmission.
kStatus_UART_TxBusyPrevious transmission still not finished; data not all written to TX register yet.
kStatus_InvalidArgumentInvalid argument.
void UART_TransferAbortSend ( UART_Type *  base,
uart_handle_t *  handle 
)

This function aborts the interrupt-driven data sending. The user can get the remainBytes to find out how many bytes are not sent out.

Parameters
baseUART peripheral base address.
handleUART handle pointer.
status_t UART_TransferGetSendCount ( UART_Type *  base,
uart_handle_t *  handle,
uint32_t *  count 
)

This function gets the number of bytes written to the UART TX register by using the interrupt method.

Parameters
baseUART peripheral base address.
handleUART handle pointer.
countSend bytes count.
Return values
kStatus_NoTransferInProgressNo send in progress.
kStatus_InvalidArgumentThe parameter is invalid.
kStatus_SuccessGet successfully through the parameter count;
status_t UART_TransferReceiveNonBlocking ( UART_Type *  base,
uart_handle_t *  handle,
uart_transfer_t *  xfer,
size_t *  receivedBytes 
)

This function receives data using an interrupt method. This is a non-blocking function, which returns without waiting for all data to be received. If the RX ring buffer is used and not empty, the data in the ring buffer is copied and the parameter receivedBytes shows how many bytes are copied from the ring buffer. After copying, if the data in the ring buffer is not enough to read, the receive request is saved by the UART driver. When the new data arrives, the receive request is serviced first. When all data is received, the UART driver notifies the upper layer through a callback function and passes the status parameter kStatus_UART_RxIdle. For example, the upper layer needs 10 bytes but there are only 5 bytes in the ring buffer. The 5 bytes are copied to the xfer->data and this function returns with the parameter receivedBytes set to 5. For the left 5 bytes, newly arrived data is saved from the xfer->data[5]. When 5 bytes are received, the UART driver notifies the upper layer. If the RX ring buffer is not enabled, this function enables the RX and RX interrupt to receive data to the xfer->data. When all data is received, the upper layer is notified.

Parameters
baseUART peripheral base address.
handleUART handle pointer.
xferUART transfer structure, see uart_transfer_t.
receivedBytesBytes received from the ring buffer directly.
Return values
kStatus_SuccessSuccessfully queue the transfer into transmit queue.
kStatus_UART_RxBusyPrevious receive request is not finished.
kStatus_InvalidArgumentInvalid argument.
void UART_TransferAbortReceive ( UART_Type *  base,
uart_handle_t *  handle 
)

This function aborts the interrupt-driven data receiving. The user can get the remainBytes to know how many bytes are not received yet.

Parameters
baseUART peripheral base address.
handleUART handle pointer.
status_t UART_TransferGetReceiveCount ( UART_Type *  base,
uart_handle_t *  handle,
uint32_t *  count 
)

This function gets the number of bytes that have been received.

Parameters
baseUART peripheral base address.
handleUART handle pointer.
countReceive bytes count.
Return values
kStatus_NoTransferInProgressNo receive in progress.
kStatus_InvalidArgumentParameter is invalid.
kStatus_SuccessGet successfully through the parameter count;
void UART_TransferHandleIRQ ( UART_Type *  base,
uart_handle_t *  handle 
)

This function handles the UART transmit and receive IRQ request.

Parameters
baseUART peripheral base address.
handleUART handle pointer.
static void UART_EnableTxDMA ( UART_Type *  base,
bool  enable 
)
inlinestatic

This function enables or disables the transmit request when the transmitter has one or more slots available in the TxFIFO. The fill level in the TxFIFO that generates the DMA request is controlled by the TXTL bits.

Parameters
baseUART peripheral base address.
enableTrue to enable, false to disable.
static void UART_EnableRxDMA ( UART_Type *  base,
bool  enable 
)
inlinestatic

This function enables or disables the receive request when the receiver has data in the RxFIFO. The fill level in the RxFIFO at which a DMA request is generated is controlled by the RXTL bits .

Parameters
baseUART peripheral base address.
enableTrue to enable, false to disable.
static void UART_SetTxFifoWatermark ( UART_Type *  base,
uint8_t  watermark 
)
inlinestatic
   A maskable interrupt is generated whenever the data level in
   the TxFIFO falls below the Tx FIFO watermark.
Parameters
baseUART base pointer.
watermarkThe Tx FIFO watermark.
static void UART_SetRxFifoWatermark ( UART_Type *  base,
uint8_t  watermark 
)
inlinestatic
   A maskable interrupt is generated whenever the data level in
   the RxFIFO reaches the Rx FIFO watermark.
Parameters
baseUART base pointer.
watermarkThe Rx FIFO watermark.
static void UART_EnableAutoBaudRate ( UART_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseUART base pointer.
enableEnable/Disable Automatic Baud Rate Detection feature.
  • true: Enable Automatic Baud Rate Detection feature.
  • false: Disable Automatic Baud Rate Detection feature.
static bool UART_IsAutoBaudRateComplete ( UART_Type *  base)
inlinestatic
Parameters
baseUART base pointer.
Returns
- true: Automatic baud rate detection has finished.
  • false: Automatic baud rate detection has not finished.

Variable Documentation

uint32_t uart_config_t::baudRate_Bps
uart_parity_mode_t uart_config_t::parityMode
uart_stop_bit_count_t uart_config_t::stopBitCount
uint8_t* uart_transfer_t::data
size_t uart_transfer_t::dataSize
uint8_t* volatile uart_handle_t::txData
volatile size_t uart_handle_t::txDataSize
size_t uart_handle_t::txDataSizeAll
uint8_t* volatile uart_handle_t::rxData
volatile size_t uart_handle_t::rxDataSize
size_t uart_handle_t::rxDataSizeAll
uint8_t* uart_handle_t::rxRingBuffer
size_t uart_handle_t::rxRingBufferSize
volatile uint16_t uart_handle_t::rxRingBufferHead
volatile uint16_t uart_handle_t::rxRingBufferTail
uart_transfer_callback_t uart_handle_t::callback
void* uart_handle_t::userData
volatile uint8_t uart_handle_t::txState