The SDK provides a peripheral driver for the CACHE Controller of MCUXpresso SDK devices.
The CACHE driver is created to the help the user more easily operate the cache memory. The LPCAC contains a code bus cache and system bus cache if the system bus cache is supported (the system bus cache is SoC-specific). The code bus cache ranges from 0x00000000 ~ 0x1FFFFFFF and the system bus ranges from 0x20000000 ~ 0xFFFFFFFF.
The APIs for basic operations are included the following three groups: 1L. The L1-specific cache driver API. This group provides the IP-specific cache controller drivers. The L1 caches in this arch is the AHB Low Power Cache Controller (LPCAC). The driver API name in this level is L1 cache controller specific.
2L. The unified L1 cache driver API. For ease of use, we try to unify the L1 cache driver API as much as possible in this group. APIs of this type directly call the L1 specific cache driver API and are unified to the same name. Due to the cache controller specification, it is impossible to provide all L1 cache-unified APIs for LPCAC.
3L. The unified cache driver API. This group is provided for the unified cache driver APIs for combining L1 and L2 cache maintain operations. This is provided for SDK drivers (DMA, ENET, USDHC, etc) which should do the cache maintenance in their transactional APIs. This is because in this arch, there is no L2 cache so the unified cache driver API directly calls only L1 cache driver APIs.
Function groups
L1 CACHE Operation {#L1CACHE MaintainOperation}
This function group provides Enable/Disable APIs. This function group only provides the cache invalidate operation beacuse the LPCAC is write through mode. By default, the cache mode is write through with allocation. The above cache maintains are provided for code bus cache and might provide for system bus cache if it is supported in the future.
The SDK provides a peripheral driver for the CACHE Controller of MCUXpresso SDK devices.
CACHE driver is created to help user to operate the cache memory more easy. The LPLMEM contains code bus cache and system bus cache if the system bus cache is supported (the system bus cache is soc specific). The code bus cache is ranged from 0x00000000 ~ 0x1FFFFFFF and the system bus is ranged from 0x20000000 ~ 0xFFFFFFFF.
The APIs for basic operations are including the following three groups: 1L. The L1 specific cache driver API. This group provides the IP specific cache controller drivers. The L1 caches in this arch is the AHB Low-Power Local Memory Controller (LPLMEM). The driver API name in this level is L1 cache controller specific.
2L. The unified L1 cache driver API. For ease of use, we try to unify the L1 cache driver API as much as possible in this group. APIs of this type directly call the L1 specific cache driver API and are unified to the same name. Due to the cache controller specification, it is impossible to provide all L1 cache unified APIs for LPLMEM.
3L. The unified cache driver API. This group is provided for unified cache driver APIs for combining L1 and L2 cache maintain operations. This is provided for SDK drivers (DMA, ENET, USDHC, etc) which should do the cache maintenance in their transactional APIs. This is because in this arch, there is no L2 cache so the unified cache driver API directly call only L1 cache driver APIs.
Function groups
L1 CACHE Operation {#L1CACHE MaintainOperation}
This function group provides Enable/Disable APIs. This function group only provides the cache invalidate operation beacuse the LPLMEM is write through mode. By default, the cache mode is write through with allocation. The above cache maintains are provided for code bus cache and might provide for system bus cache if it is supported in the future.
| void L1CACHE_InvalidateICacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
- Parameters
-
| address | The start address of the memory to be invalidated. |
| size_byte | The memory size. |
| static void L1CACHE_InvalidateDCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The start address of the memory to be invalidated. |
| size_byte | The memory size. |
| static void L1CACHE_CleanDCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
The cache is write through mode, so there is nothing to do with the cache flush/clean operation.
- Parameters
-
| address | The start address of the memory to be cleaned. |
| size_byte | The memory size. |
| static void L1CACHE_CleanInvalidateDCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The start address of the memory to be clean and invalidated. |
| size_byte | The memory size. |
| static void ICACHE_InvalidateByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The physical address. |
| size_byte | size of the memory to be invalidated. |
| static void DCACHE_InvalidateByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The physical address. |
| size_byte | size of the memory to be invalidated. |
| static void DCACHE_CleanByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The physical address. |
| size_byte | size of the memory to be cleaned. |
| static void DCACHE_CleanInvalidateByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The physical address. |
| size_byte | size of the memory to be Cleaned and Invalidated. |