![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | uart_dma_handle_t |
| UART DMA handle. More... | |
Typedefs | |
| typedef void(* | uart_dma_transfer_callback_t )(UART_Type *base, uart_dma_handle_t *handle, status_t status, void *userData) |
| UART transfer callback function. More... | |
Driver version | |
| #define | FSL_UART_DMA_DRIVER_VERSION (MAKE_VERSION(2, 2, 0)) |
| UART DMA driver version 2.2.0. More... | |
eDMA transactional | |
| void | UART_TransferCreateHandleDMA (UART_Type *base, uart_dma_handle_t *handle, uart_dma_transfer_callback_t callback, void *userData, dma_handle_t *txDmaHandle, dma_handle_t *rxDmaHandle) |
| Initializes the UART handle which is used in transactional functions and sets the callback. More... | |
| status_t | UART_TransferSendDMA (UART_Type *base, uart_dma_handle_t *handle, uart_transfer_t *xfer) |
| Sends data using DMA. More... | |
| status_t | UART_TransferReceiveDMA (UART_Type *base, uart_dma_handle_t *handle, uart_transfer_t *xfer) |
| Receives data using DMA. More... | |
| void | UART_TransferAbortSendDMA (UART_Type *base, uart_dma_handle_t *handle) |
| Aborts the send data using DMA. More... | |
| void | UART_TransferAbortReceiveDMA (UART_Type *base, uart_dma_handle_t *handle) |
| Aborts the received data using DMA. More... | |
| status_t | UART_TransferGetSendCountDMA (UART_Type *base, uart_dma_handle_t *handle, uint32_t *count) |
| Gets the number of bytes written to UART TX register. More... | |
| status_t | UART_TransferGetReceiveCountDMA (UART_Type *base, uart_dma_handle_t *handle, uint32_t *count) |
| Gets the number of bytes that have been received. More... | |
| struct _uart_dma_handle |
Data Fields | |
| UART_Type * | base |
| UART peripheral base address. More... | |
| uart_dma_transfer_callback_t | callback |
| Callback function. More... | |
| void * | userData |
| UART callback function parameter. More... | |
| size_t | rxDataSizeAll |
| Size of the data to receive. More... | |
| size_t | txDataSizeAll |
| Size of the data to send out. More... | |
| dma_handle_t * | txDmaHandle |
| The DMA TX channel used. More... | |
| dma_handle_t * | rxDmaHandle |
| The DMA RX channel used. More... | |
| volatile uint8_t | txState |
| TX transfer state. More... | |
| volatile uint8_t | rxState |
| RX transfer state. | |
| UART_Type* uart_dma_handle_t::base |
| uart_dma_transfer_callback_t uart_dma_handle_t::callback |
| void* uart_dma_handle_t::userData |
| size_t uart_dma_handle_t::rxDataSizeAll |
| size_t uart_dma_handle_t::txDataSizeAll |
| dma_handle_t* uart_dma_handle_t::txDmaHandle |
| dma_handle_t* uart_dma_handle_t::rxDmaHandle |
| volatile uint8_t uart_dma_handle_t::txState |
| #define FSL_UART_DMA_DRIVER_VERSION (MAKE_VERSION(2, 2, 0)) |
| typedef void(* uart_dma_transfer_callback_t)(UART_Type *base, uart_dma_handle_t *handle, status_t status, void *userData) |
| void UART_TransferCreateHandleDMA | ( | UART_Type * | base, |
| uart_dma_handle_t * | handle, | ||
| uart_dma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | txDmaHandle, | ||
| dma_handle_t * | rxDmaHandle | ||
| ) |
| base | UART peripheral base address. |
| handle | Pointer to the uart_dma_handle_t structure. |
| callback | UART callback, NULL means no callback. |
| userData | User callback function data. |
| rxDmaHandle | User requested DMA handle for the RX DMA transfer. |
| txDmaHandle | User requested DMA handle for the TX DMA transfer. |
| status_t UART_TransferSendDMA | ( | UART_Type * | base, |
| uart_dma_handle_t * | handle, | ||
| uart_transfer_t * | xfer | ||
| ) |
This function sends data using DMA. This is non-blocking function, which returns right away. When all data is sent, the send callback function is called.
| base | UART peripheral base address. |
| handle | UART handle pointer. |
| xfer | UART DMA transfer structure. See uart_transfer_t. |
| kStatus_Success | if succeeded; otherwise failed. |
| kStatus_UART_TxBusy | Previous transfer ongoing. |
| kStatus_InvalidArgument | Invalid argument. |
| status_t UART_TransferReceiveDMA | ( | UART_Type * | base, |
| uart_dma_handle_t * | handle, | ||
| uart_transfer_t * | xfer | ||
| ) |
This function receives data using DMA. This is non-blocking function, which returns right away. When all data is received, the receive callback function is called.
| base | UART peripheral base address. |
| handle | Pointer to the uart_dma_handle_t structure. |
| xfer | UART DMA transfer structure. See uart_transfer_t. |
| kStatus_Success | if succeeded; otherwise failed. |
| kStatus_UART_RxBusy | Previous transfer on going. |
| kStatus_InvalidArgument | Invalid argument. |
| void UART_TransferAbortSendDMA | ( | UART_Type * | base, |
| uart_dma_handle_t * | handle | ||
| ) |
This function aborts the sent data using DMA.
| base | UART peripheral base address. |
| handle | Pointer to uart_dma_handle_t structure. |
| void UART_TransferAbortReceiveDMA | ( | UART_Type * | base, |
| uart_dma_handle_t * | handle | ||
| ) |
This function abort receive data which using DMA.
| base | UART peripheral base address. |
| handle | Pointer to uart_dma_handle_t structure. |
| status_t UART_TransferGetSendCountDMA | ( | UART_Type * | base, |
| uart_dma_handle_t * | handle, | ||
| uint32_t * | count | ||
| ) |
This function gets the number of bytes written to UART TX register by DMA.
| base | UART peripheral base address. |
| handle | UART handle pointer. |
| count | Send bytes count. |
| kStatus_NoTransferInProgress | No send in progress. |
| kStatus_InvalidArgument | Parameter is invalid. |
| kStatus_Success | Get successfully through the parameter count; |
| status_t UART_TransferGetReceiveCountDMA | ( | UART_Type * | base, |
| uart_dma_handle_t * | handle, | ||
| uint32_t * | count | ||
| ) |
This function gets the number of bytes that have been received.
| base | UART peripheral base address. |
| handle | UART handle pointer. |
| count | Receive bytes count. |
| kStatus_NoTransferInProgress | No receive in progress. |
| kStatus_InvalidArgument | Parameter is invalid. |
| kStatus_Success | Get successfully through the parameter count; |