The MCUXpresso SDK provides a peripheral clock driver for the SYSCON module of MCUXpresso SDK devices.
Function description
Clock driver provides these functions:
- Functions to initialize the Core clock to given frequency
- Functions to configure the clock selection muxes.
- Functions to setup peripheral clock dividers
- Functions to set the flash wait states for the input freuqency
- Functions to get the frequency of the selected clock
- Functions to set PLL frequency
SYSCON Clock frequency functions
SYSCON clock module provides clocks, such as MCLKCLK, ADCCLK, DMICCLK, MCGFLLCLK, FXCOMCLK, WDTOSC, RTCOSC, USBCLK, and SYSPLL. The functions CLOCK_EnableClock() and CLOCK_DisableClock() enables and disables the various clocks. CLOCK_SetupFROClocking() initializes the FRO to 12 MHz, 48 MHz, or 96 MHz frequency. CLOCK_SetupPLLData(), CLOCK_SetupSystemPLLPrec(), and CLOCK_SetPLLFreq() functions are used to setup the PLL. The SYSCON clock driver provides functions to get the frequency of these clocks, such as CLOCK_GetFreq(), CLOCK_GetFro12MFreq(), CLOCK_GetExtClkFreq(), CLOCK_GetWdtOscFreq(), CLOCK_GetFroHfFreq(), CLOCK_GetPllOutFreq(), CLOCK_GetOsc32KFreq(), CLOCK_GetCoreSysClkFreq(), CLOCK_GetI2SMClkFreq(), CLOCK_GetFlexCommClkFreq, and CLOCK_GetAsyncApbClkFreq.
SYSCON clock Selection Muxes
The SYSCON clock driver provides the function to configure the clock selected. The function CLOCK_AttachClk() is implemented for this. The function selects the clock source for a particular peripheral like MAINCLK, DMIC, FLEXCOMM, USB, ADC, and PLL.
SYSCON clock dividers
The SYSCON clock module provides the function to setup the peripheral clock dividers. The function CLOCK_SetClkDiv() configures the CLKDIV registers for various periperals like USB, DMIC, I2S, SYSTICK, AHB, ADC, and also CLKOUT and TRACE functions.
SYSCON flash wait states
The SYSCON clock driver provides the function CLOCK_SetFLASHAccessCyclesForFreq() that configures FLASHCFG register with a selected FLASHTIM value.
Typical use case
POWER_DisablePD(kPDRUNCFG_PD_FRO_EN); /*!< Ensure FRO is on so that we can switch to its 12MHz mode temporarily
|
| struct | pll_config_t |
| | PLL configuration structure. More...
|
| |
| struct | pll_setup_t |
| | PLL setup structure This structure can be used to pre-build a PLL setup configuration at run-time and quickly set the PLL to the configuration. More...
|
| |
|
| enum | clock_ip_name_t |
| | Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More...
|
| |
| enum | clock_name_t {
kCLOCK_CoreSysClk,
kCLOCK_BusClk,
kCLOCK_FroHf,
kCLOCK_Fro12M,
kCLOCK_ExtClk,
kCLOCK_PllOut,
kCLOCK_UsbClk,
kCLOCK_WdtOsc,
kCLOCK_Frg,
kCLOCK_AsyncApbClk,
kCLOCK_FlexI2S
} |
| | Clock name used to get clock frequency. More...
|
| |
| enum | async_clock_src_t {
kCLOCK_AsyncMainClk = 0,
kCLOCK_AsyncFro12Mhz
} |
| |
| enum | clock_flashtim_t {
kCLOCK_Flash1Cycle = 0,
kCLOCK_Flash2Cycle,
kCLOCK_Flash3Cycle,
kCLOCK_Flash4Cycle,
kCLOCK_Flash5Cycle,
kCLOCK_Flash6Cycle,
kCLOCK_Flash7Cycle
} |
| | FLASH Access time definitions. More...
|
| |
| enum | ss_progmodfm_t {
kSS_MF_512 = (0 << 20),
kSS_MF_384 = (1 << 20),
kSS_MF_256 = (2 << 20),
kSS_MF_128 = (3 << 20),
kSS_MF_64 = (4 << 20),
kSS_MF_32 = (5 << 20),
kSS_MF_24 = (6 << 20),
kSS_MF_16 = (7 << 20)
} |
| | PLL Spread Spectrum (SS) Programmable modulation frequency See (MF) field in the SYSPLLSSCTRL1 register in the UM. More...
|
| |
| enum | ss_progmoddp_t {
kSS_MR_K0 = (0 << 23),
kSS_MR_K1 = (1 << 23),
kSS_MR_K1_5 = (2 << 23),
kSS_MR_K2 = (3 << 23),
kSS_MR_K3 = (4 << 23),
kSS_MR_K4 = (5 << 23),
kSS_MR_K6 = (6 << 23),
kSS_MR_K8 = (7 << 23)
} |
| | PLL Spread Spectrum (SS) Programmable frequency modulation depth See (MR) field in the SYSPLLSSCTRL1 register in the UM. More...
|
| |
| enum | ss_modwvctrl_t {
kSS_MC_NOC = (0 << 26),
kSS_MC_RECC = (2 << 26),
kSS_MC_MAXC = (3 << 26)
} |
| | PLL Spread Spectrum (SS) Modulation waveform control See (MC) field in the SYSPLLSSCTRL1 register in the UM. More...
|
| |
| enum | pll_error_t {
kStatus_PLL_Success = MAKE_STATUS(kStatusGroup_Generic, 0),
kStatus_PLL_OutputTooLow = MAKE_STATUS(kStatusGroup_Generic, 1),
kStatus_PLL_OutputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 2),
kStatus_PLL_InputTooLow = MAKE_STATUS(kStatusGroup_Generic, 3),
kStatus_PLL_InputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 4),
kStatus_PLL_OutsideIntLimit = MAKE_STATUS(kStatusGroup_Generic, 5)
} |
| | PLL status definitions. More...
|
| |
| enum | clock_usb_src_t {
kCLOCK_UsbSrcFro = (uint32_t)kCLOCK_FroHf,
kCLOCK_UsbSrcSystemPll = (uint32_t)kCLOCK_PllOut,
kCLOCK_UsbSrcMainClock = (uint32_t)kCLOCK_CoreSysClk,
kCLOCK_UsbSrcNone
} |
| | USB clock source definition. More...
|
| |
|
| static void | CLOCK_SetFLASHAccessCycles (clock_flashtim_t clks) |
| | Set FLASH memory access time in clocks. More...
|
| |
| status_t | CLOCK_SetupFROClocking (uint32_t iFreq) |
| | Initialize the Core clock to given frequency (12, 48 or 96 MHz). Turns on FRO and uses default CCO, if freq is 12000000, then high speed output is off, else high speed output is enabled. More...
|
| |
| void | CLOCK_AttachClk (clock_attach_id_t connection) |
| | Configure the clock selection muxes. More...
|
| |
| clock_attach_id_t | CLOCK_GetClockAttachId (clock_attach_id_t attachId) |
| | Get the actual clock attach id. This fuction uses the offset in input attach id, then it reads the actual source value in the register and combine the offset to obtain an actual attach id. More...
|
| |
| void | CLOCK_SetClkDiv (clock_div_name_t div_name, uint32_t divided_by_value, bool reset) |
| | Setup peripheral clock dividers. More...
|
| |
| void | CLOCK_SetFLASHAccessCyclesForFreq (uint32_t iFreq) |
| | Set the flash wait states for the input freuqency. More...
|
| |
| uint32_t | CLOCK_GetFreq (clock_name_t clockName) |
| | Return Frequency of selected clock. More...
|
| |
| uint32_t | CLOCK_GetFRGInputClock (void) |
| | Return Input frequency for the Fractional baud rate generator. More...
|
| |
| uint32_t | CLOCK_GetDmicClkFreq (void) |
| | Return Input frequency for the DMIC. More...
|
| |
| uint32_t | CLOCK_GetFrgClkFreq (void) |
| | Return Input frequency for the FRG. More...
|
| |
| uint32_t | CLOCK_SetFRGClock (uint32_t freq) |
| | Set output of the Fractional baud rate generator. More...
|
| |
| uint32_t | CLOCK_GetFro12MFreq (void) |
| | Return Frequency of FRO 12MHz. More...
|
| |
| uint32_t | CLOCK_GetExtClkFreq (void) |
| | Return Frequency of External Clock. More...
|
| |
| uint32_t | CLOCK_GetWdtOscFreq (void) |
| | Return Frequency of Watchdog Oscillator. More...
|
| |
| uint32_t | CLOCK_GetFroHfFreq (void) |
| | Return Frequency of High-Freq output of FRO. More...
|
| |
| uint32_t | CLOCK_GetUsbClkFreq (void) |
| | Return Frequency of USB. More...
|
| |
| uint32_t | CLOCK_GetPllOutFreq (void) |
| | Return Frequency of PLL. More...
|
| |
| uint32_t | CLOCK_GetOsc32KFreq (void) |
| | Return Frequency of 32kHz osc. More...
|
| |
| uint32_t | CLOCK_GetCoreSysClkFreq (void) |
| | Return Frequency of Core System. More...
|
| |
| uint32_t | CLOCK_GetI2SMClkFreq (void) |
| | Return Frequency of I2S MCLK Clock. More...
|
| |
| uint32_t | CLOCK_GetFlexCommClkFreq (uint32_t id) |
| | Return Frequency of Flexcomm functional Clock. More...
|
| |
| uint32_t | CLOCK_GetAdcClkFreq (void) |
| | Return Frequency of Adc Clock. More...
|
| |
| __STATIC_INLINE async_clock_src_t | CLOCK_GetAsyncApbClkSrc (void) |
| | Return Asynchronous APB Clock source. More...
|
| |
| uint32_t | CLOCK_GetAsyncApbClkFreq (void) |
| | Return Frequency of Asynchronous APB Clock. More...
|
| |
| uint32_t | CLOCK_GetSystemPLLInClockRate (void) |
| | Return System PLL input clock rate. More...
|
| |
| uint32_t | CLOCK_GetSystemPLLOutClockRate (bool recompute) |
| | Return System PLL output clock rate. More...
|
| |
| __STATIC_INLINE void | CLOCK_SetBypassPLL (bool bypass) |
| | Enables and disables PLL bypass mode. More...
|
| |
| __STATIC_INLINE bool | CLOCK_IsSystemPLLLocked (void) |
| | Check if PLL is locked or not. More...
|
| |
| void | CLOCK_SetStoredPLLClockRate (uint32_t rate) |
| | Store the current PLL rate. More...
|
| |
| uint32_t | CLOCK_GetSystemPLLOutFromSetup (pll_setup_t *pSetup) |
| | Return System PLL output clock rate from setup structure. More...
|
| |
| pll_error_t | CLOCK_SetupPLLData (pll_config_t *pControl, pll_setup_t *pSetup) |
| | Set PLL output based on the passed PLL setup data. More...
|
| |
| pll_error_t | CLOCK_SetupSystemPLLPrec (pll_setup_t *pSetup, uint32_t flagcfg) |
| | Set PLL output from PLL setup structure (precise frequency) More...
|
| |
| pll_error_t | CLOCK_SetPLLFreq (const pll_setup_t *pSetup) |
| | Set PLL output from PLL setup structure (precise frequency) More...
|
| |
| void | CLOCK_SetupSystemPLLMult (uint32_t multiply_by, uint32_t input_freq) |
| | Set PLL output based on the multiplier and input frequency. More...
|
| |
| static void | CLOCK_DisableUsbfs0Clock (void) |
| | Disable USB FS clock. More...
|
| |
This structure can be used to configure the settings for a PLL setup structure. Fill in the desired configuration for the PLL and call the PLL setup function to fill in a PLL setup structure.
Data Fields |
|
uint32_t | desiredRate |
| | Desired PLL rate in Hz.
|
| |
|
uint32_t | inputRate |
| | PLL input clock in Hz, only used if PLL_CONFIGFLAG_USEINRATE flag is set.
|
| |
|
uint32_t | flags |
| | PLL configuration flags, Or'ed value of PLL_CONFIGFLAG_* definitions.
|
| |
|
ss_progmodfm_t | ss_mf |
| | SS Programmable modulation frequency, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag.
|
| |
|
ss_progmoddp_t | ss_mr |
| | SS Programmable frequency modulation depth, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag.
|
| |
|
ss_modwvctrl_t | ss_mc |
| | SS Modulation waveform control, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag.
|
| |
|
bool | mfDither |
| | false for fixed modulation frequency or true for dithering, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag
|
| |
It can be populated with the PLL setup function. If powering up or waiting for PLL lock, the PLL input clock source should be configured prior to PLL setup.
Data Fields |
|
uint32_t | syspllctrl |
| | PLL control register SYSPLLCTRL.
|
| |
|
uint32_t | syspllndec |
| | PLL NDEC register SYSPLLNDEC.
|
| |
|
uint32_t | syspllpdec |
| | PLL PDEC register SYSPLLPDEC.
|
| |
|
uint32_t | syspllssctrl [2] |
| | PLL SSCTL registers SYSPLLSSCTRL.
|
| |
|
uint32_t | pllRate |
| | Acutal PLL rate.
|
| |
|
uint32_t | flags |
| | PLL setup flags, Or'ed value of PLL_SETUPFLAG_* definitions.
|
| |
| #define CLOCK_USR_CFG_PLL_CONFIG_CACHE_COUNT 2U |
Once define this MACRO to be non-zero value, CLOCK_PllGetConfig() function would cache the recent calulation and accelerate the execution to get the right settings.
Value:{ \
kCLOCK_FlexComm0, kCLOCK_FlexComm1, kCLOCK_FlexComm2, kCLOCK_FlexComm3, kCLOCK_FlexComm4, kCLOCK_FlexComm5, \
kCLOCK_FlexComm6, kCLOCK_FlexComm7 \
}
Value:{ \
kCLOCK_MinUart0, kCLOCK_MinUart1, kCLOCK_MinUart2, kCLOCK_MinUart3, kCLOCK_MinUart4, kCLOCK_MinUart5, \
kCLOCK_MinUart6, kCLOCK_MinUart7 \
}
Value:{ \
kCLOCK_BI2c0, kCLOCK_BI2c1, kCLOCK_BI2c2, kCLOCK_BI2c3, kCLOCK_BI2c4, kCLOCK_BI2c5, kCLOCK_BI2c6, kCLOCK_BI2c7 \
}
Value:{ \
kCLOCK_LSpi0, kCLOCK_LSpi1, kCLOCK_LSpi2, kCLOCK_LSpi3, kCLOCK_LSpi4, kCLOCK_LSpi5, kCLOCK_LSpi6, kCLOCK_LSpi7 \
}
Value:{ \
kCLOCK_FlexI2s0, kCLOCK_FlexI2s1, kCLOCK_FlexI2s2, kCLOCK_FlexI2s3, kCLOCK_FlexI2s4, kCLOCK_FlexI2s5, \
kCLOCK_FlexI2s6, kCLOCK_FlexI2s7 \
}
Value:{ \
kCLOCK_Ct32b0, kCLOCK_Ct32b1, kCLOCK_Ct32b2, kCLOCK_Ct32b3, kCLOCK_Ct32b4 \
}
Value:{ \
kCLOCK_Gpio0, kCLOCK_Gpio1 \
}
Value:{ \
kCLOCK_Gint, kCLOCK_Gint \
}
GINT0 & GINT1 share same slot
| #define CLK_GATE_REG_OFFSET_SHIFT 8U |
| #define CLK_ATTACH_ID |
( |
|
mux, |
|
|
|
sel, |
|
|
|
pos |
|
) |
| ((((uint32_t)(mux) << 0U) | (((uint32_t)(sel) + 1UL) & 0xFU) << 8U) << ((pos)*12U)) |
[4 bits for choice, 0 means invalid choice] [8 bits mux ID]*
| #define PLL_CONFIGFLAG_USEINRATE (1U << 0U) |
When the PLL_CONFIGFLAG_USEINRATE flag is selected, the 'InputRate' field in the configuration structure must be assigned with the expected PLL frequency. If the PLL_CONFIGFLAG_USEINRATE is not used, 'InputRate' is ignored in the configuration function and the driver will determine the PLL rate from the currently selected PLL source. This flag might be used to configure the PLL input clock more accurately when using the WDT oscillator or a more dyanmic CLKIN source.
When the PLL_CONFIGFLAG_FORCENOFRACT flag is selected, the PLL hardware for the automatic bandwidth selection, Spread Spectrum (SS) support, and fractional M-divider are not used.
Flag to use InputRate in PLL configuration structure for setup
| #define PLL_SETUPFLAG_POWERUP (1U << 0U) |
Setup will power on the PLL after setup
| Enumerator |
|---|
| kCLOCK_CoreSysClk |
Core/system clock (aka MAIN_CLK)
|
| kCLOCK_BusClk |
Bus clock (AHB clock)
|
| kCLOCK_FroHf |
FRO48/96.
|
| kCLOCK_Fro12M |
FRO12M.
|
| kCLOCK_ExtClk |
External Clock.
|
| kCLOCK_PllOut |
PLL Output.
|
| kCLOCK_UsbClk |
USB input.
|
| kCLOCK_WdtOsc |
Watchdog Oscillator.
|
| kCLOCK_Frg |
Frg Clock.
|
| kCLOCK_AsyncApbClk |
Async APB clock.
|
| kCLOCK_FlexI2S |
FlexI2S clock.
|
Clock source selections for the asynchronous APB clock
| Enumerator |
|---|
| kCLOCK_AsyncMainClk |
Main System clock.
|
| kCLOCK_AsyncFro12Mhz |
12MHz FRO
|
| Enumerator |
|---|
| kCLOCK_Flash1Cycle |
Flash accesses use 1 CPU clock.
|
| kCLOCK_Flash2Cycle |
Flash accesses use 2 CPU clocks.
|
| kCLOCK_Flash3Cycle |
Flash accesses use 3 CPU clocks.
|
| kCLOCK_Flash4Cycle |
Flash accesses use 4 CPU clocks.
|
| kCLOCK_Flash5Cycle |
Flash accesses use 5 CPU clocks.
|
| kCLOCK_Flash6Cycle |
Flash accesses use 6 CPU clocks.
|
| kCLOCK_Flash7Cycle |
Flash accesses use 7 CPU clocks.
|
| Enumerator |
|---|
| kSS_MF_512 |
Nss = 512 (fm ? 3.9 - 7.8 kHz)
|
| kSS_MF_384 |
Nss ?= 384 (fm ? 5.2 - 10.4 kHz)
|
| kSS_MF_256 |
Nss = 256 (fm ? 7.8 - 15.6 kHz)
|
| kSS_MF_128 |
Nss = 128 (fm ? 15.6 - 31.3 kHz)
|
| kSS_MF_64 |
Nss = 64 (fm ? 32.3 - 64.5 kHz)
|
| kSS_MF_32 |
Nss = 32 (fm ? 62.5- 125 kHz)
|
| kSS_MF_24 |
Nss ?= 24 (fm ? 83.3- 166.6 kHz)
|
| kSS_MF_16 |
Nss = 16 (fm ? 125- 250 kHz)
|
| Enumerator |
|---|
| kSS_MR_K0 |
k = 0 (no spread spectrum)
|
| kSS_MR_K1 |
k = 1
|
| kSS_MR_K1_5 |
k = 1.5
|
| kSS_MR_K2 |
k = 2
|
| kSS_MR_K3 |
k = 3
|
| kSS_MR_K4 |
k = 4
|
| kSS_MR_K6 |
k = 6
|
| kSS_MR_K8 |
k = 8
|
Compensation for low pass filtering of the PLL to get a triangular modulation at the output of the PLL, giving a flat frequency spectrum.
| Enumerator |
|---|
| kSS_MC_NOC |
no compensation
|
| kSS_MC_RECC |
recommended setting
|
| kSS_MC_MAXC |
max.
compensation
|
| Enumerator |
|---|
| kStatus_PLL_Success |
PLL operation was successful.
|
| kStatus_PLL_OutputTooLow |
PLL output rate request was too low.
|
| kStatus_PLL_OutputTooHigh |
PLL output rate request was too high.
|
| kStatus_PLL_InputTooLow |
PLL input rate is too low.
|
| kStatus_PLL_InputTooHigh |
PLL input rate is too high.
|
| kStatus_PLL_OutsideIntLimit |
Requested output rate isn't possible.
|
| Enumerator |
|---|
| kCLOCK_UsbSrcFro |
Use FRO 96 or 48 MHz.
|
| kCLOCK_UsbSrcSystemPll |
Use System PLL output.
|
| kCLOCK_UsbSrcMainClock |
Use Main clock.
|
| kCLOCK_UsbSrcNone |
Use None, this may be selected in order to reduce power when no output is needed.
|
- Parameters
-
| clks | : Clock cycles for FLASH access |
- Returns
- Nothing
| status_t CLOCK_SetupFROClocking |
( |
uint32_t |
iFreq | ) |
|
- Parameters
-
| iFreq | : Desired frequency (must be one of CLK_FRO_12MHZ or CLK_FRO_48MHZ or CLK_FRO_96MHZ) |
- Returns
- returns success or fail status.
| void CLOCK_AttachClk |
( |
clock_attach_id_t |
connection | ) |
|
- Parameters
-
| connection | : Clock to be configured. |
- Returns
- Nothing
| clock_attach_id_t CLOCK_GetClockAttachId |
( |
clock_attach_id_t |
attachId | ) |
|
- Parameters
-
| attachId | : Clock attach id to get. |
- Returns
- Clock source value.
| void CLOCK_SetClkDiv |
( |
clock_div_name_t |
div_name, |
|
|
uint32_t |
divided_by_value, |
|
|
bool |
reset |
|
) |
| |
- Parameters
-
| div_name | : Clock divider name |
| divided_by_value,: | Value to be divided |
| reset | : Whether to reset the divider counter. |
- Returns
- Nothing
| void CLOCK_SetFLASHAccessCyclesForFreq |
( |
uint32_t |
iFreq | ) |
|
- Parameters
-
- Returns
- Nothing
- Returns
- Frequency of selected clock
| uint32_t CLOCK_GetFRGInputClock |
( |
void |
| ) |
|
- Returns
- Input Frequency for FRG
| uint32_t CLOCK_GetDmicClkFreq |
( |
void |
| ) |
|
- Returns
- Input Frequency for DMIC
| uint32_t CLOCK_GetFrgClkFreq |
( |
void |
| ) |
|
- Returns
- Input Frequency for FRG
| uint32_t CLOCK_SetFRGClock |
( |
uint32_t |
freq | ) |
|
- Parameters
-
| freq | : Desired output frequency |
- Returns
- Error Code 0 - fail 1 - success
| uint32_t CLOCK_GetFro12MFreq |
( |
void |
| ) |
|
- Returns
- Frequency of FRO 12MHz
| uint32_t CLOCK_GetExtClkFreq |
( |
void |
| ) |
|
- Returns
- Frequency of External Clock. If no external clock is used returns 0.
| uint32_t CLOCK_GetWdtOscFreq |
( |
void |
| ) |
|
- Returns
- Frequency of Watchdog Oscillator
| uint32_t CLOCK_GetFroHfFreq |
( |
void |
| ) |
|
- Returns
- Frequency of High-Freq output of FRO
| uint32_t CLOCK_GetUsbClkFreq |
( |
void |
| ) |
|
| uint32_t CLOCK_GetPllOutFreq |
( |
void |
| ) |
|
| uint32_t CLOCK_GetOsc32KFreq |
( |
void |
| ) |
|
- Returns
- Frequency of 32kHz osc
| uint32_t CLOCK_GetCoreSysClkFreq |
( |
void |
| ) |
|
- Returns
- Frequency of Core System
| uint32_t CLOCK_GetI2SMClkFreq |
( |
void |
| ) |
|
- Returns
- Frequency of I2S MCLK Clock
| uint32_t CLOCK_GetFlexCommClkFreq |
( |
uint32_t |
id | ) |
|
- Returns
- Frequency of Flexcomm functional Clock
| uint32_t CLOCK_GetAdcClkFreq |
( |
void |
| ) |
|
- Returns
- Frequency of Adc Clock.
- Returns
- Asynchronous APB CLock source
| uint32_t CLOCK_GetAsyncApbClkFreq |
( |
void |
| ) |
|
- Returns
- Frequency of Asynchronous APB Clock Clock
| uint32_t CLOCK_GetSystemPLLInClockRate |
( |
void |
| ) |
|
- Returns
- System PLL input clock rate
| uint32_t CLOCK_GetSystemPLLOutClockRate |
( |
bool |
recompute | ) |
|
- Parameters
-
| recompute | : Forces a PLL rate recomputation if true |
- Returns
- System PLL output clock rate
- Note
- The PLL rate is cached in the driver in a variable as the rate computation function can take some time to perform. It is recommended to use 'false' with the 'recompute' parameter.
| __STATIC_INLINE void CLOCK_SetBypassPLL |
( |
bool |
bypass | ) |
|
bypass : true to bypass PLL (PLL output = PLL input, false to disable bypass
- Returns
- System PLL output clock rate
| __STATIC_INLINE bool CLOCK_IsSystemPLLLocked |
( |
void |
| ) |
|
- Returns
- true if the PLL is locked, false if not locked
| void CLOCK_SetStoredPLLClockRate |
( |
uint32_t |
rate | ) |
|
- Parameters
-
| rate,: | Current rate of the PLL |
- Returns
- Nothing
| uint32_t CLOCK_GetSystemPLLOutFromSetup |
( |
pll_setup_t * |
pSetup | ) |
|
- Parameters
-
| pSetup | : Pointer to a PLL setup structure |
- Returns
- System PLL output clock rate calculated from the setup structure
- Parameters
-
| pControl | : Pointer to populated PLL control structure to generate setup with |
| pSetup | : Pointer to PLL setup structure to be filled |
- Returns
- PLL_ERROR_SUCCESS on success, or PLL setup error code
- Note
- Actual frequency for setup may vary from the desired frequency based on the accuracy of input clocks, rounding, non-fractional PLL mode, etc.
- Parameters
-
| pSetup | : Pointer to populated PLL setup structure |
| flagcfg | : Flag configuration for PLL config structure |
- Returns
- PLL_ERROR_SUCCESS on success, or PLL setup error code
- Note
- This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the PLL, wait for PLL lock, and adjust system voltages to the new PLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
- Parameters
-
| pSetup | : Pointer to populated PLL setup structure |
- Returns
- kStatus_PLL_Success on success, or PLL setup error code
- Note
- This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the PLL, wait for PLL lock, and adjust system voltages to the new PLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
| void CLOCK_SetupSystemPLLMult |
( |
uint32_t |
multiply_by, |
|
|
uint32_t |
input_freq |
|
) |
| |
- Parameters
-
| multiply_by | : multiplier |
| input_freq | : Clock input frequency of the PLL |
- Returns
- Nothing
- Note
- Unlike the Chip_Clock_SetupSystemPLLPrec() function, this function does not disable or enable PLL power, wait for PLL lock, or adjust system voltages. These must be done in the application. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
| static void CLOCK_DisableUsbfs0Clock |
( |
void |
| ) |
|
|
inlinestatic |