The MCUXpresso SDK provides a peripheral driver for the Flash Signature generator module of MCUXpresso SDK devices.
The flash module contains a built-in signature generator. This generator can produce a 128-bit signature from a range of flash memory. A typical usage is to verify the flashed contents against a calculated signature (for example, during programming). The signature generator can also be accessed via an IAP function call or ISP command.
Generate flash signature
-
FMC_GenerateFlashSignature() function generates flash signature for a specified address range.
This example code shows how to generate 128-bit flash signature using the FMC driver.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/fmc
This function initialize FMC module with user configuration
- Parameters
-
| base | The FMC peripheral base address. |
| config | pointer to user configuration structure. |
| void FMC_Deinit |
( |
FMC_Type * |
base | ) |
|
This function De-initialize FMC module.
- Parameters
-
| base | The FMC peripheral base address. |
This function provides default configuration for fmc module, the default wait states value is 5.
- Parameters
-
| config | pointer to user configuration structure. |
| void FMC_GenerateFlashSignature |
( |
FMC_Type * |
base, |
|
|
uint32_t |
startAddress, |
|
|
uint32_t |
length, |
|
|
fmc_flash_signature_t * |
flashSignature |
|
) |
| |
This function generates hardware flash signature for specified address range.
- Note
- This function needs to be excuted out of flash memory.
- Parameters
-
| base | The FMC peripheral base address. |
| startAddress | Flash start address for signature generation. |
| length | Length of address range. |
| flashSignature | Pointer which stores the generated flash signarue. |