![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | flexcan_edma_handle_t | 
| FlexCAN eDMA handle.  More... | |
Typedefs | |
| typedef void(* | flexcan_edma_transfer_callback_t )(CAN_Type *base, flexcan_edma_handle_t *handle, status_t status, void *userData) | 
| FlexCAN transfer callback function.  More... | |
Driver version | |
| #define | FSL_FLEXCAN_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 5, 0)) | 
| FlexCAN EDMA driver version 2.5.0.  More... | |
eDMA transactional | |
| void | FLEXCAN_TransferCreateHandleEDMA (CAN_Type *base, flexcan_edma_handle_t *handle, flexcan_edma_transfer_callback_t callback, void *userData, edma_handle_t *rxFifoEdmaHandle) | 
| Initializes the FlexCAN handle, which is used in transactional functions.  More... | |
| void | FLEXCAN_PrepareTransfConfiguration (CAN_Type *base, flexcan_fifo_transfer_t *pFifoXfer, edma_transfer_config_t *pEdmaConfig) | 
| Prepares the eDMA transfer configuration for FLEXCAN Legacy RX FIFO.  More... | |
| status_t | FLEXCAN_StartTransferDatafromRxFIFO (CAN_Type *base, flexcan_edma_handle_t *handle, edma_transfer_config_t *pEdmaConfig) | 
| Start Transfer Data from the FLEXCAN Legacy Rx FIFO using eDMA.  More... | |
| status_t | FLEXCAN_TransferReceiveFifoEDMA (CAN_Type *base, flexcan_edma_handle_t *handle, flexcan_fifo_transfer_t *pFifoXfer) | 
| Receives the CAN Message from the Rx FIFO using eDMA.  More... | |
| void | FLEXCAN_TransferAbortReceiveFifoEDMA (CAN_Type *base, flexcan_edma_handle_t *handle) | 
| Aborts the receive process which used eDMA.  More... | |
| struct _flexcan_edma_handle | 
Data Fields | |
| flexcan_edma_transfer_callback_t | callback | 
| Callback function.  More... | |
| void * | userData | 
| FlexCAN callback function parameter.  More... | |
| edma_handle_t * | rxFifoEdmaHandle | 
| The EDMA Rx FIFO channel used.  More... | |
| volatile uint8_t | rxFifoState | 
| Rx FIFO transfer state.  More... | |
| flexcan_edma_transfer_callback_t flexcan_edma_handle_t::callback | 
| void* flexcan_edma_handle_t::userData | 
| edma_handle_t* flexcan_edma_handle_t::rxFifoEdmaHandle | 
| volatile uint8_t flexcan_edma_handle_t::rxFifoState | 
| #define FSL_FLEXCAN_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 5, 0)) | 
| typedef void(* flexcan_edma_transfer_callback_t)(CAN_Type *base, flexcan_edma_handle_t *handle, status_t status, void *userData) | 
| void FLEXCAN_TransferCreateHandleEDMA | ( | CAN_Type * | base, | 
| flexcan_edma_handle_t * | handle, | ||
| flexcan_edma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | rxFifoEdmaHandle | ||
| ) | 
| base | FlexCAN peripheral base address. | 
| handle | Pointer to flexcan_edma_handle_t structure. | 
| callback | The callback function. | 
| userData | The parameter of the callback function. | 
| rxFifoEdmaHandle | User-requested DMA handle for Rx FIFO DMA transfer. | 
| void FLEXCAN_PrepareTransfConfiguration | ( | CAN_Type * | base, | 
| flexcan_fifo_transfer_t * | pFifoXfer, | ||
| edma_transfer_config_t * | pEdmaConfig | ||
| ) | 
This function prepares the eDMA transfer configuration structure according to FLEXCAN Legacy RX FIFO.
| base | FlexCAN peripheral base address. | 
| pFifoXfer | FlexCAN Rx FIFO EDMA transfer structure, see flexcan_fifo_transfer_t. | 
| pEdmaConfig | The user configuration structure of type edma_transfer_t. | 
| status_t FLEXCAN_StartTransferDatafromRxFIFO | ( | CAN_Type * | base, | 
| flexcan_edma_handle_t * | handle, | ||
| edma_transfer_config_t * | pEdmaConfig | ||
| ) | 
This function to Update edma transfer confiugration and Start eDMA transfer
| base | FlexCAN peripheral base address. | 
| handle | Pointer to flexcan_edma_handle_t structure. | 
| pEdmaConfig | The user configuration structure of type edma_transfer_t. | 
| kStatus_Success | if succeed, others failed. | 
| kStatus_FLEXCAN_RxFifoBusy | Previous transfer ongoing. | 
| status_t FLEXCAN_TransferReceiveFifoEDMA | ( | CAN_Type * | base, | 
| flexcan_edma_handle_t * | handle, | ||
| flexcan_fifo_transfer_t * | pFifoXfer | ||
| ) | 
This function receives the CAN Message using eDMA. This is a non-blocking function, which returns right away. After the CAN Message is received, the receive callback function is called.
| base | FlexCAN peripheral base address. | 
| handle | Pointer to flexcan_edma_handle_t structure. | 
| pFifoXfer | FlexCAN Rx FIFO EDMA transfer structure, see flexcan_fifo_transfer_t. | 
| kStatus_Success | if succeed, others failed. | 
| kStatus_FLEXCAN_RxFifoBusy | Previous transfer ongoing. | 
| void FLEXCAN_TransferAbortReceiveFifoEDMA | ( | CAN_Type * | base, | 
| flexcan_edma_handle_t * | handle | ||
| ) | 
This function aborts the receive process which used eDMA.
| base | FlexCAN peripheral base address. | 
| handle | Pointer to flexcan_edma_handle_t structure. |