The MCUXpresso SDK provides a peripheral driver for the General-Purpose Input/Output (GPIO) module of MCUXpresso SDK devices.
Typical use case
Output Operation
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/gpio 
Input Operation
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/gpio 
 | 
| static void  | GPIO_PinWrite (GPIO_Type *base, uint32_t pin, uint8_t output) | 
|   | Sets the output level of the multiple GPIO pins to the logic 1 or 0.  More...
  | 
|   | 
| static void  | GPIO_PortSet (GPIO_Type *base, uint32_t mask) | 
|   | Sets the output level of the multiple GPIO pins to the logic 1.  More...
  | 
|   | 
| static void  | GPIO_PortClear (GPIO_Type *base, uint32_t mask) | 
|   | Sets the output level of the multiple GPIO pins to the logic 0.  More...
  | 
|   | 
| static void  | GPIO_PortToggle (GPIO_Type *base, uint32_t mask) | 
|   | Reverses the current output logic of the multiple GPIO pins.  More...
  | 
|   | 
 | 
| static uint32_t  | GPIO_PinRead (GPIO_Type *base, uint32_t pin) | 
|   | Reads the current input value of the GPIO port.  More...
  | 
|   | 
      
        
          | void GPIO_PinInit  | 
          ( | 
          GPIO_Type *  | 
          base,  | 
        
        
           | 
           | 
          uint32_t  | 
          pin,  | 
        
        
           | 
           | 
          const gpio_pin_config_t *  | 
          config  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
To initialize the GPIO, define a pin configuration, as either input or output, in the user file. Then, call the GPIO_PinInit() function.
This is an example to define an input pin or an output pin configuration. 
* Define a digital input pin configuration,
* {
*   0,
* }
* Define a digital output pin configuration,
* {
*   0,
* }
* 
- Parameters
 - 
  
    | base | GPIO peripheral base pointer (GPIOA, GPIOB, GPIOC, and so on.)  | 
    | pin | GPIO port pin number  | 
    | config | GPIO pin configuration pointer  | 
  
   
 
 
  
  
      
        
          | static void GPIO_PinWrite  | 
          ( | 
          GPIO_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          pin,  | 
         
        
           | 
           | 
          uint8_t  | 
          output  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
- Parameters
 - 
  
    | base | GPIO peripheral base pointer (GPIOA, GPIOB, GPIOC, and so on.)  | 
    | pin | GPIO pin number  | 
    | output | GPIO pin output logic level.
- 0: corresponding pin output low-logic level.
 
- 1: corresponding pin output high-logic level. 
 
 
 | 
  
   
 
 
  
  
      
        
          | static void GPIO_PortSet  | 
          ( | 
          GPIO_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          mask  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
- Parameters
 - 
  
    | base | GPIO peripheral base pointer (GPIOA, GPIOB, GPIOC, and so on.)  | 
    | mask | GPIO pin number macro  | 
  
   
 
 
  
  
      
        
          | static void GPIO_PortClear  | 
          ( | 
          GPIO_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          mask  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
- Parameters
 - 
  
    | base | GPIO peripheral base pointer (GPIOA, GPIOB, GPIOC, and so on.)  | 
    | mask | GPIO pin number macro  | 
  
   
 
 
  
  
      
        
          | static void GPIO_PortToggle  | 
          ( | 
          GPIO_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          mask  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
- Parameters
 - 
  
    | base | GPIO peripheral base pointer (GPIOA, GPIOB, GPIOC, and so on.)  | 
    | mask | GPIO pin number macro  | 
  
   
 
 
  
  
      
        
          | static uint32_t GPIO_PinRead  | 
          ( | 
          GPIO_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          pin  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
- Parameters
 - 
  
    | base | GPIO peripheral base pointer (GPIOA, GPIOB, GPIOC, and so on.)  | 
    | pin | GPIO pin number  | 
  
   
- Return values
 - 
  
    | GPIO | port input value
- 0: corresponding pin input low-logic level.
 
- 1: corresponding pin input high-logic level. 
 
 
 | 
  
   
 
 
      
        
          | uint32_t GPIO_PortGetInterruptFlags  | 
          ( | 
          GPIO_Type *  | 
          base | ) | 
           | 
        
      
 
If a pin is configured to generate the DMA request, the corresponding flag is cleared automatically at the completion of the requested DMA transfer. Otherwise, the flag remains set until a logic one is written to that flag. If configured for a level sensitive interrupt that remains asserted, the flag is set again immediately.
- Parameters
 - 
  
    | base | GPIO peripheral base pointer (GPIOA, GPIOB, GPIOC, and so on.)  | 
  
   
- Return values
 - 
  
    | The | current GPIO port interrupt status flag, for example, 0x00010001 means the pin 0 and 17 have the interrupt.  | 
  
   
 
 
      
        
          | void GPIO_PortClearInterruptFlags  | 
          ( | 
          GPIO_Type *  | 
          base,  | 
        
        
           | 
           | 
          uint32_t  | 
          mask  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | base | GPIO peripheral base pointer (GPIOA, GPIOB, GPIOC, and so on.)  | 
    | mask | GPIO pin number macro  |