![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the Reset Control Module (RCM) module of MCUXpresso SDK devices.
Data Structures | |
struct | rcm_reset_pin_filter_config_t |
Reset pin filter configuration. More... | |
Enumerations | |
enum | rcm_reset_source_t { kRCM_SourceWakeup = RCM_SRS0_WAKEUP_MASK, kRCM_SourceLvd = RCM_SRS0_LVD_MASK, kRCM_SourceLoc = RCM_SRS0_LOC_MASK, kRCM_SourceWdog = RCM_SRS0_WDOG_MASK, kRCM_SourcePin = RCM_SRS0_PIN_MASK, kRCM_SourcePor = RCM_SRS0_POR_MASK, kRCM_SourceLockup = RCM_SRS1_LOCKUP_MASK << 8U, kRCM_SourceSw = RCM_SRS1_SW_MASK << 8U, kRCM_SourceMdmap = RCM_SRS1_MDM_AP_MASK << 8U, kRCM_SourceSackerr = RCM_SRS1_SACKERR_MASK << 8U } |
System Reset Source Name definitions. More... | |
enum | rcm_run_wait_filter_mode_t { kRCM_FilterDisable = 0U, kRCM_FilterBusClock = 1U, kRCM_FilterLpoClock = 2U } |
Reset pin filter select in Run and Wait modes. More... | |
Driver version | |
#define | FSL_RCM_DRIVER_VERSION (MAKE_VERSION(2, 0, 3)) |
RCM driver version 2.0.3. More... | |
Reset Control Module APIs | |
static uint32_t | RCM_GetPreviousResetSources (RCM_Type *base) |
Gets the reset source status which caused a previous reset. More... | |
void | RCM_ConfigureResetPinFilter (RCM_Type *base, const rcm_reset_pin_filter_config_t *config) |
Configures the reset pin filter. More... | |
struct rcm_reset_pin_filter_config_t |
Data Fields | |
bool | enableFilterInStop |
Reset pin filter select in stop mode. More... | |
rcm_run_wait_filter_mode_t | filterInRunWait |
Reset pin filter in run/wait mode. More... | |
uint8_t | busClockFilterCount |
Reset pin bus clock filter width. More... | |
bool rcm_reset_pin_filter_config_t::enableFilterInStop |
rcm_run_wait_filter_mode_t rcm_reset_pin_filter_config_t::filterInRunWait |
uint8_t rcm_reset_pin_filter_config_t::busClockFilterCount |
#define FSL_RCM_DRIVER_VERSION (MAKE_VERSION(2, 0, 3)) |
enum rcm_reset_source_t |
|
inlinestatic |
This function gets the current reset source status. Use source masks defined in the rcm_reset_source_t to get the desired source status.
This is an example.
base | RCM peripheral base address. |
void RCM_ConfigureResetPinFilter | ( | RCM_Type * | base, |
const rcm_reset_pin_filter_config_t * | config | ||
) |
This function sets the reset pin filter including the filter source, filter width, and so on.
base | RCM peripheral base address. |
config | Pointer to the configuration structure. |