MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
SDMA: Smart Direct Memory Access (SDMA) Controller Driver

Overview

The MCUXpresso SDK provides a peripheral driver for the Smart Direct Memory Access (SDMA) of devices.

Typical use case

SDMA Operation

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/sdma

Data Structures

struct  sdma_config_t
 SDMA global configuration structure. More...
 
struct  sdma_multi_fifo_config_t
 SDMA multi fifo configurations. More...
 
struct  sdma_sw_done_config_t
 SDMA sw done configurations. More...
 
struct  sdma_p2p_config_t
 SDMA peripheral to peripheral R7 config. More...
 
struct  sdma_transfer_config_t
 SDMA transfer configuration. More...
 
struct  sdma_buffer_descriptor_t
 SDMA buffer descriptor structure. More...
 
struct  sdma_channel_control_t
 SDMA channel control descriptor structure. More...
 
struct  sdma_context_data_t
 SDMA context structure for each channel. More...
 
struct  sdma_handle_t
 SDMA transfer handle structure. More...
 

Typedefs

typedef void(* sdma_callback )(struct _sdma_handle *handle, void *userData, bool transferDone, uint32_t bdIndex)
 Define callback function for SDMA. More...
 

Enumerations

enum  sdma_transfer_size_t {
  kSDMA_TransferSize1Bytes = 0x1U,
  kSDMA_TransferSize2Bytes = 0x2U,
  kSDMA_TransferSize3Bytes = 0x3U,
  kSDMA_TransferSize4Bytes = 0x0U
}
 SDMA transfer configuration. More...
 
enum  sdma_bd_status_t {
  kSDMA_BDStatusDone = 0x1U,
  kSDMA_BDStatusWrap = 0x2U,
  kSDMA_BDStatusContinuous = 0x4U,
  kSDMA_BDStatusInterrupt = 0x8U,
  kSDMA_BDStatusError = 0x10U,
  kSDMA_BDStatusLast,
  kSDMA_BDStatusExtend = 0x80U
}
 SDMA buffer descriptor status. More...
 
enum  sdma_bd_command_t {
  kSDMA_BDCommandSETDM = 0x1U,
  kSDMA_BDCommandGETDM = 0x2U,
  kSDMA_BDCommandSETPM = 0x4U,
  kSDMA_BDCommandGETPM = 0x6U,
  kSDMA_BDCommandSETCTX = 0x7U,
  kSDMA_BDCommandGETCTX = 0x3U
}
 SDMA buffer descriptor command. More...
 
enum  sdma_context_switch_mode_t {
  kSDMA_ContextSwitchModeStatic = 0x0U,
  kSDMA_ContextSwitchModeDynamicLowPower,
  kSDMA_ContextSwitchModeDynamicWithNoLoop,
  kSDMA_ContextSwitchModeDynamic
}
 SDMA context switch mode. More...
 
enum  sdma_clock_ratio_t {
  kSDMA_HalfARMClockFreq = 0x0U,
  kSDMA_ARMClockFreq
}
 SDMA core clock frequency ratio to the ARM DMA interface. More...
 
enum  sdma_transfer_type_t {
  kSDMA_MemoryToMemory = 0x0U,
  kSDMA_PeripheralToMemory,
  kSDMA_MemoryToPeripheral,
  kSDMA_PeripheralToPeripheral
}
 SDMA transfer type. More...
 
enum  sdma_peripheral_t {
  kSDMA_PeripheralTypeMemory = 0x0,
  kSDMA_PeripheralTypeUART,
  kSDMA_PeripheralTypeUART_SP,
  kSDMA_PeripheralTypeSPDIF,
  kSDMA_PeripheralNormal,
  kSDMA_PeripheralNormal_SP,
  kSDMA_PeripheralMultiFifoPDM,
  kSDMA_PeripheralMultiFifoSaiRX,
  kSDMA_PeripheralMultiFifoSaiTX,
  kSDMA_PeripheralASRCM2P,
  kSDMA_PeripheralASRCP2M,
  kSDMA_PeripheralASRCP2P
}
 Peripheral type use SDMA. More...
 
enum  {
  kStatus_SDMA_ERROR = MAKE_STATUS(kStatusGroup_SDMA, 0),
  kStatus_SDMA_Busy = MAKE_STATUS(kStatusGroup_SDMA, 1)
}
 _sdma_transfer_status SDMA transfer status More...
 
enum  {
  kSDMA_MultiFifoWatermarkLevelMask = 0xFFFU,
  kSDMA_MultiFifoNumsMask = 0xFU,
  kSDMA_MultiFifoOffsetMask = 0xFU,
  kSDMA_MultiFifoSwDoneMask = 0x1U,
  kSDMA_MultiFifoSwDoneSelectorMask = 0xFU
}
 _sdma_multi_fifo_mask SDMA multi fifo mask More...
 
enum  {
  kSDMA_MultiFifoWatermarkLevelShift = 0U,
  kSDMA_MultiFifoNumsShift = 12U,
  kSDMA_MultiFifoOffsetShift = 16U,
  kSDMA_MultiFifoSwDoneShift = 23U,
  kSDMA_MultiFifoSwDoneSelectorShift = 24U
}
 _sdma_multi_fifo_shift SDMA multi fifo shift More...
 
enum  {
  kSDMA_DoneChannel0 = 0U,
  kSDMA_DoneChannel1 = 1U,
  kSDMA_DoneChannel2 = 2U,
  kSDMA_DoneChannel3 = 3U,
  kSDMA_DoneChannel4 = 4U,
  kSDMA_DoneChannel5 = 5U,
  kSDMA_DoneChannel6 = 6U,
  kSDMA_DoneChannel7 = 7U
}
 _sdma_done_channel SDMA done channel More...
 
enum  sdma_done_src_t {
  kSDMA_DoneSrcSW = 0U,
  kSDMA_DoneSrcHwEvent0U = 1U,
  kSDMA_DoneSrcHwEvent1U = 2U,
  kSDMA_DoneSrcHwEvent2U = 3U,
  kSDMA_DoneSrcHwEvent3U = 4U,
  kSDMA_DoneSrcHwEvent4U = 5U,
  kSDMA_DoneSrcHwEvent5U = 6U,
  kSDMA_DoneSrCHwEvent6U = 7U,
  kSDMA_DoneSrcHwEvent7U = 8U,
  kSDMA_DoneSrcHwEvent8U = 9U,
  kSDMA_DoneSrcHwEvent9U = 10U,
  kSDMA_DoneSrcHwEvent10U = 11U,
  kSDMA_DoneSrcHwEvent11U = 12U,
  kSDMA_DoneSrcHwEvent12U = 13U,
  kSDMA_DoneSrcHwEvent13U = 14U,
  kSDMA_DoneSrcHwEvent14U = 15U,
  kSDMA_DoneSrcHwEvent15U = 16U,
  kSDMA_DoneSrcHwEvent16U = 17U,
  kSDMA_DoneSrcHwEvent17U = 18U,
  kSDMA_DoneSrcHwEvent18U = 19U,
  kSDMA_DoneSrcHwEvent19U = 20U,
  kSDMA_DoneSrcHwEvent20U = 21U,
  kSDMA_DoneSrcHwEvent21U = 22U,
  kSDMA_DoneSrcHwEvent22U = 23U,
  kSDMA_DoneSrcHwEvent23U = 24U,
  kSDMA_DoneSrcHwEvent24U = 25U,
  kSDMA_DoneSrcHwEvent25U = 26U,
  kSDMA_DoneSrcHwEvent26U = 27U,
  kSDMA_DoneSrcHwEvent27U = 28U,
  kSDMA_DoneSrcHwEvent28U = 29U,
  kSDMA_DoneSrcHwEvent29U = 30U,
  kSDMA_DoneSrcHwEvent30U = 31U,
  kSDMA_DoneSrcHwEvent31U = 32U
}
 SDMA done source. More...
 

Driver version

#define FSL_SDMA_DRIVER_VERSION   (MAKE_VERSION(2, 3, 0))
 SDMA driver version. More...
 

SDMA initialization and de-initialization

void SDMA_Init (SDMAARM_Type *base, const sdma_config_t *config)
 Initializes the SDMA peripheral. More...
 
void SDMA_Deinit (SDMAARM_Type *base)
 Deinitializes the SDMA peripheral. More...
 
void SDMA_GetDefaultConfig (sdma_config_t *config)
 Gets the SDMA default configuration structure. More...
 
void SDMA_ResetModule (SDMAARM_Type *base)
 Sets all SDMA core register to reset status. More...
 

SDMA Channel Operation

static void SDMA_EnableChannelErrorInterrupts (SDMAARM_Type *base, uint32_t channel)
 Enables the interrupt source for the SDMA error. More...
 
static void SDMA_DisableChannelErrorInterrupts (SDMAARM_Type *base, uint32_t channel)
 Disables the interrupt source for the SDMA error. More...
 

SDMA Buffer Descriptor Operation

void SDMA_ConfigBufferDescriptor (sdma_buffer_descriptor_t *bd, uint32_t srcAddr, uint32_t destAddr, sdma_transfer_size_t busWidth, size_t bufferSize, bool isLast, bool enableInterrupt, bool isWrap, sdma_transfer_type_t type)
 Sets buffer descriptor contents. More...
 

SDMA Channel Transfer Operation

static void SDMA_SetChannelPriority (SDMAARM_Type *base, uint32_t channel, uint8_t priority)
 Set SDMA channel priority. More...
 
static void SDMA_SetSourceChannel (SDMAARM_Type *base, uint32_t source, uint32_t channelMask)
 Set SDMA request source mapping channel. More...
 
static void SDMA_StartChannelSoftware (SDMAARM_Type *base, uint32_t channel)
 Start a SDMA channel by software trigger. More...
 
static void SDMA_StartChannelEvents (SDMAARM_Type *base, uint32_t channel)
 Start a SDMA channel by hardware events. More...
 
static void SDMA_StopChannel (SDMAARM_Type *base, uint32_t channel)
 Stop a SDMA channel. More...
 
void SDMA_SetContextSwitchMode (SDMAARM_Type *base, sdma_context_switch_mode_t mode)
 Set the SDMA context switch mode. More...
 

SDMA Channel Status Operation

static uint32_t SDMA_GetChannelInterruptStatus (SDMAARM_Type *base)
 Gets the SDMA interrupt status of all channels. More...
 
static void SDMA_ClearChannelInterruptStatus (SDMAARM_Type *base, uint32_t mask)
 Clear the SDMA channel interrupt status of specific channels. More...
 
static uint32_t SDMA_GetChannelStopStatus (SDMAARM_Type *base)
 Gets the SDMA stop status of all channels. More...
 
static void SDMA_ClearChannelStopStatus (SDMAARM_Type *base, uint32_t mask)
 Clear the SDMA channel stop status of specific channels. More...
 
static uint32_t SDMA_GetChannelPendStatus (SDMAARM_Type *base)
 Gets the SDMA channel pending status of all channels. More...
 
static void SDMA_ClearChannelPendStatus (SDMAARM_Type *base, uint32_t mask)
 Clear the SDMA channel pending status of specific channels. More...
 
static uint32_t SDMA_GetErrorStatus (SDMAARM_Type *base)
 Gets the SDMA channel error status. More...
 
bool SDMA_GetRequestSourceStatus (SDMAARM_Type *base, uint32_t source)
 Gets the SDMA request source pending status. More...
 

SDMA Transactional Operation

void SDMA_CreateHandle (sdma_handle_t *handle, SDMAARM_Type *base, uint32_t channel, sdma_context_data_t *context)
 Creates the SDMA handle. More...
 
void SDMA_InstallBDMemory (sdma_handle_t *handle, sdma_buffer_descriptor_t *BDPool, uint32_t BDCount)
 Installs the BDs memory pool into the SDMA handle. More...
 
void SDMA_SetCallback (sdma_handle_t *handle, sdma_callback callback, void *userData)
 Installs a callback function for the SDMA transfer. More...
 
void SDMA_SetMultiFifoConfig (sdma_transfer_config_t *config, uint32_t fifoNums, uint32_t fifoOffset)
 multi fifo configurations. More...
 
void SDMA_EnableSwDone (SDMAARM_Type *base, sdma_transfer_config_t *config, uint8_t sel, sdma_peripheral_t type)
 enable sdma sw done feature. More...
 
void SDMA_SetDoneConfig (SDMAARM_Type *base, sdma_transfer_config_t *config, sdma_peripheral_t type, sdma_done_src_t doneSrc)
 sdma channel done configurations. More...
 
void SDMA_LoadScript (SDMAARM_Type *base, uint32_t destAddr, void *srcAddr, size_t bufferSizeBytes)
 load script to sdma program memory. More...
 
void SDMA_DumpScript (SDMAARM_Type *base, uint32_t srcAddr, void *destAddr, size_t bufferSizeBytes)
 dump script from sdma program memory. More...
 
void SDMA_PrepareTransfer (sdma_transfer_config_t *config, uint32_t srcAddr, uint32_t destAddr, uint32_t srcWidth, uint32_t destWidth, uint32_t bytesEachRequest, uint32_t transferSize, uint32_t eventSource, sdma_peripheral_t peripheral, sdma_transfer_type_t type)
 Prepares the SDMA transfer structure. More...
 
void SDMA_PrepareP2PTransfer (sdma_transfer_config_t *config, uint32_t srcAddr, uint32_t destAddr, uint32_t srcWidth, uint32_t destWidth, uint32_t bytesEachRequest, uint32_t transferSize, uint32_t eventSource, uint32_t eventSource1, sdma_peripheral_t peripheral, sdma_p2p_config_t *p2p)
 Prepares the SDMA P2P transfer structure. More...
 
void SDMA_SubmitTransfer (sdma_handle_t *handle, const sdma_transfer_config_t *config)
 Submits the SDMA transfer request. More...
 
void SDMA_StartTransfer (sdma_handle_t *handle)
 SDMA starts transfer. More...
 
void SDMA_StopTransfer (sdma_handle_t *handle)
 SDMA stops transfer. More...
 
void SDMA_AbortTransfer (sdma_handle_t *handle)
 SDMA aborts transfer. More...
 
uint32_t SDMA_GetTransferredBytes (sdma_handle_t *handle)
 Get transferred bytes while not using BD pools. More...
 
bool SDMA_IsPeripheralInSPBA (uint32_t addr)
 Judge if address located in SPBA. More...
 
void SDMA_HandleIRQ (sdma_handle_t *handle)
 SDMA IRQ handler for complete a buffer descriptor transfer. More...
 

Data Structure Documentation

struct sdma_config_t

Data Fields

bool enableRealTimeDebugPin
 If enable real-time debug pin, default is closed to reduce power consumption. More...
 
bool isSoftwareResetClearLock
 If software reset clears the LOCK bit which prevent writing SDMA scripts into SDMA. More...
 
sdma_clock_ratio_t ratio
 SDMA core clock ratio to ARM platform DMA interface.
 

Field Documentation

bool sdma_config_t::enableRealTimeDebugPin
bool sdma_config_t::isSoftwareResetClearLock
struct sdma_multi_fifo_config_t

Data Fields

uint8_t fifoNums
 fifo numbers
 
uint8_t fifoOffset
 offset between multi fifo data register address
 
struct sdma_sw_done_config_t

Data Fields

bool enableSwDone
 true is enable sw done, false is disable
 
uint8_t swDoneSel
 sw done channel number per peripheral type
 
struct sdma_p2p_config_t

Data Fields

uint8_t sourceWatermark
 lower watermark value
 
uint8_t destWatermark
 higher water makr value
 
bool continuousTransfer
 0: the amount of samples to be transferred is equal to the cont field of mode word 1: the amount of samples to be transferred is unknown and script will keep on transferring as long as both events are detected and script must be stopped by application. More...
 

Field Documentation

bool sdma_p2p_config_t::continuousTransfer
struct sdma_transfer_config_t

This structure configures the source/destination transfer attribute.

Data Fields

uint32_t srcAddr
 Source address of the transfer.
 
uint32_t destAddr
 Destination address of the transfer.
 
sdma_transfer_size_t srcTransferSize
 Source data transfer size. More...
 
sdma_transfer_size_t destTransferSize
 Destination data transfer size. More...
 
uint32_t bytesPerRequest
 Bytes to transfer in a minor loop.
 
uint32_t transferSzie
 Bytes to transfer for this descriptor.
 
uint32_t scriptAddr
 SDMA script address located in SDMA ROM. More...
 
uint32_t eventSource
 Event source number for the channel. More...
 
uint32_t eventSource1
 event source 1
 
bool isEventIgnore
 True means software trigger, false means hardware trigger.
 
bool isSoftTriggerIgnore
 If ignore the HE bit, 1 means use hardware events trigger, 0 means software trigger.
 
sdma_transfer_type_t type
 Transfer type, transfer type used to decide the SDMA script. More...
 
sdma_multi_fifo_config_t multiFifo
 multi fifo configurations
 
sdma_sw_done_config_t swDone
 sw done selector
 
uint32_t watermarkLevel
 watermark level
 
uint32_t eventMask0
 event mask 0
 
uint32_t eventMask1
 event mask 1
 

Field Documentation

sdma_transfer_size_t sdma_transfer_config_t::srcTransferSize
sdma_transfer_size_t sdma_transfer_config_t::destTransferSize
uint32_t sdma_transfer_config_t::scriptAddr
uint32_t sdma_transfer_config_t::eventSource

0 means no event, use software trigger

sdma_transfer_type_t sdma_transfer_config_t::type
struct sdma_buffer_descriptor_t

This structure is a buffer descriptor, this structure describes the buffer start address and other options

Data Fields

uint32_t count: 16
 Bytes of the buffer length for this buffer descriptor. More...
 
uint32_t status: 8
 E,R,I,C,W,D status bits stored here.
 
uint32_t command: 8
 command mostlky used for channel 0
 
uint32_t bufferAddr
 Buffer start address for this descriptor. More...
 
uint32_t extendBufferAddr
 External buffer start address, this is an optional for a transfer. More...
 

Field Documentation

uint32_t sdma_buffer_descriptor_t::count
uint32_t sdma_buffer_descriptor_t::bufferAddr
uint32_t sdma_buffer_descriptor_t::extendBufferAddr
struct sdma_channel_control_t

Data Fields

uint32_t currentBDAddr
 Address of current buffer descriptor processed.
 
uint32_t baseBDAddr
 The start address of the buffer descriptor array.
 
uint32_t channelDesc
 Optional for transfer.
 
uint32_t status
 Channel status.
 
struct sdma_context_data_t

This structure can be load into SDMA core, with this structure, SDMA scripts can start work.

Data Fields

uint32_t GeneralReg [8]
 8 general regsiters used for SDMA RISC core
 
struct sdma_handle_t

Data Fields

sdma_callback callback
 Callback function for major count exhausted. More...
 
void * userData
 Callback function parameter. More...
 
SDMAARM_Type * base
 SDMA peripheral base address. More...
 
sdma_buffer_descriptor_t * BDPool
 Pointer to memory stored BD arrays. More...
 
uint32_t bdCount
 How many buffer descriptor.
 
uint32_t bdIndex
 How many buffer descriptor.
 
uint32_t eventSource
 Event source count for the channel.
 
uint32_t eventSource1
 Event source 1 count for the channel.
 
sdma_context_data_t * context
 Channel context to exectute in SDMA.
 
uint8_t channel
 SDMA channel number. More...
 
uint8_t priority
 SDMA channel priority.
 
uint8_t flags
 The status of the current channel. More...
 

Field Documentation

sdma_callback sdma_handle_t::callback
void* sdma_handle_t::userData
SDMAARM_Type* sdma_handle_t::base
sdma_buffer_descriptor_t* sdma_handle_t::BDPool
uint8_t sdma_handle_t::channel
uint8_t sdma_handle_t::flags

Macro Definition Documentation

#define FSL_SDMA_DRIVER_VERSION   (MAKE_VERSION(2, 3, 0))

Version 2.3.0.

Typedef Documentation

typedef void(* sdma_callback)(struct _sdma_handle *handle, void *userData, bool transferDone, uint32_t bdIndex)

Enumeration Type Documentation

Enumerator
kSDMA_TransferSize1Bytes 

Source/Destination data transfer size is 1 byte every time.

kSDMA_TransferSize2Bytes 

Source/Destination data transfer size is 2 bytes every time.

kSDMA_TransferSize3Bytes 

Source/Destination data transfer size is 3 bytes every time.

kSDMA_TransferSize4Bytes 

Source/Destination data transfer size is 4 bytes every time.

Enumerator
kSDMA_BDStatusDone 

BD ownership, 0 means ARM core owns the BD, while 1 means SDMA owns BD.

kSDMA_BDStatusWrap 

While this BD is last one, the next BD will be the first one.

kSDMA_BDStatusContinuous 

Buffer is allowed to transfer/receive to/from multiple buffers.

kSDMA_BDStatusInterrupt 

While this BD finished, send an interrupt.

kSDMA_BDStatusError 

Error occurred on buffer descriptor command.

kSDMA_BDStatusLast 

This BD is the last BD in this array.

It means the transfer ended after this buffer

kSDMA_BDStatusExtend 

Buffer descriptor extend status for SDMA scripts.

Enumerator
kSDMA_BDCommandSETDM 

Load SDMA data memory from ARM core memory buffer.

kSDMA_BDCommandGETDM 

Copy SDMA data memory to ARM core memory buffer.

kSDMA_BDCommandSETPM 

Load SDMA program memory from ARM core memory buffer.

kSDMA_BDCommandGETPM 

Copy SDMA program memory to ARM core memory buffer.

kSDMA_BDCommandSETCTX 

Load context for one channel into SDMA RAM from ARM platform memory buffer.

kSDMA_BDCommandGETCTX 

Copy context for one channel from SDMA RAM to ARM platform memory buffer.

Enumerator
kSDMA_ContextSwitchModeStatic 

SDMA context switch mode static.

kSDMA_ContextSwitchModeDynamicLowPower 

SDMA context switch mode dynamic with low power.

kSDMA_ContextSwitchModeDynamicWithNoLoop 

SDMA context switch mode dynamic with no loop.

kSDMA_ContextSwitchModeDynamic 

SDMA context switch mode dynamic.

Enumerator
kSDMA_HalfARMClockFreq 

SDMA core clock frequency half of ARM platform.

kSDMA_ARMClockFreq 

SDMA core clock frequency equals to ARM platform.

Enumerator
kSDMA_MemoryToMemory 

Transfer from memory to memory.

kSDMA_PeripheralToMemory 

Transfer from peripheral to memory.

kSDMA_MemoryToPeripheral 

Transfer from memory to peripheral.

kSDMA_PeripheralToPeripheral 

Transfer from peripheral to peripheral.

Enumerator
kSDMA_PeripheralTypeMemory 

Peripheral DDR memory.

kSDMA_PeripheralTypeUART 

UART use SDMA.

kSDMA_PeripheralTypeUART_SP 

UART instance in SPBA use SDMA.

kSDMA_PeripheralTypeSPDIF 

SPDIF use SDMA.

kSDMA_PeripheralNormal 

Normal peripheral use SDMA.

kSDMA_PeripheralNormal_SP 

Normal peripheral in SPBA use SDMA.

kSDMA_PeripheralMultiFifoPDM 

multi fifo PDM

kSDMA_PeripheralMultiFifoSaiRX 

multi fifo sai rx use SDMA

kSDMA_PeripheralMultiFifoSaiTX 

multi fifo sai tx use SDMA

kSDMA_PeripheralASRCM2P 

asrc m2p

kSDMA_PeripheralASRCP2M 

asrc p2m

kSDMA_PeripheralASRCP2P 

asrc p2p

anonymous enum
Enumerator
kStatus_SDMA_ERROR 

SDMA context error.

kStatus_SDMA_Busy 

Channel is busy and can't handle the transfer request.

anonymous enum
Enumerator
kSDMA_MultiFifoWatermarkLevelMask 

multi fifo watermark level mask

kSDMA_MultiFifoNumsMask 

multi fifo nums mask

kSDMA_MultiFifoOffsetMask 

multi fifo offset mask

kSDMA_MultiFifoSwDoneMask 

multi fifo sw done mask

kSDMA_MultiFifoSwDoneSelectorMask 

multi fifo sw done selector mask

anonymous enum
Enumerator
kSDMA_MultiFifoWatermarkLevelShift 

multi fifo watermark level shift

kSDMA_MultiFifoNumsShift 

multi fifo nums shift

kSDMA_MultiFifoOffsetShift 

multi fifo offset shift

kSDMA_MultiFifoSwDoneShift 

multi fifo sw done shift

kSDMA_MultiFifoSwDoneSelectorShift 

multi fifo sw done selector shift

anonymous enum
Enumerator
kSDMA_DoneChannel0 

SDMA done channel 0.

kSDMA_DoneChannel1 

SDMA done channel 1.

kSDMA_DoneChannel2 

SDMA done channel 2.

kSDMA_DoneChannel3 

SDMA done channel 3.

kSDMA_DoneChannel4 

SDMA done channel 4.

kSDMA_DoneChannel5 

SDMA done channel 5.

kSDMA_DoneChannel6 

SDMA done channel 6.

kSDMA_DoneChannel7 

SDMA done channel 7.

Enumerator
kSDMA_DoneSrcSW 

software done

kSDMA_DoneSrcHwEvent0U 

HW event 0 is used for DONE event.

kSDMA_DoneSrcHwEvent1U 

HW event 1 is used for DONE event.

kSDMA_DoneSrcHwEvent2U 

HW event 2 is used for DONE event.

kSDMA_DoneSrcHwEvent3U 

HW event 3 is used for DONE event.

kSDMA_DoneSrcHwEvent4U 

HW event 4 is used for DONE event.

kSDMA_DoneSrcHwEvent5U 

HW event 5 is used for DONE event.

kSDMA_DoneSrCHwEvent6U 

HW event 6 is used for DONE event.

kSDMA_DoneSrcHwEvent7U 

HW event 7 is used for DONE event.

kSDMA_DoneSrcHwEvent8U 

HW event 8 is used for DONE event.

kSDMA_DoneSrcHwEvent9U 

HW event 9 is used for DONE event.

kSDMA_DoneSrcHwEvent10U 

HW event 10 is used for DONE event.

kSDMA_DoneSrcHwEvent11U 

HW event 11 is used for DONE event.

kSDMA_DoneSrcHwEvent12U 

HW event 12 is used for DONE event.

kSDMA_DoneSrcHwEvent13U 

HW event 13 is used for DONE event.

kSDMA_DoneSrcHwEvent14U 

HW event 14 is used for DONE event.

kSDMA_DoneSrcHwEvent15U 

HW event 15 is used for DONE event.

kSDMA_DoneSrcHwEvent16U 

HW event 16 is used for DONE event.

kSDMA_DoneSrcHwEvent17U 

HW event 17 is used for DONE event.

kSDMA_DoneSrcHwEvent18U 

HW event 18 is used for DONE event.

kSDMA_DoneSrcHwEvent19U 

HW event 19 is used for DONE event.

kSDMA_DoneSrcHwEvent20U 

HW event 20 is used for DONE event.

kSDMA_DoneSrcHwEvent21U 

HW event 21 is used for DONE event.

kSDMA_DoneSrcHwEvent22U 

HW event 22 is used for DONE event.

kSDMA_DoneSrcHwEvent23U 

HW event 23 is used for DONE event.

kSDMA_DoneSrcHwEvent24U 

HW event 24 is used for DONE event.

kSDMA_DoneSrcHwEvent25U 

HW event 25 is used for DONE event.

kSDMA_DoneSrcHwEvent26U 

HW event 26 is used for DONE event.

kSDMA_DoneSrcHwEvent27U 

HW event 27 is used for DONE event.

kSDMA_DoneSrcHwEvent28U 

HW event 28 is used for DONE event.

kSDMA_DoneSrcHwEvent29U 

HW event 29 is used for DONE event.

kSDMA_DoneSrcHwEvent30U 

HW event 30 is used for DONE event.

kSDMA_DoneSrcHwEvent31U 

HW event 31 is used for DONE event.

Function Documentation

void SDMA_Init ( SDMAARM_Type *  base,
const sdma_config_t *  config 
)

This function ungates the SDMA clock and configures the SDMA peripheral according to the configuration structure.

Parameters
baseSDMA peripheral base address.
configA pointer to the configuration structure, see "sdma_config_t".
Note
This function enables the minor loop map feature.
void SDMA_Deinit ( SDMAARM_Type *  base)

This function gates the SDMA clock.

Parameters
baseSDMA peripheral base address.
void SDMA_GetDefaultConfig ( sdma_config_t *  config)

This function sets the configuration structure to default values. The default configuration is set to the following values.

* config.enableRealTimeDebugPin = false;
* config.isSoftwareResetClearLock = true;
* config.ratio = kSDMA_HalfARMClockFreq;
*
Parameters
configA pointer to the SDMA configuration structure.
void SDMA_ResetModule ( SDMAARM_Type *  base)

If only reset ARM core, SDMA register cannot return to reset value, shall call this function to reset all SDMA register to reset value. But the internal status cannot be reset.

Parameters
baseSDMA peripheral base address.
static void SDMA_EnableChannelErrorInterrupts ( SDMAARM_Type *  base,
uint32_t  channel 
)
inlinestatic

Enable this will trigger an interrupt while SDMA occurs error while executing scripts.

Parameters
baseSDMA peripheral base address.
channelSDMA channel number.
static void SDMA_DisableChannelErrorInterrupts ( SDMAARM_Type *  base,
uint32_t  channel 
)
inlinestatic
Parameters
baseSDMA peripheral base address.
channelSDMA channel number.
void SDMA_ConfigBufferDescriptor ( sdma_buffer_descriptor_t *  bd,
uint32_t  srcAddr,
uint32_t  destAddr,
sdma_transfer_size_t  busWidth,
size_t  bufferSize,
bool  isLast,
bool  enableInterrupt,
bool  isWrap,
sdma_transfer_type_t  type 
)

This function sets the descriptor contents such as source, dest address and status bits.

Parameters
bdPointer to the buffer descriptor structure.
srcAddrSource address for the buffer descriptor.
destAddrDestination address for the buffer descriptor.
busWidthThe transfer width, it only can be a member of sdma_transfer_size_t.
bufferSizeBuffer size for this descriptor, this number shall less than 0xFFFF. If need to transfer a big size, shall divide into several buffer descriptors.
isLastIs the buffer descriptor the last one for the channel to transfer. If only one descriptor used for the channel, this bit shall set to TRUE.
enableInterruptIf trigger an interrupt while this buffer descriptor transfer finished.
isWrapIs the buffer descriptor need to be wrapped. While this bit set to true, it will automatically wrap to the first buffer descrtiptor to do transfer.
typeTransfer type, memory to memory, peripheral to memory or memory to peripheral.
static void SDMA_SetChannelPriority ( SDMAARM_Type *  base,
uint32_t  channel,
uint8_t  priority 
)
inlinestatic

This function sets the channel priority. The default value is 0 for all channels, priority 0 will prevents channel from starting, so the priority must be set before start a channel.

Parameters
baseSDMA peripheral base address.
channelSDMA channel number.
prioritySDMA channel priority.
static void SDMA_SetSourceChannel ( SDMAARM_Type *  base,
uint32_t  source,
uint32_t  channelMask 
)
inlinestatic

This function sets which channel will be triggered by the dma request source.

Parameters
baseSDMA peripheral base address.
sourceSDMA dma request source number.
channelMaskSDMA channel mask. 1 means channel 0, 2 means channel 1, 4 means channel 3. SDMA supports an event trigger multi-channel. A channel can also be triggered by several source events.
static void SDMA_StartChannelSoftware ( SDMAARM_Type *  base,
uint32_t  channel 
)
inlinestatic

This function start a channel.

Parameters
baseSDMA peripheral base address.
channelSDMA channel number.
static void SDMA_StartChannelEvents ( SDMAARM_Type *  base,
uint32_t  channel 
)
inlinestatic

This function start a channel.

Parameters
baseSDMA peripheral base address.
channelSDMA channel number.
static void SDMA_StopChannel ( SDMAARM_Type *  base,
uint32_t  channel 
)
inlinestatic

This function stops a channel.

Parameters
baseSDMA peripheral base address.
channelSDMA channel number.
void SDMA_SetContextSwitchMode ( SDMAARM_Type *  base,
sdma_context_switch_mode_t  mode 
)
Parameters
baseSDMA peripheral base address.
modeSDMA context switch mode.
static uint32_t SDMA_GetChannelInterruptStatus ( SDMAARM_Type *  base)
inlinestatic
Parameters
baseSDMA peripheral base address.
Returns
The interrupt status for all channels. Check the relevant bits for specific channel.
static void SDMA_ClearChannelInterruptStatus ( SDMAARM_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseSDMA peripheral base address.
maskThe interrupt status need to be cleared.
static uint32_t SDMA_GetChannelStopStatus ( SDMAARM_Type *  base)
inlinestatic
Parameters
baseSDMA peripheral base address.
Returns
The stop status for all channels. Check the relevant bits for specific channel.
static void SDMA_ClearChannelStopStatus ( SDMAARM_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseSDMA peripheral base address.
maskThe stop status need to be cleared.
static uint32_t SDMA_GetChannelPendStatus ( SDMAARM_Type *  base)
inlinestatic
Parameters
baseSDMA peripheral base address.
Returns
The pending status for all channels. Check the relevant bits for specific channel.
static void SDMA_ClearChannelPendStatus ( SDMAARM_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseSDMA peripheral base address.
maskThe pending status need to be cleared.
static uint32_t SDMA_GetErrorStatus ( SDMAARM_Type *  base)
inlinestatic

SDMA channel error flag is asserted while an incoming DMA request was detected and it triggers a channel that is already pending or being serviced. This probably means there is an overflow of data for that channel.

Parameters
baseSDMA peripheral base address.
Returns
The error status for all channels. Check the relevant bits for specific channel.
bool SDMA_GetRequestSourceStatus ( SDMAARM_Type *  base,
uint32_t  source 
)
Parameters
baseSDMA peripheral base address.
sourceDMA request source number.
Returns
True means the request source is pending, otherwise not pending.
void SDMA_CreateHandle ( sdma_handle_t *  handle,
SDMAARM_Type *  base,
uint32_t  channel,
sdma_context_data_t *  context 
)

This function is called if using the transactional API for SDMA. This function initializes the internal state of the SDMA handle.

Parameters
handleSDMA handle pointer. The SDMA handle stores callback function and parameters.
baseSDMA peripheral base address.
channelSDMA channel number.
contextContext structure for the channel to download into SDMA. Users shall make sure the context located in a non-cacheable memory, or it will cause SDMA run fail. Users shall not touch the context contents, it only be filled by SDMA driver in SDMA_SubmitTransfer function.
void SDMA_InstallBDMemory ( sdma_handle_t *  handle,
sdma_buffer_descriptor_t *  BDPool,
uint32_t  BDCount 
)

This function is called after the SDMA_CreateHandle to use multi-buffer feature.

Parameters
handleSDMA handle pointer.
BDPoolA memory pool to store BDs. It must be located in non-cacheable address.
BDCountThe number of BD slots.
void SDMA_SetCallback ( sdma_handle_t *  handle,
sdma_callback  callback,
void *  userData 
)

This callback is called in the SDMA IRQ handler. Use the callback to do something after the current major loop transfer completes.

Parameters
handleSDMA handle pointer.
callbackSDMA callback function pointer.
userDataA parameter for the callback function.
void SDMA_SetMultiFifoConfig ( sdma_transfer_config_t *  config,
uint32_t  fifoNums,
uint32_t  fifoOffset 
)

This api is used to support multi fifo for SDMA, if user want to get multi fifo data, then this api shoule be called before submit transfer.

Parameters
configtransfer configurations.
fifoNumsfifo numbers that multi fifo operation perform.
fifoOffsetoffset between multififo address.
void SDMA_EnableSwDone ( SDMAARM_Type *  base,
sdma_transfer_config_t *  config,
uint8_t  sel,
sdma_peripheral_t  type 
)
Parameters
baseSDMA base.
configtransfer configurations.
selsw done selector.
typeperipheral type is used to determine the corresponding peripheral sw done selector bit.
void SDMA_SetDoneConfig ( SDMAARM_Type *  base,
sdma_transfer_config_t *  config,
sdma_peripheral_t  type,
sdma_done_src_t  doneSrc 
)
Parameters
baseSDMA base.
configtransfer configurations.
typeperipheral type.
doneSrcreference sdma_done_src_t.
void SDMA_LoadScript ( SDMAARM_Type *  base,
uint32_t  destAddr,
void *  srcAddr,
size_t  bufferSizeBytes 
)
Parameters
baseSDMA base.
destAddrdest script address, should be SDMA program memory address.
srcAddrsource address of target script.
bufferSizeBytesbytes size of script.
void SDMA_DumpScript ( SDMAARM_Type *  base,
uint32_t  srcAddr,
void *  destAddr,
size_t  bufferSizeBytes 
)
Parameters
baseSDMA base.
srcAddrshould be SDMA program memory address.
destAddraddress to store scripts.
bufferSizeBytesbytes size of script.
void SDMA_PrepareTransfer ( sdma_transfer_config_t *  config,
uint32_t  srcAddr,
uint32_t  destAddr,
uint32_t  srcWidth,
uint32_t  destWidth,
uint32_t  bytesEachRequest,
uint32_t  transferSize,
uint32_t  eventSource,
sdma_peripheral_t  peripheral,
sdma_transfer_type_t  type 
)

This function prepares the transfer configuration structure according to the user input.

Parameters
configThe user configuration structure of type sdma_transfer_t.
srcAddrSDMA transfer source address.
destAddrSDMA transfer destination address.
srcWidthSDMA transfer source address width(bytes).
destWidthSDMA transfer destination address width(bytes).
bytesEachRequestSDMA transfer bytes per channel request.
transferSizeSDMA transfer bytes to be transferred.
eventSourceEvent source number for the transfer, if use software trigger, just write 0.
peripheralPeripheral type, used to decide if need to use some special scripts.
typeSDMA transfer type. Used to decide the correct SDMA script address in SDMA ROM.
Note
The data address and the data width must be consistent. For example, if the SRC is 4 bytes, the source address must be 4 bytes aligned, or it results in source address error.
void SDMA_PrepareP2PTransfer ( sdma_transfer_config_t *  config,
uint32_t  srcAddr,
uint32_t  destAddr,
uint32_t  srcWidth,
uint32_t  destWidth,
uint32_t  bytesEachRequest,
uint32_t  transferSize,
uint32_t  eventSource,
uint32_t  eventSource1,
sdma_peripheral_t  peripheral,
sdma_p2p_config_t *  p2p 
)

This function prepares the transfer configuration structure according to the user input.

Parameters
configThe user configuration structure of type sdma_transfer_t.
srcAddrSDMA transfer source address.
destAddrSDMA transfer destination address.
srcWidthSDMA transfer source address width(bytes).
destWidthSDMA transfer destination address width(bytes).
bytesEachRequestSDMA transfer bytes per channel request.
transferSizeSDMA transfer bytes to be transferred.
eventSourceEvent source number for the transfer.
eventSource1Event source1 number for the transfer.
peripheralPeripheral type, used to decide if need to use some special scripts.
p2psdma p2p configuration pointer.
Note
The data address and the data width must be consistent. For example, if the SRC is 4 bytes, the source address must be 4 bytes aligned, or it results in source address error.
void SDMA_SubmitTransfer ( sdma_handle_t *  handle,
const sdma_transfer_config_t *  config 
)

This function submits the SDMA transfer request according to the transfer configuration structure.

Parameters
handleSDMA handle pointer.
configPointer to SDMA transfer configuration structure.
void SDMA_StartTransfer ( sdma_handle_t *  handle)

This function enables the channel request. Users can call this function after submitting the transfer request or before submitting the transfer request.

Parameters
handleSDMA handle pointer.
void SDMA_StopTransfer ( sdma_handle_t *  handle)

This function disables the channel request to pause the transfer. Users can call SDMA_StartTransfer() again to resume the transfer.

Parameters
handleSDMA handle pointer.
void SDMA_AbortTransfer ( sdma_handle_t *  handle)

This function disables the channel request and clear transfer status bits. Users can submit another transfer after calling this API.

Parameters
handleDMA handle pointer.
uint32_t SDMA_GetTransferredBytes ( sdma_handle_t *  handle)

This function returns the buffer descriptor count value if not using buffer descriptor. While do a simple transfer, which only uses one descriptor, the SDMA driver inside handle the buffer descriptor. In uart receive case, it can tell users how many data already received, also it can tells users how many data transfferd while error occurred. Notice, the count would not change while transfer is on-going using default SDMA script.

Parameters
handleDMA handle pointer.
Returns
Transferred bytes.
bool SDMA_IsPeripheralInSPBA ( uint32_t  addr)
Parameters
addrAddress which need to judge.
returnTrue means located in SPBA, false means not.
void SDMA_HandleIRQ ( sdma_handle_t *  handle)

This function clears the interrupt flags and also handle the CCB for the channel.

Parameters
handleSDMA handle pointer.