Kinetis SDK v.2.0 API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

SHA Functional Operation

status_t SHA_Init (SHA_Type *base, sha_ctx_t *ctx, sha_algo_t algo)
 Initialize HASH context. More...
 
status_t SHA_Update (SHA_Type *base, sha_ctx_t *ctx, const uint8_t *message, size_t messageSize)
 Add data to current HASH. More...
 
status_t SHA_Finish (SHA_Type *base, sha_ctx_t *ctx, uint8_t *output, size_t *outputSize)
 Finalize hashing. More...
 
void SHA_ClkInit (SHA_Type *base)
 Start SHA clock. More...
 
void SHA_ClkDeinit (SHA_Type *base)
 Stop SHA clock. More...
 

Function Documentation

status_t SHA_Init ( SHA_Type *  base,
sha_ctx_t ctx,
sha_algo_t  algo 
)

This function initializes new hash context.

Parameters
baseSHA peripheral base address
[out]ctxOutput hash context
algoUnderlaying algorithm to use for hash computation. Either SHA-1 or SHA-256.
Returns
Status of initialization
status_t SHA_Update ( SHA_Type *  base,
sha_ctx_t ctx,
const uint8_t *  message,
size_t  messageSize 
)

Add data to current HASH. This can be called repeatedly with an arbitrary amount of data to be hashed.

Parameters
baseSHA peripheral base address
[in,out]ctxHASH context
messageInput message
messageSizeSize of input message in bytes
Returns
Status of the hash update operation
status_t SHA_Finish ( SHA_Type *  base,
sha_ctx_t ctx,
uint8_t *  output,
size_t *  outputSize 
)

Outputs the final hash and erases the context. SHA-1 or SHA-256 padding bits are automatically added by this function.

Parameters
baseSHA peripheral base address
[in,out]ctxHASH context
[out]outputOutput hash data
[in,out]outputSizeOn input, determines the size of bytes of the output array. On output, tells how many bytes have been written to output.
Returns
Status of the hash finish operation
void SHA_ClkInit ( SHA_Type *  base)

Start SHA clock

Parameters
baseSHA peripheral base address
void SHA_ClkDeinit ( SHA_Type *  base)

Stop SHA clock

Parameters
baseSHA peripheral base address