![]() |
Kinetis SDK v.2.0 API Reference Manual
Rev. 0
NXP Semiconductors
|
Files | |
file | fsl_usart_freertos.h |
Data Structures | |
struct | rtos_usart_config |
FLEX USART configuration structure. More... | |
struct | usart_rtos_handle_t |
FLEX USART FreeRTOS handle. More... | |
Driver version | |
#define | FSL_USART_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 1, 0)) |
USART freertos driver version 2.0.1. More... | |
USART RTOS Operation | |
int | USART_RTOS_Init (usart_rtos_handle_t *handle, usart_handle_t *t_handle, const struct rtos_usart_config *cfg) |
Initializes a USART instance for operation in RTOS. More... | |
int | USART_RTOS_Deinit (usart_rtos_handle_t *handle) |
Deinitializes a USART instance for operation. More... | |
USART transactional Operation | |
int | USART_RTOS_Send (usart_rtos_handle_t *handle, const uint8_t *buffer, uint32_t length) |
Sends data in the background. More... | |
int | USART_RTOS_Receive (usart_rtos_handle_t *handle, uint8_t *buffer, uint32_t length, size_t *received) |
Receives data. More... | |
struct rtos_usart_config |
Data Fields | |
USART_Type * | base |
USART base address. | |
uint32_t | srcclk |
USART source clock in Hz. | |
uint32_t | baudrate |
Desired communication speed. | |
usart_parity_mode_t | parity |
Parity setting. | |
usart_stop_bit_count_t | stopbits |
Number of stop bits to use. | |
uint8_t * | buffer |
Buffer for background reception. | |
uint32_t | buffer_size |
Size of buffer for background reception. | |
struct usart_rtos_handle_t |
Data Fields | |
USART_Type * | base |
USART base address. | |
usart_transfer_t | txTransfer |
TX transfer structure. | |
usart_transfer_t | rxTransfer |
RX transfer structure. | |
SemaphoreHandle_t | rxSemaphore |
RX semaphore for resource sharing. | |
SemaphoreHandle_t | txSemaphore |
TX semaphore for resource sharing. | |
EventGroupHandle_t | rxEvent |
RX completion event. | |
EventGroupHandle_t | txEvent |
TX completion event. | |
void * | t_state |
Transactional state of the underlying driver. | |
#define FSL_USART_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 1, 0)) |
int USART_RTOS_Init | ( | usart_rtos_handle_t * | handle, |
usart_handle_t * | t_handle, | ||
const struct rtos_usart_config * | cfg | ||
) |
handle | The RTOS USART handle, the pointer to allocated space for RTOS context. |
t_handle | The pointer to allocated space where to store transactional layer internal state. |
cfg | The pointer to the parameters required to configure the USART after initialization. |
int USART_RTOS_Deinit | ( | usart_rtos_handle_t * | handle | ) |
This function deinitializes the USART module, sets all register values to reset value, and releases the resources.
handle | The RTOS USART handle. |
int USART_RTOS_Send | ( | usart_rtos_handle_t * | handle, |
const uint8_t * | buffer, | ||
uint32_t | length | ||
) |
This function sends data. It is a synchronous API. If the hardware buffer is full, the task is in the blocked state.
handle | The RTOS USART handle. |
buffer | The pointer to buffer to send. |
length | The number of bytes to send. |
int USART_RTOS_Receive | ( | usart_rtos_handle_t * | handle, |
uint8_t * | buffer, | ||
uint32_t | length, | ||
size_t * | received | ||
) |
This function receives data from USART. It is a synchronous API. If data is immediately available, it is returned immediately and the number of bytes received.
handle | The RTOS USART handle. |
buffer | The pointer to buffer where to write received data. |
length | The number of bytes to receive. |
received | The pointer to a variable of size_t where the number of received data is filled. |