MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
IRTC: IRTC Driver

Overview

The MCUXpresso SDK provides a driver for the IRTC module of MCUXpresso SDK devices.

Data Structures

struct  irtc_datetime_t
 Structure is used to hold the date and time. More...
 
struct  irtc_daylight_time_t
 Structure is used to hold the daylight saving time. More...
 
struct  irtc_tamper_config_t
 Structure is used to define the parameters to configure a RTC tamper event. More...
 
struct  irtc_config_t
 RTC config structure. More...
 

Enumerations

enum  irtc_filter_clock_source_t {
  kIRTC_32K = 0x0,
  kIRTC_512 = 0x1,
  kIRTC_128 = 0x2,
  kIRTC_64 = 0x3,
  kIRTC_16 = 0x4,
  kIRTC_8 = 0x5,
  kIRTC_4 = 0x6,
  kIRTC_2 = 0x7
}
 IRTC filter clock source options. More...
 
enum  irtc_tamper_pins_t {
  kIRTC_Tamper_0 = 0U,
  kIRTC_Tamper_1,
  kIRTC_Tamper_2,
  kIRTC_Tamper_3
}
 IRTC Tamper pins. More...
 
enum  irtc_interrupt_enable_t {
  kIRTC_TamperInterruptEnable = RTC_IER_TAMPER_IE_MASK,
  kIRTC_AlarmInterruptEnable = RTC_IER_ALM_IE_MASK,
  kIRTC_DayInterruptEnable = RTC_IER_DAY_IE_MASK,
  kIRTC_HourInterruptEnable = RTC_IER_HOUR_IE_MASK,
  kIRTC_MinInterruptEnable = RTC_IER_MIN_IE_MASK,
  kIRTC_1hzInterruptEnable = RTC_IER_IE_1HZ_MASK,
  kIRTC_2hzInterruptEnable = RTC_IER_IE_2HZ_MASK,
  kIRTC_4hzInterruptEnable = RTC_IER_IE_4HZ_MASK,
  kIRTC_8hzInterruptEnable = RTC_IER_IE_8HZ_MASK,
  kIRTC_16hzInterruptEnable = RTC_IER_IE_16HZ_MASK,
  kIRTC_32hzInterruptEnable = RTC_IER_IE_32HZ_MASK,
  kIRTC_64hzInterruptEnable = RTC_IER_IE_64HZ_MASK,
  kIRTC_128hzInterruptEnable = RTC_IER_IE_128HZ_MASK,
  kIRTC_256hzInterruptEnable = RTC_IER_IE_256HZ_MASK,
  kIRTC_512hzInterruptEnable = RTC_IER_IE_512HZ_MASK
}
 List of IRTC interrupts. More...
 
enum  irtc_status_flags_t {
  kIRTC_TamperFlag = RTC_ISR_TAMPER_IS_MASK,
  kIRTC_AlarmFlag = RTC_ISR_ALM_IS_MASK,
  kIRTC_DayFlag = RTC_ISR_DAY_IS_MASK,
  kIRTC_HourFlag = RTC_ISR_HOUR_IS_MASK,
  kIRTC_MinFlag = RTC_ISR_MIN_IS_MASK,
  kIRTC_1hzFlag = RTC_ISR_IS_1HZ_MASK,
  kIRTC_2hzFlag = RTC_ISR_IS_2HZ_MASK,
  kIRTC_4hzFlag = RTC_ISR_IS_4HZ_MASK,
  kIRTC_8hzFlag = RTC_ISR_IS_8HZ_MASK,
  kIRTC_16hzFlag = RTC_ISR_IS_16HZ_MASK,
  kIRTC_32hzFlag = RTC_ISR_IS_32HZ_MASK,
  kIRTC_64hzFlag = RTC_ISR_IS_64HZ_MASK,
  kIRTC_128hzFlag = RTC_ISR_IS_128HZ_MASK,
  kIRTC_256hzFlag = RTC_ISR_IS_256HZ_MASK,
  kIRTC_512hzFlag = RTC_ISR_IS_512HZ_MASK,
  kIRTC_InvalidFlag = (RTC_STATUS_INVAL_BIT_MASK << 16),
  kIRTC_WriteProtFlag = (RTC_STATUS_WRITE_PROT_EN_MASK << 16),
  kIRTC_CpuLowVoltFlag = (RTC_STATUS_CPU_LOW_VOLT_MASK << 16),
  kIRTC_ResetSrcFlag = (RTC_STATUS_RST_SRC_MASK << 16),
  kIRTC_CmpIntFlag = (RTC_STATUS_CMP_INT_MASK << 16),
  kIRTC_BusErrFlag = (RTC_STATUS_BUS_ERR_MASK << 16),
  kIRTC_CmpDoneFlag = (RTC_STATUS_CMP_DONE_MASK << 16)
}
 List of IRTC flags. More...
 
enum  irtc_alarm_match_t {
  kRTC_MatchSecMinHr = 0,
  kRTC_MatchSecMinHrDay = 1,
  kRTC_MatchSecMinHrDayMnth = 2,
  kRTC_MatchSecMinHrDayMnthYr = 3
}
 IRTC alarm match options. More...
 
enum  irtc_osc_cap_load_t {
  kIRTC_Capacitor2p = (1U << 1),
  kIRTC_Capacitor4p = (1U << 2),
  kIRTC_Capacitor8p = (1U << 3),
  kIRTC_Capacitor16p = (1U << 4)
}
 List of RTC Oscillator capacitor load settings. More...
 

Functions

static void IRTC_SetOscCapLoad (RTC_Type *base, uint16_t capLoad)
 This function sets the specified capacitor configuration for the RTC oscillator. More...
 
status_t IRTC_SetWriteProtection (RTC_Type *base, bool lock)
 Locks or unlocks IRTC registers for write access. More...
 
static void IRTC_Reset (RTC_Type *base)
 Performs a software reset on the IRTC module. More...
 

Driver version

#define FSL_IRTC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))
 Version. More...
 

Initialization and deinitialization

status_t IRTC_Init (RTC_Type *base, const irtc_config_t *config)
 Ungates the IRTC clock and configures the peripheral for basic operation. More...
 
static void IRTC_Deinit (RTC_Type *base)
 Gate the IRTC clock. More...
 
void IRTC_GetDefaultConfig (irtc_config_t *config)
 Fill in the IRTC config struct with the default settings. More...
 

Current Time & Alarm

status_t IRTC_SetDatetime (RTC_Type *base, const irtc_datetime_t *datetime)
 Sets the IRTC date and time according to the given time structure. More...
 
void IRTC_GetDatetime (RTC_Type *base, irtc_datetime_t *datetime)
 Gets the IRTC time and stores it in the given time structure. More...
 
status_t IRTC_SetAlarm (RTC_Type *base, const irtc_datetime_t *alarmTime)
 Sets the IRTC alarm time. More...
 
void IRTC_GetAlarm (RTC_Type *base, irtc_datetime_t *datetime)
 Returns the IRTC alarm time. More...
 

Interrupt Interface

static void IRTC_EnableInterrupts (RTC_Type *base, uint32_t mask)
 Enables the selected IRTC interrupts. More...
 
static void IRTC_DisableInterrupts (RTC_Type *base, uint32_t mask)
 Disables the selected IRTC interrupts. More...
 
static uint16_t IRTC_GetEnabledInterrupts (RTC_Type *base)
 Gets the enabled IRTC interrupts. More...
 

Status Interface

static uint32_t IRTC_GetStatusFlags (RTC_Type *base)
 Gets the IRTC status flags. More...
 
static void IRTC_ClearStatusFlags (RTC_Type *base, uint32_t mask)
 Clears the IRTC status flags. More...
 

Daylight Savings Interface

void IRTC_SetDaylightTime (RTC_Type *base, const irtc_daylight_time_t *datetime)
 Sets the IRTC daylight savings start and stop date and time. More...
 
void IRTC_GetDaylightTime (RTC_Type *base, irtc_daylight_time_t *datetime)
 Gets the IRTC daylight savings time and stores it in the given time structure. More...
 

Time Compensation Interface

void IRTC_SetCoarseCompensation (RTC_Type *base, uint8_t compensationValue, uint8_t compensationInterval)
 Enables the coarse compensation and sets the value in the IRTC compensation register. More...
 
void IRTC_SetFineCompensation (RTC_Type *base, uint8_t integralValue, uint8_t fractionValue, bool accumulateFractional)
 Enables the fine compensation and sets the value in the IRTC compensation register. More...
 

Tamper Interface

void IRTC_SetTamperParams (RTC_Type *base, irtc_tamper_pins_t tamperNumber, const irtc_tamper_config_t *tamperConfig)
 This function allows configuring the four tamper inputs. More...
 

Data Structure Documentation

struct irtc_datetime_t

Data Fields

uint16_t year
 Range from 1984 to 2239. More...
 
uint8_t month
 Range from 1 to 12. More...
 
uint8_t day
 Range from 1 to 31 (depending on month). More...
 
uint8_t weekDay
 Range from 0(Sunday) to 6(Saturday). More...
 
uint8_t hour
 Range from 0 to 23. More...
 
uint8_t minute
 Range from 0 to 59. More...
 
uint8_t second
 Range from 0 to 59. More...
 

Field Documentation

uint16_t irtc_datetime_t::year
uint8_t irtc_datetime_t::month
uint8_t irtc_datetime_t::day
uint8_t irtc_datetime_t::weekDay
uint8_t irtc_datetime_t::hour
uint8_t irtc_datetime_t::minute
uint8_t irtc_datetime_t::second
struct irtc_daylight_time_t

Data Fields

uint8_t startMonth
 Range from 1 to 12.
 
uint8_t endMonth
 Range from 1 to 12.
 
uint8_t startDay
 Range from 1 to 31 (depending on month)
 
uint8_t endDay
 Range from 1 to 31 (depending on month)
 
uint8_t startHour
 Range from 0 to 23.
 
uint8_t endHour
 Range from 0 to 23.
 
struct irtc_tamper_config_t

Data Fields

bool pinPolarity
 true: tamper has active low polarity; false: active high polarity
 
irtc_filter_clock_source_t filterClk
 Clock source for the tamper filter.
 
uint8_t filterDuration
 Tamper filter duration. More...
 

Field Documentation

uint8_t irtc_tamper_config_t::filterDuration
struct irtc_config_t

This structure holds the configuration settings for the RTC peripheral. To initialize this structure to reasonable defaults, call the IRTC_GetDefaultConfig() function and pass a pointer to your config structure instance.

The config struct can be made const so it resides in flash

Data Fields

bool wakeupSelect
 true: Tamper pin 0 is used to wakeup the chip; false: Tamper pin 0 is used as the tamper pin
 
bool timerStdMask
 true: Sampling clocks gated in standby mode; false: Sampling clocks not gated
 
irtc_alarm_match_t alrmMatch
 Pick one option from enumeration :: irtc_alarm_match_t.
 

Macro Definition Documentation

#define FSL_IRTC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))

Enumeration Type Documentation

Enumerator
kIRTC_32K 

Use 32 kHz clock source for the tamper filter.

kIRTC_512 

Use 512 Hz clock source for the tamper filter.

kIRTC_128 

Use 128 Hz clock source for the tamper filter.

kIRTC_64 

Use 64 Hz clock source for the tamper filter.

kIRTC_16 

Use 16 Hz clock source for the tamper filter.

kIRTC_8 

Use 8 Hz clock source for the tamper filter.

kIRTC_4 

Use 4 Hz clock source for the tamper filter.

kIRTC_2 

Use 2 Hz clock source for the tamper filter.

Enumerator
kIRTC_Tamper_0 

External Tamper 0.

kIRTC_Tamper_1 

External Tamper 1.

kIRTC_Tamper_2 

External Tamper 2.

kIRTC_Tamper_3 

Internal tamper, does not have filter configuration.

Enumerator
kIRTC_TamperInterruptEnable 

Tamper Interrupt Enable.

kIRTC_AlarmInterruptEnable 

Alarm Interrupt Enable.

kIRTC_DayInterruptEnable 

Days Interrupt Enable.

kIRTC_HourInterruptEnable 

Hours Interrupt Enable.

kIRTC_MinInterruptEnable 

Minutes Interrupt Enable.

kIRTC_1hzInterruptEnable 

1 Hz interval Interrupt Enable

kIRTC_2hzInterruptEnable 

2 Hz interval Interrupt Enable

kIRTC_4hzInterruptEnable 

4 Hz interval Interrupt Enable

kIRTC_8hzInterruptEnable 

8 Hz interval Interrupt Enable

kIRTC_16hzInterruptEnable 

16 Hz interval Interrupt Enable

kIRTC_32hzInterruptEnable 

32 Hz interval Interrupt Enable

kIRTC_64hzInterruptEnable 

64 Hz interval Interrupt Enable

kIRTC_128hzInterruptEnable 

128 Hz interval Interrupt Enable

kIRTC_256hzInterruptEnable 

256 Hz interval Interrupt Enable

kIRTC_512hzInterruptEnable 

512 Hz interval Interrupt Enable

Enumerator
kIRTC_TamperFlag 

Tamper Status flag.

kIRTC_AlarmFlag 

Alarm Status flag.

kIRTC_DayFlag 

Days Status flag.

kIRTC_HourFlag 

Hour Status flag.

kIRTC_MinFlag 

Minutes Status flag.

kIRTC_1hzFlag 

1 Hz interval status flag

kIRTC_2hzFlag 

2 Hz interval status flag

kIRTC_4hzFlag 

4 Hz interval status flag

kIRTC_8hzFlag 

8 Hz interval status flag

kIRTC_16hzFlag 

16 Hz interval status flag

kIRTC_32hzFlag 

32 Hz interval status flag

kIRTC_64hzFlag 

64 Hz interval status flag

kIRTC_128hzFlag 

128 Hz interval status flag

kIRTC_256hzFlag 

256 Hz interval status flag

kIRTC_512hzFlag 

512 Hz interval status flag

kIRTC_InvalidFlag 

Indicates if time/date counters are invalid.

kIRTC_WriteProtFlag 

Write protect enable status flag.

kIRTC_CpuLowVoltFlag 

CPU low voltage warning flag.

kIRTC_ResetSrcFlag 

Reset source flag.

kIRTC_CmpIntFlag 

Compensation interval status flag.

kIRTC_BusErrFlag 

Bus error flag.

kIRTC_CmpDoneFlag 

Compensation done flag.

Enumerator
kRTC_MatchSecMinHr 

Only match second, minute and hour.

kRTC_MatchSecMinHrDay 

Only match second, minute, hour and day.

kRTC_MatchSecMinHrDayMnth 

Only match second, minute, hour, day and month.

kRTC_MatchSecMinHrDayMnthYr 

Only match second, minute, hour, day, month and year.

Enumerator
kIRTC_Capacitor2p 

2pF capacitor load

kIRTC_Capacitor4p 

4pF capacitor load

kIRTC_Capacitor8p 

8pF capacitor load

kIRTC_Capacitor16p 

16pF capacitor load

Function Documentation

status_t IRTC_Init ( RTC_Type *  base,
const irtc_config_t config 
)

This function initiates a soft-reset of the IRTC module, this has not effect on DST, calendaring, standby time and tamper detect registers.

Note
This API should be called at the beginning of the application using the IRTC driver.
Parameters
baseIRTC peripheral base address
configPointer to user's IRTC config structure.
Returns
kStatus_Fail if we cannot disable register write protection
static void IRTC_Deinit ( RTC_Type *  base)
inlinestatic
Parameters
baseIRTC peripheral base address
void IRTC_GetDefaultConfig ( irtc_config_t config)

The default values are:

* config->wakeupSelect = true;
* config->timerStdMask = false;
* config->alrmMatch = kRTC_MatchSecMinHr;
*
Parameters
configPointer to user's IRTC config structure.
status_t IRTC_SetDatetime ( RTC_Type *  base,
const irtc_datetime_t datetime 
)

The IRTC counter is started after the time is set.

Parameters
baseIRTC peripheral base address
datetimePointer to structure where the date and time details to set are stored
Returns
kStatus_Success: success in setting the time and starting the IRTC kStatus_InvalidArgument: failure. An error occurs because the datetime format is incorrect.
void IRTC_GetDatetime ( RTC_Type *  base,
irtc_datetime_t datetime 
)
Parameters
baseIRTC peripheral base address
datetimePointer to structure where the date and time details are stored.
status_t IRTC_SetAlarm ( RTC_Type *  base,
const irtc_datetime_t alarmTime 
)
Parameters
baseRTC peripheral base address
alarmTimePointer to structure where the alarm time is stored.
Note
weekDay field of alarmTime is not used during alarm match and should be set to 0
Returns
kStatus_Success: success in setting the alarm kStatus_InvalidArgument: error in setting the alarm. Error occurs because the alarm datetime format is incorrect.
void IRTC_GetAlarm ( RTC_Type *  base,
irtc_datetime_t datetime 
)
Parameters
baseRTC peripheral base address
datetimePointer to structure where the alarm date and time details are stored.
static void IRTC_EnableInterrupts ( RTC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseIRTC peripheral base address
maskThe interrupts to enable. This is a logical OR of members of the enumeration ::rtc_interrupt_enable_t
static void IRTC_DisableInterrupts ( RTC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseIRTC peripheral base address
maskThe interrupts to enable. This is a logical OR of members of the enumeration ::rtc_interrupt_enable_t
static uint16_t IRTC_GetEnabledInterrupts ( RTC_Type *  base)
inlinestatic
Parameters
baseIRTC peripheral base address
Returns
The enabled interrupts. This is the logical OR of members of the enumeration ::rtc_interrupt_enable_t
static uint32_t IRTC_GetStatusFlags ( RTC_Type *  base)
inlinestatic
Parameters
baseIRTC peripheral base address
Returns
The status flags. This is the logical OR of members of the enumeration irtc_status_flags_t
static void IRTC_ClearStatusFlags ( RTC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseIRTC peripheral base address
maskThe status flags to clear. This is a logical OR of members of the enumeration irtc_status_flags_t
static void IRTC_SetOscCapLoad ( RTC_Type *  base,
uint16_t  capLoad 
)
inlinestatic
Parameters
baseIRTC peripheral base address
capLoadOscillator loads to enable. This is a logical OR of members of the enumeration irtc_osc_cap_load_t
status_t IRTC_SetWriteProtection ( RTC_Type *  base,
bool  lock 
)
Note
When the registers are unlocked, they remain in unlocked state for 2 seconds, after which they are locked automatically. After power-on-reset, the registers come out unlocked and they are locked automatically 15 seconds after power on.
Parameters
baseIRTC peripheral base address
locktrue: Lock IRTC registers; false: Unlock IRTC registers.
Returns
kStatus_Success: if lock or unlock operation is successful kStatus_Fail: if lock or unlock operation fails even after multiple retry attempts
static void IRTC_Reset ( RTC_Type *  base)
inlinestatic

Clears contents of alarm, interrupt (status and enable except tamper interrupt enable bit) registers, STATUS[CMP_DONE] and STATUS[BUS_ERR]. This has no effect on DST, calendaring, standby time and tamper detect registers.

Parameters
baseIRTC peripheral base address
void IRTC_SetDaylightTime ( RTC_Type *  base,
const irtc_daylight_time_t datetime 
)

It also enables the daylight saving bit in the IRTC control register

Parameters
baseIRTC peripheral base address
datetimePointer to a structure where the date and time details are stored.
void IRTC_GetDaylightTime ( RTC_Type *  base,
irtc_daylight_time_t datetime 
)
Parameters
baseIRTC peripheral base address
datetimePointer to a structure where the date and time details are stored.
void IRTC_SetCoarseCompensation ( RTC_Type *  base,
uint8_t  compensationValue,
uint8_t  compensationInterval 
)
Parameters
baseIRTC peripheral base address
compensationValueCompensation value is a 2's complement value.
compensationIntervalCompensation interval.
void IRTC_SetFineCompensation ( RTC_Type *  base,
uint8_t  integralValue,
uint8_t  fractionValue,
bool  accumulateFractional 
)
Parameters
baseThe IRTC peripheral base address
integralValueCompensation integral value; twos complement value of the integer part
fractionValueCompensation fraction value expressed as number of clock cycles of a fixed 4.194304Mhz clock that have to be added.
accumulateFractionalFlag indicating if we want to add to previous fractional part; true: Add to previously accumulated fractional part, false: Start afresh and overwrite current value
void IRTC_SetTamperParams ( RTC_Type *  base,
irtc_tamper_pins_t  tamperNumber,
const irtc_tamper_config_t tamperConfig 
)

The function configures the filter properties for the three external tampers. It also sets up active/passive and direction of the tamper bits, which are not available on all platforms.

Note
This function programs the tamper filter parameters. The user must gate the 32K clock to the RTC before calling this function. It is assumed that the time and date are set after this and the tamper parameters do not require to be changed again later.
Parameters
baseThe IRTC peripheral base address
tamperNumberThe IRTC tamper input to configure
tamperConfigThe IRTC tamper properties