The MCUXpresso SDK provides a peripheral driver for the PRINCE bus crypto engine module of MCUXpresso SDK devices.
..
This example code shows how to use the PRINCE driver.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/prince
|
| static void | PRINCE_EncryptEnable (PRINCE_Type *base) |
| | Enable data encryption. More...
|
| |
| static void | PRINCE_EncryptDisable (PRINCE_Type *base) |
| | Disable data encryption. More...
|
| |
| static void | PRINCE_SetMask (PRINCE_Type *base, uint64_t mask) |
| | Sets PRINCE data mask. More...
|
| |
| static void | PRINCE_SetLock (PRINCE_Type *base, uint32_t lock) |
| | Locks access for specified region registers or data mask register. More...
|
| |
| status_t | PRINCE_GenNewIV (prince_region_t region, uint8_t *iv_code, bool store, flash_config_t *flash_context) |
| | Generate new IV code. More...
|
| |
| status_t | PRINCE_LoadIV (prince_region_t region, uint8_t *iv_code) |
| | Load IV code. More...
|
| |
| status_t | PRINCE_SetEncryptForAddressRange (prince_region_t region, uint32_t start_address, uint32_t length, flash_config_t *flash_context) |
| | Allow encryption/decryption for specified address range. More...
|
| |
| status_t | PRINCE_GetRegionSREnable (PRINCE_Type *base, prince_region_t region, uint32_t *sr_enable) |
| | Gets the PRINCE Sub-Region Enable register. More...
|
| |
| status_t | PRINCE_GetRegionBaseAddress (PRINCE_Type *base, prince_region_t region, uint32_t *region_base_addr) |
| | Gets the PRINCE region base address register. More...
|
| |
| status_t | PRINCE_SetRegionIV (PRINCE_Type *base, prince_region_t region, const uint8_t iv[8]) |
| | Sets the PRINCE region IV. More...
|
| |
| status_t | PRINCE_SetRegionBaseAddress (PRINCE_Type *base, prince_region_t region, uint32_t region_base_addr) |
| | Sets the PRINCE region base address. More...
|
| |
| status_t | PRINCE_SetRegionSREnable (PRINCE_Type *base, prince_region_t region, uint32_t sr_enable) |
| | Sets the PRINCE Sub-Region Enable register. More...
|
| |
Current version: 2.0.0
Change log:
| Enumerator |
|---|
| kPRINCE_Region0 |
PRINCE region 0.
|
| kPRINCE_Region1 |
PRINCE region 1.
|
| kPRINCE_Region2 |
PRINCE region 2.
|
| Enumerator |
|---|
| kPRINCE_Region0Lock |
PRINCE region 0 lock.
|
| kPRINCE_Region1Lock |
PRINCE region 1 lock.
|
| kPRINCE_Region2Lock |
PRINCE region 2 lock.
|
| kPRINCE_MaskLock |
PRINCE mask register lock.
|
| static void PRINCE_EncryptEnable |
( |
PRINCE_Type * |
base | ) |
|
|
inlinestatic |
This function enables PRINCE on-the-fly data encryption.
- Parameters
-
| base | PRINCE peripheral address. |
| static void PRINCE_EncryptDisable |
( |
PRINCE_Type * |
base | ) |
|
|
inlinestatic |
This function disables PRINCE on-the-fly data encryption.
- Parameters
-
| base | PRINCE peripheral address. |
| static void PRINCE_SetMask |
( |
PRINCE_Type * |
base, |
|
|
uint64_t |
mask |
|
) |
| |
|
inlinestatic |
This function sets the PRINCE mask that is used to mask decrypted data.
- Parameters
-
| base | PRINCE peripheral address. |
| mask | 64-bit data mask value. |
| static void PRINCE_SetLock |
( |
PRINCE_Type * |
base, |
|
|
uint32_t |
lock |
|
) |
| |
|
inlinestatic |
This function sets lock on specified region registers or mask register.
- Parameters
-
| base | PRINCE peripheral address. |
| lock | registers to lock. This is a logical OR of members of the enumeration prince_lock_t |
This function generates new IV code and stores it into the persistent memory. This function is implemented as a wrapper of the exported ROM bootloader API. Ensure about 800 bytes free space on the stack when calling this routine with the store parameter set to true!
- Parameters
-
| region | PRINCE region index. |
| iv_code | IV code pointer used for storing the newly generated 52 bytes long IV code. |
| store | flag to allow storing the newly generated IV code into the persistent memory (FFR). param flash_context pointer to the flash driver context structure. |
- Returns
- kStatus_Success upon success
-
kStatus_Fail otherwise, kStatus_Fail is also returned if the key code for the particular PRINCE region is not present in the keystore (though new IV code has been provided)
This function enables IV code loading into the PRINCE bus encryption engine. This function is implemented as a wrapper of the exported ROM bootloader API.
- Parameters
-
| region | PRINCE region index. |
| iv_code | IV code pointer used for passing the IV code. |
- Returns
- kStatus_Success upon success
-
kStatus_Fail otherwise
This function sets the encryption/decryption for specified address range. This function is implemented as a wrapper of the exported ROM bootloader API. Ensure about 800 bytes free space on the stack when calling this routine!
- Parameters
-
| region | PRINCE region index. |
| start_address | start address of the area to be encrypted/decrypted. |
| length | length of the area to be encrypted/decrypted. param flash_context pointer to the flash driver context structure. |
- Returns
- kStatus_Success upon success
-
kStatus_Fail otherwise
This function gets PRINCE SR_ENABLE register.
- Parameters
-
| base | PRINCE peripheral address. |
| region | PRINCE region index. |
| sr_enable | Sub-Region Enable register pointer. |
- Returns
- kStatus_Success upon success
-
kStatus_InvalidArgument
This function gets PRINCE BASE_ADDR register.
- Parameters
-
| base | PRINCE peripheral address. |
| region | PRINCE region index. |
| region_base_addr | Region base address pointer. |
- Returns
- kStatus_Success upon success
-
kStatus_InvalidArgument
This function sets specified AES IV for the given region.
- Parameters
-
| base | PRINCE peripheral address. |
| region | Selection of the PRINCE region to be configured. |
| iv | 64-bit AES IV in little-endian byte order. |
This function configures PRINCE region base address.
- Parameters
-
| base | PRINCE peripheral address. |
| region | Selection of the PRINCE region to be configured. |
| region_base_addr | Base Address for region. |
This function configures PRINCE SR_ENABLE register.
- Parameters
-
| base | PRINCE peripheral address. |
| region | Selection of the PRINCE region to be configured. |
| sr_enable | Sub-Region Enable register value. |