MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
PRINCE: PRINCE bus crypto engine

Overview

The MCUXpresso SDK provides a peripheral driver for the PRINCE bus crypto engine module of MCUXpresso SDK devices.

..

This example code shows how to use the PRINCE driver.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/prince

Enumerations

enum  prince_region_t {
  kPRINCE_Region0 = 0U,
  kPRINCE_Region1 = 1U,
  kPRINCE_Region2 = 2U
}
 
enum  prince_lock_t {
  kPRINCE_Region0Lock = 1U,
  kPRINCE_Region1Lock = 2U,
  kPRINCE_Region2Lock = 4U,
  kPRINCE_MaskLock = 256U
}
 

Functions

static void PRINCE_EncryptEnable (PRINCE_Type *base)
 Enable data encryption. More...
 
static void PRINCE_EncryptDisable (PRINCE_Type *base)
 Disable data encryption. More...
 
static void PRINCE_SetMask (PRINCE_Type *base, uint64_t mask)
 Sets PRINCE data mask. More...
 
static void PRINCE_SetLock (PRINCE_Type *base, uint32_t lock)
 Locks access for specified region registers or data mask register. More...
 
status_t PRINCE_GenNewIV (prince_region_t region, uint8_t *iv_code, bool store, flash_config_t *flash_context)
 Generate new IV code. More...
 
status_t PRINCE_LoadIV (prince_region_t region, uint8_t *iv_code)
 Load IV code. More...
 
status_t PRINCE_SetEncryptForAddressRange (prince_region_t region, uint32_t start_address, uint32_t length, flash_config_t *flash_context)
 Allow encryption/decryption for specified address range. More...
 
status_t PRINCE_GetRegionSREnable (PRINCE_Type *base, prince_region_t region, uint32_t *sr_enable)
 Gets the PRINCE Sub-Region Enable register. More...
 
status_t PRINCE_GetRegionBaseAddress (PRINCE_Type *base, prince_region_t region, uint32_t *region_base_addr)
 Gets the PRINCE region base address register. More...
 
status_t PRINCE_SetRegionIV (PRINCE_Type *base, prince_region_t region, const uint8_t iv[8])
 Sets the PRINCE region IV. More...
 
status_t PRINCE_SetRegionBaseAddress (PRINCE_Type *base, prince_region_t region, uint32_t region_base_addr)
 Sets the PRINCE region base address. More...
 
status_t PRINCE_SetRegionSREnable (PRINCE_Type *base, prince_region_t region, uint32_t sr_enable)
 Sets the PRINCE Sub-Region Enable register. More...
 

Driver version

#define FSL_PRINCE_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 PRINCE driver version 2.0.0. More...
 

Macro Definition Documentation

#define FSL_PRINCE_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))

Current version: 2.0.0

Change log:

  • Version 2.0.0
    • Initial version.

Enumeration Type Documentation

Enumerator
kPRINCE_Region0 

PRINCE region 0.

kPRINCE_Region1 

PRINCE region 1.

kPRINCE_Region2 

PRINCE region 2.

Enumerator
kPRINCE_Region0Lock 

PRINCE region 0 lock.

kPRINCE_Region1Lock 

PRINCE region 1 lock.

kPRINCE_Region2Lock 

PRINCE region 2 lock.

kPRINCE_MaskLock 

PRINCE mask register lock.

Function Documentation

static void PRINCE_EncryptEnable ( PRINCE_Type *  base)
inlinestatic

This function enables PRINCE on-the-fly data encryption.

Parameters
basePRINCE peripheral address.
static void PRINCE_EncryptDisable ( PRINCE_Type *  base)
inlinestatic

This function disables PRINCE on-the-fly data encryption.

Parameters
basePRINCE peripheral address.
static void PRINCE_SetMask ( PRINCE_Type *  base,
uint64_t  mask 
)
inlinestatic

This function sets the PRINCE mask that is used to mask decrypted data.

Parameters
basePRINCE peripheral address.
mask64-bit data mask value.
static void PRINCE_SetLock ( PRINCE_Type *  base,
uint32_t  lock 
)
inlinestatic

This function sets lock on specified region registers or mask register.

Parameters
basePRINCE peripheral address.
lockregisters to lock. This is a logical OR of members of the enumeration prince_lock_t
status_t PRINCE_GenNewIV ( prince_region_t  region,
uint8_t *  iv_code,
bool  store,
flash_config_t *  flash_context 
)

This function generates new IV code and stores it into the persistent memory. This function is implemented as a wrapper of the exported ROM bootloader API. Ensure about 800 bytes free space on the stack when calling this routine with the store parameter set to true!

Parameters
regionPRINCE region index.
iv_codeIV code pointer used for storing the newly generated 52 bytes long IV code.
storeflag to allow storing the newly generated IV code into the persistent memory (FFR). param flash_context pointer to the flash driver context structure.
Returns
kStatus_Success upon success
kStatus_Fail otherwise, kStatus_Fail is also returned if the key code for the particular PRINCE region is not present in the keystore (though new IV code has been provided)
status_t PRINCE_LoadIV ( prince_region_t  region,
uint8_t *  iv_code 
)

This function enables IV code loading into the PRINCE bus encryption engine. This function is implemented as a wrapper of the exported ROM bootloader API.

Parameters
regionPRINCE region index.
iv_codeIV code pointer used for passing the IV code.
Returns
kStatus_Success upon success
kStatus_Fail otherwise
status_t PRINCE_SetEncryptForAddressRange ( prince_region_t  region,
uint32_t  start_address,
uint32_t  length,
flash_config_t *  flash_context 
)

This function sets the encryption/decryption for specified address range. This function is implemented as a wrapper of the exported ROM bootloader API. Ensure about 800 bytes free space on the stack when calling this routine!

Parameters
regionPRINCE region index.
start_addressstart address of the area to be encrypted/decrypted.
lengthlength of the area to be encrypted/decrypted. param flash_context pointer to the flash driver context structure.
Returns
kStatus_Success upon success
kStatus_Fail otherwise
status_t PRINCE_GetRegionSREnable ( PRINCE_Type *  base,
prince_region_t  region,
uint32_t *  sr_enable 
)

This function gets PRINCE SR_ENABLE register.

Parameters
basePRINCE peripheral address.
regionPRINCE region index.
sr_enableSub-Region Enable register pointer.
Returns
kStatus_Success upon success
kStatus_InvalidArgument
status_t PRINCE_GetRegionBaseAddress ( PRINCE_Type *  base,
prince_region_t  region,
uint32_t *  region_base_addr 
)

This function gets PRINCE BASE_ADDR register.

Parameters
basePRINCE peripheral address.
regionPRINCE region index.
region_base_addrRegion base address pointer.
Returns
kStatus_Success upon success
kStatus_InvalidArgument
status_t PRINCE_SetRegionIV ( PRINCE_Type *  base,
prince_region_t  region,
const uint8_t  iv[8] 
)

This function sets specified AES IV for the given region.

Parameters
basePRINCE peripheral address.
regionSelection of the PRINCE region to be configured.
iv64-bit AES IV in little-endian byte order.
status_t PRINCE_SetRegionBaseAddress ( PRINCE_Type *  base,
prince_region_t  region,
uint32_t  region_base_addr 
)

This function configures PRINCE region base address.

Parameters
basePRINCE peripheral address.
regionSelection of the PRINCE region to be configured.
region_base_addrBase Address for region.
status_t PRINCE_SetRegionSREnable ( PRINCE_Type *  base,
prince_region_t  region,
uint32_t  sr_enable 
)

This function configures PRINCE SR_ENABLE register.

Parameters
basePRINCE peripheral address.
regionSelection of the PRINCE region to be configured.
sr_enableSub-Region Enable register value.