MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

Data Structures

struct  semaphore_t
 Type for an semaphore. More...
 
struct  mutex_t
 Type for a mutex. More...
 
struct  task_control_block_t
 Task control block for bare metal. More...
 
struct  event_t
 Type for an event object. More...
 
struct  msg_queue_t
 Type for a message queue. More...
 

Macros

#define FSL_OSA_BM_TASK_ENABLE   1U
 Definition to determine whether enable TASK module. More...
 
#define FSL_OSA_BM_TIMER_NONE   0U
 Bare Metal does not use timer. More...
 
#define FSL_OSA_BM_TIMER_SYSTICK   1U
 Bare Metal uses SYSTICK as timer. More...
 
#define FSL_OSA_BM_TIMER_CONFIG   FSL_OSA_BM_TIMER_SYSTICK
 Configure what timer is used in Bare Metal. More...
 
#define OSA_WAIT_FOREVER   0xFFFFFFFFU
 Constant to pass as timeout value in order to wait indefinitely. More...
 
#define TASK_MAX_NUM   7
 How many tasks can the bare metal support. More...
 
#define FSL_OSA_TIME_RANGE   0xFFFFFFFFU
 OSA's time range in millisecond, OSA time wraps if exceeds this value. More...
 
#define OSA_DEFAULT_INT_HANDLER   ((osa_int_handler_t)(&DefaultISR))
 The default interrupt handler installed in vector table. More...
 

Typedefs

typedef void * task_param_t
 Type for task parameter.
 
typedef void(* task_t )(task_param_t param)
 Type for a task handler, returned by the OSA_TaskCreate function.
 
typedef task_control_block_t * task_handler_t
 Type for a task pointer.
 
typedef uint32_t task_stack_t
 Type for a task stack.
 
typedef uint32_t event_flags_t
 Type for an event flags group, bit 32 is reserved.
 
typedef msg_queue_t * msg_queue_handler_t
 Type for a message queue handler.
 

Functions

void DefaultISR (void)
 The default interrupt handler installed in vector table. More...
 

Thread management

#define PRIORITY_OSA_TO_RTOS(osa_prio)   (osa_prio)
 Defines a task. More...
 
#define PRIORITY_RTOS_TO_OSA(rtos_prio)   (rtos_prio)
 

Data Structure Documentation

struct semaphore_t

Data Fields

uint32_t time_start
 The time to start timeout.
 
uint32_t timeout
 Timeout to wait in milliseconds.
 
volatile bool isWaiting
 Is any task waiting for a timeout on this object.
 
volatile uint8_t semCount
 The count value of the object.
 
struct mutex_t

Data Fields

uint32_t time_start
 The time to start timeout.
 
uint32_t timeout
 Timeout to wait in milliseconds.
 
volatile bool isWaiting
 Is any task waiting for a timeout on this mutex.
 
volatile bool isLocked
 Is the object locked or not.
 
struct task_control_block_t

Data Fields

osa_task_ptr_t p_func
 Task's entry.
 
osa_task_priority_t priority
 Task's priority.
 
osa_task_param_t param
 Task's parameter.
 
bool haveToRun
 Task was signaled.
 
struct event_t

Data Fields

uint32_t time_start
 The time to start timeout.
 
uint32_t timeout
 Timeout to wait in milliseconds.
 
volatile event_flags_t flags
 The flags status.
 
task_handler_t waitingTask
 Handler to the waiting task.
 
bool autoClear
 Auto clear or manual clear.
 
volatile bool isWaiting
 Is any task waiting for a timeout on this event.
 
struct msg_queue_t

Data Fields

volatile bool isWaiting
 Is any task waiting for a timeout.
 
uint32_t time_start
 The time to start timeout.
 
uint32_t timeout
 Timeout to wait in milliseconds.
 
uint32_t size
 The size(byte) of a single message.
 
task_handler_t waitingTask
 Handler to the waiting task.
 
uint8_t * queueMem
 Points to the queue memory.
 
uint16_t number
 The number of messages in the queue.
 
uint16_t max
 The max number of queue messages.
 
uint16_t head
 Index of the next message to be read.
 
uint16_t tail
 Index of the next place to write to.
 

Macro Definition Documentation

#define FSL_OSA_BM_TASK_ENABLE   1U
#define FSL_OSA_BM_TIMER_NONE   0U
#define FSL_OSA_BM_TIMER_SYSTICK   1U
#define FSL_OSA_BM_TIMER_CONFIG   FSL_OSA_BM_TIMER_SYSTICK
#define OSA_WAIT_FOREVER   0xFFFFFFFFU
#define TASK_MAX_NUM   7
#define FSL_OSA_TIME_RANGE   0xFFFFFFFFU
#define OSA_DEFAULT_INT_HANDLER   ((osa_int_handler_t)(&DefaultISR))
#define PRIORITY_OSA_TO_RTOS (   osa_prio)    (osa_prio)

This macro defines resources for a task statically. Then, the OSA_TaskCreate creates the task based-on these resources.

Parameters
taskThe task function.
stackSizeThe stack size this task needs in bytes.

Function Documentation

void DefaultISR ( void  )