MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Multipurpose Clock Generator Lite (MCGLITE)

The MCUXpresso SDK provides a peripheral driver for the MCG_Lite module of MCUXpresso SDK devices.

Function description

The MCG_Lite driver provides three kinds of APIs:

  1. APIs to get the MCG_Lite frequency.
  2. APIs for MCG_Lite mode.
  3. APIs for OSC setup.

MCG_Lite clock frequency

The CLOCK_GetOutClkFreq(), CLOCK_GetInternalRefClkFreq() and CLOCK_GetPeriphClkFreq() functions are used to get the frequency of MCGOUTCLK, MCGIRCLK, and MCGPCLK based on the current hardware setting.

MCG_Lite mode

The function CLOCK_GetMode() gets the current MCG_Lite mode.
The function CLOCK_SetMcgliteConfig() sets the MCG_Lite to a desired configuration. The MCG_Lite cannot switch between the LIRC2M and LIRC8M. Instead, the function switches to the HIRC mode first and then switches to the target mode.

OSC configuration

To enable the OSC clock, the MCG_Lite is needed together with the OSC module. The function CLOCK_InitOsc0() uses the MCG_Lite and the OSC to initialize the OSC. The OSC should be configured based on the board design.